diff --git a/arch/arm/Kconfig b/arch/arm/Kconfig
index 17ae3420bfe6eccc40af4c599a3523b1b9f7843f..1def7c896b50902dc72b60cd61706fef9416bad1 100644 (file)
--- a/arch/arm/Kconfig
+++ b/arch/arm/Kconfig
select GENERIC_IRQ_CHIP
select HAVE_IDE
select NEED_MACH_GPIO_H
+ select TI_PRIV_EDMA
select USE_OF
select ZONE_DMA
help
help
Say Y if you want to run Linux in a Virtual Machine on Xen on ARM.
+config ARM_FLUSH_CONSOLE_ON_RESTART
+ bool "Force flush the console on restart"
+ help
+ If the console is locked while the system is rebooted, the messages
+ in the temporary logbuffer would not have propogated to all the
+ console drivers. This option forces the console lock to be
+ released if it failed to be acquired, which will cause all the
+ pending messages to be flushed.
+
endmenu
menu "Boot options"