diff --git a/arch/arm/Kconfig b/arch/arm/Kconfig
index 67874b82a4edf318ae3718ae6137393140405586..1def7c896b50902dc72b60cd61706fef9416bad1 100644 (file)
--- a/arch/arm/Kconfig
+++ b/arch/arm/Kconfig
select GENERIC_IRQ_CHIP
select HAVE_IDE
select NEED_MACH_GPIO_H
+ select TI_PRIV_EDMA
select USE_OF
select ZONE_DMA
help
to deadlock. This workaround puts DSB before executing ISB if
an abort may occur on cache maintenance.
+config ARM_ERRATA_798181
+ bool "ARM errata: TLBI/DSB failure on Cortex-A15"
+ depends on CPU_V7 && SMP
+ help
+ On Cortex-A15 (r0p0..r3p2) the TLBI*IS/DSB operations are not
+ adequately shooting down all use of the old entries. This
+ option enables the Linux kernel workaround for this erratum
+ which sends an IPI to the CPUs that are running the same ASID
+ as the one being invalidated.
+
endmenu
source "arch/arm/common/Kconfig"
default 1024 if ARCH_SHMOBILE || ARCH_TEGRA
default 355 if ARCH_U8500
default 264 if MACH_H4700
- default 512 if SOC_OMAP5
+ default 512 if SOC_OMAP5 || SOC_DRA7XX
default 288 if ARCH_VT8500
default 0
help
help
Say Y if you want to run Linux in a Virtual Machine on Xen on ARM.
+config ARM_FLUSH_CONSOLE_ON_RESTART
+ bool "Force flush the console on restart"
+ help
+ If the console is locked while the system is rebooted, the messages
+ in the temporary logbuffer would not have propogated to all the
+ console drivers. This option forces the console lock to be
+ released if it failed to be acquired, which will cause all the
+ pending messages to be flushed.
+
endmenu
menu "Boot options"