]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/blobdiff - arch/arm/Kconfig
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
[android-sdk/kernel-video.git] / arch / arm / Kconfig
index 67874b82a4edf318ae3718ae6137393140405586..1def7c896b50902dc72b60cd61706fef9416bad1 100644 (file)
@@ -932,6 +932,7 @@ config ARCH_DAVINCI
        select GENERIC_IRQ_CHIP
        select HAVE_IDE
        select NEED_MACH_GPIO_H
+       select TI_PRIV_EDMA
        select USE_OF
        select ZONE_DMA
        help
@@ -1427,6 +1428,16 @@ config ARM_ERRATA_775420
         to deadlock. This workaround puts DSB before executing ISB if
         an abort may occur on cache maintenance.
 
+config ARM_ERRATA_798181
+       bool "ARM errata: TLBI/DSB failure on Cortex-A15"
+       depends on CPU_V7 && SMP
+       help
+         On Cortex-A15 (r0p0..r3p2) the TLBI*IS/DSB operations are not
+         adequately shooting down all use of the old entries. This
+         option enables the Linux kernel workaround for this erratum
+         which sends an IPI to the CPUs that are running the same ASID
+         as the one being invalidated.
+
 endmenu
 
 source "arch/arm/common/Kconfig"
@@ -1636,7 +1647,7 @@ config ARCH_NR_GPIO
        default 1024 if ARCH_SHMOBILE || ARCH_TEGRA
        default 355 if ARCH_U8500
        default 264 if MACH_H4700
-       default 512 if SOC_OMAP5
+       default 512 if SOC_OMAP5 || SOC_DRA7XX
        default 288 if ARCH_VT8500
        default 0
        help
@@ -1865,6 +1876,15 @@ config XEN
        help
          Say Y if you want to run Linux in a Virtual Machine on Xen on ARM.
 
+config ARM_FLUSH_CONSOLE_ON_RESTART
+       bool "Force flush the console on restart"
+       help
+         If the console is locked while the system is rebooted, the messages
+         in the temporary logbuffer would not have propogated to all the
+         console drivers. This option forces the console lock to be
+         released if it failed to be acquired, which will cause all the
+         pending messages to be flushed.
+
 endmenu
 
 menu "Boot options"