index af26d974e125f826550066f31fea3387af33b460..2d5ea6b49f4a155a5e85d0eb622facf5c0d9f3b8 100644 (file)
* registers. This address is needed early so the OCP registers that
* are part of the device's address space can be ioremapped properly.
*
+ * If SYSC access is not needed, the registers will not be remapped
+ * and non-availability of MPU access is not treated as an error.
+ *
* Returns 0 on success, -EINVAL if an invalid hwmod is passed, and
* -ENXIO on absent or invalid register target address space.
*/
_save_mpu_port_index(oh);
+ /* if we don't need sysc access we don't need to ioremap */
+ if (!oh->class->sysc)
+ return 0;
+
+ /* we can't continue without MPU PORT if we need sysc access */
if (oh->_int_flags & _HWMOD_NO_MPU_PORT)
return -ENXIO;
oh->name);
/* Extract the IO space from device tree blob */
- if (!np)
+ if (!np) {
+ pr_err("omap_hwmod: %s: no dt node\n", oh->name);
return -ENXIO;
+ }
va_start = of_iomap(np, index + oh->mpu_rt_idx);
} else {
oh->name, np->name);
}
- if (oh->class->sysc) {
- r = _init_mpu_rt_base(oh, NULL, index, np);
- if (r < 0) {
- WARN(1, "omap_hwmod: %s: doesn't have mpu register target base\n",
- oh->name);
- return 0;
- }
+ r = _init_mpu_rt_base(oh, NULL, index, np);
+ if (r < 0) {
+ WARN(1, "omap_hwmod: %s: doesn't have mpu register target base\n",
+ oh->name);
+ return 0;
}
r = _init_clocks(oh, NULL);
oh->flags |= HWMOD_INIT_NO_RESET;
if (of_find_property(np, "ti,no-idle-on-init", NULL))
oh->flags |= HWMOD_INIT_NO_IDLE;
+ if (of_find_property(np, "ti,enable-opt-clks-on-reset", NULL))
+ oh->flags |= HWMOD_CONTROL_OPT_CLKS_IN_RESET;
if (of_find_property(np, "ti,no-init", NULL))
oh->flags |= HWMOD_NO_INIT;
if (of_find_property(np, "ti,no-idle", NULL))