index 3b4e65d5122b69025a1fd863ff54f807dde4f2f9..92ecf50a39d390e5abd9983dc60ae2ea996d9568 100644 (file)
#include <core/device.h>
#include <core/client.h>
+#include <core/gpuobj.h>
#include <core/class.h>
#include <subdev/device.h>
+#include <subdev/vm.h>
#include "nouveau_drm.h"
+#include "nouveau_dma.h"
#include "nouveau_agp.h"
+#include "nouveau_abi16.h"
+#include "nouveau_fbcon.h"
+#include "nouveau_fence.h"
+
+#include "nouveau_ttm.h"
int __devinit nouveau_pci_probe(struct pci_dev *, const struct pci_device_id *);
void nouveau_pci_remove(struct pci_dev *);
int nouveau_load(struct drm_device *, unsigned long);
int nouveau_unload(struct drm_device *);
-void *nouveau_newpriv(struct drm_device *);
MODULE_PARM_DESC(config, "option string to pass to driver core");
static char *nouveau_config;
static char *nouveau_debug;
module_param_named(debug, nouveau_debug, charp, 0400);
+MODULE_PARM_DESC(noaccel, "disable kernel/abi16 acceleration");
+static int nouveau_noaccel = 0;
+module_param_named(noaccel, nouveau_noaccel, int, 0400);
+
static u64
nouveau_name(struct pci_dev *pdev)
{
nouveau_cli_destroy(struct nouveau_cli *cli)
{
struct nouveau_object *client = nv_object(cli);
+ nouveau_vm_ref(NULL, &cli->base.vm, NULL);
nouveau_client_fini(&cli->base, false);
atomic_set(&client->refcount, 1);
nouveau_object_ref(NULL, &client);
}
+static void
+nouveau_accel_fini(struct nouveau_drm *drm)
+{
+ nouveau_gpuobj_ref(NULL, &drm->notify);
+ nouveau_channel_del(&drm->channel);
+ if (drm->fence)
+ nouveau_fence(drm)->dtor(drm);
+}
+
+static void
+nouveau_accel_init(struct nouveau_drm *drm)
+{
+ struct nouveau_device *device = nv_device(drm->device);
+ struct nouveau_object *object;
+ int ret;
+
+ if (nouveau_noaccel)
+ return;
+
+ /* initialise synchronisation routines */
+ if (device->card_type < NV_10) ret = nv04_fence_create(drm);
+ else if (device->chipset < 0x84) ret = nv10_fence_create(drm);
+ else if (device->card_type < NV_C0) ret = nv84_fence_create(drm);
+ else ret = nvc0_fence_create(drm);
+ if (ret) {
+ NV_ERROR(drm, "failed to initialise sync subsystem, %d\n", ret);
+ nouveau_accel_fini(drm);
+ return;
+ }
+
+ ret = nouveau_channel_new(drm, &drm->client, NVDRM_DEVICE, NVDRM_CHAN,
+ NvDmaFB, NvDmaTT, &drm->channel);
+ if (ret) {
+ NV_ERROR(drm, "failed to create kernel channel, %d\n", ret);
+ nouveau_accel_fini(drm);
+ return;
+ }
+
+ if (device->card_type < NV_C0) {
+ ret = nouveau_gpuobj_new(drm->device, NULL, 32, 0, 0,
+ &drm->notify);
+ if (ret) {
+ NV_ERROR(drm, "failed to allocate notifier, %d\n", ret);
+ nouveau_accel_fini(drm);
+ return;
+ }
+
+ ret = nouveau_object_new(nv_object(drm),
+ drm->channel->handle, NvNotify0,
+ 0x003d, &(struct nv_dma_class) {
+ .flags = NV_DMA_TARGET_VRAM |
+ NV_DMA_ACCESS_RDWR,
+ .start = drm->notify->addr,
+ .limit = drm->notify->addr + 31
+ }, sizeof(struct nv_dma_class),
+ &object);
+ if (ret) {
+ nouveau_accel_fini(drm);
+ return;
+ }
+ }
+
+
+ nouveau_bo_move_init(drm->channel);
+}
+
static int __devinit
nouveau_drm_probe(struct pci_dev *pdev, const struct pci_device_id *pent)
{
struct nouveau_device *device;
+ struct apertures_struct *aper;
+ bool boot = false;
int ret;
+ /* remove conflicting drivers (vesafb, efifb etc) */
+ aper = alloc_apertures(3);
+ if (!aper)
+ return -ENOMEM;
+
+ aper->ranges[0].base = pci_resource_start(pdev, 1);
+ aper->ranges[0].size = pci_resource_len(pdev, 1);
+ aper->count = 1;
+
+ if (pci_resource_len(pdev, 2)) {
+ aper->ranges[aper->count].base = pci_resource_start(pdev, 2);
+ aper->ranges[aper->count].size = pci_resource_len(pdev, 2);
+ aper->count++;
+ }
+
+ if (pci_resource_len(pdev, 3)) {
+ aper->ranges[aper->count].base = pci_resource_start(pdev, 3);
+ aper->ranges[aper->count].size = pci_resource_len(pdev, 3);
+ aper->count++;
+ }
+
+#ifdef CONFIG_X86
+ boot = pdev->resource[PCI_ROM_RESOURCE].flags & IORESOURCE_ROM_SHADOW;
+#endif
+ remove_conflicting_framebuffers(aper, "nouveaufb", boot);
+
ret = nouveau_device_create(pdev, nouveau_name(pdev), pci_name(pdev),
nouveau_config, nouveau_debug, &device);
if (ret)
ret = nouveau_pci_probe(pdev, pent);
if (ret) {
- nouveau_device_destroy(&device);
+ nouveau_object_ref(NULL, (struct nouveau_object **)&device);
return ret;
}
nouveau_drm_load(struct drm_device *dev, unsigned long flags)
{
struct pci_dev *pdev = dev->pdev;
+ struct nouveau_device *device;
struct nouveau_drm *drm;
int ret;
return ret;
INIT_LIST_HEAD(&drm->clients);
+ spin_lock_init(&drm->tile.lock);
drm->dev = dev;
/* make sure AGP controller is in a consistent state before we
}, sizeof(struct nv_device_class),
&drm->device);
if (ret)
- return ret;
+ goto fail_device;
nouveau_agp_reset(drm);
nouveau_object_del(nv_object(drm), NVDRM_CLIENT, NVDRM_DEVICE);
if (ret)
goto fail_device;
+ device = nv_device(drm->device);
+
/* initialise AGP */
nouveau_agp_init(drm);
- ret = nouveau_load(dev, flags);
+ if (device->card_type >= NV_50) {
+ ret = nouveau_vm_new(nv_device(drm->device), 0, (1ULL << 40),
+ 0x1000, &drm->client.base.vm);
+ if (ret)
+ goto fail_device;
+ }
+
+ ret = nouveau_ttm_init(drm);
if (ret)
goto fail_device;
+ ret = nouveau_load(dev, flags);
+ if (ret)
+ goto fail_load;
+
+ nouveau_accel_init(drm);
+ nouveau_fbcon_init(dev);
return 0;
+fail_load:
+ nouveau_ttm_fini(drm);
fail_device:
nouveau_cli_destroy(&drm->client);
return ret;
struct pci_dev *pdev = dev->pdev;
int ret;
+ nouveau_fbcon_fini(dev);
+ nouveau_accel_fini(drm);
+
ret = nouveau_unload(dev);
if (ret)
return ret;
+ nouveau_ttm_fini(drm);
nouveau_agp_fini(drm);
pci_set_drvdata(pdev, drm->client.base.device);
static void
nouveau_drm_remove(struct pci_dev *pdev)
{
- struct nouveau_device *device;
+ struct nouveau_object *device;
nouveau_pci_remove(pdev);
device = pci_get_drvdata(pdev);
- nouveau_device_destroy(&device);
+ nouveau_object_ref(NULL, &device);
+ nouveau_object_debug();
}
int
pm_state.event == PM_EVENT_PRETHAW)
return 0;
+ NV_INFO(drm, "suspending fbcon...\n");
+ nouveau_fbcon_set_suspend(dev, 1);
+
+ NV_INFO(drm, "suspending drm...\n");
ret = nouveau_pci_suspend(pdev, pm_state);
if (ret)
return ret;
+ NV_INFO(drm, "evicting buffers...\n");
+ ttm_bo_evict_mm(&drm->ttm.bdev, TTM_PL_VRAM);
+
+ if (drm->fence && nouveau_fence(drm)->suspend) {
+ if (!nouveau_fence(drm)->suspend(drm))
+ return -ENOMEM;
+ }
+
+ NV_INFO(drm, "suspending client object trees...\n");
list_for_each_entry(cli, &drm->clients, head) {
ret = nouveau_client_fini(&cli->base, true);
if (ret)
if (dev->switch_power_state == DRM_SWITCH_POWER_OFF)
return 0;
+ NV_INFO(drm, "re-enabling device...\n");
pci_set_power_state(pdev, PCI_D0);
pci_restore_state(pdev);
ret = pci_enable_device(pdev);
nouveau_agp_reset(drm);
+ NV_INFO(drm, "resuming client object trees...\n");
nouveau_client_init(&drm->client.base);
+ nouveau_agp_init(drm);
list_for_each_entry(cli, &drm->clients, head) {
nouveau_client_init(&cli->base);
}
- nouveau_agp_init(drm);
+ if (drm->fence && nouveau_fence(drm)->resume)
+ nouveau_fence(drm)->resume(drm);
return nouveau_pci_resume(pdev);
}
+int
+nouveau_drm_open(struct drm_device *dev, struct drm_file *fpriv)
+{
+ struct pci_dev *pdev = dev->pdev;
+ struct nouveau_drm *drm = nouveau_drm(dev);
+ struct nouveau_cli *cli;
+ int ret;
+
+ ret = nouveau_cli_create(pdev, fpriv->pid, sizeof(*cli), (void **)&cli);
+ if (ret)
+ return ret;
+
+ if (nv_device(drm->device)->card_type >= NV_50) {
+ ret = nouveau_vm_new(nv_device(drm->device), 0, (1ULL << 40),
+ 0x1000, &cli->base.vm);
+ if (ret) {
+ nouveau_cli_destroy(cli);
+ return ret;
+ }
+ }
+
+ fpriv->driver_priv = cli;
+
+ mutex_lock(&drm->client.mutex);
+ list_add(&cli->head, &drm->clients);
+ mutex_unlock(&drm->client.mutex);
+ return 0;
+}
+
+void
+nouveau_drm_preclose(struct drm_device *dev, struct drm_file *fpriv)
+{
+ struct nouveau_cli *cli = nouveau_cli(fpriv);
+ struct nouveau_drm *drm = nouveau_drm(dev);
+
+ if (cli->abi16)
+ nouveau_abi16_fini(cli->abi16);
+
+ mutex_lock(&drm->client.mutex);
+ list_del(&cli->head);
+ mutex_unlock(&drm->client.mutex);
+}
+
+void
+nouveau_drm_postclose(struct drm_device *dev, struct drm_file *fpriv)
+{
+ struct nouveau_cli *cli = nouveau_cli(fpriv);
+ nouveau_cli_destroy(cli);
+}
+
static struct pci_device_id
nouveau_drm_pci_table[] = {
{