diff --git a/include/linux/sched.h b/include/linux/sched.h
index 6fc8f45de4e912f1196d07a5ace4d4cc752ebe3f..ed1650699563747ea9d48ff28b7192db9bb41c66 100644 (file)
--- a/include/linux/sched.h
+++ b/include/linux/sched.h
#define TASK_DEAD 64
#define TASK_WAKEKILL 128
#define TASK_WAKING 256
-#define TASK_STATE_MAX 512
+#define TASK_PARKED 512
+#define TASK_STATE_MAX 1024
-#define TASK_STATE_TO_CHAR_STR "RSDTtZXxKW"
+#define TASK_STATE_TO_CHAR_STR "RSDTtZXxKWP"
extern char ___assert_task_state[1 - 2*!!(
sizeof(TASK_STATE_TO_CHAR_STR)-1 != ilog2(TASK_STATE_MAX)+1)];
extern void task_cputime_adjusted(struct task_struct *p, cputime_t *ut, cputime_t *st);
extern void thread_group_cputime_adjusted(struct task_struct *p, cputime_t *ut, cputime_t *st);
+extern int task_free_register(struct notifier_block *n);
+extern int task_free_unregister(struct notifier_block *n);
+
/*
* Per process flags
*/
*
* Lock the threadgroup @tsk belongs to. No new task is allowed to enter
* and member tasks aren't allowed to exit (as indicated by PF_EXITING) or
- * perform exec. This is useful for cases where the threadgroup needs to
- * stay stable across blockable operations.
+ * change ->group_leader/pid. This is useful for cases where the threadgroup
+ * needs to stay stable across blockable operations.
*
* fork and exit paths explicitly call threadgroup_change_{begin|end}() for
* synchronization. While held, no new task will be added to threadgroup
* and no existing live task will have its PF_EXITING set.
*
- * During exec, a task goes and puts its thread group through unusual
- * changes. After de-threading, exclusive access is assumed to resources
- * which are usually shared by tasks in the same group - e.g. sighand may
- * be replaced with a new one. Also, the exec'ing task takes over group
- * leader role including its pid. Exclude these changes while locked by
- * grabbing cred_guard_mutex which is used to synchronize exec path.
+ * de_thread() does threadgroup_change_{begin|end}() when a non-leader
+ * sub-thread becomes a new leader.
*/
static inline void threadgroup_lock(struct task_struct *tsk)
{
- /*
- * exec uses exit for de-threading nesting group_rwsem inside
- * cred_guard_mutex. Grab cred_guard_mutex first.
- */
- mutex_lock(&tsk->signal->cred_guard_mutex);
down_write(&tsk->signal->group_rwsem);
}
static inline void threadgroup_unlock(struct task_struct *tsk)
{
up_write(&tsk->signal->group_rwsem);
- mutex_unlock(&tsk->signal->cred_guard_mutex);
}
#else
static inline void threadgroup_change_begin(struct task_struct *tsk) {}
extern void recalc_sigpending_and_wake(struct task_struct *t);
extern void recalc_sigpending(void);
-extern void signal_wake_up(struct task_struct *t, int resume_stopped);
+extern void signal_wake_up_state(struct task_struct *t, unsigned int state);
+
+static inline void signal_wake_up(struct task_struct *t, bool resume)
+{
+ signal_wake_up_state(t, resume ? TASK_WAKEKILL : 0);
+}
+static inline void ptrace_signal_wake_up(struct task_struct *t, bool resume)
+{
+ signal_wake_up_state(t, resume ? __TASK_TRACED : 0);
+}
/*
* Wrappers for p->thread_info->cpu access. No-op on UP.