]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commit
Merge tag 'mfd-3.8-1' of git://git.kernel.org/pub/scm/linux/kernel/git/sameo/mfd-2.6
authorLinus Torvalds <torvalds@linux-foundation.org>
Mon, 17 Dec 2012 02:55:20 +0000 (18:55 -0800)
committerLinus Torvalds <torvalds@linux-foundation.org>
Mon, 17 Dec 2012 02:55:20 +0000 (18:55 -0800)
commit2dfea3803dcf70983d14ce1dcbb3e97a7459a28b
tree59bffc7389ff554585f79d7cc06021790dc2b317
parentaed606e3bc1f10753254db308d3fd8c053c41328
parent1881b68b8961a86d40c3c5c205e533515a2dc9c6
Merge tag 'mfd-3.8-1' of git://git.kernel.org/pub/scm/linux/kernel/git/sameo/mfd-2.6

Pull MFS update from Samuel Ortiz:
 "This is the MFD patch set for the 3.8 merge window.

  We have several new drivers, most of the time coming with their sub
  devices drivers:

   - Austria Microsystem's AS3711
   - Nano River's viperboard
   - TI's TPS80031, AM335x TS/ADC,
   - Realtek's MMC/memstick card reader
   - Nokia's retu

  We also got some notable cleanups and improvements:

   - tps6586x got converted to IRQ domains.
   - tps65910 and tps65090 moved to the regmap IRQ API.
   - STMPE is now Device Tree aware.
   - A general twl6040 and twl-core cleanup, with moves to the regmap
     I/O and IRQ APIs and a conversion to the recently added PWM
     framework.
   - sta2x11 gained regmap support.

  Then the rest is mostly tiny cleanups and fixes, among which we have
  Mark's wm5xxx and wm8xxx patchset."

Far amount of annoying but largely trivial conflicts.  Many due to
__devinit/exit removal, others due to one or two of the new drivers also
having come in through another tree.

* tag 'mfd-3.8-1' of git://git.kernel.org/pub/scm/linux/kernel/git/sameo/mfd-2.6: (119 commits)
  mfd: tps6507x: Convert to devm_kzalloc
  mfd: stmpe: Update DT support for stmpe driver
  mfd: wm5102: Add readback of DSP status 3 register
  mfd: arizona: Log if we fail to create the primary IRQ domain
  mfd: tps80031: MFD_TPS80031 needs to select REGMAP_IRQ
  mfd: tps80031: Add terminating entry for tps80031_id_table
  mfd: sta2x11: Fix potential NULL pointer dereference in __sta2x11_mfd_mask()
  mfd: wm5102: Add tuning for revision B
  mfd: arizona: Defer patch initialistation until after first device boot
  mfd: tps65910: Fix wrong ack_base register
  mfd: tps65910: Remove unused data
  mfd: stmpe: Get rid of irq_invert_polarity
  mfd: ab8500-core: Fix invalid free of devm_ allocated data
  mfd: wm5102: Mark DSP memory regions as volatile
  mfd: wm5102: Correct default for LDO1_CONTROL_2
  mfd: arizona: Register haptics devices
  mfd: wm8994: Make current device behaviour the default
  mfd: tps65090: MFD_TPS65090 needs to select REGMAP_IRQ
  mfd: Fix stmpe.c build when OF is not enabled
  mfd: jz4740-adc: Use devm_kzalloc
  ...
37 files changed:
drivers/gpio/Kconfig
drivers/gpio/Makefile
drivers/gpio/gpio-da9052.c
drivers/gpio/gpio-tps6586x.c
drivers/gpio/gpio-twl4030.c
drivers/iio/adc/Kconfig
drivers/iio/adc/Makefile
drivers/mfd/Kconfig
drivers/mfd/Makefile
drivers/mfd/ab8500-core.c
drivers/mfd/arizona-core.c
drivers/mfd/arizona-irq.c
drivers/mfd/da9052-core.c
drivers/mfd/db8500-prcmu.c
drivers/mfd/jz4740-adc.c
drivers/mfd/lpc_ich.c
drivers/mfd/mc13xxx-i2c.c
drivers/mfd/mc13xxx-spi.c
drivers/mfd/sta2x11-mfd.c
drivers/mfd/stmpe-i2c.c
drivers/mfd/stmpe.c
drivers/mfd/tps65090.c
drivers/mfd/tps65217.c
drivers/mfd/tps6586x.c
drivers/mfd/tps65910.c
drivers/mfd/twl-core.c
drivers/mfd/twl4030-irq.c
drivers/mfd/twl4030-madc.c
drivers/mfd/twl4030-power.c
drivers/mfd/wm5102-tables.c
drivers/mfd/wm8994-core.c
drivers/mmc/host/Makefile
drivers/power/da9052-battery.c
include/linux/mfd/arizona/registers.h
include/linux/mfd/da9055/pdata.h
include/linux/mfd/tps65090.h
include/linux/mfd/tps6586x.h