author | Rafael J. Wysocki <rafael.j.wysocki@intel.com> | |
Fri, 3 Apr 2015 21:23:37 +0000 (23:23 +0200) | ||
committer | Praneeth Bajjuri <praneeth@ti.com> | |
Tue, 24 Nov 2015 23:19:27 +0000 (17:19 -0600) | ||
commit | 2e41c7d8bc9233848ad541c788bc792db341136f | |
tree | abcc191e8bd72cb2309d26a1120b0dcdd0df7ea7 | tree | snapshot (tar.xz tar.gz zip) |
parent | 107ccfc2b8022a1b2c4faefc1930278eebc9cc95 | commit | diff |
device property: Make it possible to use secondary firmware nodes
Add a secondary pointer to struct fwnode_handle so as to make it
possible for a device to have two firmware nodes associated with
it at the same time, for example, an ACPI node and a node with
a set of properties provided by platform initialization code.
In the future that will allow device property lookup to fall back
from the primary firmware node to the secondary one if the given
property is not present there to make it easier to provide defaults
for device properties used by device drivers.
Introduce two helper routines, set_primary_fwnode() and
set_secondary_fwnode() allowing callers to add a primary/secondary
firmware node to the given device in such a way that
(1) If there's only one firmware node for that device, it will be
pointed to by the device's firmware node pointer.
(2) If both the primary and secondary firmware nodes are present,
the primary one will be pointed to by the device's firmware
node pointer, while the secondary one will be pointed to by the
primary node's secondary pointer.
(3) If one of these nodes is removed (by calling one of the new
nelpers with NULL as the second argument), the other one will
be preserved.
Make ACPI use set_primary_fwnode() for attaching its firmware nodes
to devices.
Change-Id: Ief75df58b5f447e353755ada9fc3d4efbc4d8191
Signed-off-by: Rafael J. Wysocki <rafael.j.wysocki@intel.com>
Tested-by: Heikki Krogerus <heikki.krogerus@linux.intel.com>
Acked-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Add a secondary pointer to struct fwnode_handle so as to make it
possible for a device to have two firmware nodes associated with
it at the same time, for example, an ACPI node and a node with
a set of properties provided by platform initialization code.
In the future that will allow device property lookup to fall back
from the primary firmware node to the secondary one if the given
property is not present there to make it easier to provide defaults
for device properties used by device drivers.
Introduce two helper routines, set_primary_fwnode() and
set_secondary_fwnode() allowing callers to add a primary/secondary
firmware node to the given device in such a way that
(1) If there's only one firmware node for that device, it will be
pointed to by the device's firmware node pointer.
(2) If both the primary and secondary firmware nodes are present,
the primary one will be pointed to by the device's firmware
node pointer, while the secondary one will be pointed to by the
primary node's secondary pointer.
(3) If one of these nodes is removed (by calling one of the new
nelpers with NULL as the second argument), the other one will
be preserved.
Make ACPI use set_primary_fwnode() for attaching its firmware nodes
to devices.
Change-Id: Ief75df58b5f447e353755ada9fc3d4efbc4d8191
Signed-off-by: Rafael J. Wysocki <rafael.j.wysocki@intel.com>
Tested-by: Heikki Krogerus <heikki.krogerus@linux.intel.com>
Acked-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
include/linux/fwnode.h | diff | blob | history |