author | David S. Miller <davem@davemloft.net> | |
Wed, 7 May 2014 04:27:37 +0000 (21:27 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 14 Aug 2014 01:38:26 +0000 (09:38 +0800) | ||
commit | 8f0a3c34dd189a5318c23dbb82b3c675669e10e0 | |
tree | 9cf9b684695873a6664b78727c511f638bc4526d | tree | snapshot (tar.xz tar.gz zip) |
parent | 89e69c2e74e8b45bd4ae90201e68f1762dc6edca | commit | diff |
sparc64: Don't bark so loudly about 32-bit tasks generating 64-bit fault addresses.
[ Upstream commit e5c460f46ae7ee94831cb55cb980f942aa9e5a85 ]
This was found using Dave Jone's trinity tool.
When a user process which is 32-bit performs a load or a store, the
cpu chops off the top 32-bits of the effective address before
translating it.
This is because we run 32-bit tasks with the PSTATE_AM (address
masking) bit set.
We can't run the kernel with that bit set, so when the kernel accesses
userspace no address masking occurs.
Since a 32-bit process will have no mappings in that region we will
properly fault, so we don't try to handle this using access_ok(),
which can safely just be a NOP on sparc64.
Real faults from 32-bit processes should never generate such addresses
so a bug check was added long ago, and it barks in the logs if this
happens.
But it also barks when a kernel user access causes this condition, and
that _can_ happen. For example, if a pointer passed into a system call
is "0xfffffffc" and the kernel access 4 bytes offset from that pointer.
Just handle such faults normally via the exception entries.
Signed-off-by: David S. Miller <davem@davemloft.net>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
[ Upstream commit e5c460f46ae7ee94831cb55cb980f942aa9e5a85 ]
This was found using Dave Jone's trinity tool.
When a user process which is 32-bit performs a load or a store, the
cpu chops off the top 32-bits of the effective address before
translating it.
This is because we run 32-bit tasks with the PSTATE_AM (address
masking) bit set.
We can't run the kernel with that bit set, so when the kernel accesses
userspace no address masking occurs.
Since a 32-bit process will have no mappings in that region we will
properly fault, so we don't try to handle this using access_ok(),
which can safely just be a NOP on sparc64.
Real faults from 32-bit processes should never generate such addresses
so a bug check was added long ago, and it barks in the logs if this
happens.
But it also barks when a kernel user access causes this condition, and
that _can_ happen. For example, if a pointer passed into a system call
is "0xfffffffc" and the kernel access 4 bytes offset from that pointer.
Just handle such faults normally via the exception entries.
Signed-off-by: David S. Miller <davem@davemloft.net>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
arch/sparc/mm/fault_64.c | diff | blob | history |