]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commit
nilfs2: fix fix very long mount time issue
authorVyacheslav Dubeyko <slava@dubeyko.com>
Mon, 4 Feb 2013 22:28:41 +0000 (14:28 -0800)
committerLinus Torvalds <torvalds@linux-foundation.org>
Tue, 5 Feb 2013 09:38:46 +0000 (20:38 +1100)
commita9bae189542e71f91e61a4428adf6e5a7dfe8063
tree4468b0d8bb50bfe762a02b9fd609c4265fef610d
parent6edacf05c8362f4c368991b55d85e8122cfc9a24
nilfs2: fix fix very long mount time issue

There exists a situation when GC can work in background alone without
any other filesystem activity during significant time.

The nilfs_clean_segments() method calls nilfs_segctor_construct() that
updates superblocks in the case of NILFS_SC_SUPER_ROOT and
THE_NILFS_DISCONTINUED flags are set.  But when GC is working alone the
nilfs_clean_segments() is called with unset THE_NILFS_DISCONTINUED flag.
As a result, the update of superblocks doesn't occurred all this time
and in the case of SPOR superblocks keep very old values of last super
root placement.

SYMPTOMS:

Trying to mount a NILFS2 volume after SPOR in such environment ends with
very long mounting time (it can achieve about several hours in some
cases).

REPRODUCING PATH:

1. It needs to use external USB HDD, disable automount and doesn't
   make any additional filesystem activity on the NILFS2 volume.

2. Generate temporary file with size about 100 - 500 GB (for example,
   dd if=/dev/zero of=<file_name> bs=1073741824 count=200).  The size of
   file defines duration of GC working.

3. Then it needs to delete file.

4. Start GC manually by means of command "nilfs-clean -p 0".  When you
   start GC by means of such way then, at the end, superblocks is updated
   by once.  So, for simulation of SPOR, it needs to wait sometime (15 -
   40 minutes) and simply switch off USB HDD manually.

5. Switch on USB HDD again and try to mount NILFS2 volume.  As a
   result, NILFS2 volume will mount during very long time.

REPRODUCIBILITY: 100%

FIX:

This patch adds checking that superblocks need to update and set
THE_NILFS_DISCONTINUED flag before nilfs_clean_segments() call.

Reported-by: Sergey Alexandrov <splavgm@gmail.com>
Signed-off-by: Vyacheslav Dubeyko <slava@dubeyko.com>
Tested-by: Vyacheslav Dubeyko <slava@dubeyko.com>
Acked-by: Ryusuke Konishi <konishi.ryusuke@lab.ntt.co.jp>
Tested-by: Ryusuke Konishi <konishi.ryusuke@lab.ntt.co.jp>
Cc: <stable@vger.kernel.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
fs/nilfs2/ioctl.c