]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commit
drm/omap: Take a fb reference in omap_plane_update()
authorArchit Taneja <archit@ti.com>
Tue, 9 Apr 2013 12:26:00 +0000 (15:26 +0300)
committerArchit Taneja <archit@ti.com>
Thu, 30 May 2013 15:39:26 +0000 (21:09 +0530)
commitd70dab599e57e5a96d54213b400bda01f38f1224
tree4f98c7e4a2dea3d5cf62a85a52a32c6746264866
parentc7997fc9b5e3ecd3b0c1ad734e4e3d458490c2c1
drm/omap: Take a fb reference in omap_plane_update()

When userspace calls SET_PLANE ioctl, drm core takes a reference of the fb and
passes control to the update_plane op defined by the drm driver.

In omapdrm, we have a worker thread which queues framebuffers objects received
from update_plane and displays them at the appropriate time.

It is possible that the framebuffer is destoryed by userspace between the time
of calling the ioctl and apply-worker being scheduled. If this happens, the
apply-worker holds a pointer to a framebuffer which is already destroyed.

Take an extra refernece/unreference of the fb in omap_plane_update() to prevent
this from happening. A reference is taken of the fb passed to update_plane(),
the previous framebuffer (held by plane->fb) is unreferenced. This will prevent
drm from destroying the framebuffer till the time it's unreferenced by the
apply-worker.

This is in addition to the exisitng reference/unreference in update_pin(),
which is taken for the scanout of the plane's current framebuffer, and an
unreference the previous framebuffer.

Signed-off-by: Archit Taneja <archit@ti.com>
Reviewed-by: Rob Clark <robdclark@gmail.com>
Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
drivers/gpu/drm/omapdrm/omap_plane.c