author | Pekka Enberg <penberg@kernel.org> | |
Tue, 18 Dec 2012 10:46:20 +0000 (12:46 +0200) | ||
committer | Pekka Enberg <penberg@kernel.org> | |
Tue, 18 Dec 2012 10:46:20 +0000 (12:46 +0200) |
Fix up a trivial merge conflict with commit baaf1dd ("mm/slob: use
min_t() to compare ARCH_SLAB_MINALIGN") that did not go through the slab
tree.
Conflicts:
mm/slob.c
Signed-off-by: Pekka Enberg <penberg@kernel.org>
min_t() to compare ARCH_SLAB_MINALIGN") that did not go through the slab
tree.
Conflicts:
mm/slob.c
Signed-off-by: Pekka Enberg <penberg@kernel.org>
include/linux/mm_types.h | patch | blob | history | |
include/linux/slab.h | patch | blob | history | |
include/linux/slab_def.h | patch | blob | history | |
mm/slab.c | patch | blob | history | |
mm/slab.h | patch | blob | history | |
mm/slab_common.c | patch | blob | history | |
mm/slob.c | patch | blob | history | |
mm/slub.c | patch | blob | history |
index 31f8a3af7d942545562afd1fcacf11f52a4f82a0..2fef4e720e7955547cb3070f06c083f14a800063 100644 (file)
--- a/include/linux/mm_types.h
+++ b/include/linux/mm_types.h
};
struct list_head list; /* slobs list of pages */
- struct { /* slab fields */
- struct kmem_cache *slab_cache;
- struct slab *slab_page;
- };
+ struct slab *slab_page; /* slab fields */
};
/* Remainder is not double word aligned */
#if USE_SPLIT_PTLOCKS
spinlock_t ptl;
#endif
- struct kmem_cache *slab; /* SLUB: Pointer to slab */
+ struct kmem_cache *slab_cache; /* SL[AU]B: Pointer to slab */
struct page *first_page; /* Compound tail pages */
};
diff --git a/include/linux/slab.h b/include/linux/slab.h
index 83d1a1454b7edea3bc32e91fc4b03b58e52af474..743a104151229e0efc5416cf7a54383d3ba41c82 100644 (file)
--- a/include/linux/slab.h
+++ b/include/linux/slab.h
void kmem_cache_destroy(struct kmem_cache *);
int kmem_cache_shrink(struct kmem_cache *);
void kmem_cache_free(struct kmem_cache *, void *);
-unsigned int kmem_cache_size(struct kmem_cache *);
/*
* Please use this macro to create slab caches. Simply specify the
return kmalloc_node(size, flags | __GFP_ZERO, node);
}
+/*
+ * Determine the size of a slab object
+ */
+static inline unsigned int kmem_cache_size(struct kmem_cache *s)
+{
+ return s->object_size;
+}
+
void __init kmem_cache_init_late(void);
#endif /* _LINUX_SLAB_H */
index cc290f0bdb346efe82dbe0e87985e6d015ad58e1..45c0356fdc8c086f8b392b5ff6c8813a01679a32 100644 (file)
--- a/include/linux/slab_def.h
+++ b/include/linux/slab_def.h
* (see kmem_cache_init())
* We still use [NR_CPUS] and not [1] or [0] because cache_cache
* is statically defined, so we reserve the max number of cpus.
+ *
+ * We also need to guarantee that the list is able to accomodate a
+ * pointer for each node since "nodelists" uses the remainder of
+ * available pointers.
*/
struct kmem_list3 **nodelists;
- struct array_cache *array[NR_CPUS];
+ struct array_cache *array[NR_CPUS + MAX_NUMNODES];
/*
* Do not add fields after array[]
*/
diff --git a/mm/slab.c b/mm/slab.c
index 6d5c83c6ddd5d416ce8ca5716bf38740bbb70540..2c3a2e0394db6737887cb0309c27988ca0edb621 100644 (file)
--- a/mm/slab.c
+++ b/mm/slab.c
*/
static bool pfmemalloc_active __read_mostly;
-/* Legal flag mask for kmem_cache_create(). */
-#if DEBUG
-# define CREATE_MASK (SLAB_RED_ZONE | \
- SLAB_POISON | SLAB_HWCACHE_ALIGN | \
- SLAB_CACHE_DMA | \
- SLAB_STORE_USER | \
- SLAB_RECLAIM_ACCOUNT | SLAB_PANIC | \
- SLAB_DESTROY_BY_RCU | SLAB_MEM_SPREAD | \
- SLAB_DEBUG_OBJECTS | SLAB_NOLEAKTRACE | SLAB_NOTRACK)
-#else
-# define CREATE_MASK (SLAB_HWCACHE_ALIGN | \
- SLAB_CACHE_DMA | \
- SLAB_RECLAIM_ACCOUNT | SLAB_PANIC | \
- SLAB_DESTROY_BY_RCU | SLAB_MEM_SPREAD | \
- SLAB_DEBUG_OBJECTS | SLAB_NOLEAKTRACE | SLAB_NOTRACK)
-#endif
-
/*
* kmem_bufctl_t:
*
#undef CACHE
};
-static struct arraycache_init initarray_cache __initdata =
- { {0, BOOT_CPUCACHE_ENTRIES, 1, 0} };
static struct arraycache_init initarray_generic =
{ {0, BOOT_CPUCACHE_ENTRIES, 1, 0} };
/* internal cache of cache description objs */
-static struct kmem_list3 *kmem_cache_nodelists[MAX_NUMNODES];
static struct kmem_cache kmem_cache_boot = {
- .nodelists = kmem_cache_nodelists,
.batchcount = 1,
.limit = BOOT_CPUCACHE_ENTRIES,
.shared = 1,
}
}
+/*
+ * The memory after the last cpu cache pointer is used for the
+ * the nodelists pointer.
+ */
+static void setup_nodelists_pointer(struct kmem_cache *cachep)
+{
+ cachep->nodelists = (struct kmem_list3 **)&cachep->array[nr_cpu_ids];
+}
+
/*
* Initialisation. Called after the page allocator have been initialised and
* before smp_init().
*/
void __init kmem_cache_init(void)
{
- size_t left_over;
struct cache_sizes *sizes;
struct cache_names *names;
int i;
- int order;
- int node;
kmem_cache = &kmem_cache_boot;
+ setup_nodelists_pointer(kmem_cache);
if (num_possible_nodes() == 1)
use_alien_caches = 0;
- for (i = 0; i < NUM_INIT_LISTS; i++) {
+ for (i = 0; i < NUM_INIT_LISTS; i++)
kmem_list3_init(&initkmem_list3[i]);
- if (i < MAX_NUMNODES)
- kmem_cache->nodelists[i] = NULL;
- }
+
set_up_list3s(kmem_cache, CACHE_CACHE);
/*
* 6) Resize the head arrays of the kmalloc caches to their final sizes.
*/
- node = numa_mem_id();
-
/* 1) create the kmem_cache */
- INIT_LIST_HEAD(&slab_caches);
- list_add(&kmem_cache->list, &slab_caches);
- kmem_cache->colour_off = cache_line_size();
- kmem_cache->array[smp_processor_id()] = &initarray_cache.cache;
- kmem_cache->nodelists[node] = &initkmem_list3[CACHE_CACHE + node];
/*
* struct kmem_cache size depends on nr_node_ids & nr_cpu_ids
*/
- kmem_cache->size = offsetof(struct kmem_cache, array[nr_cpu_ids]) +
- nr_node_ids * sizeof(struct kmem_list3 *);
- kmem_cache->object_size = kmem_cache->size;
- kmem_cache->size = ALIGN(kmem_cache->object_size,
- cache_line_size());
- kmem_cache->reciprocal_buffer_size =
- reciprocal_value(kmem_cache->size);
-
- for (order = 0; order < MAX_ORDER; order++) {
- cache_estimate(order, kmem_cache->size,
- cache_line_size(), 0, &left_over, &kmem_cache->num);
- if (kmem_cache->num)
- break;
- }
- BUG_ON(!kmem_cache->num);
- kmem_cache->gfporder = order;
- kmem_cache->colour = left_over / kmem_cache->colour_off;
- kmem_cache->slab_size = ALIGN(kmem_cache->num * sizeof(kmem_bufctl_t) +
- sizeof(struct slab), cache_line_size());
+ create_boot_cache(kmem_cache, "kmem_cache",
+ offsetof(struct kmem_cache, array[nr_cpu_ids]) +
+ nr_node_ids * sizeof(struct kmem_list3 *),
+ SLAB_HWCACHE_ALIGN);
+ list_add(&kmem_cache->list, &slab_caches);
/* 2+3) create the kmalloc caches */
sizes = malloc_sizes;
* bug.
*/
- sizes[INDEX_AC].cs_cachep = kmem_cache_zalloc(kmem_cache, GFP_NOWAIT);
- sizes[INDEX_AC].cs_cachep->name = names[INDEX_AC].name;
- sizes[INDEX_AC].cs_cachep->size = sizes[INDEX_AC].cs_size;
- sizes[INDEX_AC].cs_cachep->object_size = sizes[INDEX_AC].cs_size;
- sizes[INDEX_AC].cs_cachep->align = ARCH_KMALLOC_MINALIGN;
- __kmem_cache_create(sizes[INDEX_AC].cs_cachep, ARCH_KMALLOC_FLAGS|SLAB_PANIC);
- list_add(&sizes[INDEX_AC].cs_cachep->list, &slab_caches);
-
- if (INDEX_AC != INDEX_L3) {
- sizes[INDEX_L3].cs_cachep = kmem_cache_zalloc(kmem_cache, GFP_NOWAIT);
- sizes[INDEX_L3].cs_cachep->name = names[INDEX_L3].name;
- sizes[INDEX_L3].cs_cachep->size = sizes[INDEX_L3].cs_size;
- sizes[INDEX_L3].cs_cachep->object_size = sizes[INDEX_L3].cs_size;
- sizes[INDEX_L3].cs_cachep->align = ARCH_KMALLOC_MINALIGN;
- __kmem_cache_create(sizes[INDEX_L3].cs_cachep, ARCH_KMALLOC_FLAGS|SLAB_PANIC);
- list_add(&sizes[INDEX_L3].cs_cachep->list, &slab_caches);
- }
+ sizes[INDEX_AC].cs_cachep = create_kmalloc_cache(names[INDEX_AC].name,
+ sizes[INDEX_AC].cs_size, ARCH_KMALLOC_FLAGS);
+
+ if (INDEX_AC != INDEX_L3)
+ sizes[INDEX_L3].cs_cachep =
+ create_kmalloc_cache(names[INDEX_L3].name,
+ sizes[INDEX_L3].cs_size, ARCH_KMALLOC_FLAGS);
slab_early_init = 0;
* Note for systems short on memory removing the alignment will
* allow tighter packing of the smaller caches.
*/
- if (!sizes->cs_cachep) {
- sizes->cs_cachep = kmem_cache_zalloc(kmem_cache, GFP_NOWAIT);
- sizes->cs_cachep->name = names->name;
- sizes->cs_cachep->size = sizes->cs_size;
- sizes->cs_cachep->object_size = sizes->cs_size;
- sizes->cs_cachep->align = ARCH_KMALLOC_MINALIGN;
- __kmem_cache_create(sizes->cs_cachep, ARCH_KMALLOC_FLAGS|SLAB_PANIC);
- list_add(&sizes->cs_cachep->list, &slab_caches);
- }
+ if (!sizes->cs_cachep)
+ sizes->cs_cachep = create_kmalloc_cache(names->name,
+ sizes->cs_size, ARCH_KMALLOC_FLAGS);
+
#ifdef CONFIG_ZONE_DMA
- sizes->cs_dmacachep = kmem_cache_zalloc(kmem_cache, GFP_NOWAIT);
- sizes->cs_dmacachep->name = names->name_dma;
- sizes->cs_dmacachep->size = sizes->cs_size;
- sizes->cs_dmacachep->object_size = sizes->cs_size;
- sizes->cs_dmacachep->align = ARCH_KMALLOC_MINALIGN;
- __kmem_cache_create(sizes->cs_dmacachep,
- ARCH_KMALLOC_FLAGS|SLAB_CACHE_DMA| SLAB_PANIC);
- list_add(&sizes->cs_dmacachep->list, &slab_caches);
+ sizes->cs_dmacachep = create_kmalloc_cache(
+ names->name_dma, sizes->cs_size,
+ SLAB_CACHE_DMA|ARCH_KMALLOC_FLAGS);
#endif
sizes++;
names++;
ptr = kmalloc(sizeof(struct arraycache_init), GFP_NOWAIT);
- BUG_ON(cpu_cache_get(kmem_cache) != &initarray_cache.cache);
memcpy(ptr, cpu_cache_get(kmem_cache),
sizeof(struct arraycache_init));
/*
@@ -2282,7 +2224,15 @@ static int __init_refok setup_cpu_cache(struct kmem_cache *cachep, gfp_t gfp)
if (slab_state == DOWN) {
/*
- * Note: the first kmem_cache_create must create the cache
+ * Note: Creation of first cache (kmem_cache).
+ * The setup_list3s is taken care
+ * of by the caller of __kmem_cache_create
+ */
+ cachep->array[smp_processor_id()] = &initarray_generic.cache;
+ slab_state = PARTIAL;
+ } else if (slab_state == PARTIAL) {
+ /*
+ * Note: the second kmem_cache_create must create the cache
* that's used by kmalloc(24), otherwise the creation of
* further caches will BUG().
*/
/*
* If the cache that's used by kmalloc(sizeof(kmem_list3)) is
- * the first cache, then we need to set up all its list3s,
+ * the second cache, then we need to set up all its list3s,
* otherwise the creation of further caches will BUG().
*/
set_up_list3s(cachep, SIZE_AC);
else
slab_state = PARTIAL_ARRAYCACHE;
} else {
+ /* Remaining boot caches */
cachep->array[smp_processor_id()] =
kmalloc(sizeof(struct arraycache_init), gfp);
@@ -2331,11 +2282,8 @@ static int __init_refok setup_cpu_cache(struct kmem_cache *cachep, gfp_t gfp)
/**
* __kmem_cache_create - Create a cache.
- * @name: A string which is used in /proc/slabinfo to identify this cache.
- * @size: The size of objects to be created in this cache.
- * @align: The required alignment for the objects.
+ * @cachep: cache management descriptor
* @flags: SLAB flags
- * @ctor: A constructor for the objects.
*
* Returns a ptr to the cache on success, NULL on failure.
* Cannot be called within a int, but can be interrupted.
if (flags & SLAB_DESTROY_BY_RCU)
BUG_ON(flags & SLAB_POISON);
#endif
- /*
- * Always checks flags, a caller might be expecting debug support which
- * isn't available.
- */
- BUG_ON(flags & ~CREATE_MASK);
/*
* Check that size is in terms of words. This is needed to avoid
size &= ~(BYTES_PER_WORD - 1);
}
- /* calculate the final buffer alignment: */
-
- /* 1) arch recommendation: can be overridden for debug */
- if (flags & SLAB_HWCACHE_ALIGN) {
- /*
- * Default alignment: as specified by the arch code. Except if
- * an object is really small, then squeeze multiple objects into
- * one cacheline.
- */
- ralign = cache_line_size();
- while (size <= ralign / 2)
- ralign /= 2;
- } else {
- ralign = BYTES_PER_WORD;
- }
-
/*
* Redzoning and user store require word alignment or possibly larger.
* Note this will be overridden by architecture or caller mandated
size &= ~(REDZONE_ALIGN - 1);
}
- /* 2) arch mandated alignment */
- if (ralign < ARCH_SLAB_MINALIGN) {
- ralign = ARCH_SLAB_MINALIGN;
- }
/* 3) caller mandated alignment */
if (ralign < cachep->align) {
ralign = cachep->align;
else
gfp = GFP_NOWAIT;
- cachep->nodelists = (struct kmem_list3 **)&cachep->array[nr_cpu_ids];
+ setup_nodelists_pointer(cachep);
#if DEBUG
/*
}
EXPORT_SYMBOL(kfree);
-unsigned int kmem_cache_size(struct kmem_cache *cachep)
-{
- return cachep->object_size;
-}
-EXPORT_SYMBOL(kmem_cache_size);
-
/*
* This initializes kmem_list3 or resizes various caches for all nodes.
*/
diff --git a/mm/slab.h b/mm/slab.h
index 5a43c2f136212292f85e991a95a6d8f56a95f389..1cb9c9ee0e6f3875854b6f51b206925031faaf55 100644 (file)
--- a/mm/slab.h
+++ b/mm/slab.h
/* The slab cache that manages slab cache information */
extern struct kmem_cache *kmem_cache;
+unsigned long calculate_alignment(unsigned long flags,
+ unsigned long align, unsigned long size);
+
/* Functions provided by the slab allocators */
extern int __kmem_cache_create(struct kmem_cache *, unsigned long flags);
+extern struct kmem_cache *create_kmalloc_cache(const char *name, size_t size,
+ unsigned long flags);
+extern void create_boot_cache(struct kmem_cache *, const char *name,
+ size_t size, unsigned long flags);
+
#ifdef CONFIG_SLUB
struct kmem_cache *__kmem_cache_alias(const char *name, size_t size,
size_t align, unsigned long flags, void (*ctor)(void *));
#endif
+/* Legal flag mask for kmem_cache_create(), for various configurations */
+#define SLAB_CORE_FLAGS (SLAB_HWCACHE_ALIGN | SLAB_CACHE_DMA | SLAB_PANIC | \
+ SLAB_DESTROY_BY_RCU | SLAB_DEBUG_OBJECTS )
+
+#if defined(CONFIG_DEBUG_SLAB)
+#define SLAB_DEBUG_FLAGS (SLAB_RED_ZONE | SLAB_POISON | SLAB_STORE_USER)
+#elif defined(CONFIG_SLUB_DEBUG)
+#define SLAB_DEBUG_FLAGS (SLAB_RED_ZONE | SLAB_POISON | SLAB_STORE_USER | \
+ SLAB_TRACE | SLAB_DEBUG_FREE)
+#else
+#define SLAB_DEBUG_FLAGS (0)
+#endif
+
+#if defined(CONFIG_SLAB)
+#define SLAB_CACHE_FLAGS (SLAB_MEM_SPREAD | SLAB_NOLEAKTRACE | \
+ SLAB_RECLAIM_ACCOUNT | SLAB_TEMPORARY | SLAB_NOTRACK)
+#elif defined(CONFIG_SLUB)
+#define SLAB_CACHE_FLAGS (SLAB_NOLEAKTRACE | SLAB_RECLAIM_ACCOUNT | \
+ SLAB_TEMPORARY | SLAB_NOTRACK)
+#else
+#define SLAB_CACHE_FLAGS (0)
+#endif
+
+#define CACHE_CREATE_MASK (SLAB_CORE_FLAGS | SLAB_DEBUG_FLAGS | SLAB_CACHE_FLAGS)
+
int __kmem_cache_shutdown(struct kmem_cache *);
struct seq_file;
diff --git a/mm/slab_common.c b/mm/slab_common.c
index 5fb753da6cf003aac7caf992f6bacc25101c02bc..a8e76d79ee65628cb5071b00935202536262c490 100644 (file)
--- a/mm/slab_common.c
+++ b/mm/slab_common.c
}
#endif
+/*
+ * Figure out what the alignment of the objects will be given a set of
+ * flags, a user specified alignment and the size of the objects.
+ */
+unsigned long calculate_alignment(unsigned long flags,
+ unsigned long align, unsigned long size)
+{
+ /*
+ * If the user wants hardware cache aligned objects then follow that
+ * suggestion if the object is sufficiently large.
+ *
+ * The hardware cache alignment cannot override the specified
+ * alignment though. If that is greater then use it.
+ */
+ if (flags & SLAB_HWCACHE_ALIGN) {
+ unsigned long ralign = cache_line_size();
+ while (size <= ralign / 2)
+ ralign /= 2;
+ align = max(align, ralign);
+ }
+
+ if (align < ARCH_SLAB_MINALIGN)
+ align = ARCH_SLAB_MINALIGN;
+
+ return ALIGN(align, sizeof(void *));
+}
+
+
/*
* kmem_cache_create - Create a cache.
* @name: A string which is used in /proc/slabinfo to identify this cache.
@@ -109,6 +137,13 @@ struct kmem_cache *kmem_cache_create(const char *name, size_t size, size_t align
if (!kmem_cache_sanity_check(name, size) == 0)
goto out_locked;
+ /*
+ * Some allocators will constraint the set of valid flags to a subset
+ * of all flags. We expect them to define CACHE_CREATE_MASK in this
+ * case, and we'll just provide them with a sanitized version of the
+ * passed flags.
+ */
+ flags &= CACHE_CREATE_MASK;
s = __kmem_cache_alias(name, size, align, flags, ctor);
if (s)
@@ -117,7 +152,7 @@ struct kmem_cache *kmem_cache_create(const char *name, size_t size, size_t align
s = kmem_cache_zalloc(kmem_cache, GFP_KERNEL);
if (s) {
s->object_size = s->size = size;
- s->align = align;
+ s->align = calculate_alignment(flags, align, size);
s->ctor = ctor;
s->name = kstrdup(name, GFP_KERNEL);
if (!s->name) {
return slab_state >= UP;
}
+#ifndef CONFIG_SLOB
+/* Create a cache during boot when no slab services are available yet */
+void __init create_boot_cache(struct kmem_cache *s, const char *name, size_t size,
+ unsigned long flags)
+{
+ int err;
+
+ s->name = name;
+ s->size = s->object_size = size;
+ s->align = calculate_alignment(flags, ARCH_KMALLOC_MINALIGN, size);
+ err = __kmem_cache_create(s, flags);
+
+ if (err)
+ panic("Creation of kmalloc slab %s size=%zd failed. Reason %d\n",
+ name, size, err);
+
+ s->refcount = -1; /* Exempt from merging for now */
+}
+
+struct kmem_cache *__init create_kmalloc_cache(const char *name, size_t size,
+ unsigned long flags)
+{
+ struct kmem_cache *s = kmem_cache_zalloc(kmem_cache, GFP_NOWAIT);
+
+ if (!s)
+ panic("Out of memory when creating slab %s\n", name);
+
+ create_boot_cache(s, name, size, flags);
+ list_add(&s->list, &slab_caches);
+ s->refcount = 1;
+ return s;
+}
+
+#endif /* !CONFIG_SLOB */
+
+
#ifdef CONFIG_SLABINFO
static void print_slabinfo_header(struct seq_file *m)
{
diff --git a/mm/slob.c b/mm/slob.c
index 1e921c5e9576b6db64cc07fb4f4c90a8f4e2729e..795bab7d391da90fbd68cfd7c4730485db69b294 100644 (file)
--- a/mm/slob.c
+++ b/mm/slob.c
* from kmalloc are prepended with a 4-byte header with the kmalloc size.
* If kmalloc is asked for objects of PAGE_SIZE or larger, it calls
* alloc_pages() directly, allocating compound pages so the page order
- * does not have to be separately tracked, and also stores the exact
- * allocation size in page->private so that it can be used to accurately
- * provide ksize(). These objects are detected in kfree() because slob_page()
+ * does not have to be separately tracked.
+ * These objects are detected in kfree() because PageSlab()
* is false for them.
*
* SLAB is emulated on top of SLOB by simply calling constructors and
#define SLOB_UNIT sizeof(slob_t)
#define SLOB_UNITS(size) (((size) + SLOB_UNIT - 1)/SLOB_UNIT)
-#define SLOB_ALIGN L1_CACHE_BYTES
/*
* struct slob_rcu is inserted at the tail of allocated slob blocks, which
if (likely(order))
gfp |= __GFP_COMP;
ret = slob_new_pages(gfp, order, node);
- if (ret) {
- struct page *page;
- page = virt_to_page(ret);
- page->private = size;
- }
trace_kmalloc_node(caller, ret,
size, PAGE_SIZE << order, gfp, node);
unsigned int *m = (unsigned int *)(block - align);
slob_free(m, *m + align);
} else
- put_page(sp);
+ __free_pages(sp, compound_order(sp));
}
EXPORT_SYMBOL(kfree);
size_t ksize(const void *block)
{
struct page *sp;
+ int align;
+ unsigned int *m;
BUG_ON(!block);
if (unlikely(block == ZERO_SIZE_PTR))
return 0;
sp = virt_to_page(block);
- if (PageSlab(sp)) {
- int align = max_t(size_t, ARCH_KMALLOC_MINALIGN, ARCH_SLAB_MINALIGN);
- unsigned int *m = (unsigned int *)(block - align);
- return SLOB_UNITS(*m) * SLOB_UNIT;
- } else
- return sp->private;
+ if (unlikely(!PageSlab(sp)))
+ return PAGE_SIZE << compound_order(sp);
+
+ align = max_t(size_t, ARCH_KMALLOC_MINALIGN, ARCH_SLAB_MINALIGN);
+ m = (unsigned int *)(block - align);
+ return SLOB_UNITS(*m) * SLOB_UNIT;
}
EXPORT_SYMBOL(ksize);
int __kmem_cache_create(struct kmem_cache *c, unsigned long flags)
{
- size_t align = c->size;
-
if (flags & SLAB_DESTROY_BY_RCU) {
/* leave room for rcu footer at the end of object */
c->size += sizeof(struct slob_rcu);
}
c->flags = flags;
- /* ignore alignment unless it's forced */
- c->align = (flags & SLAB_HWCACHE_ALIGN) ? SLOB_ALIGN : 0;
- if (c->align < ARCH_SLAB_MINALIGN)
- c->align = ARCH_SLAB_MINALIGN;
- if (c->align < align)
- c->align = align;
-
return 0;
}
if (c->size < PAGE_SIZE) {
b = slob_alloc(c->size, flags, c->align, node);
- trace_kmem_cache_alloc_node(_RET_IP_, b, c->size,
+ trace_kmem_cache_alloc_node(_RET_IP_, b, c->object_size,
SLOB_UNITS(c->size) * SLOB_UNIT,
flags, node);
} else {
b = slob_new_pages(flags, get_order(c->size), node);
- trace_kmem_cache_alloc_node(_RET_IP_, b, c->size,
+ trace_kmem_cache_alloc_node(_RET_IP_, b, c->object_size,
PAGE_SIZE << get_order(c->size),
flags, node);
}
}
EXPORT_SYMBOL(kmem_cache_free);
-unsigned int kmem_cache_size(struct kmem_cache *c)
-{
- return c->size;
-}
-EXPORT_SYMBOL(kmem_cache_size);
-
int __kmem_cache_shutdown(struct kmem_cache *c)
{
/* No way to check for remaining objects */
diff --git a/mm/slub.c b/mm/slub.c
index 472e739278b4f36e00cec3b7ec0f6216fda7451b..9640edd2cc78e067acd29432b44ba8e19e5ff815 100644 (file)
--- a/mm/slub.c
+++ b/mm/slub.c
* the fast path and disables lockless freelists.
*/
-#define SLAB_DEBUG_FLAGS (SLAB_RED_ZONE | SLAB_POISON | SLAB_STORE_USER | \
- SLAB_TRACE | SLAB_DEBUG_FREE)
-
static inline int kmem_cache_debug(struct kmem_cache *s)
{
#ifdef CONFIG_SLUB_DEBUG
#define __OBJECT_POISON 0x80000000UL /* Poison object */
#define __CMPXCHG_DOUBLE 0x40000000UL /* Use cmpxchg_double */
-static int kmem_size = sizeof(struct kmem_cache);
-
#ifdef CONFIG_SMP
static struct notifier_block slab_notifier;
#endif
if (!check_object(s, page, object, SLUB_RED_ACTIVE))
goto out;
- if (unlikely(s != page->slab)) {
+ if (unlikely(s != page->slab_cache)) {
if (!PageSlab(page)) {
slab_err(s, page, "Attempt to free object(0x%p) "
"outside of slab", object);
- } else if (!page->slab) {
+ } else if (!page->slab_cache) {
printk(KERN_ERR
"SLUB <none>: no slab for object 0x%p.\n",
object);
goto out;
inc_slabs_node(s, page_to_nid(page), page->objects);
- page->slab = s;
+ page->slab_cache = s;
__SetPageSlab(page);
if (page->pfmemalloc)
SetPageSlabPfmemalloc(page);
else
page = container_of((struct list_head *)h, struct page, lru);
- __free_slab(page->slab, page);
+ __free_slab(page->slab_cache, page);
}
static void free_slab(struct kmem_cache *s, struct page *page)
/*
* Unfreeze all the cpu partial slabs.
*
- * This function must be called with interrupt disabled.
+ * This function must be called with interrupts disabled
+ * for the cpu using c (or some other guarantee must be there
+ * to guarantee no concurrent accesses).
*/
-static void unfreeze_partials(struct kmem_cache *s)
+static void unfreeze_partials(struct kmem_cache *s,
+ struct kmem_cache_cpu *c)
{
struct kmem_cache_node *n = NULL, *n2 = NULL;
- struct kmem_cache_cpu *c = this_cpu_ptr(s->cpu_slab);
struct page *page, *discard_page = NULL;
while ((page = c->partial)) {
@@ -1963,7 +1960,7 @@ static int put_cpu_partial(struct kmem_cache *s, struct page *page, int drain)
* set to the per node partial list.
*/
local_irq_save(flags);
- unfreeze_partials(s);
+ unfreeze_partials(s, this_cpu_ptr(s->cpu_slab));
local_irq_restore(flags);
oldpage = NULL;
pobjects = 0;
if (c->page)
flush_slab(s, c);
- unfreeze_partials(s);
+ unfreeze_partials(s, c);
}
}
void *prior;
void **object = (void *)x;
int was_frozen;
- int inuse;
struct page new;
unsigned long counters;
struct kmem_cache_node *n = NULL;
return;
do {
+ if (unlikely(n)) {
+ spin_unlock_irqrestore(&n->list_lock, flags);
+ n = NULL;
+ }
prior = page->freelist;
counters = page->counters;
set_freepointer(s, object, prior);
new.counters = counters;
was_frozen = new.frozen;
new.inuse--;
- if ((!new.inuse || !prior) && !was_frozen && !n) {
+ if ((!new.inuse || !prior) && !was_frozen) {
if (!kmem_cache_debug(s) && !prior)
}
}
- inuse = new.inuse;
} while (!cmpxchg_double_slab(s, page,
prior, counters,
return;
}
+ if (unlikely(!new.inuse && n->nr_partial > s->min_partial))
+ goto slab_empty;
+
/*
- * was_frozen may have been set after we acquired the list_lock in
- * an earlier loop. So we need to check it here again.
+ * Objects left in the slab. If it was not on the partial list before
+ * then add it.
*/
- if (was_frozen)
- stat(s, FREE_FROZEN);
- else {
- if (unlikely(!inuse && n->nr_partial > s->min_partial))
- goto slab_empty;
-
- /*
- * Objects left in the slab. If it was not on the partial list before
- * then add it.
- */
- if (unlikely(!prior)) {
- remove_full(s, page);
- add_partial(n, page, DEACTIVATE_TO_TAIL);
- stat(s, FREE_ADD_PARTIAL);
- }
+ if (kmem_cache_debug(s) && unlikely(!prior)) {
+ remove_full(s, page);
+ add_partial(n, page, DEACTIVATE_TO_TAIL);
+ stat(s, FREE_ADD_PARTIAL);
}
spin_unlock_irqrestore(&n->list_lock, flags);
return;
page = virt_to_head_page(x);
- if (kmem_cache_debug(s) && page->slab != s) {
+ if (kmem_cache_debug(s) && page->slab_cache != s) {
pr_err("kmem_cache_free: Wrong slab cache. %s but object"
- " is from %s\n", page->slab->name, s->name);
+ " is from %s\n", page->slab_cache->name, s->name);
WARN_ON_ONCE(1);
return;
}
return -ENOSYS;
}
-/*
- * Figure out what the alignment of the objects will be.
- */
-static unsigned long calculate_alignment(unsigned long flags,
- unsigned long align, unsigned long size)
-{
- /*
- * If the user wants hardware cache aligned objects then follow that
- * suggestion if the object is sufficiently large.
- *
- * The hardware cache alignment cannot override the specified
- * alignment though. If that is greater then use it.
- */
- if (flags & SLAB_HWCACHE_ALIGN) {
- unsigned long ralign = cache_line_size();
- while (size <= ralign / 2)
- ralign /= 2;
- align = max(align, ralign);
- }
-
- if (align < ARCH_SLAB_MINALIGN)
- align = ARCH_SLAB_MINALIGN;
-
- return ALIGN(align, sizeof(void *));
-}
-
static void
init_kmem_cache_node(struct kmem_cache_node *n)
{
{
unsigned long flags = s->flags;
unsigned long size = s->object_size;
- unsigned long align = s->align;
int order;
/*
size += sizeof(void *);
#endif
- /*
- * Determine the alignment based on various parameters that the
- * user specified and the dynamic determination of cache line size
- * on bootup.
- */
- align = calculate_alignment(flags, align, s->object_size);
- s->align = align;
-
/*
* SLUB stores one object immediately after another beginning from
* offset 0. In order to align the objects we have to simply size
* each object to conform to the alignment.
*/
- size = ALIGN(size, align);
+ size = ALIGN(size, s->align);
s->size = size;
if (forced_order >= 0)
order = forced_order;
s->max = s->oo;
return !!oo_objects(s->oo);
-
}
static int kmem_cache_open(struct kmem_cache *s, unsigned long flags)
return -EINVAL;
}
-/*
- * Determine the size of a slab object
- */
-unsigned int kmem_cache_size(struct kmem_cache *s)
-{
- return s->object_size;
-}
-EXPORT_SYMBOL(kmem_cache_size);
-
static void list_slab_objects(struct kmem_cache *s, struct page *page,
const char *text)
{
__setup("slub_nomerge", setup_slub_nomerge);
-static struct kmem_cache *__init create_kmalloc_cache(const char *name,
- int size, unsigned int flags)
-{
- struct kmem_cache *s;
-
- s = kmem_cache_zalloc(kmem_cache, GFP_NOWAIT);
-
- s->name = name;
- s->size = s->object_size = size;
- s->align = ARCH_KMALLOC_MINALIGN;
-
- /*
- * This function is called with IRQs disabled during early-boot on
- * single CPU so there's no need to take slab_mutex here.
- */
- if (kmem_cache_open(s, flags))
- goto panic;
-
- list_add(&s->list, &slab_caches);
- return s;
-
-panic:
- panic("Creation of kmalloc slab %s size=%d failed.\n", name, size);
- return NULL;
-}
-
/*
* Conversion table for small slabs sizes / 8 to the index in the
* kmalloc array. This is necessary for slabs < 192 since we have non power
return PAGE_SIZE << compound_order(page);
}
- return slab_ksize(page->slab);
+ return slab_ksize(page->slab_cache);
}
EXPORT_SYMBOL(ksize);
}
slab_lock(page);
- if (on_freelist(page->slab, page, object)) {
- object_err(page->slab, page, object, "Object is on free-list");
+ if (on_freelist(page->slab_cache, page, object)) {
+ object_err(page->slab_cache, page, object, "Object is on free-list");
rv = false;
} else {
rv = true;
__free_pages(page, compound_order(page));
return;
}
- slab_free(page->slab, page, object, _RET_IP_);
+ slab_free(page->slab_cache, page, object, _RET_IP_);
}
EXPORT_SYMBOL(kfree);
/*
* Used for early kmem_cache structures that were allocated using
- * the page allocator
+ * the page allocator. Allocate them properly then fix up the pointers
+ * that may be pointing to the wrong kmem_cache structure.
*/
-static void __init kmem_cache_bootstrap_fixup(struct kmem_cache *s)
+static struct kmem_cache * __init bootstrap(struct kmem_cache *static_cache)
{
int node;
+ struct kmem_cache *s = kmem_cache_zalloc(kmem_cache, GFP_NOWAIT);
- list_add(&s->list, &slab_caches);
- s->refcount = -1;
+ memcpy(s, static_cache, kmem_cache->object_size);
for_each_node_state(node, N_NORMAL_MEMORY) {
struct kmem_cache_node *n = get_node(s, node);
if (n) {
list_for_each_entry(p, &n->partial, lru)
- p->slab = s;
+ p->slab_cache = s;
#ifdef CONFIG_SLUB_DEBUG
list_for_each_entry(p, &n->full, lru)
- p->slab = s;
+ p->slab_cache = s;
#endif
}
}
+ list_add(&s->list, &slab_caches);
+ return s;
}
void __init kmem_cache_init(void)
{
+ static __initdata struct kmem_cache boot_kmem_cache,
+ boot_kmem_cache_node;
int i;
- int caches = 0;
- struct kmem_cache *temp_kmem_cache;
- int order;
- struct kmem_cache *temp_kmem_cache_node;
- unsigned long kmalloc_size;
+ int caches = 2;
if (debug_guardpage_minorder())
slub_max_order = 0;
- kmem_size = offsetof(struct kmem_cache, node) +
- nr_node_ids * sizeof(struct kmem_cache_node *);
-
- /* Allocate two kmem_caches from the page allocator */
- kmalloc_size = ALIGN(kmem_size, cache_line_size());
- order = get_order(2 * kmalloc_size);
- kmem_cache = (void *)__get_free_pages(GFP_NOWAIT | __GFP_ZERO, order);
-
- /*
- * Must first have the slab cache available for the allocations of the
- * struct kmem_cache_node's. There is special bootstrap code in
- * kmem_cache_open for slab_state == DOWN.
- */
- kmem_cache_node = (void *)kmem_cache + kmalloc_size;
+ kmem_cache_node = &boot_kmem_cache_node;
+ kmem_cache = &boot_kmem_cache;
- kmem_cache_node->name = "kmem_cache_node";
- kmem_cache_node->size = kmem_cache_node->object_size =
- sizeof(struct kmem_cache_node);
- kmem_cache_open(kmem_cache_node, SLAB_HWCACHE_ALIGN | SLAB_PANIC);
+ create_boot_cache(kmem_cache_node, "kmem_cache_node",
+ sizeof(struct kmem_cache_node), SLAB_HWCACHE_ALIGN);
hotplug_memory_notifier(slab_memory_callback, SLAB_CALLBACK_PRI);
/* Able to allocate the per node structures */
slab_state = PARTIAL;
- temp_kmem_cache = kmem_cache;
- kmem_cache->name = "kmem_cache";
- kmem_cache->size = kmem_cache->object_size = kmem_size;
- kmem_cache_open(kmem_cache, SLAB_HWCACHE_ALIGN | SLAB_PANIC);
+ create_boot_cache(kmem_cache, "kmem_cache",
+ offsetof(struct kmem_cache, node) +
+ nr_node_ids * sizeof(struct kmem_cache_node *),
+ SLAB_HWCACHE_ALIGN);
- kmem_cache = kmem_cache_alloc(kmem_cache, GFP_NOWAIT);
- memcpy(kmem_cache, temp_kmem_cache, kmem_size);
+ kmem_cache = bootstrap(&boot_kmem_cache);
/*
* Allocate kmem_cache_node properly from the kmem_cache slab.
* kmem_cache_node is separately allocated so no need to
* update any list pointers.
*/
- temp_kmem_cache_node = kmem_cache_node;
-
- kmem_cache_node = kmem_cache_alloc(kmem_cache, GFP_NOWAIT);
- memcpy(kmem_cache_node, temp_kmem_cache_node, kmem_size);
-
- kmem_cache_bootstrap_fixup(kmem_cache_node);
-
- caches++;
- kmem_cache_bootstrap_fixup(kmem_cache);
- caches++;
- /* Free temporary boot structure */
- free_pages((unsigned long)temp_kmem_cache, order);
+ kmem_cache_node = bootstrap(&boot_kmem_cache_node);
/* Now we can use the kmem_cache to allocate kmalloc slabs */
if (err)
return err;
+ /* Mutex is not taken during early boot */
+ if (slab_state <= UP)
+ return 0;
+
mutex_unlock(&slab_mutex);
err = sysfs_slab_add(s);
mutex_lock(&slab_mutex);
{
int err;
const char *name;
- int unmergeable;
-
- if (slab_state < FULL)
- /* Defer until later */
- return 0;
+ int unmergeable = slab_unmergeable(s);
- unmergeable = slab_unmergeable(s);
if (unmergeable) {
/*
* Slabcache can never be merged so we can use the name proper.