summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 3d9203c)
raw | patch | inline | side by side (parent: 3d9203c)
author | Thomas Gleixner <tglx@linutronix.de> | |
Tue, 9 Apr 2013 07:33:34 +0000 (09:33 +0200) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 25 Apr 2013 19:51:09 +0000 (12:51 -0700) |
commit f2530dc71cf0822f90bb63ea4600caaef33a66bb upstream.
The smpboot threads rely on the park/unpark mechanism which binds per
cpu threads on a particular core. Though the functionality is racy:
CPU0 CPU1 CPU2
unpark(T) wake_up_process(T)
clear(SHOULD_PARK) T runs
leave parkme() due to !SHOULD_PARK
bind_to(CPU2) BUG_ON(wrong CPU)
We cannot let the tasks move themself to the target CPU as one of
those tasks is actually the migration thread itself, which requires
that it starts running on the target cpu right away.
The solution to this problem is to prevent wakeups in park mode which
are not from unpark(). That way we can guarantee that the association
of the task to the target cpu is working correctly.
Add a new task state (TASK_PARKED) which prevents other wakeups and
use this state explicitly for the unpark wakeup.
Peter noticed: Also, since the task state is visible to userspace and
all the parked tasks are still in the PID space, its a good hint in ps
and friends that these tasks aren't really there for the moment.
The migration thread has another related issue.
CPU0 CPU1
Bring up CPU2
create_thread(T)
park(T)
wait_for_completion()
parkme()
complete()
sched_set_stop_task()
schedule(TASK_PARKED)
The sched_set_stop_task() call is issued while the task is on the
runqueue of CPU1 and that confuses the hell out of the stop_task class
on that cpu. So we need the same synchronizaion before
sched_set_stop_task().
Reported-by: Dave Jones <davej@redhat.com>
Reported-and-tested-by: Dave Hansen <dave@sr71.net>
Reported-and-tested-by: Borislav Petkov <bp@alien8.de>
Acked-by: Peter Ziljstra <peterz@infradead.org>
Cc: Srivatsa S. Bhat <srivatsa.bhat@linux.vnet.ibm.com>
Cc: dhillf@gmail.com
Cc: Ingo Molnar <mingo@kernel.org>
Link: http://lkml.kernel.org/r/alpine.LFD.2.02.1304091635430.21884@ionos
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
The smpboot threads rely on the park/unpark mechanism which binds per
cpu threads on a particular core. Though the functionality is racy:
CPU0 CPU1 CPU2
unpark(T) wake_up_process(T)
clear(SHOULD_PARK) T runs
leave parkme() due to !SHOULD_PARK
bind_to(CPU2) BUG_ON(wrong CPU)
We cannot let the tasks move themself to the target CPU as one of
those tasks is actually the migration thread itself, which requires
that it starts running on the target cpu right away.
The solution to this problem is to prevent wakeups in park mode which
are not from unpark(). That way we can guarantee that the association
of the task to the target cpu is working correctly.
Add a new task state (TASK_PARKED) which prevents other wakeups and
use this state explicitly for the unpark wakeup.
Peter noticed: Also, since the task state is visible to userspace and
all the parked tasks are still in the PID space, its a good hint in ps
and friends that these tasks aren't really there for the moment.
The migration thread has another related issue.
CPU0 CPU1
Bring up CPU2
create_thread(T)
park(T)
wait_for_completion()
parkme()
complete()
sched_set_stop_task()
schedule(TASK_PARKED)
The sched_set_stop_task() call is issued while the task is on the
runqueue of CPU1 and that confuses the hell out of the stop_task class
on that cpu. So we need the same synchronizaion before
sched_set_stop_task().
Reported-by: Dave Jones <davej@redhat.com>
Reported-and-tested-by: Dave Hansen <dave@sr71.net>
Reported-and-tested-by: Borislav Petkov <bp@alien8.de>
Acked-by: Peter Ziljstra <peterz@infradead.org>
Cc: Srivatsa S. Bhat <srivatsa.bhat@linux.vnet.ibm.com>
Cc: dhillf@gmail.com
Cc: Ingo Molnar <mingo@kernel.org>
Link: http://lkml.kernel.org/r/alpine.LFD.2.02.1304091635430.21884@ionos
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
fs/proc/array.c | patch | blob | history | |
include/linux/sched.h | patch | blob | history | |
include/trace/events/sched.h | patch | blob | history | |
kernel/kthread.c | patch | blob | history |
diff --git a/fs/proc/array.c b/fs/proc/array.c
index 6a91e6ffbcbded857c4513cee0182ec61f899b74..be3c22f5729a8385938965cee9aa317840a90030 100644 (file)
--- a/fs/proc/array.c
+++ b/fs/proc/array.c
"x (dead)", /* 64 */
"K (wakekill)", /* 128 */
"W (waking)", /* 256 */
+ "P (parked)", /* 512 */
};
static inline const char *get_task_state(struct task_struct *tsk)
diff --git a/include/linux/sched.h b/include/linux/sched.h
index d2112477ff5e0ed9a942c9698cbf8549e6087a9c..7e492701142e6cb15af7ae35d2b254d8aa64f6e6 100644 (file)
--- a/include/linux/sched.h
+++ b/include/linux/sched.h
#define TASK_DEAD 64
#define TASK_WAKEKILL 128
#define TASK_WAKING 256
-#define TASK_STATE_MAX 512
+#define TASK_PARKED 512
+#define TASK_STATE_MAX 1024
-#define TASK_STATE_TO_CHAR_STR "RSDTtZXxKW"
+#define TASK_STATE_TO_CHAR_STR "RSDTtZXxKWP"
extern char ___assert_task_state[1 - 2*!!(
sizeof(TASK_STATE_TO_CHAR_STR)-1 != ilog2(TASK_STATE_MAX)+1)];
index 5a8671e8a67ff8fa8f715311300901181555d78e..e5586caff67a973c962a3ed6bf43d4cc01664083 100644 (file)
__print_flags(__entry->prev_state & (TASK_STATE_MAX-1), "|",
{ 1, "S"} , { 2, "D" }, { 4, "T" }, { 8, "t" },
{ 16, "Z" }, { 32, "X" }, { 64, "x" },
- { 128, "W" }) : "R",
+ { 128, "K" }, { 256, "W" }, { 512, "P" }) : "R",
__entry->prev_state & TASK_STATE_MAX ? "+" : "",
__entry->next_comm, __entry->next_pid, __entry->next_prio)
);
diff --git a/kernel/kthread.c b/kernel/kthread.c
index 691dc2ef9baf241c121144799360a7e1237afcb5..9eb7fed0bbaa9895973a14e551c76de31fffe533 100644 (file)
--- a/kernel/kthread.c
+++ b/kernel/kthread.c
static void __kthread_parkme(struct kthread *self)
{
- __set_current_state(TASK_INTERRUPTIBLE);
+ __set_current_state(TASK_PARKED);
while (test_bit(KTHREAD_SHOULD_PARK, &self->flags)) {
if (!test_and_set_bit(KTHREAD_IS_PARKED, &self->flags))
complete(&self->parked);
schedule();
- __set_current_state(TASK_INTERRUPTIBLE);
+ __set_current_state(TASK_PARKED);
}
clear_bit(KTHREAD_IS_PARKED, &self->flags);
__set_current_state(TASK_RUNNING);
}
EXPORT_SYMBOL(kthread_create_on_node);
-static void __kthread_bind(struct task_struct *p, unsigned int cpu)
+static void __kthread_bind(struct task_struct *p, unsigned int cpu, long state)
{
+ /* Must have done schedule() in kthread() before we set_task_cpu */
+ if (!wait_task_inactive(p, state)) {
+ WARN_ON(1);
+ return;
+ }
/* It's safe because the task is inactive. */
do_set_cpus_allowed(p, cpumask_of(cpu));
p->flags |= PF_THREAD_BOUND;
*/
void kthread_bind(struct task_struct *p, unsigned int cpu)
{
- /* Must have done schedule() in kthread() before we set_task_cpu */
- if (!wait_task_inactive(p, TASK_UNINTERRUPTIBLE)) {
- WARN_ON(1);
- return;
- }
- __kthread_bind(p, cpu);
+ __kthread_bind(p, cpu, TASK_UNINTERRUPTIBLE);
}
EXPORT_SYMBOL(kthread_bind);
return NULL;
}
+static void __kthread_unpark(struct task_struct *k, struct kthread *kthread)
+{
+ clear_bit(KTHREAD_SHOULD_PARK, &kthread->flags);
+ /*
+ * We clear the IS_PARKED bit here as we don't wait
+ * until the task has left the park code. So if we'd
+ * park before that happens we'd see the IS_PARKED bit
+ * which might be about to be cleared.
+ */
+ if (test_and_clear_bit(KTHREAD_IS_PARKED, &kthread->flags)) {
+ if (test_bit(KTHREAD_IS_PER_CPU, &kthread->flags))
+ __kthread_bind(k, kthread->cpu, TASK_PARKED);
+ wake_up_state(k, TASK_PARKED);
+ }
+}
+
/**
* kthread_unpark - unpark a thread created by kthread_create().
* @k: thread created by kthread_create().
{
struct kthread *kthread = task_get_live_kthread(k);
- if (kthread) {
- clear_bit(KTHREAD_SHOULD_PARK, &kthread->flags);
- /*
- * We clear the IS_PARKED bit here as we don't wait
- * until the task has left the park code. So if we'd
- * park before that happens we'd see the IS_PARKED bit
- * which might be about to be cleared.
- */
- if (test_and_clear_bit(KTHREAD_IS_PARKED, &kthread->flags)) {
- if (test_bit(KTHREAD_IS_PER_CPU, &kthread->flags))
- __kthread_bind(k, kthread->cpu);
- wake_up_process(k);
- }
- }
+ if (kthread)
+ __kthread_unpark(k, kthread);
put_task_struct(k);
}
trace_sched_kthread_stop(k);
if (kthread) {
set_bit(KTHREAD_SHOULD_STOP, &kthread->flags);
- clear_bit(KTHREAD_SHOULD_PARK, &kthread->flags);
+ __kthread_unpark(k, kthread);
wake_up_process(k);
wait_for_completion(&kthread->exited);
}