]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commitdiff
Merge branch 'next' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc
authorLinus Torvalds <torvalds@linux-foundation.org>
Tue, 18 Dec 2012 17:58:09 +0000 (09:58 -0800)
committerLinus Torvalds <torvalds@linux-foundation.org>
Tue, 18 Dec 2012 17:58:09 +0000 (09:58 -0800)
Pull powerpc update from Benjamin Herrenschmidt:
 "The main highlight is probably some base POWER8 support.  There's more
  to come such as transactional memory support but that will wait for
  the next one.

  Overall it's pretty quiet, or rather I've been pretty poor at picking
  things up from patchwork and reviewing them this time around and Kumar
  no better on the FSL side it seems..."

* 'next' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc: (73 commits)
  powerpc+of: Rename and fix OF reconfig notifier error inject module
  powerpc: mpc5200: Add a3m071 board support
  powerpc/512x: don't compile any platform DIU code if the DIU is not enabled
  powerpc/mpc52xx: use module_platform_driver macro
  powerpc+of: Export of_reconfig_notifier_[register,unregister]
  powerpc/dma/raidengine: add raidengine device
  powerpc/iommu/fsl: Add PAMU bypass enable register to ccsr_guts struct
  powerpc/mpc85xx: Change spin table to cached memory
  powerpc/fsl-pci: Add PCI controller ATMU PM support
  powerpc/86xx: fsl_pcibios_fixup_bus requires CONFIG_PCI
  drivers/virt: the Freescale hypervisor driver doesn't need to check MSR[GS]
  powerpc/85xx: p1022ds: Use NULL instead of 0 for pointers
  powerpc: Disable relocation on exceptions when kexecing
  powerpc: Enable relocation on during exceptions at boot
  powerpc: Move get_longbusy_msecs into hvcall.h and remove duplicate function
  powerpc: Add wrappers to enable/disable relocation on exceptions
  powerpc: Add set_mode hcall
  powerpc: Setup relocation on exceptions for bare metal systems
  powerpc: Move initial mfspr LPCR out of __init_LPCR
  powerpc: Add relocation on exception vector handlers
  ...

13 files changed:
1  2 
arch/arm/mach-mxs/mach-mxs.c
arch/powerpc/include/asm/machdep.h
arch/powerpc/include/asm/ppc-opcode.h
arch/powerpc/include/asm/reg.h
arch/powerpc/kernel/entry_64.S
arch/powerpc/platforms/pseries/reconfig.c
arch/powerpc/sysdev/fsl_pci.c
drivers/macintosh/smu.c
drivers/of/base.c
drivers/video/Kconfig
include/linux/of.h
lib/Kconfig.debug
lib/Makefile

Simple merge
Simple merge
Simple merge
Simple merge
index e9a906c27234fe880a5c78bd9c80ef7835c712ab,ad7666695761103571c7aa5b258816d517a27392..b310a0573625dec8a672c267ab6158f8e90b37a6
@@@ -373,7 -373,9 +373,9 @@@ _GLOBAL(ret_from_fork
  _GLOBAL(ret_from_kernel_thread)
        bl      .schedule_tail
        REST_NVGPRS(r1)
 -      REST_GPR(2,r1)
+       li      r3,0
+       std     r3,0(r1)
 +      ld      r14, 0(r14)
        mtlr    r14
        mr      r3,r15
        blrl
Simple merge
Simple merge
index be846408dbc14e86dd5df8b2d511eac36be4c711,fa40402fe8d5f4fe00979a4e813958e3b45b3f1a..db8d211a0d05d4f26b8b297ecb82d9a8e0139b04
@@@ -1255,12 -1243,36 +1329,36 @@@ int of_attach_node(struct device_node *
  
        write_lock_irqsave(&devtree_lock, flags);
        np->sibling = np->parent->child;
 -      np->allnext = allnodes;
 +      np->allnext = of_allnodes;
        np->parent->child = np;
 -      allnodes = np;
 +      of_allnodes = np;
        write_unlock_irqrestore(&devtree_lock, flags);
+       of_add_proc_dt_entry(np);
+       return 0;
  }
  
+ #ifdef CONFIG_PROC_DEVICETREE
+ static void of_remove_proc_dt_entry(struct device_node *dn)
+ {
+       struct device_node *parent = dn->parent;
+       struct property *prop = dn->properties;
+       while (prop) {
+               remove_proc_entry(prop->name, dn->pde);
+               prop = prop->next;
+       }
+       if (dn->pde)
+               remove_proc_entry(dn->pde->name, parent->pde);
+ }
+ #else
+ static void of_remove_proc_dt_entry(struct device_node *dn)
+ {
+       return;
+ }
+ #endif
  /**
   * of_detach_node - "Unplug" a node from the device tree.
   *
@@@ -1274,15 -1291,23 +1377,23 @@@ int of_detach_node(struct device_node *
  
        write_lock_irqsave(&devtree_lock, flags);
  
+       if (of_node_check_flag(np, OF_DETACHED)) {
+               /* someone already detached it */
+               write_unlock_irqrestore(&devtree_lock, flags);
+               return rc;
+       }
        parent = np->parent;
-       if (!parent)
-               goto out_unlock;
+       if (!parent) {
+               write_unlock_irqrestore(&devtree_lock, flags);
+               return rc;
+       }
  
 -      if (allnodes == np)
 -              allnodes = np->allnext;
 +      if (of_allnodes == np)
 +              of_allnodes = np->allnext;
        else {
                struct device_node *prev;
 -              for (prev = allnodes;
 +              for (prev = of_allnodes;
                     prev->allnext != np;
                     prev = prev->allnext)
                        ;
Simple merge
Simple merge
index e458782f3c52ac69f88d05d10233fd32b330a7fb,c2d89f37004e6840860121b99a300c32b390686f..3a353091a90390f6b95b632408797d14908d57f3
@@@ -1192,14 -1192,14 +1192,14 @@@ config MEMORY_NOTIFIER_ERROR_INJEC
  
          If unsure, say N.
  
- config PSERIES_RECONFIG_NOTIFIER_ERROR_INJECT
-       tristate "pSeries reconfig notifier error injection module"
-       depends on PPC_PSERIES && NOTIFIER_ERROR_INJECTION
+ config OF_RECONFIG_NOTIFIER_ERROR_INJECT
+       tristate "OF reconfig notifier error injection module"
+       depends on OF_DYNAMIC && NOTIFIER_ERROR_INJECTION
        help
 -        This option provides the ability to inject artifical errors to
 +        This option provides the ability to inject artificial errors to
-         pSeries reconfig notifier chain callbacks.  It is controlled
+         OF reconfig notifier chain callbacks.  It is controlled
          through debugfs interface under
-         /sys/kernel/debug/notifier-error-inject/pSeries-reconfig/
+         /sys/kernel/debug/notifier-error-inject/OF-reconfig/
  
          If the notifier call chain should be failed with some events
          notified, write the error code to "actions/<notifier event>/error".
diff --cc lib/Makefile
Simple merge