summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 3e5e7e6)
raw | patch | inline | side by side (parent: 3e5e7e6)
author | Linus Torvalds <torvalds@linux-foundation.org> | |
Thu, 29 Jan 2015 18:51:32 +0000 (10:51 -0800) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Wed, 29 Apr 2015 08:31:55 +0000 (10:31 +0200) |
commit 33692f27597fcab536d7cbbcc8f52905133e4aa7 upstream.
The core VM already knows about VM_FAULT_SIGBUS, but cannot return a
"you should SIGSEGV" error, because the SIGSEGV case was generally
handled by the caller - usually the architecture fault handler.
That results in lots of duplication - all the architecture fault
handlers end up doing very similar "look up vma, check permissions, do
retries etc" - but it generally works. However, there are cases where
the VM actually wants to SIGSEGV, and applications _expect_ SIGSEGV.
In particular, when accessing the stack guard page, libsigsegv expects a
SIGSEGV. And it usually got one, because the stack growth is handled by
that duplicated architecture fault handler.
However, when the generic VM layer started propagating the error return
from the stack expansion in commit fee7e49d4514 ("mm: propagate error
from stack expansion even for guard page"), that now exposed the
existing VM_FAULT_SIGBUS result to user space. And user space really
expected SIGSEGV, not SIGBUS.
To fix that case, we need to add a VM_FAULT_SIGSEGV, and teach all those
duplicate architecture fault handlers about it. They all already have
the code to handle SIGSEGV, so it's about just tying that new return
value to the existing code, but it's all a bit annoying.
This is the mindless minimal patch to do this. A more extensive patch
would be to try to gather up the mostly shared fault handling logic into
one generic helper routine, and long-term we really should do that
cleanup.
Just from this patch, you can generally see that most architectures just
copied (directly or indirectly) the old x86 way of doing things, but in
the meantime that original x86 model has been improved to hold the VM
semaphore for shorter times etc and to handle VM_FAULT_RETRY and other
"newer" things, so it would be a good idea to bring all those
improvements to the generic case and teach other architectures about
them too.
Reported-and-tested-by: Takashi Iwai <tiwai@suse.de>
Tested-by: Jan Engelhardt <jengelh@inai.de>
Acked-by: Heiko Carstens <heiko.carstens@de.ibm.com> # "s390 still compiles and boots"
Cc: linux-arch@vger.kernel.org
Cc: stable@vger.kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
[shengyong: Backport to 3.14
- adjust context
- ignore modification for arch nios2, because 3.14 does not support it
- add SIGSEGV handling to powerpc/cell spu_fault.c, because 3.14 does not
separate it to copro_fault.c
- add SIGSEGV handling to mm/memory.c, because 3.14 does not separate it
to gup.c
]
Signed-off-by: Sheng Yong <shengyong1@huawei.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
The core VM already knows about VM_FAULT_SIGBUS, but cannot return a
"you should SIGSEGV" error, because the SIGSEGV case was generally
handled by the caller - usually the architecture fault handler.
That results in lots of duplication - all the architecture fault
handlers end up doing very similar "look up vma, check permissions, do
retries etc" - but it generally works. However, there are cases where
the VM actually wants to SIGSEGV, and applications _expect_ SIGSEGV.
In particular, when accessing the stack guard page, libsigsegv expects a
SIGSEGV. And it usually got one, because the stack growth is handled by
that duplicated architecture fault handler.
However, when the generic VM layer started propagating the error return
from the stack expansion in commit fee7e49d4514 ("mm: propagate error
from stack expansion even for guard page"), that now exposed the
existing VM_FAULT_SIGBUS result to user space. And user space really
expected SIGSEGV, not SIGBUS.
To fix that case, we need to add a VM_FAULT_SIGSEGV, and teach all those
duplicate architecture fault handlers about it. They all already have
the code to handle SIGSEGV, so it's about just tying that new return
value to the existing code, but it's all a bit annoying.
This is the mindless minimal patch to do this. A more extensive patch
would be to try to gather up the mostly shared fault handling logic into
one generic helper routine, and long-term we really should do that
cleanup.
Just from this patch, you can generally see that most architectures just
copied (directly or indirectly) the old x86 way of doing things, but in
the meantime that original x86 model has been improved to hold the VM
semaphore for shorter times etc and to handle VM_FAULT_RETRY and other
"newer" things, so it would be a good idea to bring all those
improvements to the generic case and teach other architectures about
them too.
Reported-and-tested-by: Takashi Iwai <tiwai@suse.de>
Tested-by: Jan Engelhardt <jengelh@inai.de>
Acked-by: Heiko Carstens <heiko.carstens@de.ibm.com> # "s390 still compiles and boots"
Cc: linux-arch@vger.kernel.org
Cc: stable@vger.kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
[shengyong: Backport to 3.14
- adjust context
- ignore modification for arch nios2, because 3.14 does not support it
- add SIGSEGV handling to powerpc/cell spu_fault.c, because 3.14 does not
separate it to copro_fault.c
- add SIGSEGV handling to mm/memory.c, because 3.14 does not separate it
to gup.c
]
Signed-off-by: Sheng Yong <shengyong1@huawei.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
29 files changed:
diff --git a/arch/alpha/mm/fault.c b/arch/alpha/mm/fault.c
index 98838a05ba6d89f0459742131010f57c38cbed05..9d0ac091a52a7d16cf1f78f402ab48c511924a24 100644 (file)
--- a/arch/alpha/mm/fault.c
+++ b/arch/alpha/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/arc/mm/fault.c b/arch/arc/mm/fault.c
index 9c69552350c49754ee056ab854a5971b460fe5f8..15879a1f864cca5b9249370cb22917aac792636a 100644 (file)
--- a/arch/arc/mm/fault.c
+++ b/arch/arc/mm/fault.c
/* TBD: switch to pagefault_out_of_memory() */
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
diff --git a/arch/avr32/mm/fault.c b/arch/avr32/mm/fault.c
index 0eca93327195077ec16bdfd99efd7294c6ab2de6..d223a8b57c1eaad282289e75089654153ab598d6 100644 (file)
--- a/arch/avr32/mm/fault.c
+++ b/arch/avr32/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/cris/mm/fault.c b/arch/cris/mm/fault.c
index 1790f22e71a21a859b2b7b1942cbbc503c2d557e..2686a7aa8ec82c50f29592840185b519522c53a7 100644 (file)
--- a/arch/cris/mm/fault.c
+++ b/arch/cris/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/frv/mm/fault.c b/arch/frv/mm/fault.c
index 9a66372fc7c76019ca874a9c3780c2fc8392266c..ec4917ddf67872aa46b60c6b067b0a67ec5417a4 100644 (file)
--- a/arch/frv/mm/fault.c
+++ b/arch/frv/mm/fault.c
@@ -168,6 +168,8 @@ asmlinkage void do_page_fault(int datammu, unsigned long esr0, unsigned long ear
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/ia64/mm/fault.c b/arch/ia64/mm/fault.c
index 7225dad87094d81e89459e5a61909fa5b2d10ca0..ba5ba7accd0d6bb4dbab34f7fc307c4306347f4a 100644 (file)
--- a/arch/ia64/mm/fault.c
+++ b/arch/ia64/mm/fault.c
*/
if (fault & VM_FAULT_OOM) {
goto out_of_memory;
+ } else if (fault & VM_FAULT_SIGSEGV) {
+ goto bad_area;
} else if (fault & VM_FAULT_SIGBUS) {
signal = SIGBUS;
goto bad_area;
diff --git a/arch/m32r/mm/fault.c b/arch/m32r/mm/fault.c
index e9c6a8014bd647eec50a66afb5bc75b076b35e4d..e3d4d4890104cc27e2eb9de2f22cb6f53f939c90 100644 (file)
--- a/arch/m32r/mm/fault.c
+++ b/arch/m32r/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/m68k/mm/fault.c b/arch/m68k/mm/fault.c
index 2bd7487440c455802dac6470ec05ac138148bfcb..b2f04aee46ecc2f7a5fb1db26d8e4279f6b6ea2e 100644 (file)
--- a/arch/m68k/mm/fault.c
+++ b/arch/m68k/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto map_err;
else if (fault & VM_FAULT_SIGBUS)
goto bus_err;
BUG();
diff --git a/arch/metag/mm/fault.c b/arch/metag/mm/fault.c
index 332680e5ebf23c7909b796c415c2273efd77ba3c..2de5dc695a87fa96d41a83e127166a7126d10df0 100644 (file)
--- a/arch/metag/mm/fault.c
+++ b/arch/metag/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
index fa4cf52aa7a6d386711690005a314ece7d67fc53..d46a5ebb7570e07869ea03b9b995374aa3bff82e 100644 (file)
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/mips/mm/fault.c b/arch/mips/mm/fault.c
index becc42bb18495adf98389bd039bc111c1893cedd..70ab5d664332694e92305331f13ed15a35ab1956 100644 (file)
--- a/arch/mips/mm/fault.c
+++ b/arch/mips/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
index 3516cbdf1ee93acb82ebef6428f79df9af104514..0c2cc5d39c8e37ce1cfe5be191902bc435c41090 100644 (file)
--- a/arch/mn10300/mm/fault.c
+++ b/arch/mn10300/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
index 0703acf7d3276811919fd3d398ada99b1b9c6d50..230ac20ae7944f71636e5083fdaf3f034eb10af2 100644 (file)
--- a/arch/openrisc/mm/fault.c
+++ b/arch/openrisc/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/parisc/mm/fault.c b/arch/parisc/mm/fault.c
index d72197f0ddb863999f1bfb62a2a81c6d60038445..d27e38874e812be462ce7a9e17892a878e607d1f 100644 (file)
--- a/arch/parisc/mm/fault.c
+++ b/arch/parisc/mm/fault.c
*/
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto bad_area;
BUG();
index 51ab9e7e6c391b9497a08730a7b5e4c625c96304..010fabf3828c03757d5a063554125431222df965 100644 (file)
--- a/arch/powerpc/mm/fault.c
+++ b/arch/powerpc/mm/fault.c
*/
fault = handle_mm_fault(mm, vma, address, flags);
if (unlikely(fault & (VM_FAULT_RETRY|VM_FAULT_ERROR))) {
+ if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
rc = mm_fault_error(regs, address, fault);
if (rc >= MM_FAULT_RETURN)
goto bail;
index 641e7273d75ae687335716c5b4e87c9afcdb98c7..62f3e4e48a0b235a0bfe6ad577feccc8a3dc36aa 100644 (file)
if (*flt & VM_FAULT_OOM) {
ret = -ENOMEM;
goto out_unlock;
- } else if (*flt & VM_FAULT_SIGBUS) {
+ } else if (*flt & (VM_FAULT_SIGBUS | VM_FAULT_SIGSEGV)) {
ret = -EFAULT;
goto out_unlock;
}
diff --git a/arch/s390/mm/fault.c b/arch/s390/mm/fault.c
index d95265b2719f8e7fb0b15305b49a52130069aebd..8e95432cc3b20fd098d4e3b640831bca670efe77 100644 (file)
--- a/arch/s390/mm/fault.c
+++ b/arch/s390/mm/fault.c
do_no_context(regs);
else
pagefault_out_of_memory();
+ } else if (fault & VM_FAULT_SIGSEGV) {
+ /* Kernel mode? Handle exceptions or die */
+ if (!user_mode(regs))
+ do_no_context(regs);
+ else
+ do_sigsegv(regs, SEGV_MAPERR);
} else if (fault & VM_FAULT_SIGBUS) {
/* Kernel mode? Handle exceptions or die */
if (!user_mode(regs))
diff --git a/arch/score/mm/fault.c b/arch/score/mm/fault.c
index 52238983527d605914853fd5415ea39617944ffe..6860beb2a280d0a4a65a67c89ad2201b33513068 100644 (file)
--- a/arch/score/mm/fault.c
+++ b/arch/score/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/sh/mm/fault.c b/arch/sh/mm/fault.c
index 541dc610150888e706977c7944c42ab1d61d7437..a58fec9b55e016df85cdfb7c214cc385e300479c 100644 (file)
--- a/arch/sh/mm/fault.c
+++ b/arch/sh/mm/fault.c
} else {
if (fault & VM_FAULT_SIGBUS)
do_sigbus(regs, error_code, address);
+ else if (fault & VM_FAULT_SIGSEGV)
+ bad_area(regs, error_code, address);
else
BUG();
}
index 59dbd46457250b050ce84a48370a4f96afa3746d..163c7871211095b12d00592b0d373dd67e136d7f 100644 (file)
--- a/arch/sparc/mm/fault_32.c
+++ b/arch/sparc/mm/fault_32.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
index 45a413e4380a8f87212204c251088b2eeb524bfc..0d6de79105b6df78c1a6567ae168aa54acaa173c 100644 (file)
--- a/arch/sparc/mm/fault_64.c
+++ b/arch/sparc/mm/fault_64.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/tile/mm/fault.c b/arch/tile/mm/fault.c
index 6c0571216a9d67f81a09ff331a601d22ae881566..c6d2a76d91a81e3c23d13d6bc101d88c7c3bc461 100644 (file)
--- a/arch/tile/mm/fault.c
+++ b/arch/tile/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/arch/um/kernel/trap.c b/arch/um/kernel/trap.c
index 974b87474a9900f1909f845d449eba90dc9b8338..53b832033d9bfc9563651117f7a434df890ab7f3 100644 (file)
--- a/arch/um/kernel/trap.c
+++ b/arch/um/kernel/trap.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM) {
goto out_of_memory;
+ } else if (fault & VM_FAULT_SIGSEGV) {
+ goto out;
} else if (fault & VM_FAULT_SIGBUS) {
err = -EACCES;
goto out;
diff --git a/arch/x86/mm/fault.c b/arch/x86/mm/fault.c
index a10c8c79216187d2faa5add449762710d51c759b..95ed5f128c6aae4011e6aa777a3690c271bd76be 100644 (file)
--- a/arch/x86/mm/fault.c
+++ b/arch/x86/mm/fault.c
if (fault & (VM_FAULT_SIGBUS|VM_FAULT_HWPOISON|
VM_FAULT_HWPOISON_LARGE))
do_sigbus(regs, error_code, address, fault);
+ else if (fault & VM_FAULT_SIGSEGV)
+ bad_area_nosemaphore(regs, error_code, address);
else
BUG();
}
diff --git a/arch/xtensa/mm/fault.c b/arch/xtensa/mm/fault.c
index b57c4f91f487efdc6b2f3f44fe43cfb12e9a7e0c..9e3571a6535c3b1bbc8535195ee40405fe9c42c0 100644 (file)
--- a/arch/xtensa/mm/fault.c
+++ b/arch/xtensa/mm/fault.c
if (unlikely(fault & VM_FAULT_ERROR)) {
if (fault & VM_FAULT_OOM)
goto out_of_memory;
+ else if (fault & VM_FAULT_SIGSEGV)
+ goto bad_area;
else if (fault & VM_FAULT_SIGBUS)
goto do_sigbus;
BUG();
diff --git a/drivers/staging/lustre/lustre/llite/vvp_io.c b/drivers/staging/lustre/lustre/llite/vvp_io.c
index 93cbfbb7e7f7ba418fd5081a0edd92ed219e7342..6096771e24005b7372e36e801f02efbdeb1d826c 100644 (file)
return 0;
}
- if (cfio->fault.ft_flags & VM_FAULT_SIGBUS) {
+ if (cfio->fault.ft_flags & (VM_FAULT_SIGBUS | VM_FAULT_SIGSEGV)) {
CDEBUG(D_PAGE, "got addr %p - SIGBUS\n", vmf->virtual_address);
return -EFAULT;
}
diff --git a/include/linux/mm.h b/include/linux/mm.h
index 46b8ab56b9dbddb3ed52df387f9ada2bbf6a40c1..a7b311dfa7422605ff6ee4df15e9d41170f90b5b 100644 (file)
--- a/include/linux/mm.h
+++ b/include/linux/mm.h
#define VM_FAULT_WRITE 0x0008 /* Special case for get_user_pages */
#define VM_FAULT_HWPOISON 0x0010 /* Hit poisoned small page */
#define VM_FAULT_HWPOISON_LARGE 0x0020 /* Hit poisoned large page. Index encoded in upper bits */
+#define VM_FAULT_SIGSEGV 0x0040
#define VM_FAULT_NOPAGE 0x0100 /* ->fault installed the pte, not return page */
#define VM_FAULT_LOCKED 0x0200 /* ->fault locked the returned page */
#define VM_FAULT_HWPOISON_LARGE_MASK 0xf000 /* encodes hpage index for large hwpoison */
-#define VM_FAULT_ERROR (VM_FAULT_OOM | VM_FAULT_SIGBUS | VM_FAULT_HWPOISON | \
- VM_FAULT_FALLBACK | VM_FAULT_HWPOISON_LARGE)
+#define VM_FAULT_ERROR (VM_FAULT_OOM | VM_FAULT_SIGBUS | VM_FAULT_SIGSEGV | \
+ VM_FAULT_HWPOISON | VM_FAULT_HWPOISON_LARGE | \
+ VM_FAULT_FALLBACK)
/* Encode hstate index for a hwpoisoned large page */
#define VM_FAULT_SET_HINDEX(x) ((x) << 12)
diff --git a/mm/ksm.c b/mm/ksm.c
index 68710e80994afed815c58b59a1a3cf421df8101f..5e706e391a02b2760093b905331cb253879dd4f6 100644 (file)
--- a/mm/ksm.c
+++ b/mm/ksm.c
else
ret = VM_FAULT_WRITE;
put_page(page);
- } while (!(ret & (VM_FAULT_WRITE | VM_FAULT_SIGBUS | VM_FAULT_OOM)));
+ } while (!(ret & (VM_FAULT_WRITE | VM_FAULT_SIGBUS | VM_FAULT_SIGSEGV | VM_FAULT_OOM)));
/*
* We must loop because handle_mm_fault() may back out if there's
* any difficulty e.g. if pte accessed bit gets updated concurrently.
diff --git a/mm/memory.c b/mm/memory.c
index 102af096cbc5d5c0d750d92fdd2183ccd4f0cc7b..120eb53f815736f680bd6ab28858022711c3818f 100644 (file)
--- a/mm/memory.c
+++ b/mm/memory.c
else
return -EFAULT;
}
- if (ret & VM_FAULT_SIGBUS)
+ if (ret & (VM_FAULT_SIGBUS |
+ VM_FAULT_SIGSEGV))
return i ? i : -EFAULT;
BUG();
}
return -ENOMEM;
if (ret & (VM_FAULT_HWPOISON | VM_FAULT_HWPOISON_LARGE))
return -EHWPOISON;
- if (ret & VM_FAULT_SIGBUS)
+ if (ret & (VM_FAULT_SIGBUS | VM_FAULT_SIGSEGV))
return -EFAULT;
BUG();
}