summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 048f4bd)
raw | patch | inline | side by side (parent: 048f4bd)
author | Nishanth Menon <nm@ti.com> | |
Sun, 22 Nov 2009 18:10:56 +0000 (10:10 -0800) | ||
committer | Tony Lindgren <tony@atomide.com> | |
Sun, 22 Nov 2009 18:24:32 +0000 (10:24 -0800) |
OMAP3630 is the latest in the family of OMAP3 devices
and among the changes it introduces are:
New OPP levels for new voltage and frequency levels. a bunch of
Bug fixes to various modules feature additions, notably with ISP,
sDMA etc.
Details about the chip is available here:
http://focus.ti.com/general/docs/wtbu/wtbuproductcontent.tsp?templateId=6123&navigationId=12836&contentId=52606
Strategy used:
Strategy to introduce this device into Linux was discussed here:
Ref: http://marc.info/?t=125343303400003&r=1&w=2
Two approaches were available:
a) Consider 3630 generation of devices as a new family of silicon
b) Consider 3630 as an offshoot of 3430 family of devices
As a common consensus, (b) seems to be more valid for 3630 as:
* There are changes which are easily handled by using "FEATURES"
infrastructure.
For details how to do this, see thread:
http://marc.info/?t=125050998500001&r=1&w=2
* Most of existing 34xx infrastructure can be reused(almost 90%+)
- so no ugly if (cpu_is_omap34xx() || cpu_is_omap36xx())
all over the place
- lesser chance of bugs due to reuse of proven code flow
- 36xx specific handling can still be done where required
within the existing infrastructure
NOTE:
* If additional 34xx series are added, OMAP3430_REV_ESXXXX can be
added on top of the existing 3630 ones are renumbered
This patch was tested on SDP3430, boot tested on 3630 platform using
3430sdp defconfig
Signed-off-by: Madhusudhan Chikkature Rajashekar <madhu.cr@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Vikram Pandita <vikram.pandita@ti.com>
Cc: Allen Pais <allen.pais@ti.com>
Cc: Anand Gadiyar <gadiyar@ti.com>
Cc: Benoit Cousson <b-cousson@ti.com>
Cc: Felipe Balbi <felipe.balbi@nokia.com>
Cc: Kevin Hilman <khilman@deeprootsystems.com>
Cc: Sanjeev Premi <premi@ti.com>
Cc: Santosh Shilimkar <santosh.shilimkar@ti.com>
Cc: Sergio Alberto Aguirre Rodriguez <saaguirre@ti.com>
Signed-off-by: Tony Lindgren <tony@atomide.com>
and among the changes it introduces are:
New OPP levels for new voltage and frequency levels. a bunch of
Bug fixes to various modules feature additions, notably with ISP,
sDMA etc.
Details about the chip is available here:
http://focus.ti.com/general/docs/wtbu/wtbuproductcontent.tsp?templateId=6123&navigationId=12836&contentId=52606
Strategy used:
Strategy to introduce this device into Linux was discussed here:
Ref: http://marc.info/?t=125343303400003&r=1&w=2
Two approaches were available:
a) Consider 3630 generation of devices as a new family of silicon
b) Consider 3630 as an offshoot of 3430 family of devices
As a common consensus, (b) seems to be more valid for 3630 as:
* There are changes which are easily handled by using "FEATURES"
infrastructure.
For details how to do this, see thread:
http://marc.info/?t=125050998500001&r=1&w=2
* Most of existing 34xx infrastructure can be reused(almost 90%+)
- so no ugly if (cpu_is_omap34xx() || cpu_is_omap36xx())
all over the place
- lesser chance of bugs due to reuse of proven code flow
- 36xx specific handling can still be done where required
within the existing infrastructure
NOTE:
* If additional 34xx series are added, OMAP3430_REV_ESXXXX can be
added on top of the existing 3630 ones are renumbered
This patch was tested on SDP3430, boot tested on 3630 platform using
3430sdp defconfig
Signed-off-by: Madhusudhan Chikkature Rajashekar <madhu.cr@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Vikram Pandita <vikram.pandita@ti.com>
Cc: Allen Pais <allen.pais@ti.com>
Cc: Anand Gadiyar <gadiyar@ti.com>
Cc: Benoit Cousson <b-cousson@ti.com>
Cc: Felipe Balbi <felipe.balbi@nokia.com>
Cc: Kevin Hilman <khilman@deeprootsystems.com>
Cc: Sanjeev Premi <premi@ti.com>
Cc: Santosh Shilimkar <santosh.shilimkar@ti.com>
Cc: Sergio Alberto Aguirre Rodriguez <saaguirre@ti.com>
Signed-off-by: Tony Lindgren <tony@atomide.com>
arch/arm/mach-omap2/id.c | patch | blob | history | |
arch/arm/plat-omap/include/plat/cpu.h | patch | blob | history |
index 88999eaf91b6d4ae8c2a287862fd1dac67e3cf77..1c151122089056a55f3e471aa30907a592fa23d0 100644 (file)
--- a/arch/arm/mach-omap2/id.c
+++ b/arch/arm/mach-omap2/id.c
hawkeye = (idcode >> 12) & 0xffff;
rev = (idcode >> 28) & 0xff;
- if (hawkeye == 0xb7ae) {
+ switch (hawkeye) {
+ case 0xb7ae:
+ /* Handle 34xx/35xx devices */
switch (rev) {
case 0: /* Take care of early samples */
case 1:
/* Use the latest known revision as default */
omap_revision = OMAP3430_REV_ES3_1;
}
+ break;
+ case 0xb891:
+ /* Handle 36xx devices */
+ switch (rev) {
+ case 0:
+ omap_revision = OMAP3630_REV_ES1_0;
+ break;
+ default:
+ /* Use the latest known revision as default */
+ omap_revision = OMAP3630_REV_ES1_0;
+ }
+ break;
+ default:
+ /* Unknown default to latest silicon rev as default*/
+ omap_revision = OMAP3630_REV_ES1_0;
}
}
* on available features. Upon detection, update the CPU id
* and CPU class bits.
*/
- if (omap3_has_iva() && omap3_has_sgx()) {
+ if (cpu_is_omap3630())
+ strcpy(cpu_name, "3630");
+ else if (omap3_has_iva() && omap3_has_sgx())
strcpy(cpu_name, "3430/3530");
- }
else if (omap3_has_sgx()) {
omap_revision = OMAP3525_REV(rev);
strcpy(cpu_name, "3525");
index a67439327de397170b6e3bb57888e9ea8e9125e8..f4f7a2f0c0361646724d207e8ad3cb3a21c9f4ca 100644 (file)
IS_OMAP_SUBCLASS(242x, 0x242)
IS_OMAP_SUBCLASS(243x, 0x243)
IS_OMAP_SUBCLASS(343x, 0x343)
+IS_OMAP_SUBCLASS(363x, 0x363)
#define cpu_is_omap7xx() 0
#define cpu_is_omap15xx() 0
#define cpu_is_omap3525() 0
#define cpu_is_omap3530() 0
#define cpu_is_omap3430() 0
+#define cpu_is_omap3630() 0
/*
* Whether we have MULTI_OMAP1 or not, we still need to distinguish
(omap3_has_sgx()) && \
(!omap3_has_iva()))
# define cpu_is_omap3530() (cpu_is_omap3430())
+# undef cpu_is_omap3630
+# define cpu_is_omap3630() is_omap363x()
#endif
# if defined(CONFIG_ARCH_OMAP4)
#define OMAP3430_REV_ES3_0 0x34303034
#define OMAP3430_REV_ES3_1 0x34304034
+#define OMAP3630_REV_ES1_0 0x36300034
+
#define OMAP35XX_CLASS 0x35000034
#define OMAP3503_REV(v) (OMAP35XX_CLASS | (0x3503 << 16) | (v << 12))
#define OMAP3515_REV(v) (OMAP35XX_CLASS | (0x3515 << 16) | (v << 12))