summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 673282b)
raw | patch | inline | side by side (parent: 673282b)
author | Peter Seiderer <ps.report@gmx.net> | |
Thu, 17 Sep 2015 19:40:12 +0000 (21:40 +0200) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 22 Oct 2015 21:39:20 +0000 (14:39 -0700) |
commit 98ce94c8df762d413b3ecb849e2b966b21606d04 upstream.
Linux cifs mount with ntlmssp against an Mac OS X (Yosemite
10.10.5) share fails in case the clocks differ more than +/-2h:
digest-service: digest-request: od failed with 2 proto=ntlmv2
digest-service: digest-request: kdc failed with -1561745592 proto=ntlmv2
Fix this by (re-)using the given server timestamp for the
ntlmv2 authentication (as Windows 7 does).
A related problem was also reported earlier by Namjae Jaen (see below):
Windows machine has extended security feature which refuse to allow
authentication when there is time difference between server time and
client time when ntlmv2 negotiation is used. This problem is prevalent
in embedded enviornment where system time is set to default 1970.
Modern servers send the server timestamp in the TargetInfo Av_Pair
structure in the challenge message [see MS-NLMP 2.2.2.1]
In [MS-NLMP 3.1.5.1.2] it is explicitly mentioned that the client must
use the server provided timestamp if present OR current time if it is
not
Reported-by: Namjae Jeon <namjae.jeon@samsung.com>
Signed-off-by: Peter Seiderer <ps.report@gmx.net>
Signed-off-by: Steve French <smfrench@gmail.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Linux cifs mount with ntlmssp against an Mac OS X (Yosemite
10.10.5) share fails in case the clocks differ more than +/-2h:
digest-service: digest-request: od failed with 2 proto=ntlmv2
digest-service: digest-request: kdc failed with -1561745592 proto=ntlmv2
Fix this by (re-)using the given server timestamp for the
ntlmv2 authentication (as Windows 7 does).
A related problem was also reported earlier by Namjae Jaen (see below):
Windows machine has extended security feature which refuse to allow
authentication when there is time difference between server time and
client time when ntlmv2 negotiation is used. This problem is prevalent
in embedded enviornment where system time is set to default 1970.
Modern servers send the server timestamp in the TargetInfo Av_Pair
structure in the challenge message [see MS-NLMP 2.2.2.1]
In [MS-NLMP 3.1.5.1.2] it is explicitly mentioned that the client must
use the server provided timestamp if present OR current time if it is
not
Reported-by: Namjae Jeon <namjae.jeon@samsung.com>
Signed-off-by: Peter Seiderer <ps.report@gmx.net>
Signed-off-by: Steve French <smfrench@gmail.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
fs/cifs/cifsencrypt.c | patch | blob | history |
diff --git a/fs/cifs/cifsencrypt.c b/fs/cifs/cifsencrypt.c
index 4934347321d379b61aa170d0f93dd4468c383000..3299778391fd2b5566b18aa1c995b74f12b38160 100644 (file)
--- a/fs/cifs/cifsencrypt.c
+++ b/fs/cifs/cifsencrypt.c
return 0;
}
+/* Server has provided av pairs/target info in the type 2 challenge
+ * packet and we have plucked it and stored within smb session.
+ * We parse that blob here to find the server given timestamp
+ * as part of ntlmv2 authentication (or local current time as
+ * default in case of failure)
+ */
+static __le64
+find_timestamp(struct cifs_ses *ses)
+{
+ unsigned int attrsize;
+ unsigned int type;
+ unsigned int onesize = sizeof(struct ntlmssp2_name);
+ unsigned char *blobptr;
+ unsigned char *blobend;
+ struct ntlmssp2_name *attrptr;
+
+ if (!ses->auth_key.len || !ses->auth_key.response)
+ return 0;
+
+ blobptr = ses->auth_key.response;
+ blobend = blobptr + ses->auth_key.len;
+
+ while (blobptr + onesize < blobend) {
+ attrptr = (struct ntlmssp2_name *) blobptr;
+ type = le16_to_cpu(attrptr->type);
+ if (type == NTLMSSP_AV_EOL)
+ break;
+ blobptr += 2; /* advance attr type */
+ attrsize = le16_to_cpu(attrptr->length);
+ blobptr += 2; /* advance attr size */
+ if (blobptr + attrsize > blobend)
+ break;
+ if (type == NTLMSSP_AV_TIMESTAMP) {
+ if (attrsize == sizeof(u64))
+ return *((__le64 *)blobptr);
+ }
+ blobptr += attrsize; /* advance attr value */
+ }
+
+ return cpu_to_le64(cifs_UnixTimeToNT(CURRENT_TIME));
+}
+
static int calc_ntlmv2_hash(struct cifs_ses *ses, char *ntlmv2_hash,
const struct nls_table *nls_cp)
{
struct ntlmv2_resp *ntlmv2;
char ntlmv2_hash[16];
unsigned char *tiblob = NULL; /* target info blob */
+ __le64 rsp_timestamp;
if (ses->server->negflavor == CIFS_NEGFLAVOR_EXTENDED) {
if (!ses->domainName) {
}
}
+ /* Must be within 5 minutes of the server (or in range +/-2h
+ * in case of Mac OS X), so simply carry over server timestamp
+ * (as Windows 7 does)
+ */
+ rsp_timestamp = find_timestamp(ses);
+
baselen = CIFS_SESS_KEY_SIZE + sizeof(struct ntlmv2_resp);
tilen = ses->auth_key.len;
tiblob = ses->auth_key.response;
(ses->auth_key.response + CIFS_SESS_KEY_SIZE);
ntlmv2->blob_signature = cpu_to_le32(0x00000101);
ntlmv2->reserved = 0;
- /* Must be within 5 minutes of the server */
- ntlmv2->time = cpu_to_le64(cifs_UnixTimeToNT(CURRENT_TIME));
+ ntlmv2->time = rsp_timestamp;
+
get_random_bytes(&ntlmv2->client_chal, sizeof(ntlmv2->client_chal));
ntlmv2->reserved2 = 0;