summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 01cf9c6)
raw | patch | inline | side by side (parent: 01cf9c6)
author | David Woodhouse <dwmw2@infradead.org> | |
Wed, 16 Sep 2015 13:10:03 +0000 (14:10 +0100) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 22 Oct 2015 21:39:17 +0000 (14:39 -0700) |
commit 03da3ff1cfcd7774c8780d2547ba0d995f7dc03d upstream.
In 2007, commit 07190a08eef36 ("Mark TSC on GeodeLX reliable")
bypassed verification of the TSC on Geode LX. However, this code
(now in the check_system_tsc_reliable() function in
arch/x86/kernel/tsc.c) was only present if CONFIG_MGEODE_LX was
set.
OpenWRT has recently started building its generic Geode target
for Geode GX, not LX, to include support for additional
platforms. This broke the timekeeping on LX-based devices,
because the TSC wasn't marked as reliable:
https://dev.openwrt.org/ticket/20531
By adding a runtime check on is_geode_lx(), we can also include
the fix if CONFIG_MGEODEGX1 or CONFIG_X86_GENERIC are set, thus
fixing the problem.
Signed-off-by: David Woodhouse <David.Woodhouse@intel.com>
Cc: Andres Salomon <dilinger@queued.net>
Cc: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Marcelo Tosatti <marcelo@kvack.org>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Thomas Gleixner <tglx@linutronix.de>
Link: http://lkml.kernel.org/r/1442409003.131189.87.camel@infradead.org
Signed-off-by: Ingo Molnar <mingo@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
In 2007, commit 07190a08eef36 ("Mark TSC on GeodeLX reliable")
bypassed verification of the TSC on Geode LX. However, this code
(now in the check_system_tsc_reliable() function in
arch/x86/kernel/tsc.c) was only present if CONFIG_MGEODE_LX was
set.
OpenWRT has recently started building its generic Geode target
for Geode GX, not LX, to include support for additional
platforms. This broke the timekeeping on LX-based devices,
because the TSC wasn't marked as reliable:
https://dev.openwrt.org/ticket/20531
By adding a runtime check on is_geode_lx(), we can also include
the fix if CONFIG_MGEODEGX1 or CONFIG_X86_GENERIC are set, thus
fixing the problem.
Signed-off-by: David Woodhouse <David.Woodhouse@intel.com>
Cc: Andres Salomon <dilinger@queued.net>
Cc: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Marcelo Tosatti <marcelo@kvack.org>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Thomas Gleixner <tglx@linutronix.de>
Link: http://lkml.kernel.org/r/1442409003.131189.87.camel@infradead.org
Signed-off-by: Ingo Molnar <mingo@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
arch/x86/kernel/tsc.c | patch | blob | history |
diff --git a/arch/x86/kernel/tsc.c b/arch/x86/kernel/tsc.c
index b20bced0090f3e7ff09d3cae941e10a11058a2f3..8bc924ff88ee1067bb1510eb827627964c9c4fec 100644 (file)
--- a/arch/x86/kernel/tsc.c
+++ b/arch/x86/kernel/tsc.c
#include <asm/hypervisor.h>
#include <asm/nmi.h>
#include <asm/x86_init.h>
+#include <asm/geode.h>
unsigned int __read_mostly cpu_khz; /* TSC clocks / usec, not used here */
EXPORT_SYMBOL(cpu_khz);
static void __init check_system_tsc_reliable(void)
{
-#ifdef CONFIG_MGEODE_LX
- /* RTSC counts during suspend */
+#if defined(CONFIG_MGEODEGX1) || defined(CONFIG_MGEODE_LX) || defined(CONFIG_X86_GENERIC)
+ if (is_geode_lx()) {
+ /* RTSC counts during suspend */
#define RTSC_SUSP 0x100
- unsigned long res_low, res_high;
+ unsigned long res_low, res_high;
- rdmsr_safe(MSR_GEODE_BUSCONT_CONF0, &res_low, &res_high);
- /* Geode_LX - the OLPC CPU has a very reliable TSC */
- if (res_low & RTSC_SUSP)
- tsc_clocksource_reliable = 1;
+ rdmsr_safe(MSR_GEODE_BUSCONT_CONF0, &res_low, &res_high);
+ /* Geode_LX - the OLPC CPU has a very reliable TSC */
+ if (res_low & RTSC_SUSP)
+ tsc_clocksource_reliable = 1;
+ }
#endif
if (boot_cpu_has(X86_FEATURE_TSC_RELIABLE))
tsc_clocksource_reliable = 1;