author | Linus Torvalds <torvalds@linux-foundation.org> | |
Mon, 17 Dec 2012 01:33:01 +0000 (17:33 -0800) | ||
committer | Linus Torvalds <torvalds@linux-foundation.org> | |
Mon, 17 Dec 2012 01:33:01 +0000 (17:33 -0800) |
Pull ext4 update from Ted Ts'o:
"There are two major features for this merge window. The first is
inline data, which allows small files or directories to be stored in
the in-inode extended attribute area. (This requires that the file
system use inodes which are at least 256 bytes or larger; 128 byte
inodes do not have any room for in-inode xattrs.)
The second new feature is SEEK_HOLE/SEEK_DATA support. This is
enabled by the extent status tree patches, and this infrastructure
will be used to further optimize ext4 in the future.
Beyond that, we have the usual collection of code cleanups and bug
fixes."
* tag 'ext4_for_linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tytso/ext4: (63 commits)
ext4: zero out inline data using memset() instead of empty_zero_page
ext4: ensure Inode flags consistency are checked at build time
ext4: Remove CONFIG_EXT4_FS_XATTR
ext4: remove unused variable from ext4_ext_in_cache()
ext4: remove redundant initialization in ext4_fill_super()
ext4: remove redundant code in ext4_alloc_inode()
ext4: use sync_inode_metadata() when syncing inode metadata
ext4: enable ext4 inline support
ext4: let fallocate handle inline data correctly
ext4: let ext4_truncate handle inline data correctly
ext4: evict inline data out if we need to strore xattr in inode
ext4: let fiemap work with inline data
ext4: let ext4_rename handle inline dir
ext4: let empty_dir handle inline dir
ext4: let ext4_delete_entry() handle inline data
ext4: make ext4_delete_entry generic
ext4: let ext4_find_entry handle inline data
ext4: create a new function search_dir
ext4: let ext4_readdir handle inline data
ext4: let add_dir_entry handle inline data properly
...
"There are two major features for this merge window. The first is
inline data, which allows small files or directories to be stored in
the in-inode extended attribute area. (This requires that the file
system use inodes which are at least 256 bytes or larger; 128 byte
inodes do not have any room for in-inode xattrs.)
The second new feature is SEEK_HOLE/SEEK_DATA support. This is
enabled by the extent status tree patches, and this infrastructure
will be used to further optimize ext4 in the future.
Beyond that, we have the usual collection of code cleanups and bug
fixes."
* tag 'ext4_for_linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tytso/ext4: (63 commits)
ext4: zero out inline data using memset() instead of empty_zero_page
ext4: ensure Inode flags consistency are checked at build time
ext4: Remove CONFIG_EXT4_FS_XATTR
ext4: remove unused variable from ext4_ext_in_cache()
ext4: remove redundant initialization in ext4_fill_super()
ext4: remove redundant code in ext4_alloc_inode()
ext4: use sync_inode_metadata() when syncing inode metadata
ext4: enable ext4 inline support
ext4: let fallocate handle inline data correctly
ext4: let ext4_truncate handle inline data correctly
ext4: evict inline data out if we need to strore xattr in inode
ext4: let fiemap work with inline data
ext4: let ext4_rename handle inline dir
ext4: let empty_dir handle inline dir
ext4: let ext4_delete_entry() handle inline data
ext4: make ext4_delete_entry generic
ext4: let ext4_find_entry handle inline data
ext4: create a new function search_dir
ext4: let ext4_readdir handle inline data
ext4: let add_dir_entry handle inline data properly
...
1 | 2 | |||
---|---|---|---|---|
fs/ext4/ext4.h | patch | | diff1 | | diff2 | | blob | history |
fs/jbd2/transaction.c | patch | | diff1 | | diff2 | | blob | history |
diff --cc fs/ext4/ext4.h
index df163da388c9ccfe82348c51be596c9fcfd8cc55,b79d613091d08539f73b167b30ef38bf2987bab4..8462eb3c33aa22c62cccb88b030edfb599e2db66
--- 1/fs/ext4/ext4.h
--- 2/fs/ext4/ext4.h
+++ b/fs/ext4/ext4.h
BUFFER_FNS(Uninit, uninit)
TAS_BUFFER_FNS(Uninit, uninit)
- BUFFER_FNS(Da_Mapped, da_mapped)
/*
- * Add new method to test wether block and inode bitmaps are properly
+ * Add new method to test whether block and inode bitmaps are properly
* initialized. With uninit_bg reading the block from disk is not enough
* to mark the bitmap uptodate. We need to also zero-out the bitmap
*/
diff --cc fs/jbd2/transaction.c
Simple merge