summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 1e80807)
raw | patch | inline | side by side (parent: 1e80807)
author | Archit Taneja <archit@ti.com> | |
Tue, 30 Apr 2013 16:50:29 +0000 (18:50 +0200) | ||
committer | Archit Taneja <archit@ti.com> | |
Thu, 30 May 2013 15:39:09 +0000 (21:09 +0530) |
- Vayu evm has a demux which decides whether i2c2 lines go to the hdmi level
shifter(and finally to the panel) or if they are in their normal state(where
i2c2 is connected to many slaves, one of which is a gpio expander to configure
the LS_OE and CT_HPD pins of the level shifter). This demux is controlled by
a mcasp based gpio. There is no mcasp-gpio driver, neither there is a clean
way to represent such a pin in DT. So the bit is toggled as a hack in the
hdmi driver itself.
- On DRA7x, hdmi phy state transition checks are failing even though hdmi phy is
transitioning correctly, ignore the phy transition checks for now.
These need to be cleaned up later.
Signed-off-by: Archit Taneja <archit@ti.com>
shifter(and finally to the panel) or if they are in their normal state(where
i2c2 is connected to many slaves, one of which is a gpio expander to configure
the LS_OE and CT_HPD pins of the level shifter). This demux is controlled by
a mcasp based gpio. There is no mcasp-gpio driver, neither there is a clean
way to represent such a pin in DT. So the bit is toggled as a hack in the
hdmi driver itself.
- On DRA7x, hdmi phy state transition checks are failing even though hdmi phy is
transitioning correctly, ignore the phy transition checks for now.
These need to be cleaned up later.
Signed-off-by: Archit Taneja <archit@ti.com>
drivers/video/omap2/dss/dss.h | patch | blob | history | |
drivers/video/omap2/dss/hdmi.c | patch | blob | history | |
drivers/video/omap2/dss/ti_hdmi_4xxx_ip.c | patch | blob | history |
index 9cf3dfd3db887238b6e8767c7d294370813223da..6212bd6877b36055dbaa796b7985a31b3e59588d 100644 (file)
bool hdmi_restart);
int omapdss_hdmi_display_3d_enable(struct omap_dss_device *dssdev,
struct s3d_disp_info *info, int code);
+void sel_i2c(void);
+void sel_hdmi(void);
int hdmi_panel_init(void);
void hdmi_panel_exit(void);
#if defined(CONFIG_OMAP4_DSS_HDMI_AUDIO) || \
index a56639c59db1a873d623117cd2776d54b23622ef..15c9d011ddc82d656798c1aced82697a3164e01f 100644 (file)
if (state == hdmi.ls_state)
return;
+ sel_i2c();
+
switch (state) {
case LS_HPD_ON:
hpd_enable = true;
udelay(300);
hdmi.ls_state = state;
+
+ sel_hdmi();
}
static int hdmi_runtime_get(void)
}
r = hdmi.ip_data.ops->phy_enable(&hdmi.ip_data);
+ /*
+ * DRA7xx doesn't show the correct PHY transition changes in the
+ * WP_PWR_CTRL register, need to investigate
+ */
+ if (omapdss_get_version() == OMAPDSS_VER_DRA7xx)
+ r = 0;
+
if (r) {
DSSDBG("Failed to start PHY\n");
goto err_phy_enable;
}
}
+static void init_sel_i2c_hdmi(void)
+{
+ void __iomem *clk_base = ioremap(0x4A009000, SZ_4K);
+ void __iomem *mcasp2_base = ioremap(0x48464000, SZ_1K);
+ void __iomem *pinmux = ioremap(0x4a003600, SZ_1K);
+ u32 val;
+
+ if (omapdss_get_version() != OMAPDSS_VER_DRA7xx)
+ goto err;
+
+ if (!clk_base || !mcasp2_base || !pinmux)
+ DSSERR("couldn't ioremap for clk or mcasp2\n");
+
+ __raw_writel(0x40000, pinmux + 0xfc);
+ /* sw supervised wkup */
+ __raw_writel(0x2, clk_base + 0x8fc);
+
+ /* enable clock domain */
+ __raw_writel(0x2, clk_base + 0x860);
+
+ /* see what status looks like */
+ val = __raw_readl(clk_base + 0x8fc);
+ printk("CM_L4PER2_CLKSTCTRL %x\n", val);
+
+ /*
+ * mcasp2 regs should be hopefully accessible, make mcasp2_aclkr
+ * a gpio, write necessary stuff to MCASP_PFUNC and PDIR
+ */
+ __raw_writel(0x1 << 29, mcasp2_base + 0x10);
+ __raw_writel(0x1 << 29, mcasp2_base + 0x14);
+
+err:
+ iounmap(clk_base);
+ iounmap(mcasp2_base);
+ iounmap(pinmux);
+}
+
+/* use this to configure the pcf8575@22 to set LS_OE and CT_HPD */
+void sel_i2c(void)
+{
+ void __iomem *base = ioremap(0x48464000, SZ_1K);
+
+ if (omapdss_get_version() != OMAPDSS_VER_DRA7xx)
+ goto err;
+
+ /* PDOUT */
+ __raw_writel(0x0, base + 0x18);
+
+ DSSDBG("PDOUT sel_i2c %x\n", __raw_readl(base + 0x18));
+
+err:
+ iounmap(base);
+}
+
+/* use this to read edid and detect hpd ? */
+void sel_hdmi(void)
+{
+ void __iomem *base = ioremap(0x48464000, SZ_1K);
+
+ if (omapdss_get_version() != OMAPDSS_VER_DRA7xx)
+ goto err;
+
+ /* PDOUT */
+ __raw_writel(0x20000000, base + 0x18);
+
+ DSSDBG("PDOUT sel_hdmi %x\n", __raw_readl(base + 0x18));
+
+err:
+ iounmap(base);
+}
+
static void __init hdmi_probe_of(struct platform_device *pdev)
{
struct device_node *node = pdev->dev.of_node;
DSSERR("failed to parse SDA gpio\n");
return;
}
+ } else if (adapter != NULL) {
+ hdmi.adap = adapter;
+
+ /*
+ * we have SEL_I2C_HDMI pin which acts as a control line to
+ * a demux which choses the i2c lines to go either to hdmi
+ * or to the other i2c2 slaves. This line is used as a mcasp2
+ * gpio. Init the gpio pin so that it can be used to control
+ * the demux.
+ */
+ init_sel_i2c_hdmi();
+ sel_i2c();
}
dssdev = dss_alloc_and_init_device(&pdev->dev);
index 6dae397a94eb5f66709958607474378c684f3d9a..d7f19376181579ff3db03d4d040b090fda1ac001 100644 (file)
else
r = hdmi_set_phy_pwr(ip_data, HDMI_PHYPWRCMD_LDOON);
+ /*
+ * DRA7xx doesn't show the correct PHY transition changes in the
+ * WP_PWR_CTRL register, need to investigate
+ */
+ if (omapdss_get_version() == OMAPDSS_VER_DRA7xx)
+ r = 0;
+
if (r) {
DSSERR("Failed to %s PHY TX power\n",
hpd ? "enable" : "disable");