summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 8580153)
raw | patch | inline | side by side (parent: 8580153)
author | San Mehat <san@android.com> | |
Mon, 14 Apr 2008 22:22:49 +0000 (15:22 -0700) | ||
committer | Arve Hjønnevåg <arve@android.com> | |
Tue, 19 Feb 2013 23:49:14 +0000 (15:49 -0800) |
This is required to support chips which use SDIO for signaling/
communication but do not implement the various card enumeration registers
as required for full SD / SDIO cards.
mmc: sdio: Fix bug where we're freeing the CIS tables we never allocated when using EMBEDDED_SDIO
mmc: Add max_blksize to embedded SDIO data
Signed-off-by: San Mehat <san@google.com>
communication but do not implement the various card enumeration registers
as required for full SD / SDIO cards.
mmc: sdio: Fix bug where we're freeing the CIS tables we never allocated when using EMBEDDED_SDIO
mmc: Add max_blksize to embedded SDIO data
Signed-off-by: San Mehat <san@google.com>
index 1972b00f801bb6c89354f186b563254f8b0ece4b..85c2e1acd15627b224a6fa7400d31c1a07cf8493 100644 (file)
--- a/drivers/mmc/core/Kconfig
+++ b/drivers/mmc/core/Kconfig
If unsure, say N.
+config MMC_EMBEDDED_SDIO
+ boolean "MMC embedded SDIO device support (EXPERIMENTAL)"
+ depends on EXPERIMENTAL
+ help
+ If you say Y here, support will be added for embedded SDIO
+ devices which do not contain the necessary enumeration
+ support in hardware to be properly detected.
+
config MMC_PARANOID_SD_INIT
bool "Enable paranoid SD card initialization (EXPERIMENTAL)"
+ depends on EXPERIMENTAL
help
If you say Y here, the MMC layer will be extra paranoid
about re-trying SD init requests. This can be a useful
index aaed7687cf094fd9659dae2892b89c9ccd89c138..816ce788f3333806520d72d8823aea9236b62a52 100644 (file)
--- a/drivers/mmc/core/core.c
+++ b/drivers/mmc/core/core.c
}
#endif
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+void mmc_set_embedded_sdio_data(struct mmc_host *host,
+ struct sdio_cis *cis,
+ struct sdio_cccr *cccr,
+ struct sdio_embedded_func *funcs,
+ int num_funcs)
+{
+ host->embedded_sdio_data.cis = cis;
+ host->embedded_sdio_data.cccr = cccr;
+ host->embedded_sdio_data.funcs = funcs;
+ host->embedded_sdio_data.num_funcs = num_funcs;
+}
+
+EXPORT_SYMBOL(mmc_set_embedded_sdio_data);
+#endif
+
static int __init mmc_init(void)
{
int ret;
index 2273ce6b6c1afbd75774e38eced2cd2d5766529e..623198972ef6c4d320b194fa989601ae14abaf9a 100644 (file)
--- a/drivers/mmc/core/sdio.c
+++ b/drivers/mmc/core/sdio.c
#include "sdio_ops.h"
#include "sdio_cis.h"
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+#include <linux/mmc/sdio_ids.h>
+#endif
+
static int sdio_read_fbr(struct sdio_func *func)
{
int ret;
goto finish;
}
- /*
- * Read the common registers.
- */
- err = sdio_read_cccr(card, ocr);
- if (err)
- goto remove;
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ if (host->embedded_sdio_data.cccr)
+ memcpy(&card->cccr, host->embedded_sdio_data.cccr, sizeof(struct sdio_cccr));
+ else {
+#endif
+ /*
+ * Read the common registers.
+ */
+ err = sdio_read_cccr(card, ocr);
+ if (err)
+ goto remove;
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ }
+#endif
- /*
- * Read the common CIS tuples.
- */
- err = sdio_read_common_cis(card);
- if (err)
- goto remove;
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ if (host->embedded_sdio_data.cis)
+ memcpy(&card->cis, host->embedded_sdio_data.cis, sizeof(struct sdio_cis));
+ else {
+#endif
+ /*
+ * Read the common CIS tuples.
+ */
+ err = sdio_read_common_cis(card);
+ if (err)
+ goto remove;
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ }
+#endif
if (oldcard) {
int same = (card->cis.vendor == oldcard->cis.vendor &&
funcs = (ocr & 0x70000000) >> 28;
card->sdio_funcs = 0;
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ if (host->embedded_sdio_data.funcs)
+ card->sdio_funcs = funcs = host->embedded_sdio_data.num_funcs;
+#endif
+
/*
* Initialize (but don't add) all present functions.
*/
for (i = 0; i < funcs; i++, card->sdio_funcs++) {
- err = sdio_init_func(host->card, i + 1);
- if (err)
- goto remove;
-
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ if (host->embedded_sdio_data.funcs) {
+ struct sdio_func *tmp;
+
+ tmp = sdio_alloc_func(host->card);
+ if (IS_ERR(tmp))
+ goto remove;
+ tmp->num = (i + 1);
+ card->sdio_func[i] = tmp;
+ tmp->class = host->embedded_sdio_data.funcs[i].f_class;
+ tmp->max_blksize = host->embedded_sdio_data.funcs[i].f_maxblksize;
+ tmp->vendor = card->cis.vendor;
+ tmp->device = card->cis.device;
+ } else {
+#endif
+ err = sdio_init_func(host->card, i + 1);
+ if (err)
+ goto remove;
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ }
+#endif
/*
* Enable Runtime PM for this func (if supported)
*/
index 5e57048e2c1d2c0fbb202600f9bfa45ffa0355c4..19edd595604a0a89d6bd73742b1850b41c6a228c 100644 (file)
#include "sdio_cis.h"
#include "sdio_bus.h"
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+#include <linux/mmc/host.h>
+#endif
+
/* show configuration fields */
#define sdio_config_attr(field, format_string) \
static ssize_t \
{
struct sdio_func *func = dev_to_sdio_func(dev);
- sdio_free_func_cis(func);
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ /*
+ * If this device is embedded then we never allocated
+ * cis tables for this func
+ */
+ if (!func->card->host->embedded_sdio_data.funcs)
+#endif
+ sdio_free_func_cis(func);
kfree(func->info);
index 0926063bff9f27e4a5ced1374f3a674155551d10..9d1d9caf2611615488fb6a94547358ce288777a9 100644 (file)
#define AMBA_MMCI_H
#include <linux/mmc/host.h>
+#include <linux/mmc/card.h>
+#include <linux/mmc/sdio_func.h>
+
+struct embedded_sdio_data {
+ struct sdio_cis cis;
+ struct sdio_cccr cccr;
+ struct sdio_embedded_func *funcs;
+ int num_funcs;
+};
/*
void *dma_rx_param;
void *dma_tx_param;
unsigned int status_irq;
+ struct embedded_sdio_data *embedded_sdio;
int (*register_status_notify)(void (*callback)(int card_present, void *dev_id), void *dev_id);
};
index 61a10c17aabd98df129c091bc82697b5faa0b09d..1a5fc1f91c208c3319bc689d269faedf885e44dc 100644 (file)
--- a/include/linux/mmc/host.h
+++ b/include/linux/mmc/host.h
unsigned int actual_clock; /* Actual HC clock rate */
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+ struct {
+ struct sdio_cis *cis;
+ struct sdio_cccr *cccr;
+ struct sdio_embedded_func *funcs;
+ int num_funcs;
+ } embedded_sdio_data;
+#endif
+
unsigned long private[0] ____cacheline_aligned;
};
extern void mmc_remove_host(struct mmc_host *);
extern void mmc_free_host(struct mmc_host *);
+#ifdef CONFIG_MMC_EMBEDDED_SDIO
+extern void mmc_set_embedded_sdio_data(struct mmc_host *host,
+ struct sdio_cis *cis,
+ struct sdio_cccr *cccr,
+ struct sdio_embedded_func *funcs,
+ int num_funcs);
+#endif
+
static inline void *mmc_priv(struct mmc_host *host)
{
return (void *)host->private;
index 50f0bc952328ba0eefdb901f31424821a8765539..54600e927b06b05c618d294edcb42772c57349bc 100644 (file)
typedef void (sdio_irq_handler_t)(struct sdio_func *);
+/*
+ * Structure used to hold embedded SDIO device data from platform layer
+ */
+struct sdio_embedded_func {
+ uint8_t f_class;
+ uint32_t f_maxblksize;
+};
+
/*
* SDIO function CIS tuple (unknown to the core)
*/