summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: bf414b3)
raw | patch | inline | side by side (parent: bf414b3)
author | Ian Campbell <Ian.Campbell@citrix.com> | |
Wed, 6 Feb 2013 23:41:35 +0000 (23:41 +0000) | ||
committer | David S. Miller <davem@davemloft.net> | |
Fri, 8 Feb 2013 04:29:28 +0000 (23:29 -0500) |
A buggy or malicious frontend should not be able to confuse netback.
If we spot anything which is not as it should be then shutdown the
device and don't try to continue with the ring in a potentially
hostile state. Well behaved and non-hostile frontends will not be
penalised.
As well as making the existing checks for such errors fatal also add a
new check that ensures that there isn't an insane number of requests
on the ring (i.e. more than would fit in the ring). If the ring
contains garbage then previously is was possible to loop over this
insane number, getting an error each time and therefore not generating
any more pending requests and therefore not exiting the loop in
xen_netbk_tx_build_gops for an externded period.
Also turn various netdev_dbg calls which no precipitate a fatal error
into netdev_err, they are rate limited because the device is shutdown
afterwards.
This fixes at least one known DoS/softlockup of the backend domain.
Signed-off-by: Ian Campbell <ian.campbell@citrix.com>
Reviewed-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com>
Acked-by: Jan Beulich <JBeulich@suse.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
If we spot anything which is not as it should be then shutdown the
device and don't try to continue with the ring in a potentially
hostile state. Well behaved and non-hostile frontends will not be
penalised.
As well as making the existing checks for such errors fatal also add a
new check that ensures that there isn't an insane number of requests
on the ring (i.e. more than would fit in the ring). If the ring
contains garbage then previously is was possible to loop over this
insane number, getting an error each time and therefore not generating
any more pending requests and therefore not exiting the loop in
xen_netbk_tx_build_gops for an externded period.
Also turn various netdev_dbg calls which no precipitate a fatal error
into netdev_err, they are rate limited because the device is shutdown
afterwards.
This fixes at least one known DoS/softlockup of the backend domain.
Signed-off-by: Ian Campbell <ian.campbell@citrix.com>
Reviewed-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com>
Acked-by: Jan Beulich <JBeulich@suse.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
drivers/net/xen-netback/common.h | patch | blob | history | |
drivers/net/xen-netback/interface.c | patch | blob | history | |
drivers/net/xen-netback/netback.c | patch | blob | history |
index 94b79c3338c4260200306f180ff053b87006faa6..9d7f1723dd8f750126337d7792a0614fea8ca601 100644 (file)
/* Notify xenvif that ring now has space to send an skb to the frontend */
void xenvif_notify_tx_completion(struct xenvif *vif);
+/* Prevent the device from generating any further traffic. */
+void xenvif_carrier_off(struct xenvif *vif);
+
/* Returns number of ring slots required to send an skb to the frontend */
unsigned int xen_netbk_count_skb_slots(struct xenvif *vif, struct sk_buff *skb);
index b7d41f8c338a8372cea8bfe6649386c6a0d8b090..b8c5193bd420030a363ba30c14e8b485a8d6c5cc 100644 (file)
return err;
}
-void xenvif_disconnect(struct xenvif *vif)
+void xenvif_carrier_off(struct xenvif *vif)
{
struct net_device *dev = vif->dev;
- if (netif_carrier_ok(dev)) {
- rtnl_lock();
- netif_carrier_off(dev); /* discard queued packets */
- if (netif_running(dev))
- xenvif_down(vif);
- rtnl_unlock();
- xenvif_put(vif);
- }
+
+ rtnl_lock();
+ netif_carrier_off(dev); /* discard queued packets */
+ if (netif_running(dev))
+ xenvif_down(vif);
+ rtnl_unlock();
+ xenvif_put(vif);
+}
+
+void xenvif_disconnect(struct xenvif *vif)
+{
+ if (netif_carrier_ok(vif->dev))
+ xenvif_carrier_off(vif);
atomic_dec(&vif->refcnt);
wait_event(vif->waiting_to_free, atomic_read(&vif->refcnt) == 0);
index f2d6b78d901d92d3965fe3bd849751f04fb7ccf3..c2e3336b4f98a8ddda64686ade22e6826aecbb29 100644 (file)
xenvif_put(vif);
}
+static void netbk_fatal_tx_err(struct xenvif *vif)
+{
+ netdev_err(vif->dev, "fatal error; disabling device\n");
+ xenvif_carrier_off(vif);
+ xenvif_put(vif);
+}
+
static int netbk_count_requests(struct xenvif *vif,
struct xen_netif_tx_request *first,
struct xen_netif_tx_request *txp,
do {
if (frags >= work_to_do) {
- netdev_dbg(vif->dev, "Need more frags\n");
+ netdev_err(vif->dev, "Need more frags\n");
+ netbk_fatal_tx_err(vif);
return -frags;
}
if (unlikely(frags >= MAX_SKB_FRAGS)) {
- netdev_dbg(vif->dev, "Too many frags\n");
+ netdev_err(vif->dev, "Too many frags\n");
+ netbk_fatal_tx_err(vif);
return -frags;
}
memcpy(txp, RING_GET_REQUEST(&vif->tx, cons + frags),
sizeof(*txp));
if (txp->size > first->size) {
- netdev_dbg(vif->dev, "Frags galore\n");
+ netdev_err(vif->dev, "Frag is bigger than frame.\n");
+ netbk_fatal_tx_err(vif);
return -frags;
}
frags++;
if (unlikely((txp->offset + txp->size) > PAGE_SIZE)) {
- netdev_dbg(vif->dev, "txp->offset: %x, size: %u\n",
+ netdev_err(vif->dev, "txp->offset: %x, size: %u\n",
txp->offset, txp->size);
+ netbk_fatal_tx_err(vif);
return -frags;
}
} while ((txp++)->flags & XEN_NETTXF_more_data);
do {
if (unlikely(work_to_do-- <= 0)) {
- netdev_dbg(vif->dev, "Missing extra info\n");
+ netdev_err(vif->dev, "Missing extra info\n");
+ netbk_fatal_tx_err(vif);
return -EBADR;
}
if (unlikely(!extra.type ||
extra.type >= XEN_NETIF_EXTRA_TYPE_MAX)) {
vif->tx.req_cons = ++cons;
- netdev_dbg(vif->dev,
+ netdev_err(vif->dev,
"Invalid extra type: %d\n", extra.type);
+ netbk_fatal_tx_err(vif);
return -EINVAL;
}
struct xen_netif_extra_info *gso)
{
if (!gso->u.gso.size) {
- netdev_dbg(vif->dev, "GSO size must not be zero.\n");
+ netdev_err(vif->dev, "GSO size must not be zero.\n");
+ netbk_fatal_tx_err(vif);
return -EINVAL;
}
/* Currently only TCPv4 S.O. is supported. */
if (gso->u.gso.type != XEN_NETIF_GSO_TYPE_TCPV4) {
- netdev_dbg(vif->dev, "Bad GSO type %d.\n", gso->u.gso.type);
+ netdev_err(vif->dev, "Bad GSO type %d.\n", gso->u.gso.type);
+ netbk_fatal_tx_err(vif);
return -EINVAL;
}
/* Get a netif from the list with work to do. */
vif = poll_net_schedule_list(netbk);
+ /* This can sometimes happen because the test of
+ * list_empty(net_schedule_list) at the top of the
+ * loop is unlocked. Just go back and have another
+ * look.
+ */
if (!vif)
continue;
+ if (vif->tx.sring->req_prod - vif->tx.req_cons >
+ XEN_NETIF_TX_RING_SIZE) {
+ netdev_err(vif->dev,
+ "Impossible number of requests. "
+ "req_prod %d, req_cons %d, size %ld\n",
+ vif->tx.sring->req_prod, vif->tx.req_cons,
+ XEN_NETIF_TX_RING_SIZE);
+ netbk_fatal_tx_err(vif);
+ continue;
+ }
+
RING_FINAL_CHECK_FOR_REQUESTS(&vif->tx, work_to_do);
if (!work_to_do) {
xenvif_put(vif);
work_to_do = xen_netbk_get_extras(vif, extras,
work_to_do);
idx = vif->tx.req_cons;
- if (unlikely(work_to_do < 0)) {
- netbk_tx_err(vif, &txreq, idx);
+ if (unlikely(work_to_do < 0))
continue;
- }
}
ret = netbk_count_requests(vif, &txreq, txfrags, work_to_do);
- if (unlikely(ret < 0)) {
- netbk_tx_err(vif, &txreq, idx - ret);
+ if (unlikely(ret < 0))
continue;
- }
+
idx += ret;
if (unlikely(txreq.size < ETH_HLEN)) {
/* No crossing a page as the payload mustn't fragment. */
if (unlikely((txreq.offset + txreq.size) > PAGE_SIZE)) {
- netdev_dbg(vif->dev,
+ netdev_err(vif->dev,
"txreq.offset: %x, size: %u, end: %lu\n",
txreq.offset, txreq.size,
(txreq.offset&~PAGE_MASK) + txreq.size);
- netbk_tx_err(vif, &txreq, idx);
+ netbk_fatal_tx_err(vif);
continue;
}
gso = &extras[XEN_NETIF_EXTRA_TYPE_GSO - 1];
if (netbk_set_skb_gso(vif, skb, gso)) {
+ /* Failure in netbk_set_skb_gso is fatal. */
kfree_skb(skb);
- netbk_tx_err(vif, &txreq, idx);
continue;
}
}