summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c8356b2)
raw | patch | inline | side by side (parent: c8356b2)
author | Peter Zijlstra <peterz@infradead.org> | |
Thu, 11 Jun 2015 12:46:43 +0000 (14:46 +0200) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 3 Mar 2016 23:06:47 +0000 (15:06 -0800) |
commit 9916e214998a4a363b152b637245e5c958067350 upstream.
Remove the direct {push,pull} balancing operations from
switched_{from,to}_dl() / prio_changed_dl() and use the balance
callback queue.
Again, err on the side of too many reschedules; since too few is a
hard bug while too many is just annoying.
Signed-off-by: Peter Zijlstra (Intel) <peterz@infradead.org>
Cc: ktkhai@parallels.com
Cc: rostedt@goodmis.org
Cc: juri.lelli@gmail.com
Cc: pang.xunlei@linaro.org
Cc: oleg@redhat.com
Cc: wanpeng.li@linux.intel.com
Cc: umgwanakikbuti@gmail.com
Link: http://lkml.kernel.org/r/20150611124742.968262663@infradead.org
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Byungchul Park <byungchul.park@lge.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Remove the direct {push,pull} balancing operations from
switched_{from,to}_dl() / prio_changed_dl() and use the balance
callback queue.
Again, err on the side of too many reschedules; since too few is a
hard bug while too many is just annoying.
Signed-off-by: Peter Zijlstra (Intel) <peterz@infradead.org>
Cc: ktkhai@parallels.com
Cc: rostedt@goodmis.org
Cc: juri.lelli@gmail.com
Cc: pang.xunlei@linaro.org
Cc: oleg@redhat.com
Cc: wanpeng.li@linux.intel.com
Cc: umgwanakikbuti@gmail.com
Link: http://lkml.kernel.org/r/20150611124742.968262663@infradead.org
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Byungchul Park <byungchul.park@lge.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
kernel/sched/deadline.c | patch | blob | history |
index ec1f21d0aa3660ce2db7bdf9d01fa6379894ea11..6ab59bb2947ba8fa74961827a56f3bb349d2f3a7 100644 (file)
--- a/kernel/sched/deadline.c
+++ b/kernel/sched/deadline.c
static int push_dl_task(struct rq *rq);
-static DEFINE_PER_CPU(struct callback_head, dl_balance_head);
+static DEFINE_PER_CPU(struct callback_head, dl_push_head);
+static DEFINE_PER_CPU(struct callback_head, dl_pull_head);
static void push_dl_tasks(struct rq *);
+static void pull_dl_task(struct rq *);
static inline void queue_push_tasks(struct rq *rq)
{
if (!has_pushable_dl_tasks(rq))
return;
- queue_balance_callback(rq, &per_cpu(dl_balance_head, rq->cpu), push_dl_tasks);
+ queue_balance_callback(rq, &per_cpu(dl_push_head, rq->cpu), push_dl_tasks);
+}
+
+static inline void queue_pull_task(struct rq *rq)
+{
+ queue_balance_callback(rq, &per_cpu(dl_pull_head, rq->cpu), pull_dl_task);
}
#else
static inline void queue_push_tasks(struct rq *rq)
{
}
+
+static inline void queue_pull_task(struct rq *rq)
+{
+}
#endif /* CONFIG_SMP */
static void enqueue_task_dl(struct rq *rq, struct task_struct *p, int flags);
* from an overloaded cpu, if any.
*/
if (!rq->dl.dl_nr_running)
- pull_dl_task(rq);
+ queue_pull_task(rq);
#endif
}
*/
static void switched_to_dl(struct rq *rq, struct task_struct *p)
{
- int check_resched = 1;
-
/*
* If p is throttled, don't consider the possibility
* of preempting rq->curr, the check will be done right
if (p->on_rq || rq->curr != p) {
#ifdef CONFIG_SMP
- if (rq->dl.overloaded && push_dl_task(rq) && rq != task_rq(p))
- /* Only reschedule if pushing failed */
- check_resched = 0;
-#endif /* CONFIG_SMP */
- if (check_resched && task_has_dl_policy(rq->curr))
+ if (rq->dl.overloaded)
+ queue_push_tasks(rq);
+#else
+ if (task_has_dl_policy(rq->curr))
check_preempt_curr_dl(rq, p, 0);
+#endif /* CONFIG_SMP */
}
}
* or lowering its prio, so...
*/
if (!rq->dl.overloaded)
- pull_dl_task(rq);
+ queue_pull_task(rq);
/*
* If we now have a earlier deadline task than p,
* then reschedule, provided p is still on this
* runqueue.
*/
- if (dl_time_before(rq->dl.earliest_dl.curr, p->dl.deadline) &&
- rq->curr == p)
+ if (dl_time_before(rq->dl.earliest_dl.curr, p->dl.deadline))
resched_task(p);
#else
/*