summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 38922e5)
raw | patch | inline | side by side (parent: 38922e5)
author | Lennart Sorensen <lsorense@csclub.uwaterloo.ca> | |
Mon, 29 Dec 2014 04:47:30 +0000 (10:17 +0530) | ||
committer | Lokesh Vutla <lokeshvutla@ti.com> | |
Fri, 2 Jan 2015 06:22:38 +0000 (11:52 +0530) |
Errata i856 for the AM572x (DRA7xx) points out that the 32.768KHz external
crystal is not enabled at power up. Instead the CPU falls back to using
an emulation for the 32KHz clock which is SYSCLK1/610. SYSCLK1 is usually
20MHz on boards so far (which gives an emulated frequency of 32.786KHz),
but can also be 19.2 or 27MHz which result in much larger drift.
Since this is used to drive the master counter at 32.768KHz * 375 /
2 = 6.144MHz, the emulated speed for 20MHz is of by 570ppm, or about 43
seconds per day, and more than the 500ppm NTP is able to tolerate.
Checking the CTRL_CORE_BOOTSTRAP register can determine if the CPU
is using the real 32.768KHz crystal or the emulated SYSCLK1/610, and
by known that the real counter frequency can be determined and used.
The real speed is then SYSCLK1 / 610 * 375 / 2 or SYSCLK1 * 75 / 244.
Signed-off-by: Len Sorensen <lsorense@csclub.uwaterloo.ca>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
crystal is not enabled at power up. Instead the CPU falls back to using
an emulation for the 32KHz clock which is SYSCLK1/610. SYSCLK1 is usually
20MHz on boards so far (which gives an emulated frequency of 32.786KHz),
but can also be 19.2 or 27MHz which result in much larger drift.
Since this is used to drive the master counter at 32.768KHz * 375 /
2 = 6.144MHz, the emulated speed for 20MHz is of by 570ppm, or about 43
seconds per day, and more than the 500ppm NTP is able to tolerate.
Checking the CTRL_CORE_BOOTSTRAP register can determine if the CPU
is using the real 32.768KHz crystal or the emulated SYSCLK1/610, and
by known that the real counter frequency can be determined and used.
The real speed is then SYSCLK1 / 610 * 375 / 2 or SYSCLK1 * 75 / 244.
Signed-off-by: Len Sorensen <lsorense@csclub.uwaterloo.ca>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
arch/arm/mach-omap2/control.h | patch | blob | history | |
arch/arm/mach-omap2/timer.c | patch | blob | history |
index 405979e4d379436c70cfd072d2c65aff9efb0186..7bd7d91ec24e802198f063b6da7d89df10dcd643 100644 (file)
#define OMAP5XXX_CONTROL_STATUS 0x134
#define OMAP5_DEVICETYPE_MASK (0x7 << 6)
+/* DRA7XX CONTROL CORE BOOTSTRAP */
+#define DRA7_CTRL_CORE_BOOTSTRAP 0x6c4
+#define DRA7_SPEEDSELECT_MASK (0x3 << 8)
+
/*
* REVISIT: This list of registers is not comprehensive - there are more
* that should be added.
index c65ed137ad5b3940c3fcd4af004b72aa3a6d472b..84d0dc9e13a942be7c709f19ad8847696bc3948f 100644 (file)
#include "soc.h"
#include "common.h"
+#include "control.h"
#include "powerdomain.h"
#include "omap-secure.h"
void __iomem *base;
static struct clk *sys_clk;
unsigned long rate;
- unsigned int reg, num, den;
+ unsigned int reg;
+ unsigned long long num, den;
base = ioremap(REALTIME_COUNTER_BASE, SZ_32);
if (!base) {
}
rate = clk_get_rate(sys_clk);
+
+ if (soc_is_dra7xx()) {
+ /*
+ * Errata i856 says the 32.768KHz crystal does not start at
+ * power on, so the CPU falls back to an emulated 32KHz clock
+ * based on sysclk / 610 instead. This causes the master counter
+ * frequency to not be 6.144MHz but at sysclk / 610 * 375 / 2
+ * (OR sysclk * 75 / 244)
+ *
+ * This affects at least the DRA7/AM572x 1.0, 1.1 revisions.
+ * Of course any board built without a populated 32.768KHz
+ * crystal would also need this fix even if the CPU is fixed
+ * later.
+ *
+ * Either case can be detected by using the two speedselect bits
+ * If they are not 0, then the 32.768KHz clock driving the
+ * coarse counter that corrects the fine counter every time it
+ * ticks is actually rate/610 rather than 32.768KHz and we
+ * should compensate to avoid the 570ppm (at 20MHz, much worse
+ * at other rates) too fast system time.
+ */
+ reg = omap_ctrl_readl(DRA7_CTRL_CORE_BOOTSTRAP);
+ if (reg & DRA7_SPEEDSELECT_MASK) {
+ num = 75;
+ den = 244;
+ goto sysclk1_based;
+ }
+ }
+
/* Numerator/denumerator values refer TRM Realtime Counter section */
switch (rate) {
case 12000000:
break;
}
+sysclk1_based:
/* Program numerator and denumerator registers */
reg = __raw_readl(base + INCREMENTER_NUMERATOR_OFFSET) &
NUMERATOR_DENUMERATOR_MASK;
reg |= den;
__raw_writel(reg, base + INCREMENTER_DENUMERATOR_RELOAD_OFFSET);
- arch_timer_freq = (rate / den) * num;
+ arch_timer_freq = DIV_ROUND_UP_ULL(rate * num, den);
set_cntfreq();
iounmap(base);