summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 7e7f9ef)
raw | patch | inline | side by side (parent: 7e7f9ef)
author | Chris Metcalf <cmetcalf@ezchip.com> | |
Thu, 25 Jun 2015 22:02:08 +0000 (15:02 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Mon, 3 Aug 2015 16:29:58 +0000 (09:29 -0700) |
commit 2528a8b8f457d7432552d0e2b6f0f4046bb702f4 upstream.
bitmap_parselist("", &mask, nmaskbits) will erroneously set bit zero in
the mask. The same bug is visible in cpumask_parselist() since it is
layered on top of the bitmask code, e.g. if you boot with "isolcpus=",
you will actually end up with cpu zero isolated.
The bug was introduced in commit 4b060420a596 ("bitmap, irq: add
smp_affinity_list interface to /proc/irq") when bitmap_parselist() was
generalized to support userspace as well as kernelspace.
Fixes: 4b060420a596 ("bitmap, irq: add smp_affinity_list interface to /proc/irq")
Signed-off-by: Chris Metcalf <cmetcalf@ezchip.com>
Cc: Rasmus Villemoes <linux@rasmusvillemoes.dk>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
bitmap_parselist("", &mask, nmaskbits) will erroneously set bit zero in
the mask. The same bug is visible in cpumask_parselist() since it is
layered on top of the bitmask code, e.g. if you boot with "isolcpus=",
you will actually end up with cpu zero isolated.
The bug was introduced in commit 4b060420a596 ("bitmap, irq: add
smp_affinity_list interface to /proc/irq") when bitmap_parselist() was
generalized to support userspace as well as kernelspace.
Fixes: 4b060420a596 ("bitmap, irq: add smp_affinity_list interface to /proc/irq")
Signed-off-by: Chris Metcalf <cmetcalf@ezchip.com>
Cc: Rasmus Villemoes <linux@rasmusvillemoes.dk>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
lib/bitmap.c | patch | blob | history |
diff --git a/lib/bitmap.c b/lib/bitmap.c
index e5c4ebe586babfa20ff91f646df8a4009bc98076..c0634aa923a6d6a7db26b3a4ead37a780550f54e 100644 (file)
--- a/lib/bitmap.c
+++ b/lib/bitmap.c
unsigned a, b;
int c, old_c, totaldigits;
const char __user __force *ubuf = (const char __user __force *)buf;
- int exp_digit, in_range;
+ int at_start, in_range;
totaldigits = c = 0;
bitmap_zero(maskp, nmaskbits);
do {
- exp_digit = 1;
+ at_start = 1;
in_range = 0;
a = b = 0;
break;
if (c == '-') {
- if (exp_digit || in_range)
+ if (at_start || in_range)
return -EINVAL;
b = 0;
in_range = 1;
- exp_digit = 1;
continue;
}
b = b * 10 + (c - '0');
if (!in_range)
a = b;
- exp_digit = 0;
+ at_start = 0;
totaldigits++;
}
if (!(a <= b))
return -EINVAL;
if (b >= nmaskbits)
return -ERANGE;
- while (a <= b) {
- set_bit(a, maskp);
- a++;
+ if (!at_start) {
+ while (a <= b) {
+ set_bit(a, maskp);
+ a++;
+ }
}
} while (buflen && c == ',');
return 0;