summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: e2c9950)
raw | patch | inline | side by side (parent: e2c9950)
author | Steven Rostedt (Red Hat) <rostedt@goodmis.org> | |
Tue, 12 Mar 2013 15:32:32 +0000 (11:32 -0400) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 28 Mar 2013 19:17:45 +0000 (12:17 -0700) |
commit 2721e72dd10f71a3ba90f59781becf02638aa0d9 upstream.
Although the swap is wrapped with a spin_lock, the assignment
of the temp buffer used to swap is not within that lock.
It needs to be moved into that lock, otherwise two swaps
happening on two different CPUs, can end up using the wrong
temp buffer to assign in the swap.
Luckily, all current callers of the swap function appear to have
their own locks. But in case something is added that allows two
different callers to call the swap, then there's a chance that
this race can trigger and corrupt the buffers.
New code is coming soon that will allow for this race to trigger.
I've Cc'd stable, so this bug will not show up if someone backports
one of the changes that can trigger this bug.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Although the swap is wrapped with a spin_lock, the assignment
of the temp buffer used to swap is not within that lock.
It needs to be moved into that lock, otherwise two swaps
happening on two different CPUs, can end up using the wrong
temp buffer to assign in the swap.
Luckily, all current callers of the swap function appear to have
their own locks. But in case something is added that allows two
different callers to call the swap, then there's a chance that
this race can trigger and corrupt the buffers.
New code is coming soon that will allow for this race to trigger.
I've Cc'd stable, so this bug will not show up if someone backports
one of the changes that can trigger this bug.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
kernel/trace/trace.c | patch | blob | history |
diff --git a/kernel/trace/trace.c b/kernel/trace/trace.c
index 3c13e46d7d24e1ecbdeb532f6538354f6eca7ddf..30d9b71d5256421ddb39cf563fba09a44c54060c 100644 (file)
--- a/kernel/trace/trace.c
+++ b/kernel/trace/trace.c
void
update_max_tr(struct trace_array *tr, struct task_struct *tsk, int cpu)
{
- struct ring_buffer *buf = tr->buffer;
+ struct ring_buffer *buf;
if (trace_stop_count)
return;
}
arch_spin_lock(&ftrace_max_lock);
+ buf = tr->buffer;
tr->buffer = max_tr.buffer;
max_tr.buffer = buf;