]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commitdiff
Merge tag 'iommu-updates-v3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/joro...
authorLinus Torvalds <torvalds@linux-foundation.org>
Thu, 20 Dec 2012 18:07:25 +0000 (10:07 -0800)
committerLinus Torvalds <torvalds@linux-foundation.org>
Thu, 20 Dec 2012 18:07:25 +0000 (10:07 -0800)
Pull IOMMU updates from Joerg Roedel:
 "A few new features this merge-window.  The most important one is
  probably, that dma-debug now warns if a dma-handle is not checked with
  dma_mapping_error by the device driver.  This requires minor changes
  to some architectures which make use of dma-debug.  Most of these
  changes have the respective Acks by the Arch-Maintainers.

  Besides that there are updates to the AMD IOMMU driver for refactor
  the IOMMU-Groups support and to make sure it does not trigger a
  hardware erratum.

  The OMAP changes (for which I pulled in a branch from Tony Lindgren's
  tree) have a conflict in linux-next with the arm-soc tree.  The
  conflict is in the file arch/arm/mach-omap2/clock44xx_data.c which is
  deleted in the arm-soc tree.  It is safe to delete the file too so
  solve the conflict.  Similar changes are done in the arm-soc tree in
  the common clock framework migration.  A missing hunk from the patch
  in the IOMMU tree will be submitted as a seperate patch when the
  merge-window is closed."

* tag 'iommu-updates-v3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/joro/iommu: (29 commits)
  ARM: dma-mapping: support debug_dma_mapping_error
  ARM: OMAP4: hwmod data: ipu and dsp to use parent clocks instead of leaf clocks
  iommu/omap: Adapt to runtime pm
  iommu/omap: Migrate to hwmod framework
  iommu/omap: Keep mmu enabled when requested
  iommu/omap: Remove redundant clock handling on ISR
  iommu/amd: Remove obsolete comment
  iommu/amd: Don't use 512GB pages
  iommu/tegra: smmu: Move bus_set_iommu after probe for multi arch
  iommu/tegra: gart: Move bus_set_iommu after probe for multi arch
  iommu/tegra: smmu: Remove unnecessary PTC/TLB flush all
  tile: dma_debug: add debug_dma_mapping_error support
  sh: dma_debug: add debug_dma_mapping_error support
  powerpc: dma_debug: add debug_dma_mapping_error support
  mips: dma_debug: add debug_dma_mapping_error support
  microblaze: dma-mapping: support debug_dma_mapping_error
  ia64: dma_debug: add debug_dma_mapping_error support
  c6x: dma_debug: add debug_dma_mapping_error support
  ARM64: dma_debug: add debug_dma_mapping_error support
  intel-iommu: Prevent devices with RMRRs from being placed into SI Domain
  ...

1  2 
arch/arm/include/asm/dma-mapping.h
arch/arm/mach-omap2/devices.c
arch/arm/mach-omap2/omap_hwmod_44xx_data.c
drivers/iommu/intel-iommu.c
drivers/iommu/tegra-smmu.c

Simple merge
Simple merge
Simple merge
Simple merge