summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 412d32e)
raw | patch | inline | side by side (parent: 412d32e)
author | Tejun Heo <tj@kernel.org> | |
Sun, 2 Dec 2012 00:23:42 +0000 (16:23 -0800) | ||
committer | Tejun Heo <tj@kernel.org> | |
Sun, 2 Dec 2012 00:43:18 +0000 (16:43 -0800) |
8376fe22c7 ("workqueue: implement mod_delayed_work[_on]()")
implemented mod_delayed_work[_on]() using the improved
try_to_grab_pending(). The function is later used, among others, to
replace [__]candel_delayed_work() + queue_delayed_work() combinations.
Unfortunately, a delayed_work item w/ zero @delay is handled slightly
differently by mod_delayed_work_on() compared to
queue_delayed_work_on(). The latter skips timer altogether and
directly queues it using queue_work_on() while the former schedules
timer which will expire on the closest tick. This means, when @delay
is zero, that [__]cancel_delayed_work() + queue_delayed_work_on()
makes the target item immediately executable while
mod_delayed_work_on() may induce delay of upto a full tick.
This somewhat subtle difference breaks some of the converted users.
e.g. block queue plugging uses delayed_work for deferred processing
and uses mod_delayed_work_on() when the queue needs to be immediately
unplugged. The above problem manifested as noticeably higher number
of context switches under certain circumstances.
The difference in behavior was caused by missing special case handling
for 0 delay in mod_delayed_work_on() compared to
queue_delayed_work_on(). Joonsoo Kim posted a patch to add it -
("workqueue: optimize mod_delayed_work_on() when @delay == 0")[1].
The patch was queued for 3.8 but it was described as optimization and
I missed that it was a correctness issue.
As both queue_delayed_work_on() and mod_delayed_work_on() use
__queue_delayed_work() for queueing, it seems that the better approach
is to move the 0 delay special handling to the function instead of
duplicating it in mod_delayed_work_on().
Fix the problem by moving 0 delay special case handling from
queue_delayed_work_on() to __queue_delayed_work(). This replaces
Joonsoo's patch.
[1] http://thread.gmane.org/gmane.linux.kernel/1379011/focus=1379012
Signed-off-by: Tejun Heo <tj@kernel.org>
Reported-and-tested-by: Anders Kaseorg <andersk@MIT.EDU>
Reported-and-tested-by: Zlatko Calusic <zlatko.calusic@iskon.hr>
LKML-Reference: <alpine.DEB.2.00.1211280953350.26602@dr-wily.mit.edu>
LKML-Reference: <50A78AA9.5040904@iskon.hr>
Cc: Joonsoo Kim <js1304@gmail.com>
implemented mod_delayed_work[_on]() using the improved
try_to_grab_pending(). The function is later used, among others, to
replace [__]candel_delayed_work() + queue_delayed_work() combinations.
Unfortunately, a delayed_work item w/ zero @delay is handled slightly
differently by mod_delayed_work_on() compared to
queue_delayed_work_on(). The latter skips timer altogether and
directly queues it using queue_work_on() while the former schedules
timer which will expire on the closest tick. This means, when @delay
is zero, that [__]cancel_delayed_work() + queue_delayed_work_on()
makes the target item immediately executable while
mod_delayed_work_on() may induce delay of upto a full tick.
This somewhat subtle difference breaks some of the converted users.
e.g. block queue plugging uses delayed_work for deferred processing
and uses mod_delayed_work_on() when the queue needs to be immediately
unplugged. The above problem manifested as noticeably higher number
of context switches under certain circumstances.
The difference in behavior was caused by missing special case handling
for 0 delay in mod_delayed_work_on() compared to
queue_delayed_work_on(). Joonsoo Kim posted a patch to add it -
("workqueue: optimize mod_delayed_work_on() when @delay == 0")[1].
The patch was queued for 3.8 but it was described as optimization and
I missed that it was a correctness issue.
As both queue_delayed_work_on() and mod_delayed_work_on() use
__queue_delayed_work() for queueing, it seems that the better approach
is to move the 0 delay special handling to the function instead of
duplicating it in mod_delayed_work_on().
Fix the problem by moving 0 delay special case handling from
queue_delayed_work_on() to __queue_delayed_work(). This replaces
Joonsoo's patch.
[1] http://thread.gmane.org/gmane.linux.kernel/1379011/focus=1379012
Signed-off-by: Tejun Heo <tj@kernel.org>
Reported-and-tested-by: Anders Kaseorg <andersk@MIT.EDU>
Reported-and-tested-by: Zlatko Calusic <zlatko.calusic@iskon.hr>
LKML-Reference: <alpine.DEB.2.00.1211280953350.26602@dr-wily.mit.edu>
LKML-Reference: <50A78AA9.5040904@iskon.hr>
Cc: Joonsoo Kim <js1304@gmail.com>
kernel/workqueue.c | patch | blob | history |
diff --git a/kernel/workqueue.c b/kernel/workqueue.c
index ac25db111f4828d2674f15205c1bb513556c6668..084aa47bac820498f932ae6ff54158414e48e889 100644 (file)
--- a/kernel/workqueue.c
+++ b/kernel/workqueue.c
BUG_ON(timer_pending(timer));
BUG_ON(!list_empty(&work->entry));
+ /*
+ * If @delay is 0, queue @dwork->work immediately. This is for
+ * both optimization and correctness. The earliest @timer can
+ * expire is on the closest next tick and delayed_work users depend
+ * on that there's no such delay when @delay is 0.
+ */
+ if (!delay) {
+ __queue_work(cpu, wq, &dwork->work);
+ return;
+ }
+
timer_stats_timer_set_start_info(&dwork->timer);
/*
bool ret = false;
unsigned long flags;
- if (!delay)
- return queue_work_on(cpu, wq, &dwork->work);
-
/* read the comment in __queue_work() */
local_irq_save(flags);