]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commitdiff
Merge branch 'wireless'
authorDavid S. Miller <davem@davemloft.net>
Fri, 1 Feb 2013 19:50:16 +0000 (14:50 -0500)
committerDavid S. Miller <davem@davemloft.net>
Fri, 1 Feb 2013 19:50:16 +0000 (14:50 -0500)
John W. Linville says:

====================
This is a small batch of fixes intended for the 3.8 stream...

There are two pulls from Johannes.  Regarding mac80211, Johannes says:

"One fix from Dan for a possible memory overrun."

Regarding iwlwifi,  Johannes says:

"I have one fix from Emmanuel reverting a previous fix that caused
more trouble than it's worth."

Along with those:

Arend van Spriel fixes a fatal error in brcsmac related to tx status processing.

Bing Zhao corrects a problem where mwifiex would fail to complete a scan
in the event of an IE processing error.

Larry Finger fixes a thinko in rtlwifi in which the wrong skb variable
was being used in some cases.

Rafał Miłecki fixes a thinko in an ID check in the bcma flash code.
====================

Signed-off-by: David S. Miller <davem@davemloft.net>

Trivial merge