summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b694514)
raw | patch | inline | side by side (parent: b694514)
author | Archit Taneja <archit@ti.com> | |
Tue, 16 Apr 2013 10:14:37 +0000 (15:44 +0530) | ||
committer | Archit Taneja <archit@ti.com> | |
Thu, 30 May 2013 14:34:15 +0000 (20:04 +0530) |
TFCS9700 is a 800x480 DPI LCD panel found on the Vayu display daughter card.
The card also contains an i2c brightness controller/gpio expander(TLCxxxx) which
drives a pwm signal for the panel and also provides some gpios to configure some
of the panel pins.
Add the DPI panel driver as an omapdss driver, and add the i2c controller as a
client driver in the same file for now. In the longer run, we would have a
separate mfd driver for the TLC chip.
Signed-off-by: Archit Taneja <archit@ti.com>
The card also contains an i2c brightness controller/gpio expander(TLCxxxx) which
drives a pwm signal for the panel and also provides some gpios to configure some
of the panel pins.
Add the DPI panel driver as an omapdss driver, and add the i2c controller as a
client driver in the same file for now. In the longer run, we would have a
separate mfd driver for the TLC chip.
Signed-off-by: Archit Taneja <archit@ti.com>
drivers/video/omap2/displays/Kconfig | patch | blob | history | |
drivers/video/omap2/displays/Makefile | patch | blob | history | |
drivers/video/omap2/displays/panel-tfcs9700.c | [new file with mode: 0644] | patch | blob |
include/video/omap-panel-tfcs9700.h | [new file with mode: 0644] | patch | blob |
index 2535345b7cd3a2835eff85ff5f76d1fd0f93bb5f..0f480fa17c6481ba6d2e7a6e0c7ac43960612c03 100644 (file)
A mini-projector used in TI's SDP4430 and EVM boards
For more info please visit http://www.dlp.com/projector/
A mini-projector used in TI's SDP4430 and EVM boards
For more info please visit http://www.dlp.com/projector/
+config PANEL_TFCS9700
+ tristate "Three Five DPI panel"
+ depends on OMAP2_DSS_DPI && I2C
+ help
+ A TFT LCD DPI panel used on the LCD daughter board of Vayu EVM
+
config PANEL_TAAL
tristate "Taal DSI Panel"
depends on OMAP2_DSS_DSI
config PANEL_TAAL
tristate "Taal DSI Panel"
depends on OMAP2_DSS_DSI
index f866c6024c7a731f92bd05b4acdecd7918dd44c5..bb27e88844abe9b3cd59a1127eac02f6217c63c9 100644 (file)
obj-$(CONFIG_PANEL_NEC_NL8048HL11_01B) += panel-nec-nl8048hl11-01b.o
obj-$(CONFIG_PANEL_TAAL) += panel-taal.o
obj-$(CONFIG_PANEL_NEC_NL8048HL11_01B) += panel-nec-nl8048hl11-01b.o
obj-$(CONFIG_PANEL_TAAL) += panel-taal.o
+obj-$(CONFIG_PANEL_TFCS9700) += panel-tfcs9700.o
+
obj-$(CONFIG_PANEL_LG4591) += panel-lg4591.o
obj-$(CONFIG_PANEL_PICODLP) += panel-picodlp.o
obj-$(CONFIG_PANEL_TPO_TD043MTEA1) += panel-tpo-td043mtea1.o
obj-$(CONFIG_PANEL_LG4591) += panel-lg4591.o
obj-$(CONFIG_PANEL_PICODLP) += panel-picodlp.o
obj-$(CONFIG_PANEL_TPO_TD043MTEA1) += panel-tpo-td043mtea1.o
diff --git a/drivers/video/omap2/displays/panel-tfcs9700.c b/drivers/video/omap2/displays/panel-tfcs9700.c
--- /dev/null
@@ -0,0 +1,471 @@
+/*
+ * Copyright (C) 2013 Texas Instruments Inc
+ *
+ * This program is free software; you can redistribute it and/or modify it
+ * under the terms of the GNU General Public License version 2 as published by
+ * the Free Software Foundation.
+ *
+ * This program is distributed in the hope that it will be useful, but WITHOUT
+ * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
+ * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for
+ * more details.
+ *
+ * You should have received a copy of the GNU General Public License along with
+ * this program. If not, see <http://www.gnu.org/licenses/>.
+ */
+
+#include <linux/module.h>
+#include <linux/slab.h>
+#include <linux/delay.h>
+#include <linux/err.h>
+#include <linux/i2c.h>
+#include <linux/gpio.h>
+#include <linux/of_gpio.h>
+#include <linux/of_i2c.h>
+#include <linux/of.h>
+#include <linux/regmap.h>
+
+#include <video/omapdss.h>
+#include <video/omap-panel-tfcs9700.h>
+
+#define TLC_NAME "tlc59108"
+#define TLC_I2C_ADDR 0x40
+
+#define TLC59108_MODE1 0x00
+#define TLC59108_PWM2 0x04
+#define TLC59108_LEDOUT0 0x0c
+#define TLC59108_LEDOUT1 0x0d
+
+struct tlc_data {
+ struct device *dev;
+ struct regmap *regmap;
+ int p_gpio;
+};
+
+static const struct omap_video_timings tfc_s9700_default_timings = {
+ .x_res = 800,
+ .y_res = 480,
+
+ .pixel_clock = 29232,
+
+ .hfp = 41,
+ .hsw = 49,
+ .hbp = 41,
+
+ .vfp = 13,
+ .vsw = 4,
+ .vbp = 29,
+
+ .vsync_level = OMAPDSS_SIG_ACTIVE_LOW,
+ .hsync_level = OMAPDSS_SIG_ACTIVE_LOW,
+ .data_pclk_edge = OMAPDSS_DRIVE_SIG_RISING_EDGE,
+ .de_level = OMAPDSS_SIG_ACTIVE_HIGH,
+ .sync_pclk_edge = OMAPDSS_DRIVE_SIG_OPPOSITE_EDGES,
+};
+
+struct panel_drv_data {
+ struct omap_dss_device *dssdev;
+
+ struct i2c_client *tlc_client;
+ struct mutex lock;
+
+ int dith;
+};
+
+static int tlc_init(struct i2c_client *client)
+{
+ struct tlc_data *data = dev_get_drvdata(&client->dev);
+ struct regmap *map = data->regmap;
+
+ /* init the TLC chip */
+ regmap_write(map, TLC59108_MODE1, 0x01);
+
+ /*
+ * set LED1(AVDD) to ON state(default), enable LED2 in PWM mode, enable
+ * LED0 to OFF state
+ */
+ regmap_write(map, TLC59108_LEDOUT0, 0x21);
+
+ /* set LED2 PWM to full freq */
+ regmap_write(map, TLC59108_PWM2, 0xff);
+
+ /* set LED4(UPDN) and LED6(MODE3) to OFF state */
+ regmap_write(map, TLC59108_LEDOUT1, 0x11);
+
+ return 0;
+}
+
+static int tlc_uninit(struct i2c_client *client)
+{
+ struct tlc_data *data = dev_get_drvdata(&client->dev);
+ struct regmap *map = data->regmap;
+
+ /* clear TLC chip regs */
+ regmap_write(map, TLC59108_PWM2, 0x0);
+ regmap_write(map, TLC59108_LEDOUT0, 0x0);
+ regmap_write(map, TLC59108_LEDOUT1, 0x0);
+
+ regmap_write(map, TLC59108_MODE1, 0x0);
+
+ return 0;
+}
+
+static int tfc_s9700_power_on(struct omap_dss_device *dssdev)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+ int r;
+
+ if (dssdev->state == OMAP_DSS_DISPLAY_ACTIVE)
+ return 0;
+
+ omapdss_dpi_set_timings(dssdev, &dssdev->panel.timings);
+ omapdss_dpi_set_data_lines(dssdev, dssdev->phy.dpi.data_lines);
+
+ r = omapdss_dpi_display_enable(dssdev);
+ if (r)
+ goto err0;
+
+ tlc_init(ddata->tlc_client);
+
+ return 0;
+err0:
+ return r;
+}
+
+static void tfc_s9700_power_off(struct omap_dss_device *dssdev)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+
+ if (dssdev->state != OMAP_DSS_DISPLAY_ACTIVE)
+ return;
+
+ tlc_uninit(ddata->tlc_client);
+
+ omapdss_dpi_display_disable(dssdev);
+}
+
+static int tfc_s9700_probe_of(struct omap_dss_device *dssdev,
+ struct panel_drv_data *ddata)
+{
+ struct device_node *node = dssdev->dev.of_node;
+ struct device_node *tlc;
+ struct i2c_client *client;
+ int r, datalines;
+
+ r = of_property_read_u32(node, "data-lines", &datalines);
+ if (r) {
+ dev_err(&dssdev->dev, "failed to parse datalines");
+ return r;
+ }
+
+ tlc = of_parse_phandle(node, "tlc", 0);
+ if (!tlc) {
+ dev_err(&dssdev->dev, "could not find tlc device\n");
+ return -EINVAL;
+ }
+
+ client = of_find_i2c_device_by_node(tlc);
+ if (!client) {
+ dev_err(&dssdev->dev, "failed to find tlc i2c client device\n");
+ return -EINVAL;
+ }
+
+ ddata->tlc_client = client;
+
+ dssdev->phy.dpi.data_lines = datalines;
+
+ return 0;
+}
+
+static struct i2c_board_info tlc_i2c_board_info = {
+ I2C_BOARD_INFO(TLC_NAME, TLC_I2C_ADDR),
+};
+
+static int tfc_s9700_probe(struct omap_dss_device *dssdev)
+{
+ struct panel_drv_data *ddata;
+ int r;
+
+ ddata = devm_kzalloc(&dssdev->dev, sizeof(*ddata), GFP_KERNEL);
+ if (!ddata)
+ return -ENOMEM;
+
+ dssdev->panel.timings = tfc_s9700_default_timings;
+
+ ddata->dssdev = dssdev;
+ mutex_init(&ddata->lock);
+
+ if (dssdev->dev.of_node) {
+ r = tfc_s9700_probe_of(dssdev, ddata);
+ if (r)
+ return r;
+ } else if (dssdev->data) {
+ struct tfc_s9700_platform_data *pdata = dssdev->data;
+ struct i2c_client *client;
+ struct i2c_adapter *adapter;
+ int tlc_adapter_id;
+
+ dssdev->phy.dpi.data_lines = pdata->datalines;
+
+ tlc_adapter_id = pdata->tlc_adapter_id;
+
+ adapter = i2c_get_adapter(tlc_adapter_id);
+ if (!adapter) {
+ dev_err(&dssdev->dev, "can't get i2c adapter\n");
+ return -ENODEV;
+ }
+
+ client = i2c_new_device(adapter, &tlc_i2c_board_info);
+ if (!client) {
+ dev_err(&dssdev->dev, "can't add i2c device\n");
+ return -ENODEV;
+ }
+
+ ddata->tlc_client = client;
+ } else {
+ return -EINVAL;
+ }
+
+
+ if (dssdev->phy.dpi.data_lines == 24)
+ ddata->dith = 0;
+ else if (dssdev->phy.dpi.data_lines == 18)
+ ddata->dith = 1;
+ else
+ return -EINVAL;
+
+ dev_set_drvdata(&dssdev->dev, ddata);
+
+ return 0;
+}
+
+static void __exit tfc_s9700_remove(struct omap_dss_device *dssdev)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+
+ mutex_lock(&ddata->lock);
+
+ dev_set_drvdata(&dssdev->dev, NULL);
+
+ mutex_unlock(&ddata->lock);
+}
+
+static int tfc_s9700_enable(struct omap_dss_device *dssdev)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+ int r;
+
+ mutex_lock(&ddata->lock);
+
+ r = tfc_s9700_power_on(dssdev);
+ if (r == 0)
+ dssdev->state = OMAP_DSS_DISPLAY_ACTIVE;
+
+ mutex_unlock(&ddata->lock);
+
+ return r;
+}
+
+static void tfc_s9700_disable(struct omap_dss_device *dssdev)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+
+ mutex_lock(&ddata->lock);
+
+ tfc_s9700_power_off(dssdev);
+
+ dssdev->state = OMAP_DSS_DISPLAY_DISABLED;
+
+ mutex_unlock(&ddata->lock);
+}
+
+static void tfc_s9700_set_timings(struct omap_dss_device *dssdev,
+ struct omap_video_timings *timings)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+
+ mutex_lock(&ddata->lock);
+ omapdss_dpi_set_timings(dssdev, timings);
+ dssdev->panel.timings = *timings;
+ mutex_unlock(&ddata->lock);
+}
+
+static void tfc_s9700_get_timings(struct omap_dss_device *dssdev,
+ struct omap_video_timings *timings)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+
+ mutex_lock(&ddata->lock);
+ *timings = dssdev->panel.timings;
+ mutex_unlock(&ddata->lock);
+}
+
+static int tfc_s9700_check_timings(struct omap_dss_device *dssdev,
+ struct omap_video_timings *timings)
+{
+ struct panel_drv_data *ddata = dev_get_drvdata(&dssdev->dev);
+ int r;
+
+ mutex_lock(&ddata->lock);
+ r = dpi_check_timings(dssdev, timings);
+ mutex_unlock(&ddata->lock);
+
+ return r;
+}
+
+#if defined(CONFIG_OF)
+static const struct of_device_id tfc_s9700_of_match[] = {
+ {
+ .compatible = "ti,tfc_s9700",
+ },
+ {},
+};
+
+MODULE_DEVICE_TABLE(of, tfc_s9700_of_match);
+#else
+#define dss_of_match NULL
+#endif
+
+static struct omap_dss_driver tfc_s9700_driver = {
+ .probe = tfc_s9700_probe,
+ .remove = __exit_p(tfc_s9700_remove),
+
+ .enable = tfc_s9700_enable,
+ .disable = tfc_s9700_disable,
+
+ .set_timings = tfc_s9700_set_timings,
+ .get_timings = tfc_s9700_get_timings,
+ .check_timings = tfc_s9700_check_timings,
+
+ .driver = {
+ .name = "tfc_s9700",
+ .owner = THIS_MODULE,
+ .of_match_table = tfc_s9700_of_match,
+ },
+};
+
+struct regmap_config tlc59108_regmap_config = {
+ .reg_bits = 8,
+ .val_bits = 8,
+};
+
+static int tlc59108_i2c_probe(struct i2c_client *client,
+ const struct i2c_device_id *id)
+{
+ int r;
+ struct regmap *regmap;
+ struct tlc_data *data;
+ struct device *dev = &client->dev;
+ struct device_node *node = dev->of_node;
+ unsigned int val;
+ int gpio;
+
+ regmap = devm_regmap_init_i2c(client, &tlc59108_regmap_config);
+ if (IS_ERR(regmap)) {
+ r = PTR_ERR(regmap);
+ dev_err(&client->dev, "Failed to init regmap: %d\n", r);
+ return r;
+ }
+
+ data = devm_kzalloc(dev, sizeof(struct tlc_data), GFP_KERNEL);
+ if (!data)
+ return -ENOMEM;
+
+ gpio = of_get_gpio(node, 0);
+
+ if (gpio_is_valid(gpio)) {
+ data->p_gpio = gpio;
+ } else if (gpio == -ENOENT) {
+ data->p_gpio = -1;
+ } else {
+ dev_err(dev, "failed to parse Power gpio\n");
+ return gpio;
+ }
+
+ if (gpio_is_valid(data->p_gpio)) {
+ r = devm_gpio_request_one(dev, data->p_gpio, GPIOF_OUT_INIT_LOW,
+ "tfc_s9700 p_gpio");
+ if (r) {
+ dev_err(dev, "Failed to request Power GPIO %d\n",
+ data->p_gpio);
+ return r;
+ }
+ }
+
+ dev_set_drvdata(dev, data);
+ data->dev = dev;
+ data->regmap = regmap;
+
+ msleep(10);
+
+ /* Try to read a TLC register to verify if i2c works */
+ r = regmap_read(data->regmap, TLC59108_MODE1, &val);
+ if (r < 0) {
+ dev_err(dev, "Failed to set MODE1: %d\n", r);
+ return r;
+ }
+
+ dev_info(dev, "Successfully initialized %s\n", TLC_NAME);
+
+ return 0;
+}
+
+static int tlc59108_i2c_remove(struct i2c_client *client)
+{
+ struct tlc_data *data = dev_get_drvdata(&client->dev);
+
+ if (gpio_is_valid(data->p_gpio))
+ gpio_set_value_cansleep(data->p_gpio, 1);
+
+ return 0;
+}
+
+static const struct i2c_device_id tlc59108_id[] = {
+ { TLC_NAME, 0 },
+ { }
+};
+MODULE_DEVICE_TABLE(i2c, tlc59108_id);
+
+static const struct of_device_id tlc59108_of_match[] = {
+ { .compatible = "ti,tlc59108", },
+ { },
+};
+MODULE_DEVICE_TABLE(of, tlc59108_of_match);
+
+static struct i2c_driver tlc59108_i2c_driver = {
+ .driver = {
+ .owner = THIS_MODULE,
+ .name = TLC_NAME,
+ .of_match_table = tlc59108_of_match,
+ },
+ .id_table = tlc59108_id,
+ .probe = tlc59108_i2c_probe,
+ .remove = tlc59108_i2c_remove,
+};
+
+static int __init tfc_s9700_init(void)
+{
+ int r;
+
+ r = i2c_add_driver(&tlc59108_i2c_driver);
+ if (r) {
+ printk(KERN_WARNING "tlc59108 driver" \
+ " registration failed\n");
+ return r;
+ }
+
+ r = omap_dss_register_driver(&tfc_s9700_driver);
+ if (r)
+ i2c_del_driver(&tlc59108_i2c_driver);
+
+ return r;
+}
+
+static void __exit tfc_s9700_exit(void)
+{
+ omap_dss_unregister_driver(&tfc_s9700_driver);
+}
+
+module_init(tfc_s9700_init);
+module_exit(tfc_s9700_exit);
+MODULE_LICENSE("GPL");
diff --git a/include/video/omap-panel-tfcs9700.h b/include/video/omap-panel-tfcs9700.h
--- /dev/null
@@ -0,0 +1,11 @@
+#ifndef __PANEL_TFCS9700_H
+#define __PANEL_TFCS9700_H
+/**
+ * struct : tfc s9700 panel data
+ */
+struct tfc_s9700_platform_data {
+ int p_gpio;
+ int datalines;
+ int tlc_adapter_id;
+};
+#endif /* __PANEL_PICODLP_H */