summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: b666263)
raw | patch | inline | side by side (from parent 1: b666263)
author | Chris Bagwell <chris@cnpbagwell.com> | |
Thu, 24 Jan 2013 03:37:34 +0000 (19:37 -0800) | ||
committer | Dmitry Torokhov <dmitry.torokhov@gmail.com> | |
Thu, 24 Jan 2013 03:38:52 +0000 (19:38 -0800) |
Logic sets a value and then reads it back to make sure it worked
and retries write on failures. Since read and write share a buffer,
it needs to be set back up before writing though.
Issue is not seen a lot because 1) it doesn't need to retry for
a lot of tablets and 2) a lot of failures that need a retry are
from an -ETIMEDOUT and hopefully buffer is not touched in this case.
At least one user has shown logs with buffer being modified during
-ETIMEDOUT case with linux 3.7 kernel.
Signed-off-by: Chris Bagwell <chris@cnpbagwell.com>
Signed-off-by: Dmitry Torokhov <dmitry.torokhov@gmail.com>
and retries write on failures. Since read and write share a buffer,
it needs to be set back up before writing though.
Issue is not seen a lot because 1) it doesn't need to retry for
a lot of tablets and 2) a lot of failures that need a retry are
from an -ETIMEDOUT and hopefully buffer is not touched in this case.
At least one user has shown logs with buffer being modified during
-ETIMEDOUT case with linux 3.7 kernel.
Signed-off-by: Chris Bagwell <chris@cnpbagwell.com>
Signed-off-by: Dmitry Torokhov <dmitry.torokhov@gmail.com>
drivers/input/tablet/wacom_sys.c | patch | blob | history |
index f92d34f45a1cc6ad13af95f42440021f3bafe2bf..aaf23aeae2ea428b4a26ea0cd99f20eeac32c964 100644 (file)
@@ -553,10 +553,10 @@ static int wacom_set_device_mode(struct usb_interface *intf, int report_id, int
if (!rep_data)
return error;
- rep_data[0] = report_id;
- rep_data[1] = mode;
-
do {
+ rep_data[0] = report_id;
+ rep_data[1] = mode;
+
error = wacom_set_report(intf, WAC_HID_FEATURE_REPORT,
report_id, rep_data, length, 1);
if (error >= 0)