summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: ac3d0da)
raw | patch | inline | side by side (parent: ac3d0da)
author | Oleg Nesterov <oleg@redhat.com> | |
Sun, 26 Aug 2012 19:12:11 +0000 (21:12 +0200) | ||
committer | Ingo Molnar <mingo@kernel.org> | |
Thu, 13 Sep 2012 14:47:34 +0000 (16:47 +0200) |
ed3e694d "move exit_task_work() past exit_files() et.al" destroyed
the add/exit synchronization we had, the caller itself should ensure
task_work_add() can't race with the exiting task.
However, this is not convenient/simple, and the only user which tries
to do this is buggy (see the next patch). Unless the task is current,
there is simply no way to do this in general.
Change exit_task_work()->task_work_run() to use the dummy "work_exited"
entry to let task_work_add() know it should fail.
Signed-off-by: Oleg Nesterov <oleg@redhat.com>
Signed-off-by: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: Thomas Gleixner <tglx@linutronix.de>
Link: http://lkml.kernel.org/r/20120826191211.GA4228@redhat.com
Signed-off-by: Ingo Molnar <mingo@kernel.org>
the add/exit synchronization we had, the caller itself should ensure
task_work_add() can't race with the exiting task.
However, this is not convenient/simple, and the only user which tries
to do this is buggy (see the next patch). Unless the task is current,
there is simply no way to do this in general.
Change exit_task_work()->task_work_run() to use the dummy "work_exited"
entry to let task_work_add() know it should fail.
Signed-off-by: Oleg Nesterov <oleg@redhat.com>
Signed-off-by: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: Thomas Gleixner <tglx@linutronix.de>
Link: http://lkml.kernel.org/r/20120826191211.GA4228@redhat.com
Signed-off-by: Ingo Molnar <mingo@kernel.org>
include/linux/task_work.h | patch | blob | history | |
kernel/task_work.c | patch | blob | history |
index fb46b03b18522752538bfae6e192804e9629fc2a..ca5a1cf27daeb9487303dd29d9c58a9e571ecfb4 100644 (file)
static inline void exit_task_work(struct task_struct *task)
{
- if (unlikely(task->task_works))
- task_work_run();
+ task_work_run();
}
#endif /* _LINUX_TASK_WORK_H */
diff --git a/kernel/task_work.c b/kernel/task_work.c
index f13ec0bda1d5af70713d5d237612d120141e84dd..65bd3c92d6f3a14cf9db95f9ab7e22c368457661 100644 (file)
--- a/kernel/task_work.c
+++ b/kernel/task_work.c
#include <linux/task_work.h>
#include <linux/tracehook.h>
+static struct callback_head work_exited; /* all we need is ->next == NULL */
+
int
task_work_add(struct task_struct *task, struct callback_head *work, bool notify)
{
struct callback_head *head;
- /*
- * Not inserting the new work if the task has already passed
- * exit_task_work() is the responisbility of callers.
- */
+
do {
head = ACCESS_ONCE(task->task_works);
+ if (unlikely(head == &work_exited))
+ return -ESRCH;
work->next = head;
} while (cmpxchg(&task->task_works, head, work) != head);
* If cmpxchg() fails we continue without updating pprev.
* Either we raced with task_work_add() which added the
* new entry before this work, we will find it again. Or
- * we raced with task_work_run(), *pprev == NULL.
+ * we raced with task_work_run(), *pprev == NULL/exited.
*/
raw_spin_lock_irqsave(&task->pi_lock, flags);
while ((work = ACCESS_ONCE(*pprev))) {
struct callback_head *work, *head, *next;
for (;;) {
- work = xchg(&task->task_works, NULL);
+ /*
+ * work->func() can do task_work_add(), do not set
+ * work_exited unless the list is empty.
+ */
+ do {
+ work = ACCESS_ONCE(task->task_works);
+ head = !work && (task->flags & PF_EXITING) ?
+ &work_exited : NULL;
+ } while (cmpxchg(&task->task_works, work, head) != work);
+
if (!work)
break;
/*