summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 9d93551)
raw | patch | inline | side by side (parent: 9d93551)
author | Nishanth Menon <nm@ti.com> | |
Wed, 24 Dec 2014 17:22:57 +0000 (11:22 -0600) | ||
committer | Ravikumar Kattekola <rk@ti.com> | |
Fri, 14 Aug 2015 04:51:48 +0000 (10:21 +0530) |
kernel doc has gotten bit-rotted over time. Re-sync with Locking and
Return information. document all functions properly and ensure that
./scripts/kernel-doc -v ./drivers/base/power/opp.c >/dev/null returns
no errors
Change-Id: Ib2484b1cdec48a096ecfaec2b2a55c8175554cbd
Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Rafael J. Wysocki <rafael.j.wysocki@intel.com>
Return information. document all functions properly and ensure that
./scripts/kernel-doc -v ./drivers/base/power/opp.c >/dev/null returns
no errors
Change-Id: Ib2484b1cdec48a096ecfaec2b2a55c8175554cbd
Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Rafael J. Wysocki <rafael.j.wysocki@intel.com>
drivers/base/power/opp.c | patch | blob | history |
index d49c7e748a92edeca6278859dda2d236cbc942d9..09b5debdf915e625bd2311d48f2cc11a01c9434c 100644 (file)
--- a/drivers/base/power/opp.c
+++ b/drivers/base/power/opp.c
* Search list of device OPPs for one containing matching device. Does a RCU
* reader operation to grab the pointer needed.
*
- * Returns pointer to 'struct device_opp' if found, otherwise -ENODEV or
+ * Return: pointer to 'struct device_opp' if found, otherwise -ENODEV or
* -EINVAL based on type of error.
*
* Locking: This function must be called under rcu_read_lock(). device_opp
* dev_pm_opp_get_voltage() - Gets the voltage corresponding to an available opp
* @opp: opp for which voltage has to be returned for
*
- * Return voltage in micro volt corresponding to the opp, else
+ * Return: voltage in micro volt corresponding to the opp, else
* return 0
*
* Locking: This function must be called under rcu_read_lock(). opp is a rcu
* dev_pm_opp_get_freq() - Gets the frequency corresponding to an available opp
* @opp: opp for which frequency has to be returned for
*
- * Return frequency in hertz corresponding to the opp, else
+ * Return: frequency in hertz corresponding to the opp, else
* return 0
*
* Locking: This function must be called under rcu_read_lock(). opp is a rcu
* dev_pm_opp_get_opp_count() - Get number of opps available in the opp list
* @dev: device for which we do this operation
*
- * This function returns the number of available opps if there are any,
+ * Return: This function returns the number of available opps if there are any,
* else returns 0 if none or the corresponding error value.
*
* Locking: This function takes rcu_read_lock().
* @freq: frequency to search for
* @available: true/false - match for available opp
*
- * Searches for exact match in the opp list and returns pointer to the matching
- * opp if found, else returns ERR_PTR in case of error and should be handled
- * using IS_ERR. Error return values can be:
+ * Return: Searches for exact match in the opp list and returns pointer to the
+ * matching opp if found, else returns ERR_PTR in case of error and should
+ * be handled using IS_ERR. Error return values can be:
* EINVAL: for bad pointer
* ERANGE: no match found for search
* ENODEV: if device not found in list of registered devices
* Search for the matching ceil *available* OPP from a starting freq
* for a device.
*
- * Returns matching *opp and refreshes *freq accordingly, else returns
+ * Return: matching *opp and refreshes *freq accordingly, else returns
* ERR_PTR in case of error and should be handled using IS_ERR. Error return
* values can be:
* EINVAL: for bad pointer
* Search for the matching floor *available* OPP from a starting freq
* for a device.
*
- * Returns matching *opp and refreshes *freq accordingly, else returns
+ * Return: matching *opp and refreshes *freq accordingly, else returns
* ERR_PTR in case of error and should be handled using IS_ERR. Error return
* values can be:
* EINVAL: for bad pointer
}
EXPORT_SYMBOL_GPL(dev_pm_opp_find_freq_floor);
+/**
+ * _add_device_opp() - Allocate a new device OPP table
+ * @dev: device for which we do this operation
+ *
+ * New device node which uses OPPs - used when multiple devices with OPP tables
+ * are maintained.
+ *
+ * Return: valid device_opp pointer if success, else NULL.
+ */
static struct device_opp *_add_device_opp(struct device *dev)
{
struct device_opp *dev_opp;
return dev_opp;
}
+/**
+ * _opp_add_dynamic() - Allocate a dynamic OPP.
+ * @dev: device for which we do this operation
+ * @freq: Frequency in Hz for this OPP
+ * @u_volt: Voltage in uVolts for this OPP
+ * @dynamic: Dynamically added OPPs.
+ *
+ * This function adds an opp definition to the opp list and returns status.
+ * The opp is made available by default and it can be controlled using
+ * dev_pm_opp_enable/disable functions and may be removed by dev_pm_opp_remove.
+ *
+ * NOTE: "dynamic" parameter impacts OPPs added by the of_init_opp_table and
+ * freed by of_free_opp_table.
+ *
+ * Locking: The internal device_opp and opp structures are RCU protected.
+ * Hence this function internally uses RCU updater strategy with mutex locks
+ * to keep the integrity of the internal data structures. Callers should ensure
+ * that this function is *NOT* called under RCU protection or in contexts where
+ * mutex cannot be locked.
+ *
+ * Return:
+ * 0 On success OR
+ * Duplicate OPPs (both freq and volt are same) and opp->available
+ * -EEXIST Freq are same and volt are different OR
+ * Duplicate OPPs (both freq and volt are same) and !opp->available
+ * -ENOMEM Memory allocation failure
+ */
static int _opp_add_dynamic(struct device *dev, unsigned long freq,
long u_volt, bool dynamic)
{
* mutex cannot be locked.
*
* Return:
- * 0: On success OR
+ * 0 On success OR
* Duplicate OPPs (both freq and volt are same) and opp->available
- * -EEXIST: Freq are same and volt are different OR
+ * -EEXIST Freq are same and volt are different OR
* Duplicate OPPs (both freq and volt are same) and !opp->available
- * -ENOMEM: Memory allocation failure
+ * -ENOMEM Memory allocation failure
*/
int dev_pm_opp_add(struct device *dev, unsigned long freq, unsigned long u_volt)
{
@@ -532,6 +568,10 @@ int dev_pm_opp_add(struct device *dev, unsigned long freq, unsigned long u_volt)
}
EXPORT_SYMBOL_GPL(dev_pm_opp_add);
+/**
+ * _kfree_opp_rcu() - Free OPP RCU handler
+ * @head: RCU head
+ */
static void _kfree_opp_rcu(struct rcu_head *head)
{
struct dev_pm_opp *opp =
kfree_rcu(opp, rcu_head);
}
+/**
+ * _kfree_device_rcu() - Free device_opp RCU handler
+ * @head: RCU head
+ */
static void _kfree_device_rcu(struct rcu_head *head)
{
struct device_opp *device_opp =
kfree_rcu(device_opp, rcu_head);
}
+/**
+ * _opp_remove() - Remove an OPP from a table definition
+ * @dev_opp: points back to the device_opp struct this opp belongs to
+ * @opp: pointer to the OPP to remove
+ *
+ * This function removes an opp definition from the opp list.
+ *
+ * Locking: The internal device_opp and opp structures are RCU protected.
+ * It is assumed that the caller holds required mutex for an RCU updater
+ * strategy.
+ */
static void _opp_remove(struct device_opp *dev_opp,
struct dev_pm_opp *opp)
{
* @freq: OPP to remove with matching 'freq'
*
* This function removes an opp from the opp list.
+ *
+ * Locking: The internal device_opp and opp structures are RCU protected.
+ * Hence this function internally uses RCU updater strategy with mutex locks
+ * to keep the integrity of the internal data structures. Callers should ensure
+ * that this function is *NOT* called under RCU protection or in contexts where
+ * mutex cannot be locked.
*/
void dev_pm_opp_remove(struct device *dev, unsigned long freq)
{
* Set the availability of an OPP with an RCU operation, opp_{enable,disable}
* share a common logic which is isolated here.
*
- * Returns -EINVAL for bad pointers, -ENOMEM if no memory available for the
+ * Return: -EINVAL for bad pointers, -ENOMEM if no memory available for the
* copy operation, returns 0 if no modifcation was done OR modification was
* successful.
*
* integrity of the internal data structures. Callers should ensure that
* this function is *NOT* called under RCU protection or in contexts where
* mutex locking or synchronize_rcu() blocking calls cannot be used.
+ *
+ * Return: -EINVAL for bad pointers, -ENOMEM if no memory available for the
+ * copy operation, returns 0 if no modifcation was done OR modification was
+ * successful.
*/
int dev_pm_opp_enable(struct device *dev, unsigned long freq)
{
* integrity of the internal data structures. Callers should ensure that
* this function is *NOT* called under RCU protection or in contexts where
* mutex locking or synchronize_rcu() blocking calls cannot be used.
+ *
+ * Return: -EINVAL for bad pointers, -ENOMEM if no memory available for the
+ * copy operation, returns 0 if no modifcation was done OR modification was
+ * successful.
*/
int dev_pm_opp_disable(struct device *dev, unsigned long freq)
{
/**
* dev_pm_opp_get_notifier() - find notifier_head of the device with opp
* @dev: device pointer used to lookup device OPPs.
+ *
+ * Return: pointer to notifier head if found, otherwise -ENODEV or
+ * -EINVAL based on type of error casted as pointer. value must be checked
+ * with IS_ERR to determine valid pointer or error result.
+ *
+ * Locking: This function must be called under rcu_read_lock(). dev_opp is a RCU
+ * protected pointer. The reason for the same is that the opp pointer which is
+ * returned will remain valid for use with opp_get_{voltage, freq} only while
+ * under the locked area. The pointer returned must be used prior to unlocking
+ * with rcu_read_unlock() to maintain the integrity of the pointer.
*/
struct srcu_notifier_head *dev_pm_opp_get_notifier(struct device *dev)
{
* @dev: device pointer used to lookup device OPPs.
*
* Register the initial OPP table with the OPP library for given device.
+ *
+ * Locking: The internal device_opp and opp structures are RCU protected.
+ * Hence this function indirectly uses RCU updater strategy with mutex locks
+ * to keep the integrity of the internal data structures. Callers should ensure
+ * that this function is *NOT* called under RCU protection or in contexts where
+ * mutex cannot be locked.
+ *
+ * Return:
+ * 0 On success OR
+ * Duplicate OPPs (both freq and volt are same) and opp->available
+ * -EEXIST Freq are same and volt are different OR
+ * Duplicate OPPs (both freq and volt are same) and !opp->available
+ * -ENOMEM Memory allocation failure
+ * -ENODEV when 'operating-points' property is not found or is invalid data
+ * in device node.
+ * -ENODATA when empty 'operating-points' property is found
*/
int of_init_opp_table(struct device *dev)
{
* @dev: device pointer used to lookup device OPPs.
*
* Free OPPs created using static entries present in DT.
+ *
+ * Locking: The internal device_opp and opp structures are RCU protected.
+ * Hence this function indirectly uses RCU updater strategy with mutex locks
+ * to keep the integrity of the internal data structures. Callers should ensure
+ * that this function is *NOT* called under RCU protection or in contexts where
+ * mutex cannot be locked.
*/
void of_free_opp_table(struct device *dev)
{