summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: d98c246)
raw | patch | inline | side by side (parent: d98c246)
author | Tony Luck <tony.luck@intel.com> | |
Fri, 18 Jul 2014 18:43:01 +0000 (11:43 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 31 Jul 2014 19:52:55 +0000 (12:52 -0700) |
commit 58d4e21e50ff3cc57910a8abc20d7e14375d2f61 upstream.
The "uptime" trace clock added in:
commit 8aacf017b065a805d27467843490c976835eb4a5
tracing: Add "uptime" trace clock that uses jiffies
has wraparound problems when the system has been up more
than 1 hour 11 minutes and 34 seconds. It converts jiffies
to nanoseconds using:
(u64)jiffies_to_usecs(jiffy) * 1000ULL
but since jiffies_to_usecs() only returns a 32-bit value, it
truncates at 2^32 microseconds. An additional problem on 32-bit
systems is that the argument is "unsigned long", so fixing the
return value only helps until 2^32 jiffies (49.7 days on a HZ=1000
system).
Avoid these problems by using jiffies_64 as our basis, and
not converting to nanoseconds (we do convert to clock_t because
user facing API must not be dependent on internal kernel
HZ values).
Link: http://lkml.kernel.org/p/99d63c5bfe9b320a3b428d773825a37095bf6a51.1405708254.git.tony.luck@intel.com
Fixes: 8aacf017b065 "tracing: Add "uptime" trace clock that uses jiffies"
Signed-off-by: Tony Luck <tony.luck@intel.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
The "uptime" trace clock added in:
commit 8aacf017b065a805d27467843490c976835eb4a5
tracing: Add "uptime" trace clock that uses jiffies
has wraparound problems when the system has been up more
than 1 hour 11 minutes and 34 seconds. It converts jiffies
to nanoseconds using:
(u64)jiffies_to_usecs(jiffy) * 1000ULL
but since jiffies_to_usecs() only returns a 32-bit value, it
truncates at 2^32 microseconds. An additional problem on 32-bit
systems is that the argument is "unsigned long", so fixing the
return value only helps until 2^32 jiffies (49.7 days on a HZ=1000
system).
Avoid these problems by using jiffies_64 as our basis, and
not converting to nanoseconds (we do convert to clock_t because
user facing API must not be dependent on internal kernel
HZ values).
Link: http://lkml.kernel.org/p/99d63c5bfe9b320a3b428d773825a37095bf6a51.1405708254.git.tony.luck@intel.com
Fixes: 8aacf017b065 "tracing: Add "uptime" trace clock that uses jiffies"
Signed-off-by: Tony Luck <tony.luck@intel.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
kernel/trace/trace.c | patch | blob | history | |
kernel/trace/trace_clock.c | patch | blob | history |
diff --git a/kernel/trace/trace.c b/kernel/trace/trace.c
index 7e259b2bdf44990a8c85f59f253f2ee731fa6e7b..71136720ffa189ea63c4bfea23b6fab884b9650b 100644 (file)
--- a/kernel/trace/trace.c
+++ b/kernel/trace/trace.c
{ trace_clock_local, "local", 1 },
{ trace_clock_global, "global", 1 },
{ trace_clock_counter, "counter", 0 },
- { trace_clock_jiffies, "uptime", 1 },
+ { trace_clock_jiffies, "uptime", 0 },
{ trace_clock, "perf", 1 },
ARCH_TRACE_CLOCKS
};
index 26dc348332b798eeb43a77cf2d89357512d9e8c0..57b67b1f24d1a141f88163c385e62be25cd275cf 100644 (file)
/*
* trace_jiffy_clock(): Simply use jiffies as a clock counter.
+ * Note that this use of jiffies_64 is not completely safe on
+ * 32-bit systems. But the window is tiny, and the effect if
+ * we are affected is that we will have an obviously bogus
+ * timestamp on a trace event - i.e. not life threatening.
*/
u64 notrace trace_clock_jiffies(void)
{
- u64 jiffy = jiffies - INITIAL_JIFFIES;
-
- /* Return nsecs */
- return (u64)jiffies_to_usecs(jiffy) * 1000ULL;
+ return jiffies_64_to_clock_t(jiffies_64 - INITIAL_JIFFIES);
}
/*