]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commitdiff
ARM: OMAP5 / DRA7: Introduce workaround for 801819
authorNishanth Menon <nm@ti.com>
Tue, 11 Aug 2015 19:11:33 +0000 (14:11 -0500)
committerPraneeth Bajjuri <praneeth@ti.com>
Tue, 11 Aug 2015 21:30:42 +0000 (16:30 -0500)
Add workaround for Cortex-A15 ARM erratum 801819 which says in summary
that "A livelock can occur in the L2 cache arbitration that might
prevent a snoop from completing. Under certain conditions this can
cause the system to deadlock. "

Recommended workaround is as follows:
Do both of the following:

1) Do not use the write-back no-allocate memory type.
2) Do not issue write-back cacheable stores at any time when the cache
is disabled (SCTLR.C=0) and the MMU is enabled (SCTLR.M=1). Because it
is implementation defined whether cacheable stores update the cache when
the cache is disabled it is not expected that any portable code will
execute cacheable stores when the cache is disabled.

For implementations of Cortex-A15 configured without the “L2 arbitration
register slice” option (typically one or two core systems), you must
also do the following:

3) Disable write-streaming in each CPU by setting ACTLR[28:25] = 0b1111

So, we provide an option to disable write streaming on OMAP5 and DRA7.
It is a rare condition to occur and may be enabled selectively based
on platform acceptance of risk.

Applies to: A15 revisions r2p0, r2p1, r2p2, r2p3 or r2p4 and REVIDR[3]
is set to 0.

Based on ARM errata Document revision 18.0 (22 Nov 2013)

Note: the configuration for the workaround needs to be done with
each CPU bringup, since CPU0 bringup is done by bootloader, it is
recommended to have the workaround in the bootloader, kernel also does
ensure that CPU0 has the workaround and makes the workaround active
when CPU1 gets active.

With CONFIG_SMP disabled, it is expected to be done by the bootloader.

This does show significant degradation in synthetic tests such as
mbw (https://packages.qa.debian.org/m/mbw.html)
mbw -n 100 100|grep AVG (on a test platform)
Without enabling the erratum:
AVG Method: MEMCPY  Elapsed: 0.13406  MiB: 100.00000  Copy: 745.913 MiB/s
AVG Method: DUMB    Elapsed: 0.06746  MiB: 100.00000  Copy: 1482.357 MiB/s
AVG Method: MCBLOCK Elapsed: 0.03058  MiB: 100.00000  Copy: 3270.569 MiB/s
After enabling the erratum:
AVG Method: MEMCPY  Elapsed: 0.13757  MiB: 100.00000  Copy: 726.913 MiB/s
AVG Method: DUMB    Elapsed: 0.12024  MiB: 100.00000  Copy: 831.668 MiB/s
AVG Method: MCBLOCK Elapsed: 0.09243  MiB: 100.00000  Copy: 1081.942 MiB/s

Most benchmarks are designed for specific performance analysis, so
overall usecase must be considered before making a decision to
enable/disable the erratum workaround.

Pending internal investigation, the erratum is kept disabled by default.

Suggested-by: Richard Woodruff <r-woodruff2@ti.com>
Suggested-by: Brad Griffis <bgriffis@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
[Rebase and apply to 3.14 product baseline]
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Change-Id: I1670c797fcd41126fb6357baeb7264527918df1a

arch/arm/mach-omap2/Kconfig
arch/arm/mach-omap2/omap-secure.h
arch/arm/mach-omap2/omap-smp.c

index 2cb8a000c9088081574152611568dc9d9d45a53a..9175110d12edcacd75aad46d2dac2f6569e31c9f 100644 (file)
@@ -119,6 +119,13 @@ config ARCH_OMAP2PLUS
        help
          Systems based on OMAP2, OMAP3, OMAP4 or OMAP5
 
+config OMAP5_ERRATA_801819
+        bool "Errata 801819: An eviction from L1 data cache might stall indefinitely"
+        depends on SOC_OMAP5 || SOC_DRA7XX
+        help
+          A livelock can occur in the L2 cache arbitration that might prevent
+          a snoop from completing. Under certain conditions this can cause the
+          system to deadlock.
 
 if ARCH_OMAP2PLUS
 
index 0957875de31ef907246bc2a6f348a718c07c8cb8..ba8b1c3dbcd36c63297dd1022a877c0d0efd9c1d 100644 (file)
@@ -46,6 +46,7 @@
 
 #define OMAP5_DRA7_MON_SET_CNTFRQ_INDEX        0x109
 #define OMAP5_MON_AMBA_IF_INDEX                0x108
+#define OMAP5_DRA7_MON_SET_ACR_INDEX   0x107
 
 /* Secure PPA(Primary Protected Application) APIs */
 #define OMAP4_PPA_L2_POR_INDEX         0x23
index 17550aa39d0f395fe6489c309c77a316e4cdc16c..4d89156bfb73ec7b3ac06f77ff6ca457060ef77d 100644 (file)
@@ -49,6 +49,39 @@ void __iomem *omap4_get_scu_base(void)
        return scu_base;
 }
 
+#ifdef CONFIG_OMAP5_ERRATA_801819
+void omap5_erratum_workaround_801819(void)
+{
+       u32 acr, revidr;
+       u32 acr_mask;
+
+       /* REVIDR[3] indicates erratum fix available on silicon */
+       asm volatile ("mrc p15, 0, %0, c0, c0, 6" : "=r" (revidr));
+       if (revidr & (0x1 << 3))
+               return;
+
+       asm volatile ("mrc p15, 0, %0, c1, c0, 1" : "=r" (acr));
+       /*
+        * BIT(27) - Disables streaming. All write-allocate lines allocate in
+        * the L1 or L2 cache.
+        * BIT(25) - Disables streaming. All write-allocate lines allocate in
+        * the L1 cache.
+        */
+       acr_mask = (0x3 << 25) | (0x3 << 27);
+       /* do we already have it done.. if yes, skip expensive smc */
+       if ((acr & acr_mask) == acr_mask)
+               return;
+
+       acr |= acr_mask;
+       omap_smc1(OMAP5_DRA7_MON_SET_ACR_INDEX, acr);
+
+       pr_debug("%s: ARM erratum workaround 801819 applied on CPU%d\n",
+                __func__, smp_processor_id());
+}
+#else
+static inline void omap5_erratum_workaround_801819(void) { }
+#endif
+
 static void omap4_secondary_init(unsigned int cpu)
 {
        /*
@@ -63,12 +96,15 @@ static void omap4_secondary_init(unsigned int cpu)
                omap_secure_dispatcher(OMAP4_PPA_CPU_ACTRL_SMP_INDEX,
                                                        4, 0, 0, 0, 0, 0);
 
-       /*
-        * Configure the CNTFRQ register for the secondary cpu's which
-        * indicates the frequency of the cpu local timers.
-        */
-       if (soc_is_omap54xx() || soc_is_dra7xx())
+       if (soc_is_omap54xx() || soc_is_dra7xx()) {
+               /*
+                * Configure the CNTFRQ register for the secondary cpu's which
+                * indicates the frequency of the cpu local timers.
+                */
                set_cntfreq();
+               /* Configure ACR to disable streaming WA for 801819 */
+               omap5_erratum_workaround_801819();
+       }
 
        /*
         * Synchronise with the boot thread.
@@ -217,6 +253,8 @@ static void __init omap4_smp_prepare_cpus(unsigned int max_cpus)
 
        if (cpu_is_omap446x())
                startup_addr = omap4460_secondary_startup;
+       if (soc_is_dra74x() || soc_is_omap54xx())
+               omap5_erratum_workaround_801819();
 
        /*
         * Write the address of secondary startup routine into the