summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 02cfa2a)
raw | patch | inline | side by side (parent: 02cfa2a)
author | Josef Bacik <jbacik@fusionio.com> | |
Wed, 24 Apr 2013 20:32:55 +0000 (16:32 -0400) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Sat, 11 May 2013 20:54:10 +0000 (13:54 -0700) |
commit eb384b55ae9c2055ea00c5cc87971e182d47aefa upstream.
This is the same as the fix from commit
Btrfs: fix bad extent logging
but for O_DIRECT. I missed this when I fixed the problem originally, we were
still using the em for the orig_start and orig_block_len, which would be the
merged extent. We need to use the actual extent from the on disk file extent
item, which we have to lookup to make sure it's ok to nocow anyway so just pass
in some pointers to hold this info. Thanks,
Signed-off-by: Josef Bacik <jbacik@fusionio.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
This is the same as the fix from commit
Btrfs: fix bad extent logging
but for O_DIRECT. I missed this when I fixed the problem originally, we were
still using the em for the orig_start and orig_block_len, which would be the
merged extent. We need to use the actual extent from the on disk file extent
item, which we have to lookup to make sure it's ok to nocow anyway so just pass
in some pointers to hold this info. Thanks,
Signed-off-by: Josef Bacik <jbacik@fusionio.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
fs/btrfs/inode.c | patch | blob | history |
diff --git a/fs/btrfs/inode.c b/fs/btrfs/inode.c
index 7c4e6ccdba3f7d5a254ec17bcd8e524cba77c36b..4b5398c9f62bd6d3b05a1843bc030e7248472736 100644 (file)
--- a/fs/btrfs/inode.c
+++ b/fs/btrfs/inode.c
* block must be cow'd
*/
static noinline int can_nocow_odirect(struct btrfs_trans_handle *trans,
- struct inode *inode, u64 offset, u64 len)
+ struct inode *inode, u64 offset, u64 *len,
+ u64 *orig_start, u64 *orig_block_len,
+ u64 *ram_bytes)
{
struct btrfs_path *path;
int ret;
disk_bytenr = btrfs_file_extent_disk_bytenr(leaf, fi);
backref_offset = btrfs_file_extent_offset(leaf, fi);
+ *orig_start = key.offset - backref_offset;
+ *orig_block_len = btrfs_file_extent_disk_num_bytes(leaf, fi);
+ *ram_bytes = btrfs_file_extent_ram_bytes(leaf, fi);
+
extent_end = key.offset + btrfs_file_extent_num_bytes(leaf, fi);
- if (extent_end < offset + len) {
+ if (extent_end < offset + *len) {
/* extent doesn't include our full range, must cow */
goto out;
}
*/
disk_bytenr += backref_offset;
disk_bytenr += offset - key.offset;
- num_bytes = min(offset + len, extent_end) - offset;
+ num_bytes = min(offset + *len, extent_end) - offset;
if (csum_exist_in_range(root, disk_bytenr, num_bytes))
goto out;
/*
* all of the above have passed, it is safe to overwrite this extent
* without cow
*/
+ *len = num_bytes;
ret = 1;
out:
btrfs_free_path(path);
em->block_start != EXTENT_MAP_HOLE)) {
int type;
int ret;
- u64 block_start;
+ u64 block_start, orig_start, orig_block_len, ram_bytes;
if (test_bit(EXTENT_FLAG_PREALLOC, &em->flags))
type = BTRFS_ORDERED_PREALLOC;
if (IS_ERR(trans))
goto must_cow;
- if (can_nocow_odirect(trans, inode, start, len) == 1) {
- u64 orig_start = em->orig_start;
- u64 orig_block_len = em->orig_block_len;
-
+ if (can_nocow_odirect(trans, inode, start, &len, &orig_start,
+ &orig_block_len, &ram_bytes) == 1) {
if (type == BTRFS_ORDERED_PREALLOC) {
free_extent_map(em);
em = create_pinned_em(inode, start, len,