summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: ece9210)
raw | patch | inline | side by side (parent: ece9210)
author | Tomas Henzl <thenzl@redhat.com> | |
Thu, 14 Aug 2014 14:12:39 +0000 (16:12 +0200) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Sat, 4 Jul 2015 02:49:05 +0000 (19:49 -0700) |
commit 132aa220b45d60e9b20def1e9d8be9422eed9616 upstream.
When a second(kdump) kernel starts and the hard reset method is used
the driver calls pci_disable_device without previously enabling it,
so the kernel shows a warning -
[ 16.876248] WARNING: at drivers/pci/pci.c:1431 pci_disable_device+0x84/0x90()
[ 16.882686] Device hpsa
disabling already-disabled device
...
This patch fixes it, in addition to this I tried to balance also some other pairs
of enable/disable device in the driver.
Unfortunately I wasn't able to verify the functionality for the case of a sw reset,
because of a lack of proper hw.
Signed-off-by: Tomas Henzl <thenzl@redhat.com>
Reviewed-by: Stephen M. Cameron <scameron@beardog.cce.hp.com>
Signed-off-by: Christoph Hellwig <hch@lst.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
When a second(kdump) kernel starts and the hard reset method is used
the driver calls pci_disable_device without previously enabling it,
so the kernel shows a warning -
[ 16.876248] WARNING: at drivers/pci/pci.c:1431 pci_disable_device+0x84/0x90()
[ 16.882686] Device hpsa
disabling already-disabled device
...
This patch fixes it, in addition to this I tried to balance also some other pairs
of enable/disable device in the driver.
Unfortunately I wasn't able to verify the functionality for the case of a sw reset,
because of a lack of proper hw.
Signed-off-by: Tomas Henzl <thenzl@redhat.com>
Reviewed-by: Stephen M. Cameron <scameron@beardog.cce.hp.com>
Signed-off-by: Christoph Hellwig <hch@lst.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
drivers/scsi/hpsa.c | patch | blob | history |
diff --git a/drivers/scsi/hpsa.c b/drivers/scsi/hpsa.c
index 528bff5ec91f80c268d5d595c88490c79a3a4e47..d88133ef45b9fa1cc8d69eeb853f7eae1ab2cd4c 100644 (file)
--- a/drivers/scsi/hpsa.c
+++ b/drivers/scsi/hpsa.c
/* Save the PCI command register */
pci_read_config_word(pdev, 4, &command_register);
- /* Turn the board off. This is so that later pci_restore_state()
- * won't turn the board on before the rest of config space is ready.
- */
- pci_disable_device(pdev);
pci_save_state(pdev);
/* find the first memory BAR, so we can find the cfg table */
goto unmap_cfgtable;
pci_restore_state(pdev);
- rc = pci_enable_device(pdev);
- if (rc) {
- dev_warn(&pdev->dev, "failed to enable device.\n");
- goto unmap_cfgtable;
- }
pci_write_config_word(pdev, 4, command_register);
/* Some devices (notably the HP Smart Array 5i Controller)
if (!reset_devices)
return 0;
+ /* kdump kernel is loading, we don't know in which state is
+ * the pci interface. The dev->enable_cnt is equal zero
+ * so we call enable+disable, wait a while and switch it on.
+ */
+ rc = pci_enable_device(pdev);
+ if (rc) {
+ dev_warn(&pdev->dev, "Failed to enable PCI device\n");
+ return -ENODEV;
+ }
+ pci_disable_device(pdev);
+ msleep(260); /* a randomly chosen number */
+ rc = pci_enable_device(pdev);
+ if (rc) {
+ dev_warn(&pdev->dev, "failed to enable device.\n");
+ return -ENODEV;
+ }
+
/* Reset the controller with a PCI power-cycle or via doorbell */
rc = hpsa_kdump_hard_reset_controller(pdev);
* "performant mode". Or, it might be 640x, which can't reset
* due to concerns about shared bbwc between 6402/6404 pair.
*/
- if (rc == -ENOTSUPP)
- return rc; /* just try to do the kdump anyhow. */
- if (rc)
- return -ENODEV;
+ if (rc) {
+ if (rc != -ENOTSUPP) /* just try to do the kdump anyhow. */
+ rc = -ENODEV;
+ goto out_disable;
+ }
/* Now try to get the controller to respond to a no-op */
dev_warn(&pdev->dev, "Waiting for controller to respond to no-op\n");
dev_warn(&pdev->dev, "no-op failed%s\n",
(i < 11 ? "; re-trying" : ""));
}
- return 0;
+
+out_disable:
+
+ pci_disable_device(pdev);
+ return rc;
}
static int hpsa_allocate_cmd_pool(struct ctlr_info *h)
iounmap(h->transtable);
if (h->cfgtable)
iounmap(h->cfgtable);
+ pci_disable_device(h->pdev);
pci_release_regions(h->pdev);
kfree(h);
}