summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 388979b)
raw | patch | inline | side by side (parent: 388979b)
author | Archit Taneja <archit@ti.com> | |
Tue, 26 Mar 2013 13:45:19 +0000 (19:15 +0530) | ||
committer | Archit Taneja <archit@ti.com> | |
Thu, 30 May 2013 15:39:28 +0000 (21:09 +0530) |
The omapdrm driver currently takes a config/module arg to figure out the number
of crtcs it needs to create. We could create as many crtcs as there are overlay
managers in the DSS hardware, but we don't do that because each crtc eats up
one DSS overlay, and that reduces the number of planes we can attach to a single
crtc.
Since the number of crtcs may be lesser than the number of hardware overlay
managers, we need to figure out which overlay managers to use for our crtcs. The
current approach is to use pipe2chan(), which returns a higher numbered manager
for the crtc.
The problem with this approach is that it assumes that the overlay managers we
choose will connect to the encoders the platform's panels are going to use,
this isn't true, an overlay manager connects only to a few outputs/encoders, and
choosing any overlay manager for our crtc might lead to a situation where the
encoder cannot connect to any of the crtcs we have chosen. For example, an
omap5-panda board has just one hdmi output. If num_crtc is set to 1, with the
current approach, pipe2chan will pick up the LCD2 overlay manager, which cannot
connect to the hdmi encoder at all. The only manager that could have connected
to hdmi was the TV overlay manager.
Therefore, there is a need to choose our overlay managers keeping in mind the
panels we have on that platform. The new approach iterates through all the
available panels, creates encoders and connectors for them, and then tries to
get a suitable overlay manager to create a crtc which can connect to the
encoders.
We use the dispc_channel field in omap_dss_output to retrieve the desired
overlay manager's channel number, we then check whether the manager had already
been assigned to a crtc or not. If it was already assigned to a crtc, we assume
that out of all the encoders which intend use this crtc, only one will run at a
time. If the overlay manager wan't assigned to a crtc till then, we create a
new crtc and link it with the overlay manager.
This approach just looks for the best dispc_channel for each encoder. On DSS HW,
some encoders can connect to multiple overlay managers. Since we don't try
looking for alternate overlay managers, there is a greater possibility that 2
or more encoders end up asking for the same crtc, causing only one encoder to
run at a time.
Also, this approach isn't the most optimal one, it can do either good or bad
depending on the sequence in which the panels/outputs are parsed. The optimal
way would be some sort of back tracking approach, where we improve the set of
managers we use as we iterate through the list of panels/encoders. That's
something left for later.
Signed-off-by: Archit Taneja <archit@ti.com>
Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
of crtcs it needs to create. We could create as many crtcs as there are overlay
managers in the DSS hardware, but we don't do that because each crtc eats up
one DSS overlay, and that reduces the number of planes we can attach to a single
crtc.
Since the number of crtcs may be lesser than the number of hardware overlay
managers, we need to figure out which overlay managers to use for our crtcs. The
current approach is to use pipe2chan(), which returns a higher numbered manager
for the crtc.
The problem with this approach is that it assumes that the overlay managers we
choose will connect to the encoders the platform's panels are going to use,
this isn't true, an overlay manager connects only to a few outputs/encoders, and
choosing any overlay manager for our crtc might lead to a situation where the
encoder cannot connect to any of the crtcs we have chosen. For example, an
omap5-panda board has just one hdmi output. If num_crtc is set to 1, with the
current approach, pipe2chan will pick up the LCD2 overlay manager, which cannot
connect to the hdmi encoder at all. The only manager that could have connected
to hdmi was the TV overlay manager.
Therefore, there is a need to choose our overlay managers keeping in mind the
panels we have on that platform. The new approach iterates through all the
available panels, creates encoders and connectors for them, and then tries to
get a suitable overlay manager to create a crtc which can connect to the
encoders.
We use the dispc_channel field in omap_dss_output to retrieve the desired
overlay manager's channel number, we then check whether the manager had already
been assigned to a crtc or not. If it was already assigned to a crtc, we assume
that out of all the encoders which intend use this crtc, only one will run at a
time. If the overlay manager wan't assigned to a crtc till then, we create a
new crtc and link it with the overlay manager.
This approach just looks for the best dispc_channel for each encoder. On DSS HW,
some encoders can connect to multiple overlay managers. Since we don't try
looking for alternate overlay managers, there is a greater possibility that 2
or more encoders end up asking for the same crtc, causing only one encoder to
run at a time.
Also, this approach isn't the most optimal one, it can do either good or bad
depending on the sequence in which the panels/outputs are parsed. The optimal
way would be some sort of back tracking approach, where we improve the set of
managers we use as we iterate through the list of panels/encoders. That's
something left for later.
Signed-off-by: Archit Taneja <archit@ti.com>
Signed-off-by: Tomi Valkeinen <tomi.valkeinen@ti.com>
index 2213dbf0043c4f1086b956aa9f72516ed5207130..9b0bff29d3997d8c4b1fe7624f62c676dd2eb522 100644 (file)
struct work_struct page_flip_work;
};
+uint32_t pipe2vbl(struct drm_crtc *crtc)
+{
+ struct omap_crtc *omap_crtc = to_omap_crtc(crtc);
+
+ return dispc_mgr_get_vsync_irq(omap_crtc->channel);
+}
+
/*
* Manager-ops, callbacks from output when they need to configure
* the upstream part of the video pipe.
omap_crtc->apply.pre_apply = omap_crtc_pre_apply;
omap_crtc->apply.post_apply = omap_crtc_post_apply;
- omap_crtc->apply_irq.irqmask = pipe2vbl(id);
+ omap_crtc->channel = channel;
+ omap_crtc->plane = plane;
+ omap_crtc->plane->crtc = crtc;
+ omap_crtc->name = channel_names[channel];
+ omap_crtc->pipe = id;
+
+ omap_crtc->apply_irq.irqmask = pipe2vbl(crtc);
omap_crtc->apply_irq.irq = omap_crtc_apply_irq;
omap_crtc->error_irq.irqmask =
omap_crtc->error_irq.irq = omap_crtc_error_irq;
omap_irq_register(dev, &omap_crtc->error_irq);
- omap_crtc->channel = channel;
- omap_crtc->plane = plane;
- omap_crtc->plane->crtc = crtc;
- omap_crtc->name = channel_names[channel];
- omap_crtc->pipe = id;
-
/* temporary: */
omap_crtc->mgr.id = channel;
index a3b1eedf9cbeb150cadaf78d695cafb1d98adadb..f2413b299ffb1790f454d9931c6594a106ba3ff8 100644 (file)
}
}
+static bool channel_used(struct drm_device *dev, enum omap_channel channel)
+{
+ struct omap_drm_private *priv = dev->dev_private;
+ int i;
+
+ for (i = 0; i < priv->num_crtcs; i++) {
+ struct drm_crtc *crtc = priv->crtcs[i];
+
+ if (omap_crtc_channel(crtc) == channel)
+ return true;
+ }
+
+ return false;
+}
+
static int omap_modeset_init(struct drm_device *dev)
{
struct omap_drm_private *priv = dev->dev_private;
struct omap_dss_device *dssdev = NULL;
int num_ovls = dss_feat_get_num_ovls();
- int id;
+ int num_mgrs = dss_feat_get_num_mgrs();
+ int num_crtcs;
+ int i, id = 0;
drm_mode_config_init(dev);
omap_drm_irq_install(dev);
/*
- * Create private planes and CRTCs for the last NUM_CRTCs overlay
- * plus manager:
- */
- for (id = 0; id < min(num_crtc, num_ovls); id++) {
- struct drm_plane *plane;
- struct drm_crtc *crtc;
-
- plane = omap_plane_init(dev, id, true);
- crtc = omap_crtc_init(dev, plane, pipe2chan(id), id);
-
- BUG_ON(priv->num_crtcs >= ARRAY_SIZE(priv->crtcs));
- priv->crtcs[id] = crtc;
- priv->num_crtcs++;
-
- priv->planes[id] = plane;
- priv->num_planes++;
- }
-
- /*
- * Create normal planes for the remaining overlays:
+ * We usually don't want to create a CRTC for each manager, at least
+ * not until we have a way to expose private planes to userspace.
+ * Otherwise there would not be enough video pipes left for drm planes.
+ * We use the num_crtc argument to limit the number of crtcs we create.
*/
- for (; id < num_ovls; id++) {
- struct drm_plane *plane = omap_plane_init(dev, id, false);
+ num_crtcs = min3(num_crtc, num_mgrs, num_ovls);
- BUG_ON(priv->num_planes >= ARRAY_SIZE(priv->planes));
- priv->planes[priv->num_planes++] = plane;
- }
+ dssdev = NULL;
for_each_dss_dev(dssdev) {
struct drm_connector *connector;
struct drm_encoder *encoder;
+ enum omap_channel channel;
if (!dssdev->driver) {
dev_warn(dev->dev, "%s has no driver.. skipping it\n",
drm_mode_connector_attach_encoder(connector, encoder);
+ /*
+ * if we have reached the limit of the crtcs we are allowed to
+ * create, let's not try to look for a crtc for this
+ * panel/encoder and onwards, we will, of course, populate the
+ * the possible_crtcs field for all the encoders with the final
+ * set of crtcs we create
+ */
+ if (id == num_crtcs)
+ continue;
+
+ /*
+ * get the recommended DISPC channel for this encoder. For now,
+ * we only try to get create a crtc out of the recommended, the
+ * other possible channels to which the encoder can connect are
+ * not considered.
+ */
+ channel = dssdev->output->dispc_channel;
+
+ /*
+ * if this channel hasn't already been taken by a previously
+ * allocated crtc, we create a new crtc for it
+ */
+ if (!channel_used(dev, channel)) {
+ struct drm_plane *plane;
+ struct drm_crtc *crtc;
+
+ plane = omap_plane_init(dev, id, true);
+ crtc = omap_crtc_init(dev, plane, channel, id);
+
+ BUG_ON(priv->num_crtcs >= ARRAY_SIZE(priv->crtcs));
+ priv->crtcs[id] = crtc;
+ priv->num_crtcs++;
+
+ priv->planes[id] = plane;
+ priv->num_planes++;
+
+ id++;
+ }
+ }
+
+ /*
+ * we have allocated crtcs according to the need of the panels/encoders,
+ * adding more crtcs here if needed
+ */
+ for (; id < num_crtcs; id++) {
+
+ /* find a free manager for this crtc */
+ for (i = 0; i < num_mgrs; i++) {
+ if (!channel_used(dev, i)) {
+ struct drm_plane *plane;
+ struct drm_crtc *crtc;
+
+ plane = omap_plane_init(dev, id, true);
+ crtc = omap_crtc_init(dev, plane, i, id);
+
+ BUG_ON(priv->num_crtcs >=
+ ARRAY_SIZE(priv->crtcs));
+
+ priv->crtcs[id] = crtc;
+ priv->num_crtcs++;
+
+ priv->planes[id] = plane;
+ priv->num_planes++;
+
+ break;
+ } else {
+ continue;
+ }
+ }
+
+ if (i == num_mgrs) {
+ /* this shouldn't really happen */
+ dev_err(dev->dev, "no managers left for crtc\n");
+ return -ENOMEM;
+ }
+ }
+
+ /*
+ * Create normal planes for the remaining overlays:
+ */
+ for (; id < num_ovls; id++) {
+ struct drm_plane *plane = omap_plane_init(dev, id, false);
+
+ BUG_ON(priv->num_planes >= ARRAY_SIZE(priv->planes));
+ priv->planes[priv->num_planes++] = plane;
+ }
+
+ for (i = 0; i < priv->num_encoders; i++) {
+ struct drm_encoder *encoder = priv->encoders[i];
+ struct omap_dss_device *dssdev =
+ omap_encoder_get_dssdev(encoder);
+
/* figure out which crtc's we can connect the encoder to: */
encoder->possible_crtcs = 0;
for (id = 0; id < priv->num_crtcs; id++) {
- enum omap_dss_output_id supported_outputs =
- dss_feat_get_supported_outputs(pipe2chan(id));
+ struct drm_crtc *crtc = priv->crtcs[id];
+ enum omap_channel crtc_channel;
+ enum omap_dss_output_id supported_outputs;
+
+ crtc_channel = omap_crtc_channel(crtc);
+ supported_outputs =
+ dss_feat_get_supported_outputs(crtc_channel);
+
if (supported_outputs & dssdev->output->id)
encoder->possible_crtcs |= (1 << id);
}
}
+ DBG("registered %d planes, %d crtcs, %d encoders and %d connectors\n",
+ priv->num_planes, priv->num_crtcs, priv->num_encoders,
+ priv->num_connectors);
+
dev->mode_config.min_width = 32;
dev->mode_config.min_height = 32;
index d4f997bb4ac0eaab02f6419d4c832246959bbb45..215a20dd340cc8984ddffad32b0c7c42010d06c1 100644 (file)
int omap_gem_resume(struct device *dev);
#endif
-int omap_irq_enable_vblank(struct drm_device *dev, int crtc);
-void omap_irq_disable_vblank(struct drm_device *dev, int crtc);
+int omap_irq_enable_vblank(struct drm_device *dev, int crtc_id);
+void omap_irq_disable_vblank(struct drm_device *dev, int crtc_id);
irqreturn_t omap_irq_handler(DRM_IRQ_ARGS);
void omap_irq_preinstall(struct drm_device *dev);
int omap_irq_postinstall(struct drm_device *dev);
return ALIGN(pitch, 8 * bytespp);
}
-static inline enum omap_channel pipe2chan(int pipe)
-{
- int num_mgrs = dss_feat_get_num_mgrs();
-
- /*
- * We usually don't want to create a CRTC for each manager,
- * at least not until we have a way to expose private planes
- * to userspace. Otherwise there would not be enough video
- * pipes left for drm planes. The higher #'d managers tend
- * to have more features so start in reverse order.
- */
- return num_mgrs - pipe - 1;
-}
-
/* map crtc to vblank mask */
-static inline uint32_t pipe2vbl(int crtc)
-{
- enum omap_channel channel = pipe2chan(crtc);
- return dispc_mgr_get_vsync_irq(channel);
-}
-
-static inline int crtc2pipe(struct drm_device *dev, struct drm_crtc *crtc)
-{
- struct omap_drm_private *priv = dev->dev_private;
- int i;
-
- for (i = 0; i < ARRAY_SIZE(priv->crtcs); i++)
- if (priv->crtcs[i] == crtc)
- return i;
-
- BUG(); /* bogus CRTC ptr */
- return -1;
-}
+uint32_t pipe2vbl(struct drm_crtc *crtc);
+struct omap_dss_device *omap_encoder_get_dssdev(struct drm_encoder *encoder);
/* should these be made into common util helpers?
*/
index 7e1f2ab653729edc653438d43eca1619e8c49011..c2aabe05152eb486a17345134155aa7efdac3a77 100644 (file)
struct omap_dss_device *dssdev;
};
+struct omap_dss_device *omap_encoder_get_dssdev(struct drm_encoder *encoder)
+{
+ struct omap_encoder *omap_encoder = to_omap_encoder(encoder);
+
+ return omap_encoder->dssdev;
+}
+
static void omap_encoder_destroy(struct drm_encoder *encoder)
{
struct omap_encoder *omap_encoder = to_omap_encoder(encoder);
index e01303ee00c3b9d64ac48b4e5a956450f4920435..9263db117ff8ae937dbf743ac0e8a267264d95a4 100644 (file)
* Zero on success, appropriate errno if the given @crtc's vblank
* interrupt cannot be enabled.
*/
-int omap_irq_enable_vblank(struct drm_device *dev, int crtc)
+int omap_irq_enable_vblank(struct drm_device *dev, int crtc_id)
{
struct omap_drm_private *priv = dev->dev_private;
+ struct drm_crtc *crtc = priv->crtcs[crtc_id];
unsigned long flags;
- DBG("dev=%p, crtc=%d", dev, crtc);
+ DBG("dev=%p, crtc=%d", dev, crtc_id);
dispc_runtime_get();
spin_lock_irqsave(&list_lock, flags);
* a hardware vblank counter, this routine should be a no-op, since
* interrupts will have to stay on to keep the count accurate.
*/
-void omap_irq_disable_vblank(struct drm_device *dev, int crtc)
+void omap_irq_disable_vblank(struct drm_device *dev, int crtc_id)
{
struct omap_drm_private *priv = dev->dev_private;
+ struct drm_crtc *crtc = priv->crtcs[crtc_id];
unsigned long flags;
- DBG("dev=%p, crtc=%d", dev, crtc);
+ DBG("dev=%p, crtc=%d", dev, crtc_id);
dispc_runtime_get();
spin_lock_irqsave(&list_lock, flags);
VERB("irqs: %08x", irqstatus);
- for (id = 0; id < priv->num_crtcs; id++)
- if (irqstatus & pipe2vbl(id))
+ for (id = 0; id < priv->num_crtcs; id++) {
+ struct drm_crtc *crtc = priv->crtcs[id];
+
+ if (irqstatus & pipe2vbl(crtc))
drm_handle_vblank(dev, id);
+ }
spin_lock_irqsave(&list_lock, flags);
list_for_each_entry_safe(handler, n, &priv->irq_list, node) {