summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 6fc37d2)
raw | patch | inline | side by side (parent: 6fc37d2)
author | Eduardo Valentin <eduardo.valentin@ti.com> | |
Wed, 2 Jan 2013 15:29:39 +0000 (15:29 +0000) | ||
committer | Eduardo Valentin <eduardo.valentin@ti.com> | |
Wed, 20 Mar 2013 14:26:47 +0000 (10:26 -0400) |
This patch changes the function thermal_generate_netlink_event
to receive a thermal zone device instead of a originator id.
This way, the messages will always be bound to a thermal zone.
Signed-off-by: Eduardo Valentin <eduardo.valentin@ti.com>
Reviewed-by: Durgadoss R <durgadoss.r@intel.com>
Signed-off-by: Zhang Rui <rui.zhang@intel.com>
to receive a thermal zone device instead of a originator id.
This way, the messages will always be bound to a thermal zone.
Signed-off-by: Eduardo Valentin <eduardo.valentin@ti.com>
Reviewed-by: Durgadoss R <durgadoss.r@intel.com>
Signed-off-by: Zhang Rui <rui.zhang@intel.com>
Documentation/thermal/sysfs-api.txt | patch | blob | history | |
drivers/thermal/thermal_sys.c | patch | blob | history | |
include/linux/thermal.h | patch | blob | history |
index 88c02334e35681b005ac20a1ad0dfe4a894bc1f7..526d4b90d6c197c2995f1456de78d9ca053cbe3e 100644 (file)
netlink event. Netlink socket initialization is done during the _init_
of the framework. Drivers which intend to use the notification mechanism
just need to call thermal_generate_netlink_event() with two arguments viz
-(originator, event). Typically the originator will be an integer assigned
-to a thermal_zone_device when it registers itself with the framework. The
+(originator, event). The originator is a pointer to struct thermal_zone_device
+from where the event has been originated. An integer which represents the
+thermal zone device will be used in the message to identify the zone. The
event will be one of:{THERMAL_AUX0, THERMAL_AUX1, THERMAL_CRITICAL,
THERMAL_DEV_FAULT}. Notification can be sent when the current temperature
crosses any of the configured thresholds.
index 8c8ce806180fc1d56988273175ac899741449cad..d85f51f433be49dc9f5e5f7b5db94f095555b957 100644 (file)
.name = THERMAL_GENL_MCAST_GROUP_NAME,
};
-int thermal_generate_netlink_event(u32 orig, enum events event)
+int thermal_generate_netlink_event(struct thermal_zone_device *tz,
+ enum events event)
{
struct sk_buff *skb;
struct nlattr *attr;
int result;
static unsigned int thermal_event_seqnum;
+ if (!tz)
+ return -EINVAL;
+
/* allocate memory */
size = nla_total_size(sizeof(struct thermal_genl_event)) +
nla_total_size(0);
memset(thermal_event, 0, sizeof(struct thermal_genl_event));
- thermal_event->orig = orig;
+ thermal_event->orig = tz->id;
thermal_event->event = event;
/* send multicast genetlink message */
index 883bcda7e1e45d8504e4d2169471dcf70537742b..9b78f8c6f77374ee743c2adc41cf31d592d37546 100644 (file)
--- a/include/linux/thermal.h
+++ b/include/linux/thermal.h
void thermal_unregister_governor(struct thermal_governor *);
#ifdef CONFIG_NET
-extern int thermal_generate_netlink_event(u32 orig, enum events event);
+extern int thermal_generate_netlink_event(struct thermal_zone_device *tz,
+ enum events event);
#else
-static inline int thermal_generate_netlink_event(u32 orig, enum events event)
+static int thermal_generate_netlink_event(struct thermal_zone_device *tz,
+ enum events event)
{
return 0;
}