author | Linus Torvalds <torvalds@linux-foundation.org> | |
Fri, 25 Jan 2013 18:55:21 +0000 (10:55 -0800) | ||
committer | Linus Torvalds <torvalds@linux-foundation.org> | |
Fri, 25 Jan 2013 18:55:21 +0000 (10:55 -0800) |
Pull btrfs fixes from Chris Mason:
"It turns out that we had two crc bugs when running fsx-linux in a
loop. Many thanks to Josef, Miao Xie, and Dave Sterba for nailing it
all down. Miao also has a new OOM fix in this v2 pull as well.
Ilya fixed a regression Liu Bo found in the balance ioctls for pausing
and resuming a running balance across drives.
Josef's orphan truncate patch fixes an obscure corruption we'd see
during xfstests.
Arne's patches address problems with subvolume quotas. If the user
destroys quota groups incorrectly the FS will refuse to mount.
The rest are smaller fixes and plugs for memory leaks."
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/linux-btrfs: (30 commits)
Btrfs: fix repeated delalloc work allocation
Btrfs: fix wrong max device number for single profile
Btrfs: fix missed transaction->aborted check
Btrfs: Add ACCESS_ONCE() to transaction->abort accesses
Btrfs: put csums on the right ordered extent
Btrfs: use right range to find checksum for compressed extents
Btrfs: fix panic when recovering tree log
Btrfs: do not allow logged extents to be merged or removed
Btrfs: fix a regression in balance usage filter
Btrfs: prevent qgroup destroy when there are still relations
Btrfs: ignore orphan qgroup relations
Btrfs: reorder locks and sanity checks in btrfs_ioctl_defrag
Btrfs: fix unlock order in btrfs_ioctl_rm_dev
Btrfs: fix unlock order in btrfs_ioctl_resize
Btrfs: fix "mutually exclusive op is running" error code
Btrfs: bring back balance pause/resume logic
btrfs: update timestamps on truncate()
btrfs: fix btrfs_cont_expand() freeing IS_ERR em
Btrfs: fix a bug when llseek for delalloc bytes behind prealloc extents
Btrfs: fix off-by-one in lseek
...
"It turns out that we had two crc bugs when running fsx-linux in a
loop. Many thanks to Josef, Miao Xie, and Dave Sterba for nailing it
all down. Miao also has a new OOM fix in this v2 pull as well.
Ilya fixed a regression Liu Bo found in the balance ioctls for pausing
and resuming a running balance across drives.
Josef's orphan truncate patch fixes an obscure corruption we'd see
during xfstests.
Arne's patches address problems with subvolume quotas. If the user
destroys quota groups incorrectly the FS will refuse to mount.
The rest are smaller fixes and plugs for memory leaks."
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/linux-btrfs: (30 commits)
Btrfs: fix repeated delalloc work allocation
Btrfs: fix wrong max device number for single profile
Btrfs: fix missed transaction->aborted check
Btrfs: Add ACCESS_ONCE() to transaction->abort accesses
Btrfs: put csums on the right ordered extent
Btrfs: use right range to find checksum for compressed extents
Btrfs: fix panic when recovering tree log
Btrfs: do not allow logged extents to be merged or removed
Btrfs: fix a regression in balance usage filter
Btrfs: prevent qgroup destroy when there are still relations
Btrfs: ignore orphan qgroup relations
Btrfs: reorder locks and sanity checks in btrfs_ioctl_defrag
Btrfs: fix unlock order in btrfs_ioctl_rm_dev
Btrfs: fix unlock order in btrfs_ioctl_resize
Btrfs: fix "mutually exclusive op is running" error code
Btrfs: bring back balance pause/resume logic
btrfs: update timestamps on truncate()
btrfs: fix btrfs_cont_expand() freeing IS_ERR em
Btrfs: fix a bug when llseek for delalloc bytes behind prealloc extents
Btrfs: fix off-by-one in lseek
...
14 files changed:
diff --git a/fs/btrfs/extent-tree.c b/fs/btrfs/extent-tree.c
index 521e9d4424f64f81d69d98709031a342d5ee808f..a8b8adc0507059137898cae2e058570e11843291 100644 (file)
--- a/fs/btrfs/extent-tree.c
+++ b/fs/btrfs/extent-tree.c
* We make the other tasks wait for the flush only when we can flush
* all things.
*/
- if (ret && flush == BTRFS_RESERVE_FLUSH_ALL) {
+ if (ret && flush != BTRFS_RESERVE_NO_FLUSH) {
flushing = true;
space_info->flush = 1;
}
int empty_cluster = 2 * 1024 * 1024;
struct btrfs_space_info *space_info;
int loop = 0;
- int index = 0;
+ int index = __get_raid_index(data);
int alloc_type = (data & BTRFS_BLOCK_GROUP_DATA) ?
RESERVE_ALLOC_NO_ACCOUNT : RESERVE_ALLOC;
bool found_uncached_bg = false;
&wc->flags[level]);
if (ret < 0) {
btrfs_tree_unlock_rw(eb, path->locks[level]);
+ path->locks[level] = 0;
return ret;
}
BUG_ON(wc->refs[level] == 0);
if (wc->refs[level] == 1) {
btrfs_tree_unlock_rw(eb, path->locks[level]);
+ path->locks[level] = 0;
return 1;
}
}
diff --git a/fs/btrfs/extent_map.c b/fs/btrfs/extent_map.c
index f169d6b11d7f6a093158428352a44f35d4bae952..2e8cae63d247929613ddc77e6d01761e35b04753 100644 (file)
--- a/fs/btrfs/extent_map.c
+++ b/fs/btrfs/extent_map.c
if (test_bit(EXTENT_FLAG_COMPRESSED, &prev->flags))
return 0;
+ if (test_bit(EXTENT_FLAG_LOGGING, &prev->flags) ||
+ test_bit(EXTENT_FLAG_LOGGING, &next->flags))
+ return 0;
+
if (extent_map_end(prev) == next->start &&
prev->flags == next->flags &&
prev->bdev == next->bdev &&
if (!em)
goto out;
- list_move(&em->list, &tree->modified_extents);
+ if (!test_bit(EXTENT_FLAG_LOGGING, &em->flags))
+ list_move(&em->list, &tree->modified_extents);
em->generation = gen;
clear_bit(EXTENT_FLAG_PINNED, &em->flags);
em->mod_start = em->start;
}
+void clear_em_logging(struct extent_map_tree *tree, struct extent_map *em)
+{
+ clear_bit(EXTENT_FLAG_LOGGING, &em->flags);
+ try_merge_map(tree, em);
+}
+
/**
* add_extent_mapping - add new extent map to the extent tree
* @tree: tree to insert new map in
diff --git a/fs/btrfs/extent_map.h b/fs/btrfs/extent_map.h
index 922943ce29e8caebe0a69feda2a7e481bed0d556..c6598c89cff8c48676dd6179f649ef6f0638acad 100644 (file)
--- a/fs/btrfs/extent_map.h
+++ b/fs/btrfs/extent_map.h
int __init extent_map_init(void);
void extent_map_exit(void);
int unpin_extent_cache(struct extent_map_tree *tree, u64 start, u64 len, u64 gen);
+void clear_em_logging(struct extent_map_tree *tree, struct extent_map *em);
struct extent_map *search_extent_mapping(struct extent_map_tree *tree,
u64 start, u64 len);
#endif
diff --git a/fs/btrfs/file-item.c b/fs/btrfs/file-item.c
index bd38cef4235882425c08eb6a5d10306736a14237..94aa53b387213bbfc13181163368e5e168574d77 100644 (file)
--- a/fs/btrfs/file-item.c
+++ b/fs/btrfs/file-item.c
if (!contig)
offset = page_offset(bvec->bv_page) + bvec->bv_offset;
- if (!contig && (offset >= ordered->file_offset + ordered->len ||
- offset < ordered->file_offset)) {
+ if (offset >= ordered->file_offset + ordered->len ||
+ offset < ordered->file_offset) {
unsigned long bytes_left;
sums->len = this_sum_bytes;
this_sum_bytes = 0;
diff --git a/fs/btrfs/file.c b/fs/btrfs/file.c
index 77061bf43edbae995bf55ce73dcc89bf73012400..f76b1fd160d446fb4c92fd56b8cc0ea14acc6f9a 100644 (file)
--- a/fs/btrfs/file.c
+++ b/fs/btrfs/file.c
@@ -2241,6 +2241,7 @@ static int find_desired_extent(struct inode *inode, loff_t *offset, int whence)
if (lockend <= lockstart)
lockend = lockstart + root->sectorsize;
+ lockend--;
len = lockend - lockstart + 1;
len = max_t(u64, len, root->sectorsize);
@@ -2307,9 +2308,12 @@ static int find_desired_extent(struct inode *inode, loff_t *offset, int whence)
}
}
- *offset = start;
- free_extent_map(em);
- break;
+ if (!test_bit(EXTENT_FLAG_PREALLOC,
+ &em->flags)) {
+ *offset = start;
+ free_extent_map(em);
+ break;
+ }
}
}
index 59ea2e4349c9cdbecb105a3a384376f52b0a5da6..0be7a8742a43bb502c9b9294661baaef6e5514e1 100644 (file)
{
struct btrfs_free_space_ctl *ctl = block_group->free_space_ctl;
struct btrfs_free_space *info;
- int ret = 0;
+ int ret;
+ bool re_search = false;
spin_lock(&ctl->tree_lock);
again:
+ ret = 0;
if (!bytes)
goto out_lock;
info = tree_search_offset(ctl, offset_to_bitmap(ctl, offset),
1, 0);
if (!info) {
- /* the tree logging code might be calling us before we
- * have fully loaded the free space rbtree for this
- * block group. So it is possible the entry won't
- * be in the rbtree yet at all. The caching code
- * will make sure not to put it in the rbtree if
- * the logging code has pinned it.
+ /*
+ * If we found a partial bit of our free space in a
+ * bitmap but then couldn't find the other part this may
+ * be a problem, so WARN about it.
*/
+ WARN_ON(re_search);
goto out_lock;
}
}
+ re_search = false;
if (!info->bitmap) {
unlink_free_space(ctl, info);
if (offset == info->offset) {
}
ret = remove_from_bitmap(ctl, info, &offset, &bytes);
- if (ret == -EAGAIN)
+ if (ret == -EAGAIN) {
+ re_search = true;
goto again;
+ }
BUG_ON(ret); /* logic error */
out_lock:
spin_unlock(&ctl->tree_lock);
diff --git a/fs/btrfs/inode.c b/fs/btrfs/inode.c
index 16d9e8e191e6ac34d92da08fe90b46e2de42ebf8..cc93b23ca3520c9ad7bf2919e77f61cf400c2e4c 100644 (file)
--- a/fs/btrfs/inode.c
+++ b/fs/btrfs/inode.c
[S_IFLNK >> S_SHIFT] = BTRFS_FT_SYMLINK,
};
-static int btrfs_setsize(struct inode *inode, loff_t newsize);
+static int btrfs_setsize(struct inode *inode, struct iattr *attr);
static int btrfs_truncate(struct inode *inode);
static int btrfs_finish_ordered_io(struct btrfs_ordered_extent *ordered_extent);
static noinline int cow_file_range(struct inode *inode,
continue;
}
nr_truncate++;
+
+ /* 1 for the orphan item deletion. */
+ trans = btrfs_start_transaction(root, 1);
+ if (IS_ERR(trans)) {
+ ret = PTR_ERR(trans);
+ goto out;
+ }
+ ret = btrfs_orphan_add(trans, inode);
+ btrfs_end_transaction(trans, root);
+ if (ret)
+ goto out;
+
ret = btrfs_truncate(inode);
} else {
nr_unlink++;
block_end - cur_offset, 0);
if (IS_ERR(em)) {
err = PTR_ERR(em);
+ em = NULL;
break;
}
last_byte = min(extent_map_end(em), block_end);
return err;
}
-static int btrfs_setsize(struct inode *inode, loff_t newsize)
+static int btrfs_setsize(struct inode *inode, struct iattr *attr)
{
struct btrfs_root *root = BTRFS_I(inode)->root;
struct btrfs_trans_handle *trans;
loff_t oldsize = i_size_read(inode);
+ loff_t newsize = attr->ia_size;
+ int mask = attr->ia_valid;
int ret;
if (newsize == oldsize)
return 0;
+ /*
+ * The regular truncate() case without ATTR_CTIME and ATTR_MTIME is a
+ * special case where we need to update the times despite not having
+ * these flags set. For all other operations the VFS set these flags
+ * explicitly if it wants a timestamp update.
+ */
+ if (newsize != oldsize && (!(mask & (ATTR_CTIME | ATTR_MTIME))))
+ inode->i_ctime = inode->i_mtime = current_fs_time(inode->i_sb);
+
if (newsize > oldsize) {
truncate_pagecache(inode, oldsize, newsize);
ret = btrfs_cont_expand(inode, oldsize, newsize);
set_bit(BTRFS_INODE_ORDERED_DATA_CLOSE,
&BTRFS_I(inode)->runtime_flags);
+ /*
+ * 1 for the orphan item we're going to add
+ * 1 for the orphan item deletion.
+ */
+ trans = btrfs_start_transaction(root, 2);
+ if (IS_ERR(trans))
+ return PTR_ERR(trans);
+
+ /*
+ * We need to do this in case we fail at _any_ point during the
+ * actual truncate. Once we do the truncate_setsize we could
+ * invalidate pages which forces any outstanding ordered io to
+ * be instantly completed which will give us extents that need
+ * to be truncated. If we fail to get an orphan inode down we
+ * could have left over extents that were never meant to live,
+ * so we need to garuntee from this point on that everything
+ * will be consistent.
+ */
+ ret = btrfs_orphan_add(trans, inode);
+ btrfs_end_transaction(trans, root);
+ if (ret)
+ return ret;
+
/* we don't support swapfiles, so vmtruncate shouldn't fail */
truncate_setsize(inode, newsize);
ret = btrfs_truncate(inode);
+ if (ret && inode->i_nlink)
+ btrfs_orphan_del(NULL, inode);
}
return ret;
return err;
if (S_ISREG(inode->i_mode) && (attr->ia_valid & ATTR_SIZE)) {
- err = btrfs_setsize(inode, attr->ia_size);
+ err = btrfs_setsize(inode, attr);
if (err)
return err;
}
@@ -5572,10 +5621,13 @@ struct extent_map *btrfs_get_extent_fiemap(struct inode *inode, struct page *pag
return em;
if (em) {
/*
- * if our em maps to a hole, there might
- * actually be delalloc bytes behind it
+ * if our em maps to
+ * - a hole or
+ * - a pre-alloc extent,
+ * there might actually be delalloc bytes behind it.
*/
- if (em->block_start != EXTENT_MAP_HOLE)
+ if (em->block_start != EXTENT_MAP_HOLE &&
+ !test_bit(EXTENT_FLAG_PREALLOC, &em->flags))
return em;
else
hole_em = em;
@@ -5657,6 +5709,8 @@ struct extent_map *btrfs_get_extent_fiemap(struct inode *inode, struct page *pag
*/
em->block_start = hole_em->block_start;
em->block_len = hole_len;
+ if (test_bit(EXTENT_FLAG_PREALLOC, &hole_em->flags))
+ set_bit(EXTENT_FLAG_PREALLOC, &em->flags);
} else {
em->start = range_start;
em->len = found;
/*
* 1 for the truncate slack space
- * 1 for the orphan item we're going to add
- * 1 for the orphan item deletion
* 1 for updating the inode.
*/
- trans = btrfs_start_transaction(root, 4);
+ trans = btrfs_start_transaction(root, 2);
if (IS_ERR(trans)) {
err = PTR_ERR(trans);
goto out;
min_size);
BUG_ON(ret);
- ret = btrfs_orphan_add(trans, inode);
- if (ret) {
- btrfs_end_transaction(trans, root);
- goto out;
- }
-
/*
* setattr is responsible for setting the ordered_data_close flag,
* but that is only tested during the last file release. That
ret = btrfs_orphan_del(trans, inode);
if (ret)
err = ret;
- } else if (ret && inode->i_nlink > 0) {
- /*
- * Failed to do the truncate, remove us from the in memory
- * orphan list.
- */
- ret = btrfs_orphan_del(NULL, inode);
}
if (trans) {
*/
int btrfs_start_delalloc_inodes(struct btrfs_root *root, int delay_iput)
{
- struct list_head *head = &root->fs_info->delalloc_inodes;
struct btrfs_inode *binode;
struct inode *inode;
struct btrfs_delalloc_work *work, *next;
struct list_head works;
+ struct list_head splice;
int ret = 0;
if (root->fs_info->sb->s_flags & MS_RDONLY)
return -EROFS;
INIT_LIST_HEAD(&works);
-
+ INIT_LIST_HEAD(&splice);
+again:
spin_lock(&root->fs_info->delalloc_lock);
- while (!list_empty(head)) {
- binode = list_entry(head->next, struct btrfs_inode,
+ list_splice_init(&root->fs_info->delalloc_inodes, &splice);
+ while (!list_empty(&splice)) {
+ binode = list_entry(splice.next, struct btrfs_inode,
delalloc_inodes);
+
+ list_del_init(&binode->delalloc_inodes);
+
inode = igrab(&binode->vfs_inode);
if (!inode)
- list_del_init(&binode->delalloc_inodes);
+ continue;
+
+ list_add_tail(&binode->delalloc_inodes,
+ &root->fs_info->delalloc_inodes);
spin_unlock(&root->fs_info->delalloc_lock);
- if (inode) {
- work = btrfs_alloc_delalloc_work(inode, 0, delay_iput);
- if (!work) {
- ret = -ENOMEM;
- goto out;
- }
- list_add_tail(&work->list, &works);
- btrfs_queue_worker(&root->fs_info->flush_workers,
- &work->work);
+
+ work = btrfs_alloc_delalloc_work(inode, 0, delay_iput);
+ if (unlikely(!work)) {
+ ret = -ENOMEM;
+ goto out;
}
+ list_add_tail(&work->list, &works);
+ btrfs_queue_worker(&root->fs_info->flush_workers,
+ &work->work);
+
cond_resched();
spin_lock(&root->fs_info->delalloc_lock);
}
spin_unlock(&root->fs_info->delalloc_lock);
+ list_for_each_entry_safe(work, next, &works, list) {
+ list_del_init(&work->list);
+ btrfs_wait_and_free_delalloc_work(work);
+ }
+
+ spin_lock(&root->fs_info->delalloc_lock);
+ if (!list_empty(&root->fs_info->delalloc_inodes)) {
+ spin_unlock(&root->fs_info->delalloc_lock);
+ goto again;
+ }
+ spin_unlock(&root->fs_info->delalloc_lock);
+
/* the filemap_flush will queue IO into the worker threads, but
* we have to make sure the IO is actually started and that
* ordered extents get created before we return
atomic_read(&root->fs_info->async_delalloc_pages) == 0));
}
atomic_dec(&root->fs_info->async_submit_draining);
+ return 0;
out:
list_for_each_entry_safe(work, next, &works, list) {
list_del_init(&work->list);
btrfs_wait_and_free_delalloc_work(work);
}
+
+ if (!list_empty_careful(&splice)) {
+ spin_lock(&root->fs_info->delalloc_lock);
+ list_splice_tail(&splice, &root->fs_info->delalloc_inodes);
+ spin_unlock(&root->fs_info->delalloc_lock);
+ }
return ret;
}
diff --git a/fs/btrfs/ioctl.c b/fs/btrfs/ioctl.c
index 4b4516770f055432964da1e82fe591e1e2128ef8..5b22d45d3c6a232aeed49b24cf34bb374a96ecc9 100644 (file)
--- a/fs/btrfs/ioctl.c
+++ b/fs/btrfs/ioctl.c
if (atomic_xchg(&root->fs_info->mutually_exclusive_operation_running,
1)) {
pr_info("btrfs: dev add/delete/balance/replace/resize operation in progress\n");
- return -EINPROGRESS;
+ mnt_drop_write_file(file);
+ return -EINVAL;
}
mutex_lock(&root->fs_info->volume_mutex);
printk(KERN_INFO "btrfs: resizing devid %llu\n",
(unsigned long long)devid);
}
+
device = btrfs_find_device(root->fs_info, devid, NULL, NULL);
if (!device) {
printk(KERN_INFO "btrfs: resizer unable to find device %llu\n",
ret = -EINVAL;
goto out_free;
}
- if (device->fs_devices && device->fs_devices->seeding) {
+
+ if (!device->writeable) {
printk(KERN_INFO "btrfs: resizer unable to apply on "
- "seeding device %llu\n",
+ "readonly device %llu\n",
(unsigned long long)devid);
ret = -EINVAL;
goto out_free;
kfree(vol_args);
out:
mutex_unlock(&root->fs_info->volume_mutex);
- mnt_drop_write_file(file);
atomic_set(&root->fs_info->mutually_exclusive_operation_running, 0);
+ mnt_drop_write_file(file);
return ret;
}
err = inode_permission(inode, MAY_WRITE | MAY_EXEC);
if (err)
goto out_dput;
-
- /* check if subvolume may be deleted by a non-root user */
- err = btrfs_may_delete(dir, dentry, 1);
- if (err)
- goto out_dput;
}
+ /* check if subvolume may be deleted by a user */
+ err = btrfs_may_delete(dir, dentry, 1);
+ if (err)
+ goto out_dput;
+
if (btrfs_ino(inode) != BTRFS_FIRST_FREE_OBJECTID) {
err = -EINVAL;
goto out_dput;
struct btrfs_ioctl_defrag_range_args *range;
int ret;
- if (btrfs_root_readonly(root))
- return -EROFS;
+ ret = mnt_want_write_file(file);
+ if (ret)
+ return ret;
if (atomic_xchg(&root->fs_info->mutually_exclusive_operation_running,
1)) {
pr_info("btrfs: dev add/delete/balance/replace/resize operation in progress\n");
- return -EINPROGRESS;
+ mnt_drop_write_file(file);
+ return -EINVAL;
}
- ret = mnt_want_write_file(file);
- if (ret) {
- atomic_set(&root->fs_info->mutually_exclusive_operation_running,
- 0);
- return ret;
+
+ if (btrfs_root_readonly(root)) {
+ ret = -EROFS;
+ goto out;
}
switch (inode->i_mode & S_IFMT) {
ret = -EINVAL;
}
out:
- mnt_drop_write_file(file);
atomic_set(&root->fs_info->mutually_exclusive_operation_running, 0);
+ mnt_drop_write_file(file);
return ret;
}
if (atomic_xchg(&root->fs_info->mutually_exclusive_operation_running,
1)) {
pr_info("btrfs: dev add/delete/balance/replace/resize operation in progress\n");
- return -EINPROGRESS;
+ return -EINVAL;
}
mutex_lock(&root->fs_info->volume_mutex);
1)) {
pr_info("btrfs: dev add/delete/balance/replace/resize operation in progress\n");
mnt_drop_write_file(file);
- return -EINPROGRESS;
+ return -EINVAL;
}
mutex_lock(&root->fs_info->volume_mutex);
kfree(vol_args);
out:
mutex_unlock(&root->fs_info->volume_mutex);
- mnt_drop_write_file(file);
atomic_set(&root->fs_info->mutually_exclusive_operation_running, 0);
+ mnt_drop_write_file(file);
return ret;
}
struct btrfs_fs_info *fs_info = root->fs_info;
struct btrfs_ioctl_balance_args *bargs;
struct btrfs_balance_control *bctl;
+ bool need_unlock; /* for mut. excl. ops lock */
int ret;
- int need_to_clear_lock = 0;
if (!capable(CAP_SYS_ADMIN))
return -EPERM;
if (ret)
return ret;
- mutex_lock(&fs_info->volume_mutex);
+again:
+ if (!atomic_xchg(&fs_info->mutually_exclusive_operation_running, 1)) {
+ mutex_lock(&fs_info->volume_mutex);
+ mutex_lock(&fs_info->balance_mutex);
+ need_unlock = true;
+ goto locked;
+ }
+
+ /*
+ * mut. excl. ops lock is locked. Three possibilites:
+ * (1) some other op is running
+ * (2) balance is running
+ * (3) balance is paused -- special case (think resume)
+ */
mutex_lock(&fs_info->balance_mutex);
+ if (fs_info->balance_ctl) {
+ /* this is either (2) or (3) */
+ if (!atomic_read(&fs_info->balance_running)) {
+ mutex_unlock(&fs_info->balance_mutex);
+ if (!mutex_trylock(&fs_info->volume_mutex))
+ goto again;
+ mutex_lock(&fs_info->balance_mutex);
+
+ if (fs_info->balance_ctl &&
+ !atomic_read(&fs_info->balance_running)) {
+ /* this is (3) */
+ need_unlock = false;
+ goto locked;
+ }
+
+ mutex_unlock(&fs_info->balance_mutex);
+ mutex_unlock(&fs_info->volume_mutex);
+ goto again;
+ } else {
+ /* this is (2) */
+ mutex_unlock(&fs_info->balance_mutex);
+ ret = -EINPROGRESS;
+ goto out;
+ }
+ } else {
+ /* this is (1) */
+ mutex_unlock(&fs_info->balance_mutex);
+ pr_info("btrfs: dev add/delete/balance/replace/resize operation in progress\n");
+ ret = -EINVAL;
+ goto out;
+ }
+
+locked:
+ BUG_ON(!atomic_read(&fs_info->mutually_exclusive_operation_running));
if (arg) {
bargs = memdup_user(arg, sizeof(*bargs));
if (IS_ERR(bargs)) {
ret = PTR_ERR(bargs);
- goto out;
+ goto out_unlock;
}
if (bargs->flags & BTRFS_BALANCE_RESUME) {
bargs = NULL;
}
- if (atomic_xchg(&root->fs_info->mutually_exclusive_operation_running,
- 1)) {
- pr_info("btrfs: dev add/delete/balance/replace/resize operation in progress\n");
+ if (fs_info->balance_ctl) {
ret = -EINPROGRESS;
goto out_bargs;
}
- need_to_clear_lock = 1;
bctl = kzalloc(sizeof(*bctl), GFP_NOFS);
if (!bctl) {
}
do_balance:
- ret = btrfs_balance(bctl, bargs);
/*
- * bctl is freed in __cancel_balance or in free_fs_info if
- * restriper was paused all the way until unmount
+ * Ownership of bctl and mutually_exclusive_operation_running
+ * goes to to btrfs_balance. bctl is freed in __cancel_balance,
+ * or, if restriper was paused all the way until unmount, in
+ * free_fs_info. mutually_exclusive_operation_running is
+ * cleared in __cancel_balance.
*/
+ need_unlock = false;
+
+ ret = btrfs_balance(bctl, bargs);
+
if (arg) {
if (copy_to_user(arg, bargs, sizeof(*bargs)))
ret = -EFAULT;
out_bargs:
kfree(bargs);
-out:
- if (need_to_clear_lock)
- atomic_set(&root->fs_info->mutually_exclusive_operation_running,
- 0);
+out_unlock:
mutex_unlock(&fs_info->balance_mutex);
mutex_unlock(&fs_info->volume_mutex);
+ if (need_unlock)
+ atomic_set(&fs_info->mutually_exclusive_operation_running, 0);
+out:
mnt_drop_write_file(file);
return ret;
}
goto drop_write;
}
+ if (!sa->qgroupid) {
+ ret = -EINVAL;
+ goto out;
+ }
+
trans = btrfs_join_transaction(root);
if (IS_ERR(trans)) {
ret = PTR_ERR(trans);
diff --git a/fs/btrfs/qgroup.c b/fs/btrfs/qgroup.c
index fe9d02c45f8e521f87b44d6deff3e5f8d99aa3a9..a5c856234323241c22dde18e1ee072c8bed3ccaa 100644 (file)
--- a/fs/btrfs/qgroup.c
+++ b/fs/btrfs/qgroup.c
ret = add_relation_rb(fs_info, found_key.objectid,
found_key.offset);
+ if (ret == -ENOENT) {
+ printk(KERN_WARNING
+ "btrfs: orphan qgroup relation 0x%llx->0x%llx\n",
+ (unsigned long long)found_key.objectid,
+ (unsigned long long)found_key.offset);
+ ret = 0; /* ignore the error */
+ }
if (ret)
goto out;
next2:
struct btrfs_fs_info *fs_info, u64 qgroupid)
{
struct btrfs_root *quota_root;
+ struct btrfs_qgroup *qgroup;
int ret = 0;
quota_root = fs_info->quota_root;
if (!quota_root)
return -EINVAL;
+ /* check if there are no relations to this qgroup */
+ spin_lock(&fs_info->qgroup_lock);
+ qgroup = find_qgroup_rb(fs_info, qgroupid);
+ if (qgroup) {
+ if (!list_empty(&qgroup->groups) || !list_empty(&qgroup->members)) {
+ spin_unlock(&fs_info->qgroup_lock);
+ return -EBUSY;
+ }
+ }
+ spin_unlock(&fs_info->qgroup_lock);
+
ret = del_qgroup_item(trans, quota_root, qgroupid);
spin_lock(&fs_info->qgroup_lock);
del_qgroup_rb(quota_root->fs_info, qgroupid);
-
spin_unlock(&fs_info->qgroup_lock);
return ret;
diff --git a/fs/btrfs/send.c b/fs/btrfs/send.c
index 54454542ad4073352ddcabf27fd9e0bc528e2136..321b7fb4e4417573e9c404069c6b249afb8ab488 100644 (file)
--- a/fs/btrfs/send.c
+++ b/fs/btrfs/send.c
(unsigned long)nce->ino);
if (!nce_head) {
nce_head = kmalloc(sizeof(*nce_head), GFP_NOFS);
- if (!nce_head)
+ if (!nce_head) {
+ kfree(nce);
return -ENOMEM;
+ }
INIT_LIST_HEAD(nce_head);
ret = radix_tree_insert(&sctx->name_cache, nce->ino, nce_head);
diff --git a/fs/btrfs/super.c b/fs/btrfs/super.c
index 99545df1b86c18071fed0cbf68dcbb8e745d5524..d8982e9601d37862e6405df95df15c1ba34eecb9 100644 (file)
--- a/fs/btrfs/super.c
+++ b/fs/btrfs/super.c
function, line, errstr);
return;
}
- trans->transaction->aborted = errno;
+ ACCESS_ONCE(trans->transaction->aborted) = errno;
__btrfs_std_error(root->fs_info, function, line, errno, NULL);
}
/*
diff --git a/fs/btrfs/transaction.c b/fs/btrfs/transaction.c
index 87fac9a21ea56578625536ac1229678e854ec5f7..f15494699f3b649b1fd743b6bb5e5c7764e334d6 100644 (file)
--- a/fs/btrfs/transaction.c
+++ b/fs/btrfs/transaction.c
goto cleanup_transaction;
}
- if (cur_trans->aborted) {
+ /* Stop the commit early if ->aborted is set */
+ if (unlikely(ACCESS_ONCE(cur_trans->aborted))) {
ret = cur_trans->aborted;
goto cleanup_transaction;
}
wait_event(cur_trans->writer_wait,
atomic_read(&cur_trans->num_writers) == 1);
+ /* ->aborted might be set after the previous check, so check it */
+ if (unlikely(ACCESS_ONCE(cur_trans->aborted))) {
+ ret = cur_trans->aborted;
+ goto cleanup_transaction;
+ }
/*
* the reloc mutex makes sure that we stop
* the balancing code from coming in and moving
goto cleanup_transaction;
}
+ /*
+ * The tasks which save the space cache and inode cache may also
+ * update ->aborted, check it.
+ */
+ if (unlikely(ACCESS_ONCE(cur_trans->aborted))) {
+ ret = cur_trans->aborted;
+ mutex_unlock(&root->fs_info->tree_log_mutex);
+ mutex_unlock(&root->fs_info->reloc_mutex);
+ goto cleanup_transaction;
+ }
+
btrfs_prepare_extent_commit(trans, root);
cur_trans = root->fs_info->running_transaction;
diff --git a/fs/btrfs/tree-log.c b/fs/btrfs/tree-log.c
index 83186c7e45d40db89192abad9da56628874cf5d1..9027bb1e74660758328a3d133fe58b59ddc460e6 100644 (file)
--- a/fs/btrfs/tree-log.c
+++ b/fs/btrfs/tree-log.c
if (skip_csum)
return 0;
+ if (em->compress_type) {
+ csum_offset = 0;
+ csum_len = block_len;
+ }
+
/* block start is already adjusted for the file extent offset. */
ret = btrfs_lookup_csums_range(log->fs_info->csum_root,
em->block_start + csum_offset,
em = list_entry(extents.next, struct extent_map, list);
list_del_init(&em->list);
- clear_bit(EXTENT_FLAG_LOGGING, &em->flags);
/*
* If we had an error we just need to delete everybody from our
* private list.
*/
if (ret) {
+ clear_em_logging(tree, em);
free_extent_map(em);
continue;
}
write_unlock(&tree->lock);
ret = log_one_extent(trans, inode, root, em, path);
- free_extent_map(em);
write_lock(&tree->lock);
+ clear_em_logging(tree, em);
+ free_extent_map(em);
}
WARN_ON(!list_empty(&extents));
write_unlock(&tree->lock);
diff --git a/fs/btrfs/volumes.c b/fs/btrfs/volumes.c
index 5cce6aa7401287322c31673cf039f0e32918c6c4..15f6efdf6463589531f8d1507b74c9d8afd35a3d 100644 (file)
--- a/fs/btrfs/volumes.c
+++ b/fs/btrfs/volumes.c
}
} else {
ret = btrfs_get_bdev_and_sb(device_path,
- FMODE_READ | FMODE_EXCL,
+ FMODE_WRITE | FMODE_EXCL,
root->fs_info->bdev_holder, 0,
&bdev, &bh);
if (ret)
@@ -2614,7 +2614,14 @@ static int chunk_usage_filter(struct btrfs_fs_info *fs_info, u64 chunk_offset,
cache = btrfs_lookup_block_group(fs_info, chunk_offset);
chunk_used = btrfs_block_group_used(&cache->item);
- user_thresh = div_factor_fine(cache->key.offset, bargs->usage);
+ if (bargs->usage == 0)
+ user_thresh = 0;
+ else if (bargs->usage > 100)
+ user_thresh = cache->key.offset;
+ else
+ user_thresh = div_factor_fine(cache->key.offset,
+ bargs->usage);
+
if (chunk_used < user_thresh)
ret = 0;
unset_balance_control(fs_info);
ret = del_balance_item(fs_info->tree_root);
BUG_ON(ret);
+
+ atomic_set(&fs_info->mutually_exclusive_operation_running, 0);
}
void update_ioctl_balance_args(struct btrfs_fs_info *fs_info, int lock,
out:
if (bctl->flags & BTRFS_BALANCE_RESUME)
__cancel_balance(fs_info);
- else
+ else {
kfree(bctl);
+ atomic_set(&fs_info->mutually_exclusive_operation_running, 0);
+ }
return ret;
}
ret = btrfs_balance(fs_info->balance_ctl, NULL);
}
- atomic_set(&fs_info->mutually_exclusive_operation_running, 0);
mutex_unlock(&fs_info->balance_mutex);
mutex_unlock(&fs_info->volume_mutex);
return 0;
}
- WARN_ON(atomic_xchg(&fs_info->mutually_exclusive_operation_running, 1));
tsk = kthread_run(balance_kthread, fs_info, "btrfs-balance");
if (IS_ERR(tsk))
return PTR_ERR(tsk);
btrfs_balance_sys(leaf, item, &disk_bargs);
btrfs_disk_balance_args_to_cpu(&bctl->sys, &disk_bargs);
+ WARN_ON(atomic_xchg(&fs_info->mutually_exclusive_operation_running, 1));
+
mutex_lock(&fs_info->volume_mutex);
mutex_lock(&fs_info->balance_mutex);
{ 1, 1, 2, 2, 2, 2 /* raid1 */ },
{ 1, 2, 1, 1, 1, 2 /* dup */ },
{ 1, 1, 0, 2, 1, 1 /* raid0 */ },
- { 1, 1, 0, 1, 1, 1 /* single */ },
+ { 1, 1, 1, 1, 1, 1 /* single */ },
};
static int __btrfs_alloc_chunk(struct btrfs_trans_handle *trans,