]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/commitdiff
blkcg: don't call into policy draining if root_blkg is already gone
authorTejun Heo <tj@kernel.org>
Sat, 5 Jul 2014 22:43:21 +0000 (18:43 -0400)
committerGreg Kroah-Hartman <gregkh@linuxfoundation.org>
Thu, 31 Jul 2014 19:52:55 +0000 (12:52 -0700)
commit 0b462c89e31f7eb6789713437eb551833ee16ff3 upstream.

While a queue is being destroyed, all the blkgs are destroyed and its
->root_blkg pointer is set to NULL.  If someone else starts to drain
while the queue is in this state, the following oops happens.

  NULL pointer dereference at 0000000000000028
  IP: [<ffffffff8144e944>] blk_throtl_drain+0x84/0x230
  PGD e4a1067 PUD b773067 PMD 0
  Oops: 0000 [#1] PREEMPT SMP DEBUG_PAGEALLOC
  Modules linked in: cfq_iosched(-) [last unloaded: cfq_iosched]
  CPU: 1 PID: 537 Comm: bash Not tainted 3.16.0-rc3-work+ #2
  Hardware name: Bochs Bochs, BIOS Bochs 01/01/2011
  task: ffff88000e222250 ti: ffff88000efd4000 task.ti: ffff88000efd4000
  RIP: 0010:[<ffffffff8144e944>]  [<ffffffff8144e944>] blk_throtl_drain+0x84/0x230
  RSP: 0018:ffff88000efd7bf0  EFLAGS: 00010046
  RAX: 0000000000000000 RBX: ffff880015091450 RCX: 0000000000000001
  RDX: 0000000000000000 RSI: 0000000000000000 RDI: 0000000000000000
  RBP: ffff88000efd7c10 R08: 0000000000000000 R09: 0000000000000001
  R10: ffff88000e222250 R11: 0000000000000000 R12: ffff880015091450
  R13: ffff880015092e00 R14: ffff880015091d70 R15: ffff88001508fc28
  FS:  00007f1332650740(0000) GS:ffff88001fa80000(0000) knlGS:0000000000000000
  CS:  0010 DS: 0000 ES: 0000 CR0: 000000008005003b
  CR2: 0000000000000028 CR3: 0000000009446000 CR4: 00000000000006e0
  Stack:
   ffffffff8144e8f6 ffff880015091450 0000000000000000 ffff880015091d80
   ffff88000efd7c28 ffffffff8144ae2f ffff880015091450 ffff88000efd7c58
   ffffffff81427641 ffff880015091450 ffffffff82401f00 ffff880015091450
  Call Trace:
   [<ffffffff8144ae2f>] blkcg_drain_queue+0x1f/0x60
   [<ffffffff81427641>] __blk_drain_queue+0x71/0x180
   [<ffffffff81429b3e>] blk_queue_bypass_start+0x6e/0xb0
   [<ffffffff814498b8>] blkcg_deactivate_policy+0x38/0x120
   [<ffffffff8144ec44>] blk_throtl_exit+0x34/0x50
   [<ffffffff8144aea5>] blkcg_exit_queue+0x35/0x40
   [<ffffffff8142d476>] blk_release_queue+0x26/0xd0
   [<ffffffff81454968>] kobject_cleanup+0x38/0x70
   [<ffffffff81454848>] kobject_put+0x28/0x60
   [<ffffffff81427505>] blk_put_queue+0x15/0x20
   [<ffffffff817d07bb>] scsi_device_dev_release_usercontext+0x16b/0x1c0
   [<ffffffff810bc339>] execute_in_process_context+0x89/0xa0
   [<ffffffff817d064c>] scsi_device_dev_release+0x1c/0x20
   [<ffffffff817930e2>] device_release+0x32/0xa0
   [<ffffffff81454968>] kobject_cleanup+0x38/0x70
   [<ffffffff81454848>] kobject_put+0x28/0x60
   [<ffffffff817934d7>] put_device+0x17/0x20
   [<ffffffff817d11b9>] __scsi_remove_device+0xa9/0xe0
   [<ffffffff817d121b>] scsi_remove_device+0x2b/0x40
   [<ffffffff817d1257>] sdev_store_delete+0x27/0x30
   [<ffffffff81792ca8>] dev_attr_store+0x18/0x30
   [<ffffffff8126f75e>] sysfs_kf_write+0x3e/0x50
   [<ffffffff8126ea87>] kernfs_fop_write+0xe7/0x170
   [<ffffffff811f5e9f>] vfs_write+0xaf/0x1d0
   [<ffffffff811f69bd>] SyS_write+0x4d/0xc0
   [<ffffffff81d24692>] system_call_fastpath+0x16/0x1b

776687bce42b ("block, blk-mq: draining can't be skipped even if
bypass_depth was non-zero") made it easier to trigger this bug by
making blk_queue_bypass_start() drain even when it loses the first
bypass test to blk_cleanup_queue(); however, the bug has always been
there even before the commit as blk_queue_bypass_start() could race
against queue destruction, win the initial bypass test but perform the
actual draining after blk_cleanup_queue() already destroyed all blkgs.

Fix it by skippping calling into policy draining if all the blkgs are
already gone.

Signed-off-by: Tejun Heo <tj@kernel.org>
Reported-by: Shirish Pargaonkar <spargaonkar@suse.com>
Reported-by: Sasha Levin <sasha.levin@oracle.com>
Reported-by: Jet Chen <jet.chen@intel.com>
Tested-by: Shirish Pargaonkar <spargaonkar@suse.com>
Signed-off-by: Jens Axboe <axboe@fb.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
block/blk-cgroup.c

index dd0dd2d4cecaa443047447ec20e8e57cb54911f5..d8f80e733cf81610c017cd2daf7844e8ff637df8 100644 (file)
@@ -859,6 +859,13 @@ void blkcg_drain_queue(struct request_queue *q)
 {
        lockdep_assert_held(q->queue_lock);
 
+       /*
+        * @q could be exiting and already have destroyed all blkgs as
+        * indicated by NULL root_blkg.  If so, don't confuse policies.
+        */
+       if (!q->root_blkg)
+               return;
+
        blk_throtl_drain(q);
 }