summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 06e8684)
raw | patch | inline | side by side (parent: 06e8684)
author | Mathias Krause <minipli@googlemail.com> | |
Thu, 9 Jun 2011 18:05:18 +0000 (20:05 +0200) | ||
committer | Linus Torvalds <torvalds@linux-foundation.org> | |
Thu, 9 Jun 2011 19:50:05 +0000 (12:50 -0700) |
Unconditionally changing the address limit to USER_DS and not restoring
it to its old value in the error path is wrong because it prevents us
using kernel memory on repeated calls to this function. This, in fact,
breaks the fallback of hard coded paths to the init program from being
ever successful if the first candidate fails to load.
With this patch applied switching to USER_DS is delayed until the point
of no return is reached which makes it possible to have a multi-arch
rootfs with one arch specific init binary for each of the (hard coded)
probed paths.
Since the address limit is already set to USER_DS when start_thread()
will be invoked, this redundancy can be safely removed.
Signed-off-by: Mathias Krause <minipli@googlemail.com>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: stable@kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
it to its old value in the error path is wrong because it prevents us
using kernel memory on repeated calls to this function. This, in fact,
breaks the fallback of hard coded paths to the init program from being
ever successful if the first candidate fails to load.
With this patch applied switching to USER_DS is delayed until the point
of no return is reached which makes it possible to have a multi-arch
rootfs with one arch specific init binary for each of the (hard coded)
probed paths.
Since the address limit is already set to USER_DS when start_thread()
will be invoked, this redundancy can be safely removed.
Signed-off-by: Mathias Krause <minipli@googlemail.com>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: stable@kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
arch/x86/kernel/process_32.c | patch | blob | history | |
arch/x86/kernel/process_64.c | patch | blob | history | |
fs/exec.c | patch | blob | history |
index 8d128783af47374e56412d01d0488aa12af1647b..a3d0dc59067be542d7423d2a8abbc99801c0d3f6 100644 (file)
{
set_user_gs(regs, 0);
regs->fs = 0;
- set_fs(USER_DS);
regs->ds = __USER_DS;
regs->es = __USER_DS;
regs->ss = __USER_DS;
index 6c9dd922ac0d8b34ff9cac883ef86bf8843cb912..ca6f7ab8df332992166d51c802216d350c8729cc 100644 (file)
regs->cs = _cs;
regs->ss = _ss;
regs->flags = X86_EFLAGS_IF;
- set_fs(USER_DS);
/*
* Free the old FP and other extended state
*/
diff --git a/fs/exec.c b/fs/exec.c
index ea5f748906a83218eae60cbb241aaab53cec8ac8..97e0d52d72fdd65a365f3cab7027ae22c230582e 100644 (file)
--- a/fs/exec.c
+++ b/fs/exec.c
bprm->mm = NULL; /* We're using it now */
+ set_fs(USER_DS);
current->flags &= ~(PF_RANDOMIZE | PF_KTHREAD);
flush_thread();
current->personality &= ~bprm->per_clear;
if (retval)
return retval;
- /* kernel module loader fixup */
- /* so we don't try to load run modprobe in kernel space. */
- set_fs(USER_DS);
-
retval = audit_bprm(bprm);
if (retval)
return retval;