summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 44e51b2)
raw | patch | inline | side by side (parent: 44e51b2)
author | Nishanth Menon <nm@ti.com> | |
Sat, 9 Jul 2011 21:37:21 +0000 (14:37 -0700) | ||
committer | Kevin Hilman <khilman@ti.com> | |
Fri, 5 Aug 2011 18:54:55 +0000 (11:54 -0700) |
SmartReflex should be disabled while entering low power mode due to
a) SmartReflex values are not defined for retention voltage, further
b) with SmartReflex enabled, if CPU enters lower c-states, FSM will try
to bump the voltage to current OPP's voltage for which it has entered c-state;
hence SmartReflex needs to be disabled for MPU, CORE and IVA voltage
domains in idle path before enabling auto retention voltage achievement
on the device.
However, since the current pm_runtime setup for SmartReflex devices are
setup to allow callbacks to be invoked with interrupts enabled, calling
SmartReflex enable/disable from other contexts such as idle paths
where preemption is disabled causes warnings such as the following
indicating of a potential race.
[ 82.023895] [<c04d079c>] (__irq_svc+0x3c/0x120) from [<c04d0484>] (_raw_spin_unlock_irq+0x28/0x2c)
[ 82.023895] [<c04d0484>] (_raw_spin_unlock_irq+0x28/0x2c) from [<c0323234>] (rpm_callback+0x4c/0x68)
[ 82.023956] [<c0323234>] (rpm_callback+0x4c/0x68) from [<c0323f7c>] (rpm_resume+0x338/0x53c)
[ 82.023956] [<c0323f7c>] (rpm_resume+0x338/0x53c) from [<c03243f4>] (__pm_runtime_resume+0x48/0x60)
[ 82.023986] [<c03243f4>] (__pm_runtime_resume+0x48/0x60) from [<c008aee0>] (sr_enable+0xa8/0x19c)
[ 82.023986] [<c008aee0>] (sr_enable+0xa8/0x19c) from [<c008b2fc>] (omap_sr_enable+0x50/0x90)
[ 82.024017] [<c008b2fc>] (omap_sr_enable+0x50/0x90) from [<c00888c0>] (omap4_enter_sleep+0x138/0x168)
Instead, we use pm_runtime_irq_safe to tell the PM core that callbacks can be
invoked in interrupt disabled contexts.
Acked-by: Rajendra Nayak <rnayak@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
[khilman@ti.com: minor changelog edits]
Signed-off-by: Kevin Hilman <khilman@ti.com>
a) SmartReflex values are not defined for retention voltage, further
b) with SmartReflex enabled, if CPU enters lower c-states, FSM will try
to bump the voltage to current OPP's voltage for which it has entered c-state;
hence SmartReflex needs to be disabled for MPU, CORE and IVA voltage
domains in idle path before enabling auto retention voltage achievement
on the device.
However, since the current pm_runtime setup for SmartReflex devices are
setup to allow callbacks to be invoked with interrupts enabled, calling
SmartReflex enable/disable from other contexts such as idle paths
where preemption is disabled causes warnings such as the following
indicating of a potential race.
[ 82.023895] [<c04d079c>] (__irq_svc+0x3c/0x120) from [<c04d0484>] (_raw_spin_unlock_irq+0x28/0x2c)
[ 82.023895] [<c04d0484>] (_raw_spin_unlock_irq+0x28/0x2c) from [<c0323234>] (rpm_callback+0x4c/0x68)
[ 82.023956] [<c0323234>] (rpm_callback+0x4c/0x68) from [<c0323f7c>] (rpm_resume+0x338/0x53c)
[ 82.023956] [<c0323f7c>] (rpm_resume+0x338/0x53c) from [<c03243f4>] (__pm_runtime_resume+0x48/0x60)
[ 82.023986] [<c03243f4>] (__pm_runtime_resume+0x48/0x60) from [<c008aee0>] (sr_enable+0xa8/0x19c)
[ 82.023986] [<c008aee0>] (sr_enable+0xa8/0x19c) from [<c008b2fc>] (omap_sr_enable+0x50/0x90)
[ 82.024017] [<c008b2fc>] (omap_sr_enable+0x50/0x90) from [<c00888c0>] (omap4_enter_sleep+0x138/0x168)
Instead, we use pm_runtime_irq_safe to tell the PM core that callbacks can be
invoked in interrupt disabled contexts.
Acked-by: Rajendra Nayak <rnayak@ti.com>
Signed-off-by: Nishanth Menon <nm@ti.com>
[khilman@ti.com: minor changelog edits]
Signed-off-by: Kevin Hilman <khilman@ti.com>
arch/arm/mach-omap2/smartreflex.c | patch | blob | history |
index 2ce2fb7664bc60992f7f5eebbbed3fc57345ac9e..dc8e86a54ac57c32df1b84058cf45ea71b08b497 100644 (file)
irq = platform_get_resource(pdev, IORESOURCE_IRQ, 0);
pm_runtime_enable(&pdev->dev);
+ pm_runtime_irq_safe(&pdev->dev);
sr_info->pdev = pdev;
sr_info->srid = pdev->id;