summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c05d1fe)
raw | patch | inline | side by side (parent: c05d1fe)
author | David Rientjes <rientjes@google.com> | |
Wed, 30 Jul 2014 23:08:24 +0000 (16:08 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 7 Aug 2014 21:52:37 +0000 (14:52 -0700) |
commit b104a35d32025ca740539db2808aa3385d0f30eb upstream.
The page allocator relies on __GFP_WAIT to determine if ALLOC_CPUSET
should be set in allocflags. ALLOC_CPUSET controls if a page allocation
should be restricted only to the set of allowed cpuset mems.
Transparent hugepages clears __GFP_WAIT when defrag is disabled to prevent
the fault path from using memory compaction or direct reclaim. Thus, it
is unfairly able to allocate outside of its cpuset mems restriction as a
side-effect.
This patch ensures that ALLOC_CPUSET is only cleared when the gfp mask is
truly GFP_ATOMIC by verifying it is also not a thp allocation.
Signed-off-by: David Rientjes <rientjes@google.com>
Reported-by: Alex Thorlton <athorlton@sgi.com>
Tested-by: Alex Thorlton <athorlton@sgi.com>
Cc: Bob Liu <lliubbo@gmail.com>
Cc: Dave Hansen <dave.hansen@linux.intel.com>
Cc: Hedi Berriche <hedi@sgi.com>
Cc: Hugh Dickins <hughd@google.com>
Cc: Johannes Weiner <hannes@cmpxchg.org>
Cc: Kirill A. Shutemov <kirill.shutemov@linux.intel.com>
Cc: Mel Gorman <mgorman@suse.de>
Cc: Rik van Riel <riel@redhat.com>
Cc: Srivatsa S. Bhat <srivatsa.bhat@linux.vnet.ibm.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
The page allocator relies on __GFP_WAIT to determine if ALLOC_CPUSET
should be set in allocflags. ALLOC_CPUSET controls if a page allocation
should be restricted only to the set of allowed cpuset mems.
Transparent hugepages clears __GFP_WAIT when defrag is disabled to prevent
the fault path from using memory compaction or direct reclaim. Thus, it
is unfairly able to allocate outside of its cpuset mems restriction as a
side-effect.
This patch ensures that ALLOC_CPUSET is only cleared when the gfp mask is
truly GFP_ATOMIC by verifying it is also not a thp allocation.
Signed-off-by: David Rientjes <rientjes@google.com>
Reported-by: Alex Thorlton <athorlton@sgi.com>
Tested-by: Alex Thorlton <athorlton@sgi.com>
Cc: Bob Liu <lliubbo@gmail.com>
Cc: Dave Hansen <dave.hansen@linux.intel.com>
Cc: Hedi Berriche <hedi@sgi.com>
Cc: Hugh Dickins <hughd@google.com>
Cc: Johannes Weiner <hannes@cmpxchg.org>
Cc: Kirill A. Shutemov <kirill.shutemov@linux.intel.com>
Cc: Mel Gorman <mgorman@suse.de>
Cc: Rik van Riel <riel@redhat.com>
Cc: Srivatsa S. Bhat <srivatsa.bhat@linux.vnet.ibm.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
mm/page_alloc.c | patch | blob | history |
diff --git a/mm/page_alloc.c b/mm/page_alloc.c
index 7e7f94755ab5705eef4054c730cd8157ea7c006b..62e400d00e3f3c8488d7c8167dffcb5a1b6441cf 100644 (file)
--- a/mm/page_alloc.c
+++ b/mm/page_alloc.c
gfp_to_alloc_flags(gfp_t gfp_mask)
{
int alloc_flags = ALLOC_WMARK_MIN | ALLOC_CPUSET;
- const gfp_t wait = gfp_mask & __GFP_WAIT;
+ const bool atomic = !(gfp_mask & (__GFP_WAIT | __GFP_NO_KSWAPD));
/* __GFP_HIGH is assumed to be the same as ALLOC_HIGH to save a branch. */
BUILD_BUG_ON(__GFP_HIGH != (__force gfp_t) ALLOC_HIGH);
* The caller may dip into page reserves a bit more if the caller
* cannot run direct reclaim, or if the caller has realtime scheduling
* policy or is asking for __GFP_HIGH memory. GFP_ATOMIC requests will
- * set both ALLOC_HARDER (!wait) and ALLOC_HIGH (__GFP_HIGH).
+ * set both ALLOC_HARDER (atomic == true) and ALLOC_HIGH (__GFP_HIGH).
*/
alloc_flags |= (__force int) (gfp_mask & __GFP_HIGH);
- if (!wait) {
+ if (atomic) {
/*
- * Not worth trying to allocate harder for
- * __GFP_NOMEMALLOC even if it can't schedule.
+ * Not worth trying to allocate harder for __GFP_NOMEMALLOC even
+ * if it can't schedule.
*/
- if (!(gfp_mask & __GFP_NOMEMALLOC))
+ if (!(gfp_mask & __GFP_NOMEMALLOC))
alloc_flags |= ALLOC_HARDER;
/*
- * Ignore cpuset if GFP_ATOMIC (!wait) rather than fail alloc.
- * See also cpuset_zone_allowed() comment in kernel/cpuset.c.
+ * Ignore cpuset mems for GFP_ATOMIC rather than fail, see the
+ * comment for __cpuset_node_allowed_softwall().
*/
alloc_flags &= ~ALLOC_CPUSET;
} else if (unlikely(rt_task(current)) && !in_interrupt())