summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b4d1831)
raw | patch | inline | side by side (parent: b4d1831)
author | Tejun Heo <tj@kernel.org> | |
Tue, 16 Oct 2012 22:03:15 +0000 (15:03 -0700) | ||
committer | Tejun Heo <tj@kernel.org> | |
Sat, 20 Oct 2012 23:33:12 +0000 (16:33 -0700) |
freezer_read/write() used cgroup_lock_live_group() to synchronize
against task migration into and out of the target cgroup.
cgroup_lock_live_group() grabs the internal cgroup lock and using it
from outside cgroup core leads to complex and fragile locking
dependency issues which are difficult to resolve.
Now that freezer_can_attach() is replaced with freezer_attach() and
update_if_frozen() updated, nothing requires excluding migration
against freezer state reads and changes.
This patch removes cgroup_lock_live_group() and the matching
cgroup_unlock() usages. The prone-to-bitrot, already outdated and
unnecessary global lock hierarchy documentation is replaced with
documentation in local scope.
Signed-off-by: Tejun Heo <tj@kernel.org>
Cc: Oleg Nesterov <oleg@redhat.com>
Cc: Rafael J. Wysocki <rjw@sisk.pl>
Cc: Li Zefan <lizefan@huawei.com>
against task migration into and out of the target cgroup.
cgroup_lock_live_group() grabs the internal cgroup lock and using it
from outside cgroup core leads to complex and fragile locking
dependency issues which are difficult to resolve.
Now that freezer_can_attach() is replaced with freezer_attach() and
update_if_frozen() updated, nothing requires excluding migration
against freezer state reads and changes.
This patch removes cgroup_lock_live_group() and the matching
cgroup_unlock() usages. The prone-to-bitrot, already outdated and
unnecessary global lock hierarchy documentation is replaced with
documentation in local scope.
Signed-off-by: Tejun Heo <tj@kernel.org>
Cc: Oleg Nesterov <oleg@redhat.com>
Cc: Rafael J. Wysocki <rjw@sisk.pl>
Cc: Li Zefan <lizefan@huawei.com>
kernel/cgroup_freezer.c | patch | blob | history |
index 3d45503a21a2696aa9bba958cd1b5171aea13f4d..8a92b0e52099185136ace406dcefa7129b1ba5e1 100644 (file)
--- a/kernel/cgroup_freezer.c
+++ b/kernel/cgroup_freezer.c
struct cgroup_subsys freezer_subsys;
-/* Locks taken and their ordering
- * ------------------------------
- * cgroup_mutex (AKA cgroup_lock)
- * freezer->lock
- * css_set_lock
- * task->alloc_lock (AKA task_lock)
- * task->sighand->siglock
- *
- * cgroup code forces css_set_lock to be taken before task->alloc_lock
- *
- * freezer_create(), freezer_destroy():
- * cgroup_mutex [ by cgroup core ]
- *
- * freezer_can_attach():
- * cgroup_mutex (held by caller of can_attach)
- *
- * freezer_fork() (preserving fork() performance means can't take cgroup_mutex):
- * freezer->lock
- * sighand->siglock (if the cgroup is freezing)
- *
- * freezer_read():
- * cgroup_mutex
- * freezer->lock
- * write_lock css_set_lock (cgroup iterator start)
- * task->alloc_lock
- * read_lock css_set_lock (cgroup iterator start)
- *
- * freezer_write() (freeze):
- * cgroup_mutex
- * freezer->lock
- * write_lock css_set_lock (cgroup iterator start)
- * task->alloc_lock
- * read_lock css_set_lock (cgroup iterator start)
- * sighand->siglock (fake signal delivery inside freeze_task())
- *
- * freezer_write() (unfreeze):
- * cgroup_mutex
- * freezer->lock
- * write_lock css_set_lock (cgroup iterator start)
- * task->alloc_lock
- * read_lock css_set_lock (cgroup iterator start)
- * task->alloc_lock (inside __thaw_task(), prevents race with refrigerator())
- * sighand->siglock
- */
static struct cgroup_subsys_state *freezer_create(struct cgroup *cgroup)
{
struct freezer *freezer;
}
/*
- * The call to cgroup_lock() in the freezer.state write method prevents
- * a write to that file racing against an attach, and hence we don't need
- * to worry about racing against migration.
+ * Tasks can be migrated into a different freezer anytime regardless of its
+ * current state. freezer_attach() is responsible for making new tasks
+ * conform to the current state.
+ *
+ * Freezer state changes and task migration are synchronized via
+ * @freezer->lock. freezer_attach() makes the new tasks conform to the
+ * current state and all following state changes can see the new tasks.
*/
static void freezer_attach(struct cgroup *new_cgrp, struct cgroup_taskset *tset)
{
* partially frozen when we exitted write. Caller must hold freezer->lock.
*
* Task states and freezer state might disagree while tasks are being
- * migrated into @cgroup, so we can't verify task states against @freezer
- * state here. See freezer_attach() for details.
+ * migrated into or out of @cgroup, so we can't verify task states against
+ * @freezer state here. See freezer_attach() for details.
*/
static void update_if_frozen(struct cgroup *cgroup, struct freezer *freezer)
{
struct freezer *freezer;
enum freezer_state state;
- if (!cgroup_lock_live_group(cgroup))
- return -ENODEV;
-
freezer = cgroup_freezer(cgroup);
spin_lock_irq(&freezer->lock);
update_if_frozen(cgroup, freezer);
state = freezer->state;
spin_unlock_irq(&freezer->lock);
- cgroup_unlock();
seq_puts(m, freezer_state_strs[state]);
seq_putc(m, '\n');
{
struct freezer *freezer = cgroup_freezer(cgroup);
+ /* also synchronizes against task migration, see freezer_attach() */
spin_lock_irq(&freezer->lock);
switch (goal_state) {
else
return -EINVAL;
- if (!cgroup_lock_live_group(cgroup))
- return -ENODEV;
freezer_change_state(cgroup, goal_state);
- cgroup_unlock();
return 0;
}