]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/history - fs
Merge branch 'ti-linux-3.8.y' of git://git.ti.com/ti-linux-kernel/ti-linux-kernel...
[android-sdk/kernel-video.git] / fs /
2013-04-09 Dan MurphyMerge branch 'platform-base-3.8.y' of git://gitorious...
2013-04-09 Felipe BalbiMerge branch 'omap5uevm_uart_pinctrl_dts' of git:/...
2013-04-08 Felipe BalbiMerge tag 'v3.8.6' into connectivity-linux-3.8.y
2013-04-05 Praneeth BajjuriMerge branch 'ti-linux-3.8.y' of git://git.ti.com/ti...
2013-04-05 Dan MurphyMerge branch 'linux-3.8.y' of http://git.kernel.org...
2013-04-05 Dan MurphyMerge branch 'connectivity-linux-3.8.y' of git://gitori...
2013-04-05 Josef BacikBtrfs: fix space leak when we fail to reserve metadata...
2013-04-05 J. Bruce Fieldsnfsd4: reject "negative" acl lengths
2013-04-05 Anatol Pomozovloop: prevent bdev freeing while device in use
2013-04-05 Josef BacikBtrfs: don't drop path when printing out tree errors...
2013-04-05 Josef BacikBtrfs: limit the global reserve to 512mb
2013-04-05 Chris MasonBtrfs: fix race between mmap writes and compression
2013-04-05 Jan SchmidtBtrfs: fix locking on ROOT_REPLACE operations in tree...
2013-04-05 Josef BacikBtrfs: use set_nlink if our i_nlink is 0
2013-04-05 Eric W. Biedermanuserns: Restrict when proc and sysfs can be mounted
2013-04-05 Eric W. Biedermanvfs: Carefully propogate mounts across user namespaces
2013-04-05 Eric W. Biedermanvfs: Add a mount flag to lock read only bind mounts
2013-04-05 Eric W. Biedermanuserns: Don't allow creation if the user is chrooted
2013-04-05 Al ViroNest rename_lock inside vfsmount_lock
2013-04-05 Trond MyklebustNFSv4.1: Always clear the NFS_INO_LAYOUTCOMMIT in layou...
2013-04-05 Trond MyklebustNFSv4.1: Fix a race in pNFS layoutcommit
2013-04-05 Trond MyklebustNFSv4: Fix the string length returned by the idmapper
2013-04-05 fanchaotingpnfs-block: removing DM device maybe cause oops when...
2013-04-05 Ming Leisysfs: handle failure path correctly for readdir()
2013-04-05 Ming Leisysfs: fix race between readdir and lseek
2013-04-05 Dan MurphyMerge branch 'platform-base-3.8.y' of git://gitorious...
2013-03-28 Dan MurphyMerge branch 'linux-3.8.y' of http://git.kernel.org...
2013-03-28 Jan Karaudf: Fix bitmap overflow on large filesystems with...
2013-03-28 Kent Overstreetnfsd: fix bad offset use
2013-03-28 Theodore Ts'oext4: fix data=journal fast mount/umount hang
2013-03-28 Lukas Czernerext4: use s_extent_max_zeroout_kb value as number of kb
2013-03-28 Theodore Ts'oext4: use atomic64_t for the per-flexbg free_clusters...
2013-03-28 Zheng Liuext4: fix the wrong number of the allocated blocks...
2013-03-28 Jan Karajbd2: fix use after free in jbd2_journal_dirty_metadata()
2013-03-28 Jeff Laytoncifs: ignore everything in SPNEGO blob after mechTypes
2013-03-28 Mateusz Guzikcifs: delay super block destruction until all cifsFileI...
2013-03-28 Linus Torvaldsvfs,proc: guarantee unique inodes in /proc
2013-03-28 Al Virosaner proc_get_inode() calling conventions
2013-03-28 Suman AnnaMerge branch 'platform-base-3.8.y' of git://git.ti...
2013-03-28 Dan MurphyMerge branch 'crypto-linux-3.8.y' of git://git.ti.com...
2013-03-28 Dan MurphyMerge branch 'connectivity-linux-3.8.y' of git://gitori...
2013-03-28 Archit TanejaMerge remote-tracking branch 'tero/pm-linux-3.8.y'...
2013-03-27 Tero KristoMerge remote-tracking branch 'thermal/thermal_work...
2013-03-27 Tero KristoMerge remote-tracking branch 'rnayak/platform-base...
2013-03-27 Rajendra NayakMerge tag 'v3.8.4' of git://git.kernel.org/pub/scm...
2013-03-26 Felipe BalbiMerge branch 'platform-base-3.8.y' of git://git.ti...
2013-03-25 Dan MurphyMerge branch 'connectivity-linux-3.8.y' into ti-linux...
2013-03-20 Dan MurphyMerge branch 'linux-3.8.y' into ti-linux-3.8.y
2013-03-20 Guo Chaoblock: use i_size_write() in bd_set_size()
2013-03-20 Eric Sandeenbtrfs: use rcu_barrier() to wait for bdev puts at unmount
2013-03-20 Lars-Peter Clausenext3: Fix format string issues
2013-03-18 Dan MurphyMerge branch 'linux-3.8.y' into ti-linux-3.8.y
2013-03-14 Felipe BalbiMerge branch 'cpsw-3.8.y' of git.ti.com:~mugunthanvnm...
2013-03-14 Al Virovfs: fix pipe counter breakage
2013-03-14 Mathieu DesnoyersFix: compat_rw_copy_check_uvector() misuse in aio,...
2013-03-14 Josef BacikBtrfs: cleanup orphan reservation if truncate fails
2013-03-14 Josef BacikBtrfs: account for orphan inodes properly during cleanup
2013-03-14 Pavel ShilovskyCIFS: Fix missing of oplock_read value in smb30_values...
2013-03-14 Eric W. Biedermanproc: Use nd_jump_link in proc_ns_follow_link
2013-03-14 Linus Torvaldsvfs: don't BUG_ON() if following a /proc fd pseudo...
2013-03-14 Weston Andros AdamsonNFSv4.1: Hold reference to layout hdr in layoutget
2013-03-14 Benny Halevypnfs: fix resend_to_mds for directio
2013-03-14 Trond MyklebustNFS: Don't allow NFS silly-renamed files to be deleted...
2013-03-14 Jeff Laytoncifs: ensure that cifs_get_root() only traverses direct...
2013-03-14 Josef BacikBtrfs: delete inline extents when we find them during...
2013-03-14 Josef BacikBtrfs: copy everything if we've created an inline extent
2013-03-14 Thomas Gleixnerbtrfs: Init io_lock after cloning btrfs device struct
2013-03-14 Lukas Czernerext4: convert number of blocks to clusters properly
2013-03-14 Dan MurphyMerge branch 'omap5_audio_video-3.8.y' into ti-linux...
2013-03-14 Dan MurphyMerge branch 'mailbox-linux-3.8.y' into ti-linux-3.8.y
2013-03-13 Dan MurphyMerge branch 'pm-linux-3.8.y' into ti-linux-3.8.y
2013-03-13 Tero KristoMerge branch 'am33xx-pm-linux-3.8.y' into pm-linux...
2013-03-13 Dan MurphyMerge branch 'platform-base-3.8.y' into ti-linux-3.8.y
2013-03-13 Rajendra NayakMerge branch 'crypto-sham-linux-3.8.y' into platform...
2013-03-13 Rajendra NayakMerge branch 'crypto-aes-linux-3.8.y' into platform...
2013-03-13 Rajendra NayakMerge branch 'crypto-hwmod-linux-3.8.y' into platform...
2013-03-12 Felipe BalbiMerge branch 'usbhost-omap5-3.8-y' of gitorious.ti...
2013-03-07 Dan MurphyMerge branch 'mailbox-linux-3.8.y' into ti-linux-3.8.y a
2013-03-05 Dan MurphyMerge branch 'omap5_audio_video-3.8.y' into ti-linux...
2013-03-05 Dan MurphyMerge branch 'platform-base-3.8.y' into ti-linux-3.8.y
2013-03-05 Felipe BalbiMerge branch 'omap5-sata-mmc-3.8-dt-fix' of git://gitor...
2013-03-05 Felipe BalbiMerge tag 'v3.8.2' into connectivity-linux-3.8.y
2013-03-05 Felipe BalbiMerge tag 'v3.8.1' into connectivity-linux-3.8.y
2013-03-04 Dan MurphyMerge branch 'linux-3.8.y' into ti-linux-3.8.y
2013-03-04 Felipe BalbiMerge branch 'for-linville' of git://git.kernel.org...
2013-03-03 Dave Chinnerxfs: xfs_bmap_add_attrfork_local is too generic
2013-03-03 Seiji Aguchipstore: Avoid deadlock in panic and emergency-restart...
2013-03-03 Miklos Szeredifuse: don't WARN when nlink is zero
2013-03-03 majianpengnfsd: Fix memleak
2013-03-03 Lukas Czernerext4: fix free clusters calculation in bigalloc filesystem
2013-03-03 Lukas Czernerext4: fix xattr block allocation/release with bigalloc
2013-03-03 Niu Yaweiext4: fix race in ext4_mb_add_n_trim()
2013-03-03 Theodore Ts'oext4: release sysfs kobject when failing to enable...
2013-03-03 Eryu Guanext4: check bh in ext4_read_block_bitmap()
2013-03-03 Theodore Ts'oext4: return ENOMEM if sb_getblk() fails
2013-03-03 Jan Karaext4: fix possible use-after-free with AIO
2013-03-03 Jan Karafs: Fix possible use-after-free with AIO
2013-03-03 Xiaowei.Huocfs2: ac->ac_allow_chain_relink=0 won't disable group...
2013-03-03 Jeff Liuocfs2: fix ocfs2_init_security_and_acl() to initialize...
2013-03-03 Jan Karaocfs2: fix possible use-after-free with AIO
next