Merge branch 'p-ti-android-3.8.y-video'
Merge branch 'ion' into p-ti-android-3.8.y-video
This contains the ION cleanup series and caching changes
* ion:
gpu: ion: add support for more cache operations
gpu: ion: DRA7: ensure TILER 2d mappings are shared device
ARM: dts: DRA7/OMAP5: reserve carveout buffers & fix carveout size
gpu: ion: fix omap_ion_share_fd_to_buffers api
gpu: ion: omap: add checks for carveout addresses and sizes
gpu: ion: omap: Fix TILER secure heap base address
gpu: ion: omap: re-populate flags parameters into buffer
Signed-off-by: Sundar Raman <a0393242@ti.com>
This contains the ION cleanup series and caching changes
* ion:
gpu: ion: add support for more cache operations
gpu: ion: DRA7: ensure TILER 2d mappings are shared device
ARM: dts: DRA7/OMAP5: reserve carveout buffers & fix carveout size
gpu: ion: fix omap_ion_share_fd_to_buffers api
gpu: ion: omap: add checks for carveout addresses and sizes
gpu: ion: omap: Fix TILER secure heap base address
gpu: ion: omap: re-populate flags parameters into buffer
Signed-off-by: Sundar Raman <a0393242@ti.com>
Merge branch 'p-ti-android-3.8.y-video'
gpu: ion: add support for more cache operations
Enhance ion_sync_for_device to take in cache direction
Change-Id: I78bef9c2b5cc461b5f49c6019d031a15ce1a36de
Signed-off-by: Sundar Raman <a0393242@ti.com>
Enhance ion_sync_for_device to take in cache direction
Change-Id: I78bef9c2b5cc461b5f49c6019d031a15ce1a36de
Signed-off-by: Sundar Raman <a0393242@ti.com>
gpu: ion: DRA7: ensure TILER 2d mappings are shared device
Write combined mappings are not supported for TILER 2D on DRA7
similar to OMAP5 due to h/w issue. So, shared mappings should
be used. Added the check which was missing for DRA7.
Change-Id: I8ba9bd676f2942dd6a8bd5737bab8e25c8f1cbd3
Signed-off-by: Sundar Raman <a0393242@ti.com>
Write combined mappings are not supported for TILER 2D on DRA7
similar to OMAP5 due to h/w issue. So, shared mappings should
be used. Added the check which was missing for DRA7.
Change-Id: I8ba9bd676f2942dd6a8bd5737bab8e25c8f1cbd3
Signed-off-by: Sundar Raman <a0393242@ti.com>
ARM: dts: DRA7/OMAP5: reserve carveout buffers & fix carveout size
Carveout buffers were initialized but not reserved for
DRA7. This patch adds the missing memreserves without
which there could be data corruption in highmem region.
In addition, the carveout size for TILER secure heap was programmed
wrongly to 96MB whereas it should have been 81 MB. This patch
fixes this and re-adjusts the carveout base addresses.
Change-Id: I151bd37f089aa7fbf590035ea4f612f1da12f53a
Signed-off-by: Sundar Raman <a0393242@ti.com>
Carveout buffers were initialized but not reserved for
DRA7. This patch adds the missing memreserves without
which there could be data corruption in highmem region.
In addition, the carveout size for TILER secure heap was programmed
wrongly to 96MB whereas it should have been 81 MB. This patch
fixes this and re-adjusts the carveout base addresses.
Change-Id: I151bd37f089aa7fbf590035ea4f612f1da12f53a
Signed-off-by: Sundar Raman <a0393242@ti.com>
gpu: ion: fix omap_ion_share_fd_to_buffers api
the output value from ion_share_dma_buf is a dma buf fd
buffers array was filled mistakenly as the code was ported
from k3.4 where the equivalent function ion_share used to
return pointer to ion_buffer. updated the code to upref
using ion_share_dma_buf() and get the handle to buffer using
ion_handle_buffer().
Change-Id: I3bb39f918a9dde8ee78ffa3adcab447589295fdf
Signed-off-by: Sundar Raman <a0393242@ti.com>
the output value from ion_share_dma_buf is a dma buf fd
buffers array was filled mistakenly as the code was ported
from k3.4 where the equivalent function ion_share used to
return pointer to ion_buffer. updated the code to upref
using ion_share_dma_buf() and get the handle to buffer using
ion_handle_buffer().
Change-Id: I3bb39f918a9dde8ee78ffa3adcab447589295fdf
Signed-off-by: Sundar Raman <a0393242@ti.com>
gpu: ion: omap: add checks for carveout addresses and sizes
This patch adds sanity checks on the carveout and size parameters
read from the device tree file and returns error. It also checks
if the device tree is populated and returns error accordingly.
Change-Id: Ic1f4e9d7c5f7e9361d9fe922544f9dbc105d99c3
Signed-off-by: Sundar Raman <a0393242@ti.com>
This patch adds sanity checks on the carveout and size parameters
read from the device tree file and returns error. It also checks
if the device tree is populated and returns error accordingly.
Change-Id: Ic1f4e9d7c5f7e9361d9fe922544f9dbc105d99c3
Signed-off-by: Sundar Raman <a0393242@ti.com>
gpu: ion: omap: Fix TILER secure heap base address
Access to ION TILER buffers were resulting in data aborts
because of incorrect heap base address initialization.
The omap_ion_heap_tiler_base variable was not being
initialized. With this patch the ION tests pass.
Change-Id: Ic072767a5b70b1eab37caf0a7fadb96f1da97b34
Signed-off-by: Sundar Raman <a0393242@ti.com>
Access to ION TILER buffers were resulting in data aborts
because of incorrect heap base address initialization.
The omap_ion_heap_tiler_base variable was not being
initialized. With this patch the ION tests pass.
Change-Id: Ic072767a5b70b1eab37caf0a7fadb96f1da97b34
Signed-off-by: Sundar Raman <a0393242@ti.com>
gpu: ion: omap: re-populate flags parameters into buffer
Since the flags function param of omap_tiler_heap_allocate
is used to pass the omap_tiler_info struct, pass the
actual flags param from the client inside omap_tiler_info
struct and re-populate it into the buffer struct.
Change-Id: I06f3b6125c2760f7b4bcc7f174458139d80ec000
Signed-off-by: Sundar Raman <a0393242@ti.com>
Since the flags function param of omap_tiler_heap_allocate
is used to pass the omap_tiler_info struct, pass the
actual flags param from the client inside omap_tiler_info
struct and re-populate it into the buffer struct.
Change-Id: I06f3b6125c2760f7b4bcc7f174458139d80ec000
Signed-off-by: Sundar Raman <a0393242@ti.com>
Merge branch 'p-ti-android-3.8.y-video' of git://git.ti.com/android-sdk/kernel-video into p-ti-android-3.8.y
* 'p-ti-android-3.8.y-video' of git://git.ti.com/android-sdk/kernel-video:
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
gc320: gcx: [WA] Allocate MMU page tables as non cached
gc320: Added missing programming of MTLB base second time
gc320: Increase VRAM buffers to 4
gc320: adding gcxxx support in Makefiles
gc320: Adapt GC320 driver for K3.8
devices: Initialize GC320 as part of devices init
platform_data: Added platform data for GC320
gc320: OMAP4: Adding cache-2dmanager
Change-Id: I7b240582c78cb9ba0c5d77e56ab0cf06d29a64a4
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* 'p-ti-android-3.8.y-video' of git://git.ti.com/android-sdk/kernel-video:
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
gc320: gcx: [WA] Allocate MMU page tables as non cached
gc320: Added missing programming of MTLB base second time
gc320: Increase VRAM buffers to 4
gc320: adding gcxxx support in Makefiles
gc320: Adapt GC320 driver for K3.8
devices: Initialize GC320 as part of devices init
platform_data: Added platform data for GC320
gc320: OMAP4: Adding cache-2dmanager
Change-Id: I7b240582c78cb9ba0c5d77e56ab0cf06d29a64a4
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Merge remote-tracking branch 'origin/omaplfb' into p-ti-android-3.8.y-video
This contains GC320 series
* origin/omaplfb:
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
gc320: gcx: [WA] Allocate MMU page tables as non cached
gc320: Added missing programming of MTLB base second time
gc320: Increase VRAM buffers to 4
gc320: adding gcxxx support in Makefiles
gc320: Adapt GC320 driver for K3.8
devices: Initialize GC320 as part of devices init
platform_data: Added platform data for GC320
gc320: OMAP4: Adding cache-2dmanager
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
This contains GC320 series
* origin/omaplfb:
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
gc320: gcx: [WA] Allocate MMU page tables as non cached
gc320: Added missing programming of MTLB base second time
gc320: Increase VRAM buffers to 4
gc320: adding gcxxx support in Makefiles
gc320: Adapt GC320 driver for K3.8
devices: Initialize GC320 as part of devices init
platform_data: Added platform data for GC320
gc320: OMAP4: Adding cache-2dmanager
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
This is required so that the omap_hwmod_get_mpu_rt_va()
api returns a virtual register base address for the IP.
Change-Id: I29aff07f34653c552b3eac3a1ac3f10e36b7efbb
Signed-off-by: Sundar Raman <a0393242@ti.com>
This is required so that the omap_hwmod_get_mpu_rt_va()
api returns a virtual register base address for the IP.
Change-Id: I29aff07f34653c552b3eac3a1ac3f10e36b7efbb
Signed-off-by: Sundar Raman <a0393242@ti.com>
Merge branch 'p-ti-android-3.8.y-video'
Merge branch 'p-ti-linux-3.8.y-video'
Merge branch 'omaplfb' into p-ti-android-3.8.y-video
Enabled GC320 as of this commit on J6 EVM and validated via HWC
Need to cherrypick http://review.omapzoom.org/#/c/33221/7
in addition.
Enabled GC320 as of this commit on J6 EVM and validated via HWC
Need to cherrypick http://review.omapzoom.org/#/c/33221/7
in addition.
gc320: gcx: [WA] Allocate MMU page tables as non cached
In K3.8, the cache flushing APIs for the MMU page tables are not
working correctly. Changed the allocations to non cached to
workaround the problem until the correct root cause is found.
Change-Id: Id87497b86d3d93941926f4fc417a4f8d81a5d570
Signed-off-by: Sundar Raman <a0393242@ti.com>
In K3.8, the cache flushing APIs for the MMU page tables are not
working correctly. Changed the allocations to non cached to
workaround the problem until the correct root cause is found.
Change-Id: Id87497b86d3d93941926f4fc417a4f8d81a5d570
Signed-off-by: Sundar Raman <a0393242@ti.com>
gc320: Added missing programming of MTLB base second time
This patch fixes a crash when running the bvtest test case
second time around. The MTLB base address was not programmed
second time around leading to a bad MMU state. This patch
ensures that the MTLB base is programmed correctly.
Change-Id: Iab33425bc61c1e1618c78bdb17f64cbb9d7b4309
Signed-off-by: Alexei Shlychkov <shlychkov@gmail.com>
Signed-off-by: Sundar Raman <a0393242@ti.com>
This patch fixes a crash when running the bvtest test case
second time around. The MTLB base address was not programmed
second time around leading to a bad MMU state. This patch
ensures that the MTLB base is programmed correctly.
Change-Id: Iab33425bc61c1e1618c78bdb17f64cbb9d7b4309
Signed-off-by: Alexei Shlychkov <shlychkov@gmail.com>
Signed-off-by: Sundar Raman <a0393242@ti.com>
gc320: Increase VRAM buffers to 4
With GC320 driver integrated and LCD/HDMI output using VRAM buffers
for SGX composition, it is necessary to increase the number of VRAM
buffers to 4 inorder to allow GC320 to use 2 buffers for composition
output.
Change-Id: I2a481ab9c5c16cd26ac5635b543f41e8c5929fdf
Signed-off-by: Sundar Raman <a0393242@ti.com>
With GC320 driver integrated and LCD/HDMI output using VRAM buffers
for SGX composition, it is necessary to increase the number of VRAM
buffers to 4 inorder to allow GC320 to use 2 buffers for composition
output.
Change-Id: I2a481ab9c5c16cd26ac5635b543f41e8c5929fdf
Signed-off-by: Sundar Raman <a0393242@ti.com>
gc320: adding gcxxx support in Makefiles
Ported from k3.0, commit Id 6c14dfc5c011ce3
[ David Sin <davidsin@ti.com> ]
Change-Id: Ie3b211ff273c9257b596560b6260058466152b35
Signed-off-by: Volodymyr Mieshkov <volodymyr.mieshkov@ti.com>
Signed-off-by: Sundar Raman <sunds@ti.com>
Ported from k3.0, commit Id 6c14dfc5c011ce3
[ David Sin <davidsin@ti.com> ]
Change-Id: Ie3b211ff273c9257b596560b6260058466152b35
Signed-off-by: Volodymyr Mieshkov <volodymyr.mieshkov@ti.com>
Signed-off-by: Sundar Raman <sunds@ti.com>
gc320: Adapt GC320 driver for K3.8
Modified SOC checks and a few other minor changes.
Change-Id: I426c2f017bea0384c7602dd50c0b558329d79b1a
Signed-off-by: Sundar Raman <a0393242@ti.com>
Modified SOC checks and a few other minor changes.
Change-Id: I426c2f017bea0384c7602dd50c0b558329d79b1a
Signed-off-by: Sundar Raman <a0393242@ti.com>
devices: Initialize GC320 as part of devices init
With K3.8, devices.c is used to initialize platform
devices. Added GC320 initialization here so that it is
done as part of bootup.
Change-Id: I45d3e3b18fb4b419f7a5aabfa7cea54460ffe46a
Signed-off-by: Sundar Raman <a0393242@ti.com>
With K3.8, devices.c is used to initialize platform
devices. Added GC320 initialization here so that it is
done as part of bootup.
Change-Id: I45d3e3b18fb4b419f7a5aabfa7cea54460ffe46a
Signed-off-by: Sundar Raman <a0393242@ti.com>
platform_data: Added platform data for GC320
The omap_gcx.h file which contains platform specific
structures for gc320 IP is being added as part of this
patch
Change-Id: I4889333139bb8cd3724ec99ad3e108952e585ed1
Signed-off-by: Sundar Raman <a0393242@ti.com>
The omap_gcx.h file which contains platform specific
structures for gc320 IP is being added as part of this
patch
Change-Id: I4889333139bb8cd3724ec99ad3e108952e585ed1
Signed-off-by: Sundar Raman <a0393242@ti.com>
gc320: OMAP4: Adding cache-2dmanager
Based on k3.0 commit:
p-android-omap-3.0: 43eb373199a [Jack Yen <jyen@ti.com>]
Change-Id: I7e43de75a20a1cead49e902a7fedad9d4f568855
Signed-off-by: Jack Yen <jyen@ti.com>
Signed-off-by: Volodymyr Mieshkov <volodymyr.mieshkov@ti.com>
Signed-off-by: Sundar Raman <sunds@ti.com>
Based on k3.0 commit:
p-android-omap-3.0: 43eb373199a [Jack Yen <jyen@ti.com>]
Change-Id: I7e43de75a20a1cead49e902a7fedad9d4f568855
Signed-off-by: Jack Yen <jyen@ti.com>
Signed-off-by: Volodymyr Mieshkov <volodymyr.mieshkov@ti.com>
Signed-off-by: Sundar Raman <sunds@ti.com>
OMAP: cdm data: Use sw sleep/wkup instead of hw_auto for dss
With hw_auto we are getting unpredictable lock ups with BB2D
enabled.
Change-Id: I391d4e12d9472239b1843670c684c2e7b15a6569
Signed-off-by: Sundar Raman <a0393242@ti.com>
With hw_auto we are getting unpredictable lock ups with BB2D
enabled.
Change-Id: I391d4e12d9472239b1843670c684c2e7b15a6569
Signed-off-by: Sundar Raman <a0393242@ti.com>
ARM: OMAP5/DRA7: hwmod: add ADDR_TYPE_RT to bb2d address flags
This is required so that the omap_hwmod_get_mpu_rt_va()
api returns a virtual register base address for the IP.
Change-Id: I29aff07f34653c552b3eac3a1ac3f10e36b7efbb
Signed-off-by: Sundar Raman <a0393242@ti.com>
This is required so that the omap_hwmod_get_mpu_rt_va()
api returns a virtual register base address for the IP.
Change-Id: I29aff07f34653c552b3eac3a1ac3f10e36b7efbb
Signed-off-by: Sundar Raman <a0393242@ti.com>
Merge remote-tracking branch 'omapzoom/p-ti-android-3.8.y' into p-ti-android-3.8.y-video
defconfig: android: Enable dra7-evm sound support
Enable ALSA and dra7-evm sound support as built-in features.
Change-Id: Ia3576d802f9445870e2b4cb257fa2862df47e0a7
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Enable ALSA and dra7-evm sound support as built-in features.
Change-Id: Ia3576d802f9445870e2b4cb257fa2862df47e0a7
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y:
ARM: OMAP: omap2plus_defconfig: disable USB debug flags
ARM: omap2plus_defconfig: Enable dra7-evm sound support
Change-Id: I45384b836e98f8b8a5ef44fd215ee664e84303bf
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y:
ARM: OMAP: omap2plus_defconfig: disable USB debug flags
ARM: omap2plus_defconfig: Enable dra7-evm sound support
Change-Id: I45384b836e98f8b8a5ef44fd215ee664e84303bf
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
ARM: OMAP: omap2plus_defconfig: disable USB debug flags
Disable USB debug flags from omap2plus_defconfig
Change-Id: Icfa01952faae6992d5bfc97ce8ae27f79f977e3c
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
Disable USB debug flags from omap2plus_defconfig
Change-Id: Icfa01952faae6992d5bfc97ce8ae27f79f977e3c
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
ARM: omap2plus_defconfig: Enable dra7-evm sound support
Enable ALSA and dra7-evm sound support as built-in features.
Change-Id: I3d00f20e7aeeee3a6d298183969de21e32d264b8
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Enable ALSA and dra7-evm sound support as built-in features.
Change-Id: I3d00f20e7aeeee3a6d298183969de21e32d264b8
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
defconfig: android: disable USB debug flag
Disabling USB debug flag from android defconfig
Change-Id: I4e869c4aa44ae11815808991c05a7fe3295aa8aa
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
Disabling USB debug flag from android defconfig
Change-Id: I4e869c4aa44ae11815808991c05a7fe3295aa8aa
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y: (30 commits)
ARM: dts: dra7-evm: Add HDMI sound node
OMAPDSS: HDMI: Fix GPA Channel Setting and Channel Allocation for 6-Channels
OMAPDSS: OMAP5: HDMI: Audio InfoFrame DB1 field offsets
ASoC: omap-hdmi-card: Remove redundant print
ARM: DRA7: hwmod: Fix HDMI irq number
ARM: DRA7: clocks: Fix HDMI sys_clk mux register
ASoC: DRA7: dra7-evm: HACK: Set McASP DMA reqs in sDMA crossbar
ARM: dts: dra7-evm: Add sound card node
ARM: dts: dra7: Add ATL node
ARM: dts: dra7: Add McASP nodes
ARM: dts: dra7-evm: Add audio pinctrl
ASoC: DRA7: dra7-evm: Add initial support for DRA7 EVM
ASoC: DRA7: atl: Add initial support for Audio Tracking Logic
ARM: DRA7: clocks: Append _ck to atl_clkin* and ref_clkin*
ARM: DRA7: clock: Fix the wrong ABE PLL lock frequency
ARM: DRA7: hwmod: Disable smart-idle for McASP
ASoC: davinci-mcasp: Add hw_rule for buffer_size when using AFIFO
ASoC: davinci-mcasp: Add support for using McASP DATA port
ASoC: davinci-mcasp: HACK: Add MCASP_VERSION_4 support
ASoC: davinci-mcasp: Add support for 1-channel
...
Conflicts:
arch/arm/boot/dts/dra7-evm.dts
Change-Id: I6134724d21801c94afeae8fb369f171bae901db6
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y: (30 commits)
ARM: dts: dra7-evm: Add HDMI sound node
OMAPDSS: HDMI: Fix GPA Channel Setting and Channel Allocation for 6-Channels
OMAPDSS: OMAP5: HDMI: Audio InfoFrame DB1 field offsets
ASoC: omap-hdmi-card: Remove redundant print
ARM: DRA7: hwmod: Fix HDMI irq number
ARM: DRA7: clocks: Fix HDMI sys_clk mux register
ASoC: DRA7: dra7-evm: HACK: Set McASP DMA reqs in sDMA crossbar
ARM: dts: dra7-evm: Add sound card node
ARM: dts: dra7: Add ATL node
ARM: dts: dra7: Add McASP nodes
ARM: dts: dra7-evm: Add audio pinctrl
ASoC: DRA7: dra7-evm: Add initial support for DRA7 EVM
ASoC: DRA7: atl: Add initial support for Audio Tracking Logic
ARM: DRA7: clocks: Append _ck to atl_clkin* and ref_clkin*
ARM: DRA7: clock: Fix the wrong ABE PLL lock frequency
ARM: DRA7: hwmod: Disable smart-idle for McASP
ASoC: davinci-mcasp: Add hw_rule for buffer_size when using AFIFO
ASoC: davinci-mcasp: Add support for using McASP DATA port
ASoC: davinci-mcasp: HACK: Add MCASP_VERSION_4 support
ASoC: davinci-mcasp: Add support for 1-channel
...
Conflicts:
arch/arm/boot/dts/dra7-evm.dts
Change-Id: I6134724d21801c94afeae8fb369f171bae901db6
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
ARM: dts: dra7-evm: Add HDMI sound node
Add HDMI audio node.
Change-Id: I220e56b5a45716a7f7d6bd0b32df102f16746d16
Signed-off-by: Dandawate Saket <dsaket@ti.com>
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Add HDMI audio node.
Change-Id: I220e56b5a45716a7f7d6bd0b32df102f16746d16
Signed-off-by: Dandawate Saket <dsaket@ti.com>
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
OMAPDSS: HDMI: Fix GPA Channel Setting and Channel Allocation for 6-Channels
Enable channels 0 to 5 in GPA configuration (GP_CONF1) for the
6 channels case. This fixes an issue where the Audio Sample Packet
was carrying 8 channels instead of 6 channels.
The new GPA configuration sets the sample_present.sp3 bit to 0, then
0x13 is not a valid channel allocation. So, the channel allocation is
set to a valid value (0xb), when the number of channels is 6.
Also a typo is fixed in the comments for the eight channel case.
Change-Id: I3c987a4efdaf9f9594c99dc1fca1470b53a59355
Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
Enable channels 0 to 5 in GPA configuration (GP_CONF1) for the
6 channels case. This fixes an issue where the Audio Sample Packet
was carrying 8 channels instead of 6 channels.
The new GPA configuration sets the sample_present.sp3 bit to 0, then
0x13 is not a valid channel allocation. So, the channel allocation is
set to a valid value (0xb), when the number of channels is 6.
Also a typo is fixed in the comments for the eight channel case.
Change-Id: I3c987a4efdaf9f9594c99dc1fca1470b53a59355
Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
OMAPDSS: OMAP5: HDMI: Audio InfoFrame DB1 field offsets
CHNL_COUNT is in bits 6:4 and CODING_TYPE in bits 3:0 of HDMI_CORE_FC_AUDICONF0
register, while in the CEA-861 definition DB1CC is in bits 2:0 and DB1CT in
bits 7:4.
Change-Id: Ifd6ca2c91209b7fcf31dfdc921707c0ad5c9378a
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
CHNL_COUNT is in bits 6:4 and CODING_TYPE in bits 3:0 of HDMI_CORE_FC_AUDICONF0
register, while in the CEA-861 definition DB1CC is in bits 2:0 and DB1CT in
bits 7:4.
Change-Id: Ifd6ca2c91209b7fcf31dfdc921707c0ad5c9378a
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: omap-hdmi-card: Remove redundant print
HDMI card name is already printed when card is registered in ALSA,
no need to print it again.
Change-Id: I4bbe1acc45ab647a6a28824f3cb86a14163ba054
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
HDMI card name is already printed when card is registered in ALSA,
no need to print it again.
Change-Id: I4bbe1acc45ab647a6a28824f3cb86a14163ba054
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: DRA7: hwmod: Fix HDMI irq number
HDMI_IRQ is connected to IRQ_CROSSBAR_96 in DRA7, previous IRQ number
was for OMAP5.
Change-Id: Iedff41b2e2dc253be7f6aa8a18c0c0d23a7f989d
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
HDMI_IRQ is connected to IRQ_CROSSBAR_96 in DRA7, previous IRQ number
was for OMAP5.
Change-Id: Iedff41b2e2dc253be7f6aa8a18c0c0d23a7f989d
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: DRA7: clocks: Fix HDMI sys_clk mux register
HDMI sys_clk mux uses CM_CLKSEL_HDMI_PLL_SYS register for source
selection.
Change-Id: I3c762b2ff4e845978b69482ec3422dcbc736e49c
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
HDMI sys_clk mux uses CM_CLKSEL_HDMI_PLL_SYS register for source
selection.
Change-Id: I3c762b2ff4e845978b69482ec3422dcbc736e49c
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: DRA7: dra7-evm: HACK: Set McASP DMA reqs in sDMA crossbar
McASP3 and McASP6 don't have default DMA reqs assigned in sDMA
crossbar. In the meantime, McASP3 TX/RX DMA reqs are reassigned
to sDMA_78 and 79, and McASP6 TX/RX to sDMA_62 and 63.
Change-Id: I079e181cfeccd12a121ea3f864bd8905609d09ad
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
McASP3 and McASP6 don't have default DMA reqs assigned in sDMA
crossbar. In the meantime, McASP3 TX/RX DMA reqs are reassigned
to sDMA_78 and 79, and McASP6 TX/RX to sDMA_62 and 63.
Change-Id: I079e181cfeccd12a121ea3f864bd8905609d09ad
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: dts: dra7-evm: Add sound card node
Add node for McASP-based sound card which consists of the media
DAI link that connects McASP3 and tlv320aic3106. This DAI link
in I2S mode with a bit clock of 5.6448 MHz that allows 44.1kHz,
16-bits/sample.
Change-Id: I46aaa94a68c6b3c89069b9030edf96d57d2476ef
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Add node for McASP-based sound card which consists of the media
DAI link that connects McASP3 and tlv320aic3106. This DAI link
in I2S mode with a bit clock of 5.6448 MHz that allows 44.1kHz,
16-bits/sample.
Change-Id: I46aaa94a68c6b3c89069b9030edf96d57d2476ef
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: dts: dra7: Add ATL node
ATL1 and ATL2 are the only instances enabled. ATL1 is used to supply
the audio clock for the 16-slots TDM DAI link, so it requires an output
freq of 11.2896 MHz. ATL2 is used for the I2S DAI link and is configured
to 5.6448 MHz.
Change-Id: I4cf5ed86e75aa517e1ab3dbb3de8e9227013311b
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ATL1 and ATL2 are the only instances enabled. ATL1 is used to supply
the audio clock for the 16-slots TDM DAI link, so it requires an output
freq of 11.2896 MHz. ATL2 is used for the I2S DAI link and is configured
to 5.6448 MHz.
Change-Id: I4cf5ed86e75aa517e1ab3dbb3de8e9227013311b
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: dts: dra7: Add McASP nodes
McASP3 is configured in I2S mode with AXR0 as TX and AXR1 as RX.
McASP6 is configured in TDM mode (uses same op-mode property value
than I2S) with 8-slots, AXR0 is used for TX and AXR1 for RX.
Interrupt property in both nodes is using McASP1's in the meantime
since McASP3 and McASP6 don't have default interrupt lines and have
to be assigned through IRQ crossbar.
Change-Id: I766dcbea9190083c6fe0e01501104226d480a22f
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
McASP3 is configured in I2S mode with AXR0 as TX and AXR1 as RX.
McASP6 is configured in TDM mode (uses same op-mode property value
than I2S) with 8-slots, AXR0 is used for TX and AXR1 for RX.
Interrupt property in both nodes is using McASP1's in the meantime
since McASP3 and McASP6 don't have default interrupt lines and have
to be assigned through IRQ crossbar.
Change-Id: I766dcbea9190083c6fe0e01501104226d480a22f
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: dts: dra7-evm: Add audio pinctrl
Add pinctrl entries for McASP3, McASP6 and ATL. McASP pins are
configured so that McASPs are masters in their corresponding
audio links.
Change-Id: I507ad5941cf679a4afab98fcca7cbeba5fe5cad8
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Add pinctrl entries for McASP3, McASP6 and ATL. McASP pins are
configured so that McASPs are masters in their corresponding
audio links.
Change-Id: I507ad5941cf679a4afab98fcca7cbeba5fe5cad8
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: DRA7: dra7-evm: Add initial support for DRA7 EVM
Add initial support for DRA7 EVM, it includes the media DAI link that
connects McASP3 and tlv320aic3106 in I2S mode.
DRA7xx is a high-performance, infotainment application device, based on
enhanced OMAP architecture integrated on a 28-nm technology.
Change-Id: I3be3e94e2f9c5736f236e965297d3cb9d646c7fc
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Add initial support for DRA7 EVM, it includes the media DAI link that
connects McASP3 and tlv320aic3106 in I2S mode.
DRA7xx is a high-performance, infotainment application device, based on
enhanced OMAP architecture integrated on a 28-nm technology.
Change-Id: I3be3e94e2f9c5736f236e965297d3cb9d646c7fc
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: DRA7: atl: Add initial support for Audio Tracking Logic
Add initial version of Audio Tracking Logic (ATL) driver. ATL is
used to synchronize the digital audio output to the baseband clock.
ATL produces a timing signal at the top of the audio clock tree.
Change-Id: I123ff440b8e478c12e28ff4db42d1196f0ae4f6b
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Add initial version of Audio Tracking Logic (ATL) driver. ATL is
used to synchronize the digital audio output to the baseband clock.
ATL produces a timing signal at the top of the audio clock tree.
Change-Id: I123ff440b8e478c12e28ff4db42d1196f0ae4f6b
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: DRA7: clocks: Append _ck to atl_clkin* and ref_clkin*
Suffix 'ck' is missing for 'atl_clkin*' and 'ref_clkin*' clocks in
mcasp and timer parent clock names list.
Fix also a missing "_" in 'atl_clkin3_ck'.
Change-Id: I0d1ced5c61b08c63577872a38b16390f506c9cba
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Suffix 'ck' is missing for 'atl_clkin*' and 'ref_clkin*' clocks in
mcasp and timer parent clock names list.
Fix also a missing "_" in 'atl_clkin3_ck'.
Change-Id: I0d1ced5c61b08c63577872a38b16390f506c9cba
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ARM: DRA7: clock: Fix the wrong ABE PLL lock frequency
The ABE PLL (used by ATL) was wrongly locked at twice the frequency.
Fix it and also set the dpll_abe_m2x2_ck rate explicitely so that we
have m2 set to 1.
Change-Id: I5efc593c46ee7b31f06326b361a85f27dd3310ec
Signed-off-by: Rajendra Nayak <rnayak@ti.com>
The ABE PLL (used by ATL) was wrongly locked at twice the frequency.
Fix it and also set the dpll_abe_m2x2_ck rate explicitely so that we
have m2 set to 1.
Change-Id: I5efc593c46ee7b31f06326b361a85f27dd3310ec
Signed-off-by: Rajendra Nayak <rnayak@ti.com>
ARM: DRA7: hwmod: Disable smart-idle for McASP
As per TRM, wakeup schema is not supported by McASP, so it's recommended to
use no-idle after McASP is enabled, and smart-idle after it's disabled.
Change-Id: Ia20eff9238b996dbcac4b534b4645ec93fd8bafb
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
As per TRM, wakeup schema is not supported by McASP, so it's recommended to
use no-idle after McASP is enabled, and smart-idle after it's disabled.
Change-Id: Ia20eff9238b996dbcac4b534b4645ec93fd8bafb
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Add hw_rule for buffer_size when using AFIFO
The AFIFO threshold imposes a limiation on the buffer size.
When the AFIFO is used, the buffer size (in samples) needs to be
an integer multiple of the AFIFO threshold value (wnumevt, rnumevt).
This patch adds a hw_rule to the McASP driver for version 4
of the McASP to account for the limitation on the buffer size.
Change-Id: I3bd320130b10a55d3d84defd99572526ad6469fb
Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
The AFIFO threshold imposes a limiation on the buffer size.
When the AFIFO is used, the buffer size (in samples) needs to be
an integer multiple of the AFIFO threshold value (wnumevt, rnumevt).
This patch adds a hw_rule to the McASP driver for version 4
of the McASP to account for the limitation on the buffer size.
Change-Id: I3bd320130b10a55d3d84defd99572526ad6469fb
Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
ASoC: davinci-mcasp: Add support for using McASP DATA port
By default the CFG port is used for data transfer. It
is desireable to use the DATA port so that the AFIFO
can be used on DRA7XX.
To enable DATA port usage, during the probe a check for
an IORESOURCE_MEM named "dat" is done. If the
resource is found, the data port will be used. If it is
not found, the driver will fall back to using the cfg
port.
Change-Id: I42c3cc04621354ef1fd7546f9feff003cf6b38ce
Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
By default the CFG port is used for data transfer. It
is desireable to use the DATA port so that the AFIFO
can be used on DRA7XX.
To enable DATA port usage, during the probe a check for
an IORESOURCE_MEM named "dat" is done. If the
resource is found, the data port will be used. If it is
not found, the driver will fall back to using the cfg
port.
Change-Id: I42c3cc04621354ef1fd7546f9feff003cf6b38ce
Signed-off-by: Angela Stegmaier <angelabaker@ti.com>
ASoC: davinci-mcasp: HACK: Add MCASP_VERSION_4 support
McASP IP found in DRA7xx devices is similar to the one described by
VERSION_3 (TI81xx, AM33xx), except that a different DMA mechanism
is used. A new version is introduced to use DMA4 instead (OMAP's).
Long term plan is to keep McASP driver totally agnostic of the DMA
module (sDMA or eDMA).
Change-Id: I47a2fd117b3647a5ed6562cbaa00211cb95dea3a
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
McASP IP found in DRA7xx devices is similar to the one described by
VERSION_3 (TI81xx, AM33xx), except that a different DMA mechanism
is used. A new version is introduced to use DMA4 instead (OMAP's).
Long term plan is to keep McASP driver totally agnostic of the DMA
module (sDMA or eDMA).
Change-Id: I47a2fd117b3647a5ed6562cbaa00211cb95dea3a
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Add support for 1-channel
McASP doesn't support 1-slot TDM mode needed for mono, however mono
can still be achieved by using 2-slots (or more) and transferring data
only in one slot.
Change-Id: Ic8420cf2d6cc1ee9b9c163ab592cfa347a679340
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
McASP doesn't support 1-slot TDM mode needed for mono, however mono
can still be achieved by using 2-slots (or more) and transferring data
only in one slot.
Change-Id: Ic8420cf2d6cc1ee9b9c163ab592cfa347a679340
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Pass pin inactive state via DT
The state of transmit/receive pins during inactive slots can be controlled through
DISMOD. Previously, the default state (Hi-Z) was used all the time, but that might
not fit well for all applications. So, the inactive state is passed via DT:
"tx-inactive-state" and "rx-inactive-state".
The inactive states can actually be set per serializer, but for the sake of simplicity
we only differentiate them by stream direction.
Additionally, the DISMOD macro is also fixed as the argument part was incorrect.
Change-Id: I0e099c29fde94dd59175c1017c098554c43d18fe
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
The state of transmit/receive pins during inactive slots can be controlled through
DISMOD. Previously, the default state (Hi-Z) was used all the time, but that might
not fit well for all applications. So, the inactive state is passed via DT:
"tx-inactive-state" and "rx-inactive-state".
The inactive states can actually be set per serializer, but for the sake of simplicity
we only differentiate them by stream direction.
Additionally, the DISMOD macro is also fixed as the argument part was incorrect.
Change-Id: I0e099c29fde94dd59175c1017c098554c43d18fe
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Wait until TX AFIFO is not empty
Wait until TX AFIFO has at least one audio sample before TXBUF starts
consuming data, otherwise XRUN can be hit immediately at the start of
the stream.
Change-Id: Ie94dcd16f7a00046eb043aec1ceee21ce6009fbc
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Wait until TX AFIFO has at least one audio sample before TXBUF starts
consuming data, otherwise XRUN can be hit immediately at the start of
the stream.
Change-Id: Ie94dcd16f7a00046eb043aec1ceee21ce6009fbc
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Fix receive right-rotation value
Receive right-rotation (RROT) for I2S/TDM falls in the MSB-first,
left-aligned streams whose suggested rotation value is slot size -
word size.
Change-Id: I53ac6a0a9c02cf78cc4a2f37c34b6dbc4f9a0bcc
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Receive right-rotation (RROT) for I2S/TDM falls in the MSB-first,
left-aligned streams whose suggested rotation value is slot size -
word size.
Change-Id: I53ac6a0a9c02cf78cc4a2f37c34b6dbc4f9a0bcc
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Keep TX and RX format symmetric
[TR]XFMT and [TR]XFMTCTL registers are set symmetrically in most
part of the driver, no need to keep it stream direction dependent
only in one place.
Change-Id: I8bacf75c8e5147d086ea67ab8ea5400a6affba99
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
[TR]XFMT and [TR]XFMTCTL registers are set symmetrically in most
part of the driver, no need to keep it stream direction dependent
only in one place.
Change-Id: I8bacf75c8e5147d086ea67ab8ea5400a6affba99
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Enable TX FSG for master mode
McASP is configured by default in synchronous mode so the TX frame sync
is also used for RX. If McASP is also in master mode (for FSYNC), the
transmit FSG needs to be running to provide the frame sync needed for RX.
In some cases, AFSR/ACLKR pins are not even used so AFSX/ACLKX pins have
to be active for RX too, this requires TX clock dividers to be released
from reset.
Change-Id: Iff0b7b93ed2665b7da8219e435fece512c4551e8
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
McASP is configured by default in synchronous mode so the TX frame sync
is also used for RX. If McASP is also in master mode (for FSYNC), the
transmit FSG needs to be running to provide the frame sync needed for RX.
In some cases, AFSR/ACLKR pins are not even used so AFSX/ACLKX pins have
to be active for RX too, this requires TX clock dividers to be released
from reset.
Change-Id: Iff0b7b93ed2665b7da8219e435fece512c4551e8
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Remove unnecesary runtime PM calls
Runtime PM calls in trigger() are not symmetric, this causes that
usage counter always keeps increasing. Similarly, runtime PM calls
in driver probe() and remove() are not needed since ASoC already
takes care of calling the appropriate runtime PM calls as required
during stream lifecycle.
Change-Id: I29ef47d9dce3b21db47b54c50d1c64b2fe82d804
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Runtime PM calls in trigger() are not symmetric, this causes that
usage counter always keeps increasing. Similarly, runtime PM calls
in driver probe() and remove() are not needed since ASoC already
takes care of calling the appropriate runtime PM calls as required
during stream lifecycle.
Change-Id: I29ef47d9dce3b21db47b54c50d1c64b2fe82d804
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Apply symmetry on sample bits
McASP instances with unified clock/sync domain share the same BCLK
and FSYNC for playback and capture, hence the slot size has to be
symmetric.
Change-Id: Ia0bc75f39aeeda05196ed73a393518f88f21a568
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
McASP instances with unified clock/sync domain share the same BCLK
and FSYNC for playback and capture, hence the slot size has to be
symmetric.
Change-Id: Ia0bc75f39aeeda05196ed73a393518f88f21a568
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Active slots depend on active serializers
Active slots count depends on the number of channels in the stream
and the number of active serializers. Each serializer will handle
at most the number of channels specified via 'tdm-slots' parameter
in DT.
There are two possible scenarios:
- Single serializer: channel count fits in the max slots supported by
McASP serializers, active slots is same as channel count
- Multiple serializers: channel count is bigger than max slots supported
by a serializer. Channel count determines how many serializers are
needed at their max slot count configuration
Change-Id: I690a8518a807b70cebdbeb131979d68bfb86e4fe
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Active slots count depends on the number of channels in the stream
and the number of active serializers. Each serializer will handle
at most the number of channels specified via 'tdm-slots' parameter
in DT.
There are two possible scenarios:
- Single serializer: channel count fits in the max slots supported by
McASP serializers, active slots is same as channel count
- Multiple serializers: channel count is bigger than max slots supported
by a serializer. Channel count determines how many serializers are
needed at their max slot count configuration
Change-Id: I690a8518a807b70cebdbeb131979d68bfb86e4fe
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: davinci-mcasp: Simplify channels retrieval
Channels can be extracted using params_channels() macro.
Change-Id: Ia48497cbb6d3b49d6e1ced9f3241d3e0dd4011ea
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
Channels can be extracted using params_channels() macro.
Change-Id: Ia48497cbb6d3b49d6e1ced9f3241d3e0dd4011ea
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
ASoC: omap-pcm: Initialize DMA slave config
OMAP DMA engine driver does parameter checking on src_addr_width and
dst_addr_width which can contain an invalid value if the DMA slave
config struct is not initialized.
Change-Id: I9ce81a7f069be08485d8c105d5430ddd2e398fd5
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
OMAP DMA engine driver does parameter checking on src_addr_width and
dst_addr_width which can contain an invalid value if the DMA slave
config struct is not initialized.
Change-Id: I9ce81a7f069be08485d8c105d5430ddd2e398fd5
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
defconfig: android: enable user space wake lock support
Enable CONFIG_PM_WAKELOCKS in defconfig for user space wakelock
operations using sysfs entries.
Change-Id: I737fb2d258991087cd8bea445fabdb04027ff0e5
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
Enable CONFIG_PM_WAKELOCKS in defconfig for user space wakelock
operations using sysfs entries.
Change-Id: I737fb2d258991087cd8bea445fabdb04027ff0e5
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
Merge remote-tracking branch 'remotes/gitomapzoom/p-ti-android-3.8.y' into p-ti-android-3.8.y-video
android: defconfig: enable android usb flags
Enabling android usb specific flags
Change-Id: I50dee0fa992a7704bad152658194b3f8de2fc69f
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
[Enable the android flags correctly in defconfig]
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Enabling android usb specific flags
Change-Id: I50dee0fa992a7704bad152658194b3f8de2fc69f
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
[Enable the android flags correctly in defconfig]
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
HACK: DRA7xx: usb: dwc3: set mailbox in gadget pullup.
On DRA7xx EVM, there is no vbus sensing. Hence the mailbox is required to
be set when the android gagdet pullup is called.
When the IO expander driver is available and senses vbus, it should write to
the dwc3 mailbox.
Change-Id: I78850c8ab243d4acc94b6327996849d13704802d
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
On DRA7xx EVM, there is no vbus sensing. Hence the mailbox is required to
be set when the android gagdet pullup is called.
When the IO expander driver is available and senses vbus, it should write to
the dwc3 mailbox.
Change-Id: I78850c8ab243d4acc94b6327996849d13704802d
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
android: usb: dwc3: Ensure the OUT request sizes are valid
Backport fix from K3.4.
Refer commit:6170c26e89640f5c38dfc7b3a214f83cb98b9047
usb: gadget: android: fix adb to work with Synopsys UDC
The DWC3 USB device controller requires all OUT transfer request
lengths to be a multiple of max packet size
Refer: commit: 98346f7db
Align with above patch to have bulk-OUT transfer size be
divisible by maxpacket size.
Change-Id: I552d65d58fc5f414be2ddb33ffa37c5f6819373a
Signed-off-by: Vikram Pandita <vikram.pandita@ti.com>
Signed-off-by: Moiz Sonasath <m-sonasath@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Backport fix from K3.4.
Refer commit:6170c26e89640f5c38dfc7b3a214f83cb98b9047
usb: gadget: android: fix adb to work with Synopsys UDC
The DWC3 USB device controller requires all OUT transfer request
lengths to be a multiple of max packet size
Refer: commit: 98346f7db
Align with above patch to have bulk-OUT transfer size be
divisible by maxpacket size.
Change-Id: I552d65d58fc5f414be2ddb33ffa37c5f6819373a
Signed-off-by: Vikram Pandita <vikram.pandita@ti.com>
Signed-off-by: Moiz Sonasath <m-sonasath@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
android: hack: usb: gadget: android: remove audio function
Remove audio function to avoid compilation break.
Change-Id: Iaf4684d8e1b3e8e7b5427f313906940e727aa8cd
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Remove audio function to avoid compilation break.
Change-Id: Iaf4684d8e1b3e8e7b5427f313906940e727aa8cd
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
android: usb: gadget: Allow kernel boot with android gadget.
This patch allows a kernel with android gadget enabled to boot.
Issues fixed:
- Allows the android gadget probe to get deferred if a udc gadget is
unavailable.
- Check added for udc gadget availability first before "any" android
initialization.
Change-Id: If6c46d32a32994367d95a57af1e231beafa7bb8a
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
This patch allows a kernel with android gadget enabled to boot.
Issues fixed:
- Allows the android gadget probe to get deferred if a udc gadget is
unavailable.
- Check added for udc gadget availability first before "any" android
initialization.
Change-Id: If6c46d32a32994367d95a57af1e231beafa7bb8a
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
android: usb: gadget: udc_core: Check for android compile flag.
It is incorrect to comment out usb_gadget_connect() if the android gadget is
not compiled in.
Change-Id: If7f4a7e4f79a0a93aa976605184e3c82e7a71c4e
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
It is incorrect to comment out usb_gadget_connect() if the android gadget is
not compiled in.
Change-Id: If7f4a7e4f79a0a93aa976605184e3c82e7a71c4e
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y:
dra7x: dts: pinctrl: Adding drv1/2_vbus pinctrl config to dra7x DT
usb: dra7x: Enable init rate for dpll usb
dra7xx: usb: dwc: device tree entrees for 2 usb_otg_ss
HACK: usb: dwc3: dwc3 wrapper update for multiple usb subsystems
usb: dwc3-omap: wrapper dwc3_omap_mailbox updated ret val
usb: phy: omap_control_usb: addition of a dummy control register
usb: omap_control_usb: addition of a phy variation.
usb: phy: omap_control_usb: removal of globals
usb: phy: enable phy drivers to use the device node for optional clock names.
usb: dwc3: update the maxpacket based on the maximum_speed
Change-Id: I61c584e5062101924c42e9ee9f01f4cccbfe1381
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y:
dra7x: dts: pinctrl: Adding drv1/2_vbus pinctrl config to dra7x DT
usb: dra7x: Enable init rate for dpll usb
dra7xx: usb: dwc: device tree entrees for 2 usb_otg_ss
HACK: usb: dwc3: dwc3 wrapper update for multiple usb subsystems
usb: dwc3-omap: wrapper dwc3_omap_mailbox updated ret val
usb: phy: omap_control_usb: addition of a dummy control register
usb: omap_control_usb: addition of a phy variation.
usb: phy: omap_control_usb: removal of globals
usb: phy: enable phy drivers to use the device node for optional clock names.
usb: dwc3: update the maxpacket based on the maximum_speed
Change-Id: I61c584e5062101924c42e9ee9f01f4cccbfe1381
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
dra7x: dts: pinctrl: Adding drv1/2_vbus pinctrl config to dra7x DT
Add drv1_vbus pincontrol configuration to dra7-evm dts.
select muxmode 0, and enable drv1_vbus slewctrl and pulldown
Add drvr2_vbus pincontrol configuration to dra7-evm dts.
select muxmode 0, and enable drv1_vbus slewctrl and pulldown
Change-Id: I49135549c92e7860b832a4fcdae15853f1475695
Signed-off-by: Ravi Babu <ravibabu@ti.com>
Signed-off-by: Nikhil Devshatwar <nikhil.nd@ti.com>
Signed-off-by: Somnath Mukherjee <somnath@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Add drv1_vbus pincontrol configuration to dra7-evm dts.
select muxmode 0, and enable drv1_vbus slewctrl and pulldown
Add drvr2_vbus pincontrol configuration to dra7-evm dts.
select muxmode 0, and enable drv1_vbus slewctrl and pulldown
Change-Id: I49135549c92e7860b832a4fcdae15853f1475695
Signed-off-by: Ravi Babu <ravibabu@ti.com>
Signed-off-by: Nikhil Devshatwar <nikhil.nd@ti.com>
Signed-off-by: Somnath Mukherjee <somnath@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: dra7x: Enable init rate for dpll usb
Add init rate fout=960Mhz to configure USB dpll
USB dpll is not locked correctly through the pm runtime
Change-Id: I51feacb546052120eb62be17f4119a7bb46d1c90
Signed-off-by: Nikhil Devshatwar <nikhil.nd@ti.com>
Signed-off-by: Somnath Mukherjee <somnath@ti.com>
Add init rate fout=960Mhz to configure USB dpll
USB dpll is not locked correctly through the pm runtime
Change-Id: I51feacb546052120eb62be17f4119a7bb46d1c90
Signed-off-by: Nikhil Devshatwar <nikhil.nd@ti.com>
Signed-off-by: Somnath Mukherjee <somnath@ti.com>
dra7xx: usb: dwc: device tree entrees for 2 usb_otg_ss
This introduces 2 usb otg subsystems to the dra7xx device tree.
Change-Id: I32df149d262fb527802faf528d7aa506fb883cef
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
This introduces 2 usb otg subsystems to the dra7xx device tree.
Change-Id: I32df149d262fb527802faf528d7aa506fb883cef
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
HACK: usb: dwc3: dwc3 wrapper update for multiple usb subsystems
Allow a separate dma mask per usb_otg_ss instance.
REVISIT: This is based on the name of the node in the device tree and ugly.
Temporary to get DRA7xx going and hardly scalable.
"_omap" global still exists and the only reason his works is because dra7xx
does not use the palmas driver.
Change-Id: Iff9d09e837c1556516c28c42f7a3f41a2315befc
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Allow a separate dma mask per usb_otg_ss instance.
REVISIT: This is based on the name of the node in the device tree and ugly.
Temporary to get DRA7xx going and hardly scalable.
"_omap" global still exists and the only reason his works is because dra7xx
does not use the palmas driver.
Change-Id: Iff9d09e837c1556516c28c42f7a3f41a2315befc
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: dwc3-omap: wrapper dwc3_omap_mailbox updated ret val
Instead of returning IRQ_NONE, it returns a 0 on success.
This allows it to be called if needed from a non irq function routine
nicely.
Change-Id: Ic7db386a91bd6661f686c519d04d57a3c1e0407b
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Instead of returning IRQ_NONE, it returns a 0 on success.
This allows it to be called if needed from a non irq function routine
nicely.
Change-Id: Ic7db386a91bd6661f686c519d04d57a3c1e0407b
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: phy: omap_control_usb: addition of a dummy control register
This patch introduces a "dummy control register" to turn on addition
clocks for phy tpe 3.
Change-Id: I7ed4400e496a92940944637684bb5586f93da713
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
This patch introduces a "dummy control register" to turn on addition
clocks for phy tpe 3.
Change-Id: I7ed4400e496a92940944637684bb5586f93da713
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: omap_control_usb: addition of a phy variation.
Another phy type on dra7xx inspired the addition of a OMAP_CTRL_DEV_TYPE3
type of omap_control_usb system.
This phy is different in 2 ways
- usb2 only
- the power on is in different register with bit definitions dissimilar to
dev_conf.
Change-Id: I39969ea675ff9916aa746b5168784ba99119a54f
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Another phy type on dra7xx inspired the addition of a OMAP_CTRL_DEV_TYPE3
type of omap_control_usb system.
This phy is different in 2 ways
- usb2 only
- the power on is in different register with bit definitions dissimilar to
dev_conf.
Change-Id: I39969ea675ff9916aa746b5168784ba99119a54f
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: phy: omap_control_usb: removal of globals
This patch removes the use of a global omap_control_usb.
This allows
- Multiple instances of the omap_control_usb when required such as in DRA7xx.
- The device node is looked up using the phandle.
Change-Id: Ib5bf866b00f945430c055344d6344d4edfc38882
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
This patch removes the use of a global omap_control_usb.
This allows
- Multiple instances of the omap_control_usb when required such as in DRA7xx.
- The device node is looked up using the phandle.
Change-Id: Ib5bf866b00f945430c055344d6344d4edfc38882
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: phy: enable phy drivers to use the device node for optional clock names.
Allow the device drivers to use the required optional clock names
from the DT node data.This allows scalability when multiple usb_otg_ss
instances are in use.
Change-Id: Id4a941855d6011a195d5cc796d6b1861624f8f56
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Allow the device drivers to use the required optional clock names
from the DT node data.This allows scalability when multiple usb_otg_ss
instances are in use.
Change-Id: Id4a941855d6011a195d5cc796d6b1861624f8f56
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: dwc3: update the maxpacket based on the maximum_speed
During initialization of endpoints, the maximum_speed is used
to determine the maxpacket size of the control endpoint.
For non control endpoints it appears alright to set the maxpacketsize to
be 1024 for the controller, but the function dwc3_gadget_get_maxpacket() is
introduced merely for consistency.
Change-Id: Iececaa685f1dd1901d254bbdf8d83c517bab8c72
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
During initialization of endpoints, the maximum_speed is used
to determine the maxpacket size of the control endpoint.
For non control endpoints it appears alright to set the maxpacketsize to
be 1024 for the controller, but the function dwc3_gadget_get_maxpacket() is
introduced merely for consistency.
Change-Id: Iececaa685f1dd1901d254bbdf8d83c517bab8c72
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
android: defconfig: unified defconfig for all omap platforms
for now, lets keep a unified defconfig for both omap5 evm and
dra7 evm platforms.
REVISIT: We will diverge later based on program needs to have seperate
memory footprint to make the configurable option compile or runtime.
{ Based on customer requirements }.
Change-Id: I9877c8678dedbc22b6d47a72c1fc7b28b3e8a647
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
for now, lets keep a unified defconfig for both omap5 evm and
dra7 evm platforms.
REVISIT: We will diverge later based on program needs to have seperate
memory footprint to make the configurable option compile or runtime.
{ Based on customer requirements }.
Change-Id: I9877c8678dedbc22b6d47a72c1fc7b28b3e8a647
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y:
arm: dts: dra7xx: Add voltage-tolerance to avs_mpu and avs_gpu
Change-Id: I919d3a7089a8ef8f158f338853dd21b65a863cd9
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y:
arm: dts: dra7xx: Add voltage-tolerance to avs_mpu and avs_gpu
Change-Id: I919d3a7089a8ef8f158f338853dd21b65a863cd9
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
arm: dts: dra7xx: Add voltage-tolerance to avs_mpu and avs_gpu
Without voltage tolerance, regulator code tries to set exact voltage
and this results in a falilure if this value differs even slightly
from what pmic expects. Adding a voltage-tolerance of 1% handles the
case where these voltage values differ slightly.
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
Without voltage tolerance, regulator code tries to set exact voltage
and this results in a falilure if this value differs even slightly
from what pmic expects. Adding a voltage-tolerance of 1% handles the
case where these voltage values differ slightly.
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y:
clk: omap5: Add CLK_SET_RATE_PARENT flag to gpu clocks
clk: dra7xx: Add CLK_SET_RATE_PARENT flag to gpu clocks
Change-Id: Ie676c6535e575f87a7ce6f978dd574898de2ace8
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y:
clk: omap5: Add CLK_SET_RATE_PARENT flag to gpu clocks
clk: dra7xx: Add CLK_SET_RATE_PARENT flag to gpu clocks
Change-Id: Ie676c6535e575f87a7ce6f978dd574898de2ace8
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
clk: omap5: Add CLK_SET_RATE_PARENT flag to gpu clocks
clk_set_rate finds the topmost clock that needs to be changed
in order to set the desired clock to a particular frequency.
This is done only if CLK_SET_RATE_PARENT flag is set for a clock.
gpu_core_gclk_mux and gpu_hyd_gclk_mux need to have this flag
enabled in order for clk_set_rate to propagate to to their parent.
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
clk_set_rate finds the topmost clock that needs to be changed
in order to set the desired clock to a particular frequency.
This is done only if CLK_SET_RATE_PARENT flag is set for a clock.
gpu_core_gclk_mux and gpu_hyd_gclk_mux need to have this flag
enabled in order for clk_set_rate to propagate to to their parent.
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
clk: dra7xx: Add CLK_SET_RATE_PARENT flag to gpu clocks
clk_set_rate finds the topmost clock that needs to be changed
in order to set the desired clock to a particular frequency.
This is done only if CLK_SET_RATE_PARENT flag is set for a clock.
gpu_core_gclk_mux and gpu_hyd_gclk_mux need to have this flag
enabled in order for clk_set_rate to propagate to to their parent.
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
clk_set_rate finds the topmost clock that needs to be changed
in order to set the desired clock to a particular frequency.
This is done only if CLK_SET_RATE_PARENT flag is set for a clock.
gpu_core_gclk_mux and gpu_hyd_gclk_mux need to have this flag
enabled in order for clk_set_rate to propagate to to their parent.
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y:
ARM: OMAP5: board-generic: Modify the machine name
Change-Id: Ic6f400e3bded71a2b2dcc44c7c5ad467558dc478
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y:
ARM: OMAP5: board-generic: Modify the machine name
Change-Id: Ic6f400e3bded71a2b2dcc44c7c5ad467558dc478
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
ARM: OMAP5: board-generic: Modify the machine name
Changing the machine name to "OMAP5 panda board".
This is needed to populate the correct device name to sdk.
Revisit: Will change the name to official omap5 platform
name "OMAP5432 EVM board" later.
For now, lets keep it in a way so that userspace understands
and populates accordingly.
Change-Id: I857d53e732220fe7bd2324ce3620ef511a39bebd
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Changing the machine name to "OMAP5 panda board".
This is needed to populate the correct device name to sdk.
Revisit: Will change the name to official omap5 platform
name "OMAP5432 EVM board" later.
For now, lets keep it in a way so that userspace understands
and populates accordingly.
Change-Id: I857d53e732220fe7bd2324ce3620ef511a39bebd
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y:
regulator: core: Make set_voltage_tol() try for mid-range first
Change-Id: Ifa9a0ed287cbd0cdb9cd217e5b9952c8154b36eb
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y:
regulator: core: Make set_voltage_tol() try for mid-range first
Change-Id: Ifa9a0ed287cbd0cdb9cd217e5b9952c8154b36eb
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
OMAPDSS: DSSCOMP: Avoid DSSCOMP compilation by default.
Compile DSSCOMP only when TILER and ION both components are
included in def config.
Change-Id: I221264a80f2426cc52d45902a83fcd6e9a001fce
Signed-off-by: Dandawate Saket <dsaket@ti.com>
Compile DSSCOMP only when TILER and ION both components are
included in def config.
Change-Id: I221264a80f2426cc52d45902a83fcd6e9a001fce
Signed-off-by: Dandawate Saket <dsaket@ti.com>
regulator: core: Make set_voltage_tol() try for mid-range first
The expected semantic for something expressed as a tolerance is that it
should deliver the specified value with some deviation allowed but this
is not what set_voltage_tol() currently does. Instead it just passes
the maximum possible range to set_voltage() which will typically result
in a voltage aimed at lower than the target voltage.
Instead first try to set a voltage between the target voltage and the
upper limit, then fall back on the full range. This will be much more
robust against physical variation in systems and makes the API behave
more like users would expect.
Signed-off-by: Mark Brown <broonie@linaro.org>
[cherry-pick from
https://git.kernel.org/cgit/linux/kernel/git/broonie/regulator.git/commit/?h=topic/core&id=dc9ceed6a12aff627c81e01ada191e8a23fcbe3e
]
Change-Id: I52e88a886e4277e5f7d9f97192931290b9775eab
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
The expected semantic for something expressed as a tolerance is that it
should deliver the specified value with some deviation allowed but this
is not what set_voltage_tol() currently does. Instead it just passes
the maximum possible range to set_voltage() which will typically result
in a voltage aimed at lower than the target voltage.
Instead first try to set a voltage between the target voltage and the
upper limit, then fall back on the full range. This will be much more
robust against physical variation in systems and makes the API behave
more like users would expect.
Signed-off-by: Mark Brown <broonie@linaro.org>
[cherry-pick from
https://git.kernel.org/cgit/linux/kernel/git/broonie/regulator.git/commit/?h=topic/core&id=dc9ceed6a12aff627c81e01ada191e8a23fcbe3e
]
Change-Id: I52e88a886e4277e5f7d9f97192931290b9775eab
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
OMAPDSS: OMAPFB: Fix OMAPFB compilation break
Fix OMAPFB compilation break because the Fb support
functions were not compiled.
Change-Id: If73ed83af6b7dc94859ef0ca8aead46bc06ea424
Signed-off-by: Dandawate Saket <dsaket@ti.com>
Fix OMAPFB compilation break because the Fb support
functions were not compiled.
Change-Id: If73ed83af6b7dc94859ef0ca8aead46bc06ea424
Signed-off-by: Dandawate Saket <dsaket@ti.com>
android: defconfig: OMAPDSS: DSSCOMP: OMAPLFB: Enabling dual FB configuration for multidisplay feature
Enabling dual FB configuration for multidisplay feature
updating CMDLINE for omapfb accordingly
Change-Id: I1d503cd8dfd955a3eb60871ca03eec2dc1a52560
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Enabling dual FB configuration for multidisplay feature
updating CMDLINE for omapfb accordingly
Change-Id: I1d503cd8dfd955a3eb60871ca03eec2dc1a52560
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
android: defconfig: usb: Enable all usb drivers as built in.
DWC3, XHCI, PHY and OMAP_CONTROL are all set to be built-in vs modules.
Change-Id: I5e2c3dd4a10f7bda0a981eb44465c594d2bc2002
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
DWC3, XHCI, PHY and OMAP_CONTROL are all set to be built-in vs modules.
Change-Id: I5e2c3dd4a10f7bda0a981eb44465c594d2bc2002
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Merge branch 'p-ti-linux-3.8.y' into p-ti-android-3.8.y
* p-ti-linux-3.8.y:
omap5: device tree: usb: Specify optional clock names in dt
usb: phy: protect against NULL phy pointers
usb: dwc3: core: make USB3 PHY optional
usb: dwc3: adapt to use dr_mode device tree helper
usb: dwc3: make maximum-speed a per-instance attribute
usb: common: introduce of_usb_get_maximum_speed()
usb: add devicetree helpers for determining dr_mode and phy_type
dra7xx : usb3_phy: Updated dpll M,N values.
ARM: OMAP: omap2plus_defconfig: Enable Kernel Preemption
Change-Id: I94360aac84a025cf25ef7220c16110e146918029
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
* p-ti-linux-3.8.y:
omap5: device tree: usb: Specify optional clock names in dt
usb: phy: protect against NULL phy pointers
usb: dwc3: core: make USB3 PHY optional
usb: dwc3: adapt to use dr_mode device tree helper
usb: dwc3: make maximum-speed a per-instance attribute
usb: common: introduce of_usb_get_maximum_speed()
usb: add devicetree helpers for determining dr_mode and phy_type
dra7xx : usb3_phy: Updated dpll M,N values.
ARM: OMAP: omap2plus_defconfig: Enable Kernel Preemption
Change-Id: I94360aac84a025cf25ef7220c16110e146918029
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
omap5: device tree: usb: Specify optional clock names in dt
Specify the optional clock names in the device tree.
This is required for scalablity.
Change-Id: Id80d0c0c92d1bb676f1fc713a20f668e3b0ee161
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Specify the optional clock names in the device tree.
This is required for scalablity.
Change-Id: Id80d0c0c92d1bb676f1fc713a20f668e3b0ee161
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
usb: phy: protect against NULL phy pointers
In order to decrease the amount of work done
by PHY users, allow NULL phy pointers to be
passed.
[Backport from 3.10 patch http://www.spinics.net/lists/linux-usb/msg88622.html
- Ignored what could not be applied for 3.8
]
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Change-Id: Ic921172d92214a4d0f8c840b6869beb7d320ff4a
In order to decrease the amount of work done
by PHY users, allow NULL phy pointers to be
passed.
[Backport from 3.10 patch http://www.spinics.net/lists/linux-usb/msg88622.html
- Ignored what could not be applied for 3.8
]
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
Change-Id: Ic921172d92214a4d0f8c840b6869beb7d320ff4a
usb: dwc3: core: make USB3 PHY optional
If we want a port to work at any speed lower than Superspeed, it makes no
sense to even initialize/power up the USB3 transceiver, provided it won't
be used. We can use the oportunity to save some power and leave the
superspeed transceiver powered off. There is at least one such case which
is Texas Instruments' AM437x which has one of its USB3 ports without a matching
USB3 PHY (that port is hardwired to work on USB2 only).
http://git.kernel.org/cgit/linux/kernel/git/balbi/usb.git/commit/
?h=testing&id=d7e39d414310e098540605be2051d5187797be34
Change-Id: I61639c4d58aac671a5aade67814981dc6d20f2e6
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>
If we want a port to work at any speed lower than Superspeed, it makes no
sense to even initialize/power up the USB3 transceiver, provided it won't
be used. We can use the oportunity to save some power and leave the
superspeed transceiver powered off. There is at least one such case which
is Texas Instruments' AM437x which has one of its USB3 ports without a matching
USB3 PHY (that port is hardwired to work on USB2 only).
http://git.kernel.org/cgit/linux/kernel/git/balbi/usb.git/commit/
?h=testing&id=d7e39d414310e098540605be2051d5187797be34
Change-Id: I61639c4d58aac671a5aade67814981dc6d20f2e6
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ruchika Kharwar <ruchika@ti.com>