Linux v2.6.13-rc7
Too many changes to release a final 2.6.13.
Too many changes to release a final 2.6.13.
[PATCH] Fix IXP4xx CLOCK_TICK_RATE
As pointed out in the following thread, the CLOCK_TICK_RATE setting for
IXP4xx is incorrect b/c the HW ignores the lowest 2 bits of the LATCH
value.
http://lists.arm.linux.org.uk/pipermail/linux-arm-kernel/2005-August/030950.html
Tnx to George Anziger and Egil Hjelmeland for finding the issue.
Signed-off-by: Deepak Saxena <dsaxena@plexity.net>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
As pointed out in the following thread, the CLOCK_TICK_RATE setting for
IXP4xx is incorrect b/c the HW ignores the lowest 2 bits of the LATCH
value.
http://lists.arm.linux.org.uk/pipermail/linux-arm-kernel/2005-August/030950.html
Tnx to George Anziger and Egil Hjelmeland for finding the issue.
Signed-off-by: Deepak Saxena <dsaxena@plexity.net>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] cpu_exclusive sched domains on partial nodes temp fix
This keeps the kernel/cpuset.c routine update_cpu_domains() from
invoking the sched.c routine partition_sched_domains() if the cpuset in
question doesn't fall on node boundaries.
I have boot tested this on an SN2, and with the help of a couple of ad
hoc printk's, determined that it does indeed avoid calling the
partition_sched_domains() routine on partial nodes.
I did not directly verify that this avoids setting up bogus sched
domains or avoids the oops that Hawkes saw.
This patch imposes a silent artificial constraint on which cpusets can
be used to define dynamic sched domains.
This patch should allow proceeding with this new feature in 2.6.13 for
the configurations in which it is useful (node alligned sched domains)
while avoiding trying to setup sched domains in the less useful cases
that can cause the kernel corruption and oops.
Signed-off-by: Paul Jackson <pj@sgi.com>
Acked-by: Ingo Molnar <mingo@elte.hu>
Acked-by: Dinakar Guniguntala <dino@in.ibm.com>
Acked-by: John Hawkes <hawkes@sgi.com>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
This keeps the kernel/cpuset.c routine update_cpu_domains() from
invoking the sched.c routine partition_sched_domains() if the cpuset in
question doesn't fall on node boundaries.
I have boot tested this on an SN2, and with the help of a couple of ad
hoc printk's, determined that it does indeed avoid calling the
partition_sched_domains() routine on partial nodes.
I did not directly verify that this avoids setting up bogus sched
domains or avoids the oops that Hawkes saw.
This patch imposes a silent artificial constraint on which cpusets can
be used to define dynamic sched domains.
This patch should allow proceeding with this new feature in 2.6.13 for
the configurations in which it is useful (node alligned sched domains)
while avoiding trying to setup sched domains in the less useful cases
that can cause the kernel corruption and oops.
Signed-off-by: Paul Jackson <pj@sgi.com>
Acked-by: Ingo Molnar <mingo@elte.hu>
Acked-by: Dinakar Guniguntala <dino@in.ibm.com>
Acked-by: John Hawkes <hawkes@sgi.com>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Merge head 'upstream-fixes' of master.kernel.org:/pub/scm/linux/kernel/git/jgarzik/misc-2.6
Merge head 'upstream-fixes' of master.kernel.org:/pub/scm/linux/kernel/git/jgarzik/libata-dev
[PATCH] x86_64: Don't oops at boot when empty Opteron node has IO
The code to detect IO links on Opteron would not check
if the node had actually memory. This could lead to pci_bus_to_node
returning an invalid node, which might cause crashes later
when dma_alloc_coherent passes it to page_alloc_node().
The bug has been there forever but for some reason
it is causing now crashes.
Signed-off-by: Andi Kleen <ak@suse.de>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
The code to detect IO links on Opteron would not check
if the node had actually memory. This could lead to pci_bus_to_node
returning an invalid node, which might cause crashes later
when dma_alloc_coherent passes it to page_alloc_node().
The bug has been there forever but for some reason
it is causing now crashes.
Signed-off-by: Andi Kleen <ak@suse.de>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] usbnet oops fix
There's a "return the wrong SKB" error in the GL620A cable minidriver
(for "usbnet") which can oops. This would not appear when talking
Linux-to-Linux, only Linux-to-Windows (for recent Linuxes).
Signed-off-by: David Brownell <dbrownell@users.sourceforge.net>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
There's a "return the wrong SKB" error in the GL620A cable minidriver
(for "usbnet") which can oops. This would not appear when talking
Linux-to-Linux, only Linux-to-Windows (for recent Linuxes).
Signed-off-by: David Brownell <dbrownell@users.sourceforge.net>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] i386: fix incorrect FP signal code
i386 floating-point exception handling has a bug that can cause error
code 0 to be sent instead of the proper code during signal delivery.
This is caused by unconditionally checking the IS and c1 bits from the
FPU status word when they are not always relevant. The IS bit tells
whether an exception is a stack fault and is only relevant when the
exception is IE (invalid operation.) The C1 bit determines whether a
stack fault is overflow or underflow and is only relevant when IS and IE
are set.
Signed-off-by: Chuck Ebbert <76306.1226@compuserve.com>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
i386 floating-point exception handling has a bug that can cause error
code 0 to be sent instead of the proper code during signal delivery.
This is caused by unconditionally checking the IS and c1 bits from the
FPU status word when they are not always relevant. The IS bit tells
whether an exception is a stack fault and is only relevant when the
exception is IE (invalid operation.) The C1 bit determines whether a
stack fault is overflow or underflow and is only relevant when IS and IE
are set.
Signed-off-by: Chuck Ebbert <76306.1226@compuserve.com>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Merge master.kernel.org:/pub/scm/linux/kernel/git/davem/net-2.6
[PATCH] s390 __CHECKER__ ifdefs
remove the bogus games with explicit ifdefs on __CHECKER__
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
remove the bogus games with explicit ifdefs on __CHECKER__
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] %t... in vsnprintf
handling of %t... (ptrdiff_t) in vsnprintf
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
handling of %t... (ptrdiff_t) in vsnprintf
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] ad1980 makefile fix
ac97_plugin_ad1980 should trigger build of ac97_codec
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
ac97_plugin_ad1980 should trigger build of ac97_codec
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (non-modular SCSI drivers)
non-modular scsi drivers depend on built-in scsi
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
non-modular scsi drivers depend on built-in scsi
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (missing dependencies on PCI in sound/*)
a bunch of PCI-only drivers didn't have the right dependency
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
a bunch of PCI-only drivers didn't have the right dependency
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] missing exports on m32r
missing exports on m32r
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
missing exports on m32r
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] qualifiers in return types - easy cases
a bunch of functions switched from volatile to __attribute__((noreturn)) and
from const to __attribute_pure__
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
a bunch of functions switched from volatile to __attribute__((noreturn)) and
from const to __attribute_pure__
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] typo fix in qdio.c
dumb typo: u32 volatile * mistyped as u32 * volatile
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
dumb typo: u32 volatile * mistyped as u32 * volatile
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] emac netpoll fix
netpoll is void(struct net_device *), not int(struct net_device *)
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
netpoll is void(struct net_device *), not int(struct net_device *)
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] vidc gcc4 fix
removes an extern for a static variable.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
removes an extern for a static variable.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] broken inline asm on s390 (misuse of labels)
use of explicit labels in inline asm is a Bad Idea(tm), since gcc can
decide to inline the function in several places. Fixed by use of 1f/f:
instead of .Lfitsin/.Lfitsin:
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
use of explicit labels in inline asm is a Bad Idea(tm), since gcc can
decide to inline the function in several places. Fixed by use of 1f/f:
instead of .Lfitsin/.Lfitsin:
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] m32r_sio gcc4 fixes
extern declaration followed by static in drivers/serial/m32r_sio.c
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
extern declaration followed by static in drivers/serial/m32r_sio.c
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] m32r icu_data gcc4 fixes
either icu_data declaration for SMP case should be taken out of m32102.h,
or its declarations for m32700ut and opsput should not be static for SMP.
Patch does the latter - judging by comments in m32102.h it is intended to
be non-static.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
either icu_data declaration for SMP case should be taken out of m32102.h,
or its declarations for m32700ut and opsput should not be static for SMP.
Patch does the latter - judging by comments in m32102.h it is intended to
be non-static.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] m32r smp.h gcc4 fixes
extern on physid_2_cpu[] does not belong in smp.h - the thing is static.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
extern on physid_2_cpu[] does not belong in smp.h - the thing is static.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] alpha spinlock code and bogus constraints
"=m" (lock->lock) / "1" (lock->lock) makes gcc4 unhappy; fixed by s/1/m/,
same as in case of i386 rwsem.h where such variant had been accepted
by both Linus and rth.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
"=m" (lock->lock) / "1" (lock->lock) makes gcc4 unhappy; fixed by s/1/m/,
same as in case of i386 rwsem.h where such variant had been accepted
by both Linus and rth.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] alpha xchg fix
alpha xchg has to be a macro - alpha disables always_inline and if that
puppy does not get inlined, we immediately blow up on undefined reference.
Happens even on gcc3; with gcc4 that happens a _lot_.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
alpha xchg has to be a macro - alpha disables always_inline and if that
puppy does not get inlined, we immediately blow up on undefined reference.
Happens even on gcc3; with gcc4 that happens a _lot_.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] missing include in pcmcia_resource.c
missing include of asm/irq.h
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
missing include of asm/irq.h
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] alpha gcc4 warnings
on UP smp_call_function() is expanded to expression. Alpha oprofile
calls that puppy and ignores the return value. And has -Werror for
arch/*...
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
on UP smp_call_function() is expanded to expression. Alpha oprofile
calls that puppy and ignores the return value. And has -Werror for
arch/*...
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (sparc32 drivers/char dependencies)
since sparc32 Kconfig includes drivers/char/Kconfig (instead of duplicating
its parts) we need several new dependencies there to exclude the stuff
broken on sparc32 and not excluded by existing dependencies.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
since sparc32 Kconfig includes drivers/char/Kconfig (instead of duplicating
its parts) we need several new dependencies there to exclude the stuff
broken on sparc32 and not excluded by existing dependencies.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (emac dependencient)
emac doesn't build modular; ibm_emac_debug doesn't build at all (missing
headers).
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
emac doesn't build modular; ibm_emac_debug doesn't build at all (missing
headers).
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (CONFIG_PM on 44x)
CONFIG_PM is broken on 44x; removed duplicate entry for CONFIG_PM, made
the inclusion of generic one conditional on BROKEN || !44x.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
CONFIG_PM is broken on 44x; removed duplicate entry for CONFIG_PM, made
the inclusion of generic one conditional on BROKEN || !44x.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (ppc 4xx and early serial)
a bunch of ppc 4xx variants unconditionally calls early_serial_setup() and
therefore needs SERIAL_8250
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
a bunch of ppc 4xx variants unconditionally calls early_serial_setup() and
therefore needs SERIAL_8250
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (IRQ_ALL_CPUS vs. MV64360)
MV64360 does not support IRQ_ALL_CPUS - see arch/ppc/kernel/mv64360_pic.c.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
MV64360 does not support IRQ_ALL_CPUS - see arch/ppc/kernel/mv64360_pic.c.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (ppc32 SMP dependencies)
ppc SMP is supported only for 6xx/POWER3/POWER4 - i.e. ones that have
PPC_STD_MMU. Dependency fixed.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Acked-by: Paul Mackerras <paulus@samba.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
ppc SMP is supported only for 6xx/POWER3/POWER4 - i.e. ones that have
PPC_STD_MMU. Dependency fixed.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Acked-by: Paul Mackerras <paulus@samba.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (VGA console on arm/versatile)
VGA console doesn't exist (or build) on arm/versatile; dependency fixed.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
VGA console doesn't exist (or build) on arm/versatile; dependency fixed.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (amba on arm/versatile)
AMBA_PL010 is broken on arm/versatile; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
AMBA_PL010 is broken on arm/versatile; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (acornscsi)
acornscsi had been broken for a long time; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
acornscsi had been broken for a long time; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (M32R_PLDSIO dependecies)
M32R_PLDSIO depends on subarchitecture providing PLD_ESIO0CR and
friends.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
M32R_PLDSIO depends on subarchitecture providing PLD_ESIO0CR and
friends.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (parport_pc on m32r)
parport_pc shouldn't be picked on m32r (no asm/parport.h, for starters)
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
parport_pc shouldn't be picked on m32r (no asm/parport.h, for starters)
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (airo_cs on m32r)
airo_cs is broken on m32r; marked as such. [Proper fix would involve
separating PCI-dependent parts and making sure they don't get in the
way _and_ arranging for asm/scatterlist.h getting picked on m32r]
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
airo_cs is broken on m32r; marked as such. [Proper fix would involve
separating PCI-dependent parts and making sure they don't get in the
way _and_ arranging for asm/scatterlist.h getting picked on m32r]
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (tms380tr and ISA_DMA_API)
ISA parts of tms380tr are using ISA DMA helpers and should depend on
ISA_DMA_API.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
ISA parts of tms380tr are using ISA DMA helpers and should depend on
ISA_DMA_API.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (arv)
arv uses constants provided only by include/asm-m32r/m32700ut/m32700ut_lan.h
It won't build for any subarchitecture other than M32700UT; marked as such.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
arv uses constants provided only by include/asm-m32r/m32700ut/m32700ut_lan.h
It won't build for any subarchitecture other than M32700UT; marked as such.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (infiniband and PCI)
infiniband uses PCI helpers all over the place (including the core parts) and
won't build without PCI.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
infiniband uses PCI helpers all over the place (including the core parts) and
won't build without PCI.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (DEBUG_PAGEALLOC on m32r)
DEBUG_PAGEALLOC is broken on m32r - the option had been blindly copied from
i386; kernel_map_pages() had not and that's what is needed for DEBUG_PAGEALLOC
to work (or link, while we are at it).
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
DEBUG_PAGEALLOC is broken on m32r - the option had been blindly copied from
i386; kernel_map_pages() had not and that's what is needed for DEBUG_PAGEALLOC
to work (or link, while we are at it).
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (PCI on m32r)
PCI support is broken on m32r (pci_map_... missing, etc.); marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
PCI support is broken on m32r (pci_map_... missing, etc.); marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (PMAC_BACKLIGHT on ppc64)
PMAC_BACKLIGHT is broken on ppc64; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
PMAC_BACKLIGHT is broken on ppc64; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (HISAX_FRITZPCI on ppc64)
HISAX_FRITZPCI is broken on ppc64; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
HISAX_FRITZPCI is broken on ppc64; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (m32r genrtc)
genrtc is not for m32r; marked as such. Probably ought to put that into
arch/* - list of "don't build it on <platform>" is getting too long.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
genrtc is not for m32r; marked as such. Probably ought to put that into
arch/* - list of "don't build it on <platform>" is getting too long.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (m32r NUMA)
NUMA is broken on m32r; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
NUMA is broken on m32r; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (ISA_DMA_API and sound/*)
fixed kconfig dependencies on ISA_DMA_API for parts of sound/* that rely
on it.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
fixed kconfig dependencies on ISA_DMA_API for parts of sound/* that rely
on it.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (epca on 64bit)
epca is broken on 64bit; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
epca is broken on 64bit; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (arm SMP)
SMP is broken on arm; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
SMP is broken on arm; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Kconfig fix (alpha NUMA)
NUMA is broken on alpha; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
NUMA is broken on alpha; marked as such
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[ROSE]: Fix typo in rose_route_frame() locking fix.
Signed-off-by: David S. Miller <davem@davemloft.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
[PATCH] zd1201 kmalloc size fix
Noticed by Coverity checker.
(akpm: I stole this from Greg's tree and used the (IMO) tidier sizeof(*p)
construct).
Signed-off-by: Alexey Dobriyan <adobriyan@gmail.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Noticed by Coverity checker.
(akpm: I stole this from Greg's tree and used the (IMO) tidier sizeof(*p)
construct).
Signed-off-by: Alexey Dobriyan <adobriyan@gmail.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] md: make sure resync gets started when array starts.
We weren't actually waking up the md thread after setting
MD_RECOVERY_NEEDED when assembling an array, so it is possible to lose a
race and not actually start resync.
So add a call to md_wakeup_thread, and while we are at it, remove all the
"if (mddev->thread)" guards as md_wake_thread does its own checking.
Signed-off-by: Neil Brown <neilb@cse.unsw.edu.au>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
We weren't actually waking up the md thread after setting
MD_RECOVERY_NEEDED when assembling an array, so it is possible to lose a
race and not actually start resync.
So add a call to md_wakeup_thread, and while we are at it, remove all the
"if (mddev->thread)" guards as md_wake_thread does its own checking.
Signed-off-by: Neil Brown <neilb@cse.unsw.edu.au>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] preempt race in getppid
With CONFIG_PREEMPT && !CONFIG_SMP, it's possible for sys_getppid to
return a bogus value if the parent's task_struct gets reallocated after
current->group_leader->real_parent is read:
asmlinkage long sys_getppid(void)
{
int pid;
struct task_struct *me = current;
struct task_struct *parent;
parent = me->group_leader->real_parent;
RACE HERE => for (;;) {
pid = parent->tgid;
#ifdef CONFIG_SMP
{
struct task_struct *old = parent;
/*
* Make sure we read the pid before re-reading the
* parent pointer:
*/
smp_rmb();
parent = me->group_leader->real_parent;
if (old != parent)
continue;
}
#endif
break;
}
return pid;
}
If the process gets preempted at the indicated point, the parent process
can go ahead and call exit() and then get wait()'d on to reap its
task_struct. When the preempted process gets resumed, it will not do any
further checks of the parent pointer on !CONFIG_SMP: it will read the
bad pid and return.
So, the same algorithm used when SMP is enabled should be used when
preempt is enabled, which will recheck ->real_parent in this case.
Signed-off-by: David Meybohm <dmeybohmlkml@bellsouth.net>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
With CONFIG_PREEMPT && !CONFIG_SMP, it's possible for sys_getppid to
return a bogus value if the parent's task_struct gets reallocated after
current->group_leader->real_parent is read:
asmlinkage long sys_getppid(void)
{
int pid;
struct task_struct *me = current;
struct task_struct *parent;
parent = me->group_leader->real_parent;
RACE HERE => for (;;) {
pid = parent->tgid;
#ifdef CONFIG_SMP
{
struct task_struct *old = parent;
/*
* Make sure we read the pid before re-reading the
* parent pointer:
*/
smp_rmb();
parent = me->group_leader->real_parent;
if (old != parent)
continue;
}
#endif
break;
}
return pid;
}
If the process gets preempted at the indicated point, the parent process
can go ahead and call exit() and then get wait()'d on to reap its
task_struct. When the preempted process gets resumed, it will not do any
further checks of the parent pointer on !CONFIG_SMP: it will read the
bad pid and return.
So, the same algorithm used when SMP is enabled should be used when
preempt is enabled, which will recheck ->real_parent in this case.
Signed-off-by: David Meybohm <dmeybohmlkml@bellsouth.net>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Merge master.kernel.org:/pub/scm/linux/kernel/git/davem/net-2.6
[ROSE]: Fix missing unlocks in rose_route_frame()
Noticed by Coverity checker.
Signed-off-by: David S. Miller <davem@davemloft.net>
Noticed by Coverity checker.
Signed-off-by: David S. Miller <davem@davemloft.net>
[TCP]: Document non-trivial locking path in tcp_v{4,6}_get_port().
This trips up a lot of folks reading this code.
Put an unlikely() around the port-exhaustion test
for good measure.
Signed-off-by: David S. Miller <davem@davemloft.net>
This trips up a lot of folks reading this code.
Put an unlikely() around the port-exhaustion test
for good measure.
Signed-off-by: David S. Miller <davem@davemloft.net>
[TCP]: Unconditionally clear TCP_NAGLE_PUSH in skb_entail().
Intention of this bit is to force pushing of the existing
send queue when TCP_CORK or TCP_NODELAY state changes via
setsockopt().
But it's easy to create a situation where the bit never
clears. For example, if the send queue starts empty:
1) set TCP_NODELAY
2) clear TCP_NODELAY
3) set TCP_CORK
4) do small write()
The current code will leave TCP_NAGLE_PUSH set after that
sequence. Unconditionally clearing the bit when new data
is added via skb_entail() solves the problem.
Signed-off-by: David S. Miller <davem@davemloft.net>
Intention of this bit is to force pushing of the existing
send queue when TCP_CORK or TCP_NODELAY state changes via
setsockopt().
But it's easy to create a situation where the bit never
clears. For example, if the send queue starts empty:
1) set TCP_NODELAY
2) clear TCP_NODELAY
3) set TCP_CORK
4) do small write()
The current code will leave TCP_NAGLE_PUSH set after that
sequence. Unconditionally clearing the bit when new data
is added via skb_entail() solves the problem.
Signed-off-by: David S. Miller <davem@davemloft.net>
[PKT_SCHED]: Fix missing qdisc_destroy() in qdisc_create_dflt()
qdisc_create_dflt() is missing to destroy the newly allocated
default qdisc if the initialization fails resulting in leaks
of all kinds. The only caller in mainline which may trigger
this bug is sch_tbf.c in tbf_create_dflt_qdisc().
Note: qdisc_create_dflt() doesn't fulfill the official locking
requirements of qdisc_destroy() but since the qdisc could
never be seen by the outside world this doesn't matter
and it can stay as-is until the locking of pkt_sched
is cleaned up.
Signed-off-by: Thomas Graf <tgraf@suug.ch>
Signed-off-by: David S. Miller <davem@davemloft.net>
qdisc_create_dflt() is missing to destroy the newly allocated
default qdisc if the initialization fails resulting in leaks
of all kinds. The only caller in mainline which may trigger
this bug is sch_tbf.c in tbf_create_dflt_qdisc().
Note: qdisc_create_dflt() doesn't fulfill the official locking
requirements of qdisc_destroy() but since the qdisc could
never be seen by the outside world this doesn't matter
and it can stay as-is until the locking of pkt_sched
is cleaned up.
Signed-off-by: Thomas Graf <tgraf@suug.ch>
Signed-off-by: David S. Miller <davem@davemloft.net>
[SCTP]: Add SENTINEL to SCTP MIB stats
Add SNMP_MIB_SENTINEL to the definition of the sctp_snmp_list so that
the output routine in proc correctly terminates. This was causing some
problems running on ia64 systems.
Signed-off-by: Vlad Yasevich <vladislav.yasevich@hp.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
Add SNMP_MIB_SENTINEL to the definition of the sctp_snmp_list so that
the output routine in proc correctly terminates. This was causing some
problems running on ia64 systems.
Signed-off-by: Vlad Yasevich <vladislav.yasevich@hp.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
[AX25]: UID fixes
o Brown paperbag bug - ax25_findbyuid() was always returning a NULL pointer
as the result. Breaks ROSE completly and AX.25 if UID policy set to deny.
o While the list structure of AX.25's UID to callsign mapping table was
properly protected by a spinlock, it's elements were not refcounted
resulting in a race between removal and usage of an element.
Signed-off-by: Ralf Baechle DL5RB <ralf@linux-mips.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
o Brown paperbag bug - ax25_findbyuid() was always returning a NULL pointer
as the result. Breaks ROSE completly and AX.25 if UID policy set to deny.
o While the list structure of AX.25's UID to callsign mapping table was
properly protected by a spinlock, it's elements were not refcounted
resulting in a race between removal and usage of an element.
Signed-off-by: Ralf Baechle DL5RB <ralf@linux-mips.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
[NET]: Fix socket bitop damage
The socket flag cleanups that went into 2.6.12-rc1 are basically oring
the flags of an old socket into the socket just being created.
Unfortunately that one was just initialized by sock_init_data(), so already
has SOCK_ZAPPED set. As the result zapped sockets are created and all
incoming connection will fail due to this bug which again was carefully
replicated to at least AX.25, NET/ROM or ROSE.
In order to keep the abstraction alive I've introduced sock_copy_flags()
to copy the socket flags from one sockets to another and used that
instead of the bitwise copy thing. Anyway, the idea here has probably
been to copy all flags, so sock_copy_flags() should be the right thing.
With this the ham radio protocols are usable again, so I hope this will
make it into 2.6.13.
Signed-off-by: Ralf Baechle DL5RB <ralf@linux-mips.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
The socket flag cleanups that went into 2.6.12-rc1 are basically oring
the flags of an old socket into the socket just being created.
Unfortunately that one was just initialized by sock_init_data(), so already
has SOCK_ZAPPED set. As the result zapped sockets are created and all
incoming connection will fail due to this bug which again was carefully
replicated to at least AX.25, NET/ROM or ROSE.
In order to keep the abstraction alive I've introduced sock_copy_flags()
to copy the socket flags from one sockets to another and used that
instead of the bitwise copy thing. Anyway, the idea here has probably
been to copy all flags, so sock_copy_flags() should be the right thing.
With this the ham radio protocols are usable again, so I hope this will
make it into 2.6.13.
Signed-off-by: Ralf Baechle DL5RB <ralf@linux-mips.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
[NETFILTER]: Fix HW checksum handling in ip_queue/ip6_queue
The checksum needs to be filled in on output, after mangling a packet
ip_summed needs to be reset.
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
The checksum needs to be filled in on output, after mangling a packet
ip_summed needs to be reset.
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
[IPV4]: Fix negative timer loop with lots of ipv4 peers.
From: Dave Johnson <djohnson+linux-kernel@sw.starentnetworks.com>
Found this bug while doing some scaling testing that created 500K inet
peers.
peer_check_expire() in net/ipv4/inetpeer.c isn't using inet_peer_gc_mintime
correctly and will end up creating an expire timer with less than the
minimum duration, and even zero/negative if enough active peers are
present.
If >65K peers, the timer will be less than inet_peer_gc_mintime, and with
>70K peers, the timer duration will reach zero and go negative.
The timer handler will continue to schedule another zero/negative timer in
a loop until peers can be aged. This can continue for at least a few
minutes or even longer if the peers remain active due to arriving packets
while the loop is occurring.
Bug is present in both 2.4 and 2.6. Same patch will apply to both just
fine.
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
From: Dave Johnson <djohnson+linux-kernel@sw.starentnetworks.com>
Found this bug while doing some scaling testing that created 500K inet
peers.
peer_check_expire() in net/ipv4/inetpeer.c isn't using inet_peer_gc_mintime
correctly and will end up creating an expire timer with less than the
minimum duration, and even zero/negative if enough active peers are
present.
If >65K peers, the timer will be less than inet_peer_gc_mintime, and with
>70K peers, the timer duration will reach zero and go negative.
The timer handler will continue to schedule another zero/negative timer in
a loop until peers can be aged. This can continue for at least a few
minutes or even longer if the peers remain active due to arriving packets
while the loop is occurring.
Bug is present in both 2.4 and 2.6. Same patch will apply to both just
fine.
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
[RPC]: Kill bogus kmap in krb5
While I was going through the crypto users recently, I noticed this
bogus kmap in sunrpc. It's totally unnecessary since the crypto
layer will do its own kmap before touching the data. Besides, the
kmap is throwing the return value away.
Signed-off-by: Herbert Xu <herbert@gondor.apana.org.au>
Signed-off-by: David S. Miller <davem@davemloft.net>
While I was going through the crypto users recently, I noticed this
bogus kmap in sunrpc. It's totally unnecessary since the crypto
layer will do its own kmap before touching the data. Besides, the
kmap is throwing the return value away.
Signed-off-by: Herbert Xu <herbert@gondor.apana.org.au>
Signed-off-by: David S. Miller <davem@davemloft.net>
[TCP]: Do TSO deferral even if tail SKB can go out now.
If the tail SKB fits into the window, it is still
benefitical to defer until the goal percentage of
the window is available. This give the application
time to feed more data into the send queue and thus
results in larger TSO frames going out.
Patch from Dmitry Yusupov <dima@neterion.com>.
Signed-off-by: David S. Miller <davem@davemloft.net>
If the tail SKB fits into the window, it is still
benefitical to defer until the goal percentage of
the window is available. This give the application
time to feed more data into the send queue and thus
results in larger TSO frames going out.
Patch from Dmitry Yusupov <dima@neterion.com>.
Signed-off-by: David S. Miller <davem@davemloft.net>
[IA64] Fix simulator boot (for real this time).
Thanks to Stephane, we've now worked out the real cause of the
`Linux will not boot on simulator' problem. Turns out it's a stack
overflow because the stack pointer wasn't being initialised properly
in boot_head.S (it was being initialised to the lowest instead of the
highest address of the stack, so the first push started to overwrite
data in the BSS).
Signed-off-by: Peter Chubb <peterc@gelato.unsw.edu.au>
Signed-off-by: Tony Luck <tony.luck@intel.com>
Thanks to Stephane, we've now worked out the real cause of the
`Linux will not boot on simulator' problem. Turns out it's a stack
overflow because the stack pointer wasn't being initialised properly
in boot_head.S (it was being initialised to the lowest instead of the
highest address of the stack, so the first push started to overwrite
data in the BSS).
Signed-off-by: Peter Chubb <peterc@gelato.unsw.edu.au>
Signed-off-by: Tony Luck <tony.luck@intel.com>
[IA64] backout incorrect fix for simulator boot issue
Earlier fix in 4aec0fb12267718c750475f3404337ad13caa8f5 just
masked the real problem.
Signed-off-by: Tony Luck <tony.luck@intel.com>
Earlier fix in 4aec0fb12267718c750475f3404337ad13caa8f5 just
masked the real problem.
Signed-off-by: Tony Luck <tony.luck@intel.com>
Pull prarit-bus-sysdata into release branch
libata: release prep (bump versions, etc.)
- bump versions where necessary
- remove two duplicated+outdated doc comments
- add MODULE_VERSION() to AHCI driver
- bump versions where necessary
- remove two duplicated+outdated doc comments
- add MODULE_VERSION() to AHCI driver
[PATCH] i810_audio: fix release_region misordering in error exit from i810_probe
Re-order release_region calls in i810_probe to properly unwind preceding
allocations.
Signed-off-by: John W. Linville <linville@tuxdriver.com>
Signed-off-by: Jeff Garzik <jgarzik@pobox.com>
Re-order release_region calls in i810_probe to properly unwind preceding
allocations.
Signed-off-by: John W. Linville <linville@tuxdriver.com>
Signed-off-by: Jeff Garzik <jgarzik@pobox.com>
Auto-update from upstream
Don't allow normal users to set idle IO priority
It has all the normal priority inversion problems.
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
It has all the normal priority inversion problems.
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[NETFILTER]: Fix HW checksum handling in TCPMSS target
Most importantly, remove bogus BUG() in receive path.
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
Most importantly, remove bogus BUG() in receive path.
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
[NETFILTER]: Fix HW checksum handling in ECN target
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
[NETFILTER]: Fix ECN target TCP marking
An incorrect check made it bail out before doing anything.
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
An incorrect check made it bail out before doing anything.
Signed-off-by: Patrick McHardy <kaber@trash.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
[PATCH] freevxfs: fix breakage introduced by symlink fixes
Signed-off-by: Alexey Dobriyan <adobriyan@gmail.com>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Signed-off-by: Alexey Dobriyan <adobriyan@gmail.com>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
befs: fix up missed follow_link declaration change
We'd updated the prototype and the return value, but not the function
declaration itself.
We'd updated the prototype and the return value, but not the function
declaration itself.
[PATCH] x86_64: Fix race in TSC synchronization
Plug a race in TSC synchronization
We need to do tsc_sync_wait() before the CPU is set online to prevent
multiple CPUs from doing it in parallel - which won't work because TSC
sync has global unprotected state.
Signed-off-by: Andi Kleen <ak@suse.de>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Plug a race in TSC synchronization
We need to do tsc_sync_wait() before the CPU is set online to prevent
multiple CPUs from doing it in parallel - which won't work because TSC
sync has global unprotected state.
Signed-off-by: Andi Kleen <ak@suse.de>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] x86_64: Don't print exceptions for ltrace
Don't printk exceptions for ltrace
Signed-off-by: Andi Kleen <ak@suse.de>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Don't printk exceptions for ltrace
Signed-off-by: Andi Kleen <ak@suse.de>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Merge master.kernel.org:/pub/scm/linux/kernel/git/davem/net-2.6
Merge master.kernel.org:/pub/scm/linux/kernel/git/davem/sparc-2.6
[PATCH] NFSv4: unbalanced BKL in nfs_atomic_lookup()
Added missing unlock_kernel() to NFSv4 atomic lookup.
Signed-off-by: Steve Dickson <steved@redhat.com>
Signed-off-by: Trond Myklebust <Trond.Myklebust@netapp.com>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Added missing unlock_kernel() to NFSv4 atomic lookup.
Signed-off-by: Steve Dickson <steved@redhat.com>
Signed-off-by: Trond Myklebust <Trond.Myklebust@netapp.com>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Mobil Pentium 4 HT and the NMI
I'm trying to get the nmi working with my laptop (IBM ThinkPad G41) and after
debugging it a while, I found that the nmi code doesn't want to set it up for
this particular CPU.
Here I have:
$ cat /proc/cpuinfo
processor : 0
vendor_id : GenuineIntel
cpu family : 15
model : 4
model name : Mobile Intel(R) Pentium(R) 4 CPU 3.33GHz
stepping : 1
cpu MHz : 3320.084
cache size : 1024 KB
physical id : 0
siblings : 2
core id : 0
cpu cores : 1
fdiv_bug : no
hlt_bug : no
f00f_bug : no
coma_bug : no
fpu : yes
fpu_exception : yes
cpuid level : 3
wp : yes
flags : fpu vme de pse tsc msr pae mce cx8 apic sep mtrr pge
mca cmov pat pse36 clflush dts acpi mmx fxsr sse sse2 ss ht tm pbe pni
monitor ds_cpl est tm2 cid xtpr
bogomips : 6642.39
processor : 1
vendor_id : GenuineIntel
cpu family : 15
model : 4
model name : Mobile Intel(R) Pentium(R) 4 CPU 3.33GHz
stepping : 1
cpu MHz : 3320.084
cache size : 1024 KB
physical id : 0
siblings : 2
core id : 0
cpu cores : 1
fdiv_bug : no
hlt_bug : no
f00f_bug : no
coma_bug : no
fpu : yes
fpu_exception : yes
cpuid level : 3
wp : yes
flags : fpu vme de pse tsc msr pae mce cx8 apic sep mtrr pge
mca cmov pat pse36 clflush dts acpi mmx fxsr sse sse2 ss ht tm pbe pni
monitor ds_cpl est tm2 cid xtpr
bogomips : 6637.46
And the following code shows:
$ cat linux-2.6.13-rc6/arch/i386/kernel/nmi.c
[...]
void setup_apic_nmi_watchdog (void)
{
switch (boot_cpu_data.x86_vendor) {
case X86_VENDOR_AMD:
if (boot_cpu_data.x86 != 6 && boot_cpu_data.x86 != 15)
return;
setup_k7_watchdog();
break;
case X86_VENDOR_INTEL:
switch (boot_cpu_data.x86) {
case 6:
if (boot_cpu_data.x86_model > 0xd)
return;
setup_p6_watchdog();
break;
case 15:
if (boot_cpu_data.x86_model > 0x3)
return;
Here I get boot_cpu_data.x86_model == 0x4. So I decided to change it and
reboot. I now seem to have a working NMI. So, unless there's something know
to be bad about this processor and the NMI. I'm submitting the following
patch.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Acked-by: Zwane Mwaikambo <zwane@arm.linux.org.uk>
Acked-by: Mikael Pettersson <mikpe@csd.uu.se>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
I'm trying to get the nmi working with my laptop (IBM ThinkPad G41) and after
debugging it a while, I found that the nmi code doesn't want to set it up for
this particular CPU.
Here I have:
$ cat /proc/cpuinfo
processor : 0
vendor_id : GenuineIntel
cpu family : 15
model : 4
model name : Mobile Intel(R) Pentium(R) 4 CPU 3.33GHz
stepping : 1
cpu MHz : 3320.084
cache size : 1024 KB
physical id : 0
siblings : 2
core id : 0
cpu cores : 1
fdiv_bug : no
hlt_bug : no
f00f_bug : no
coma_bug : no
fpu : yes
fpu_exception : yes
cpuid level : 3
wp : yes
flags : fpu vme de pse tsc msr pae mce cx8 apic sep mtrr pge
mca cmov pat pse36 clflush dts acpi mmx fxsr sse sse2 ss ht tm pbe pni
monitor ds_cpl est tm2 cid xtpr
bogomips : 6642.39
processor : 1
vendor_id : GenuineIntel
cpu family : 15
model : 4
model name : Mobile Intel(R) Pentium(R) 4 CPU 3.33GHz
stepping : 1
cpu MHz : 3320.084
cache size : 1024 KB
physical id : 0
siblings : 2
core id : 0
cpu cores : 1
fdiv_bug : no
hlt_bug : no
f00f_bug : no
coma_bug : no
fpu : yes
fpu_exception : yes
cpuid level : 3
wp : yes
flags : fpu vme de pse tsc msr pae mce cx8 apic sep mtrr pge
mca cmov pat pse36 clflush dts acpi mmx fxsr sse sse2 ss ht tm pbe pni
monitor ds_cpl est tm2 cid xtpr
bogomips : 6637.46
And the following code shows:
$ cat linux-2.6.13-rc6/arch/i386/kernel/nmi.c
[...]
void setup_apic_nmi_watchdog (void)
{
switch (boot_cpu_data.x86_vendor) {
case X86_VENDOR_AMD:
if (boot_cpu_data.x86 != 6 && boot_cpu_data.x86 != 15)
return;
setup_k7_watchdog();
break;
case X86_VENDOR_INTEL:
switch (boot_cpu_data.x86) {
case 6:
if (boot_cpu_data.x86_model > 0xd)
return;
setup_p6_watchdog();
break;
case 15:
if (boot_cpu_data.x86_model > 0x3)
return;
Here I get boot_cpu_data.x86_model == 0x4. So I decided to change it and
reboot. I now seem to have a working NMI. So, unless there's something know
to be bad about this processor and the NMI. I'm submitting the following
patch.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Acked-by: Zwane Mwaikambo <zwane@arm.linux.org.uk>
Acked-by: Mikael Pettersson <mikpe@csd.uu.se>
Signed-off-by: Andrew Morton <akpm@osdl.org>
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] Fix up symlink function pointers
This fixes up the symlink functions for the calling convention change:
* afs, autofs4, befs, devfs, freevxfs, jffs2, jfs, ncpfs, procfs,
smbfs, sysvfs, ufs, xfs - prototype change for ->follow_link()
* befs, smbfs, xfs - same for ->put_link()
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
This fixes up the symlink functions for the calling convention change:
* afs, autofs4, befs, devfs, freevxfs, jffs2, jfs, ncpfs, procfs,
smbfs, sysvfs, ufs, xfs - prototype change for ->follow_link()
* befs, smbfs, xfs - same for ->put_link()
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
Fix nasty ncpfs symlink handling bug.
This bug could cause oopses and page state corruption, because ncpfs
used the generic page-cache symlink handlign functions. But those
functions only work if the page cache is guaranteed to be "stable", ie a
page that was installed when the symlink walk was started has to still
be installed in the page cache at the end of the walk.
We could have fixed ncpfs to not use the generic helper routines, but it
is in many ways much cleaner to instead improve on the symlink walking
helper routines so that they don't require that absolute stability.
We do this by allowing "follow_link()" to return a error-pointer as a
cookie, which is fed back to the cleanup "put_link()" routine. This
also simplifies NFS symlink handling.
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
This bug could cause oopses and page state corruption, because ncpfs
used the generic page-cache symlink handlign functions. But those
functions only work if the page cache is guaranteed to be "stable", ie a
page that was installed when the symlink walk was started has to still
be installed in the page cache at the end of the walk.
We could have fixed ncpfs to not use the generic helper routines, but it
is in many ways much cleaner to instead improve on the symlink walking
helper routines so that they don't require that absolute stability.
We do this by allowing "follow_link()" to return a error-pointer as a
cookie, which is fed back to the cleanup "put_link()" routine. This
also simplifies NFS symlink handling.
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[PATCH] jffs2: fix symlink error handling
The current calling conventions for ->follow_link() are already fairly
complex.
What we have is
1) you can return -error; then you must release nameidata yourself
and ->put_link() will _not_ be called.
2) you can do nd_set_link(nd, ERR_PTR(-error)) and return 0
3) you can do nd_set_link(nd, path) and return 0
4) you can return 0 (after having moved nameidata yourself)
jffs2 follow_link() is broken - it has an exit where it returns
-EIO and leaks nameidata.
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
The current calling conventions for ->follow_link() are already fairly
complex.
What we have is
1) you can return -error; then you must release nameidata yourself
and ->put_link() will _not_ be called.
2) you can do nd_set_link(nd, ERR_PTR(-error)) and return 0
3) you can do nd_set_link(nd, path) and return 0
4) you can return 0 (after having moved nameidata yourself)
jffs2 follow_link() is broken - it has an exit where it returns
-EIO and leaks nameidata.
Signed-off-by: Linus Torvalds <torvalds@osdl.org>
[SPARC]: Fix weak aliases
sparc_ksyms.c used to declare weak alias to several gcc intrinsics. It
doesn't work with gcc4 anymore - it wants a declaration for the thing
we are aliasing to and that's not going to happen for something like
.mul, etc. Replaced with direct injection of weak alias on the assembler
level - .weak <alias> followed by <alias> = <aliased>; that works on all
gcc versions.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: David S. Miller <davem@davemloft.net>
sparc_ksyms.c used to declare weak alias to several gcc intrinsics. It
doesn't work with gcc4 anymore - it wants a declaration for the thing
we are aliasing to and that's not going to happen for something like
.mul, etc. Replaced with direct injection of weak alias on the assembler
level - .weak <alias> followed by <alias> = <aliased>; that works on all
gcc versions.
Signed-off-by: Al Viro <viro@parcelfarce.linux.theplanet.co.uk>
Signed-off-by: David S. Miller <davem@davemloft.net>
[SPARC64]: Move kernel unaligned trap handlers into assembler file.
GCC 4.x really dislikes the games we are playing in
unaligned.c, and the cleanest way to fix this is to
move things into assembler.
Noted by Al Viro.
Signed-off-by: David S. Miller <davem@davemloft.net>
GCC 4.x really dislikes the games we are playing in
unaligned.c, and the cleanest way to fix this is to
move things into assembler.
Noted by Al Viro.
Signed-off-by: David S. Miller <davem@davemloft.net>
[SPARC]: Deal with glibc changing macro names in modpost.c
GLIBC 2.3.4 and later changed the STT_REGISTER macro to
STT_SPARC_REGISTER, so we need to cope with that somehow.
Original patch from fabbione, reposted by Ben Collins.
Signed-off-by: David S. Miller <davem@davemloft.net>
GLIBC 2.3.4 and later changed the STT_REGISTER macro to
STT_SPARC_REGISTER, so we need to cope with that somehow.
Original patch from fabbione, reposted by Ben Collins.
Signed-off-by: David S. Miller <davem@davemloft.net>
[TG3]: Update driver version and reldate.
Signed-off-by: David S. Miller <davem@davemloft.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
[TG3]: Fix SerDes detection
A problem was reported by Grant Grundler on an HP rx8620 using IOX
Core LAN partno(A7109-6) 5701 copper NIC. The tg3 driver mistakenly
detects this NIC as having a SerDes PHY and link does not come up as a
result.
The problem was caused by an incorrectly programmed eeprom that set the
NIC_SRAM_DATA_CFG_PHY_TYPE_FIBER bit in the NIC_SRAM_DATA_CFG location.
This patch will override the NIC_SRAM_DATA_CFG_PHY_TYPE_FIBER bit if a
valid PHY ID is read from the MII registers on older 570x chips where
the MII interface is not used on SerDes chips. On newer chips such as
the 5780 that use MII for both copper and SerDes, SerDes detection must
rely on the eeprom.
This patch will make the SerDes detection identical to versions 3.25 and
older.
Signed-off-by: Michael Chan <mchan@broadcom.com>
Acked-by: Grant Grundler <iod00d@hp.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
A problem was reported by Grant Grundler on an HP rx8620 using IOX
Core LAN partno(A7109-6) 5701 copper NIC. The tg3 driver mistakenly
detects this NIC as having a SerDes PHY and link does not come up as a
result.
The problem was caused by an incorrectly programmed eeprom that set the
NIC_SRAM_DATA_CFG_PHY_TYPE_FIBER bit in the NIC_SRAM_DATA_CFG location.
This patch will override the NIC_SRAM_DATA_CFG_PHY_TYPE_FIBER bit if a
valid PHY ID is read from the MII registers on older 570x chips where
the MII interface is not used on SerDes chips. On newer chips such as
the 5780 that use MII for both copper and SerDes, SerDes detection must
rely on the eeprom.
This patch will make the SerDes detection identical to versions 3.25 and
older.
Signed-off-by: Michael Chan <mchan@broadcom.com>
Acked-by: Grant Grundler <iod00d@hp.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
Auto-update from upstream
Merge master.kernel.org:/pub/scm/linux/kernel/git/bart/ide-2.6
Merge head 'upstream-fixes' of master.kernel.org:/pub/scm/linux/kernel/git/jgarzik/netdev-2.6
Merge master.kernel.org:/pub/scm/linux/kernel/git/davem/sparc-2.6
[IA64] remove unused function __ia64_get_io_port_base
Not only was this unused, but its somewhat eccentric declaration
of "static inline const unsigned long" gives gcc4 heartburn.
Signed-off-by: Tony Luck <tony.luck@intel.com>
Not only was this unused, but its somewhat eccentric declaration
of "static inline const unsigned long" gives gcc4 heartburn.
Signed-off-by: Tony Luck <tony.luck@intel.com>
[IPCOMP]: Fix false smp_processor_id warning
This patch fixes a false-positive from debug_smp_processor_id().
The processor ID is only used to look up crypto_tfm objects.
Any processor ID is acceptable here as long as it is one that is
iterated on by for_each_cpu().
Signed-off-by: Herbert Xu <herbert@gondor.apana.org.au>
Signed-off-by: David S. Miller <davem@davemloft.net>
This patch fixes a false-positive from debug_smp_processor_id().
The processor ID is only used to look up crypto_tfm objects.
Any processor ID is acceptable here as long as it is one that is
iterated on by for_each_cpu().
Signed-off-by: Herbert Xu <herbert@gondor.apana.org.au>
Signed-off-by: David S. Miller <davem@davemloft.net>