]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/log
android-sdk/kernel-video.git
12 years agoLinux 3.1-rc2 v3.1-rc2
Linus Torvalds [Sun, 14 Aug 2011 22:09:08 +0000 (15:09 -0700)]
Linux 3.1-rc2

12 years agomm: fix wrong vmap address calculations with odd NR_CPUS values
Clemens Ladisch [Tue, 21 Jun 2011 20:09:50 +0000 (22:09 +0200)]
mm: fix wrong vmap address calculations with odd NR_CPUS values

Commit db64fe02258f ("mm: rewrite vmap layer") introduced code that does
address calculations under the assumption that VMAP_BLOCK_SIZE is a
power of two.  However, this might not be true if CONFIG_NR_CPUS is not
set to a power of two.

Wrong vmap_block index/offset values could lead to memory corruption.
However, this has never been observed in practice (or never been
diagnosed correctly); what caught this was the BUG_ON in vb_alloc() that
checks for inconsistent vmap_block indices.

To fix this, ensure that VMAP_BLOCK_SIZE always is a power of two.

BugLink: https://bugzilla.kernel.org/show_bug.cgi?id=31572
Reported-by: Pavel Kysilka <goldenfish@linuxsoft.cz>
Reported-by: Matias A. Fonzo <selk@dragora.org>
Signed-off-by: Clemens Ladisch <clemens@ladisch.de>
Signed-off-by: Stefan Richter <stefanr@s5r6.in-berlin.de>
Cc: Nick Piggin <npiggin@suse.de>
Cc: Jeremy Fitzhardinge <jeremy@goop.org>
Cc: Krzysztof Helt <krzysztof.h1@poczta.fm>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: 2.6.28+ <stable@kernel.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/cjb/mmc
Linus Torvalds [Sun, 14 Aug 2011 19:28:15 +0000 (12:28 -0700)]
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/cjb/mmc

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/cjb/mmc:
  mmc: remove unused "ddr" parameter in struct mmc_ios
  mmc: dw_mmc: Fix DDR mode support.
  mmc: core: use defined R1_STATE_PRG macro for card status
  mmc: sdhci: use f_max instead of host->clock for timeouts
  mmc: sdhci: move timeout_clk calculation farther down
  mmc: sdhci: check host->clock before using it as a denominator
  mmc: Revert "mmc: sdhci: Fix SDHCI_QUIRK_TIMEOUT_USES_SDCLK"
  mmc: tmio: eliminate unused variable 'mmc' warning
  mmc: esdhc-imx: fix card interrupt loss on freescale eSDHC
  mmc: sdhci-s3c: Fix build for header change
  mmc: dw_mmc: Fix mask in IDMAC_SET_BUFFER1_SIZE macro
  mmc: cb710: fix possible pci_dev leak in cb710_pci_configure()
  mmc: core: Detect eMMC v4.5 ext_csd entries
  mmc: mmc_test: avoid stalled file in debugfs
  mmc: sdhci-s3c: add BROKEN_ADMA_ZEROLEN_DESC quirk
  mmc: sdhci: pxav3: controller needs 32 bit ADMA addressing
  mmc: sdhci: fix retuning timer wrongly deleted in sdhci_tasklet_finish

12 years agoMerge branch 'hwmon-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/groec...
Linus Torvalds [Sun, 14 Aug 2011 01:37:28 +0000 (18:37 -0700)]
Merge branch 'hwmon-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/groeck/staging

* 'hwmon-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/groeck/staging:
  hwmon: (ibmaem) add missing kfree
  hwmon: (pmbus/lm25066) Ignore byte writes to non-zero pages
  hwmon: (pmbus) Virtualize pmbus_write_byte

12 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound-2.6
Linus Torvalds [Sun, 14 Aug 2011 01:36:28 +0000 (18:36 -0700)]
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound-2.6

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound-2.6:
  ASoC: Fix compile warning in wm8750.c
  ASoC: omap: Update e-mail address of Jarkko Nikula
  ASoC: SAMSUNG: Add I2S0 internal dma driver
  ASoC: Terminate WM8750 SPI device ID table
  ASoC: Add missing break in WM8994 probe
  ALSA: snd-usb-caiaq: Correct offset fields of outbound iso_frame_desc
  ALSA: azt3328 - adjust error handling code to include debugging code
  ALSA: hda - Add CONFIG_SND_HDA_POWER_SAVE to stac_vrefout_set()
  ALSA: usb-audio - Add quirk for BOSS Micro BR-80
  ASoC: Fix typo in wm8750 spi_ids
  ASoC: Fix warning in Speyside WM8962
  ASoC: Fix SPI driver binding for WM8987
  ASoC: Fix binding of WM8750 on Jive
  ASoC: WM8903: Free IRQ on device removal
  ASoC: Tegra: wm8903 machine driver: Allow re-insertion of module
  ASoC: Tegra: tegra_pcm_deallocate_dma_buffer: Don't OOPS

12 years agoDocumentation: befs.txt: no maintainer, orphaned
Marcos Souza [Sat, 13 Aug 2011 19:34:59 +0000 (12:34 -0700)]
Documentation: befs.txt: no maintainer, orphaned

Remove the name of Sergey Kostyliov as maintainer of befs.
In the MAINTAINERS file, befs is orphaned.

Signed-off-by: Marcos Souza <marcos.mage@gmail.com>
Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoDocumentation: SubmittingDrivers: fix Linus's git tree URL
Ralf Thielow [Sat, 13 Aug 2011 19:34:57 +0000 (12:34 -0700)]
Documentation: SubmittingDrivers: fix Linus's git tree URL

Change resource URL to new git tree -
(http://git.kernel.org/?p=linux/kernel/git/torvalds/linux.git).

Signed-off-by: Ralf Thielow <ralf.thielow@googlemail.com>
Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoDocumentation: add Ramoops usage description
Sergiu Iordache [Sat, 13 Aug 2011 19:34:56 +0000 (12:34 -0700)]
Documentation: add Ramoops usage description

Add a documentation file describing the usage of Ramoops

Signed-off-by: Sergiu Iordache <sergiu@chromium.org>
Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoDocumentation: email-clients: Add better Thunderbird information
Paul Mcquade [Sat, 13 Aug 2011 19:34:54 +0000 (12:34 -0700)]
Documentation: email-clients: Add better Thunderbird information

Add better Thunderbird information.
Add Thunderbird Registry instructions to:
  Enable UTF8 & Preformat mode
  Disable HTML mode

Signed-off-by: Paul McQuade <paulmcquad@gmail.com>
Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoDocumentation: kernel-parameters.txt cleanups
Randy Dunlap [Sat, 13 Aug 2011 19:34:52 +0000 (12:34 -0700)]
Documentation: kernel-parameters.txt cleanups

General cleanups to kernel-parameters.txt:
 - add missing $ARCH that are being used/referenced
 - alphabetize the parameter restrictions list
 - spell "IA-64" as listed in arch/ia64/Kconfig instead of "IA64"
 - remove trailing whitespace
 - use hyphen in 32-bit etc.

Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoDocumentation: add ARM user_debug to kernel-parameters.txt
Stephen Boyd [Sat, 13 Aug 2011 19:34:50 +0000 (12:34 -0700)]
Documentation: add ARM user_debug to kernel-parameters.txt

Usually kernel parameters are documented in kernel-parameters.txt
but user_debug is only documented in the Kconfig. Document the
option and point to the Kconfig help text for more info.

Signed-off-by: Stephen Boyd <sboyd@codeaurora.org>
Cc: Russell King <linux@arm.linux.org.uk>
Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoDocumentation: drop Linux Source Driver from kernel-docs references
Luis de Bethencourt [Sat, 13 Aug 2011 19:34:47 +0000 (12:34 -0700)]
Documentation: drop Linux Source Driver from kernel-docs references

Dropping LSD (Linux Source Driver) since it hasn't been available
for a long time.

Signed-off-by: Luis de Bethencourt <luis@debethencourt.com>
Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoDocumentation: fix spelling error in SubmittingPatches
Zac Storer [Sat, 13 Aug 2011 19:34:45 +0000 (12:34 -0700)]
Documentation: fix spelling error in SubmittingPatches

Fixed a spelling error.

Signed-off-by: Zac Storer <zac.3.14159@gmail.com>
Signed-off-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agommc: remove unused "ddr" parameter in struct mmc_ios
Jaehoon Chung [Mon, 8 Aug 2011 09:10:52 +0000 (18:10 +0900)]
mmc: remove unused "ddr" parameter in struct mmc_ios

"mmc: dw_mmc: Fix DDR mode support" removed the last user.

Signed-off-by: Jaehoon Chung <jh80.chung@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: dw_mmc: Fix DDR mode support.
Seungwon Jeon [Fri, 5 Aug 2011 03:35:03 +0000 (12:35 +0900)]
mmc: dw_mmc: Fix DDR mode support.

Host driver can't get a hint of DDR mode through ios->ddr flag anymore.
ios->timing is currently used to inform DDR mode as a substitute.
And capability of MMC_CAP_MMC_HIGHSPEED is added for DDR support.

Signed-off-by: Seungwon Jeon <tgih.jun@samsung.com>
Acked-by: Will Newton <will.newton@imgtec.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: core: use defined R1_STATE_PRG macro for card status
Jaehoon Chung [Wed, 10 Aug 2011 09:46:28 +0000 (18:46 +0900)]
mmc: core: use defined R1_STATE_PRG macro for card status

Signed-off-by: Jaehoon Chung <jh80.chung@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: sdhci: use f_max instead of host->clock for timeouts
Andy Shevchenko [Wed, 3 Aug 2011 15:36:01 +0000 (18:36 +0300)]
mmc: sdhci: use f_max instead of host->clock for timeouts

When timeout_clk is calculated the host->clock could be zero.
So, instead of host->clock the calculation now uses mmc->f_max.

Signed-off-by: Andy Shevchenko <andriy.shevchenko@linux.intel.com>
Cc: Mark Brown <broonie@opensource.wolfsonmicro.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: sdhci: move timeout_clk calculation farther down
Andy Shevchenko [Wed, 3 Aug 2011 15:36:00 +0000 (18:36 +0300)]
mmc: sdhci: move timeout_clk calculation farther down

This moves the calculation below the assignment of mmc->f_max, which
we need for calculating timeout_clk in the next patch in this series.

Signed-off-by: Andy Shevchenko <andriy.shevchenko@linux.intel.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: sdhci: check host->clock before using it as a denominator
Andy Shevchenko [Wed, 3 Aug 2011 15:35:59 +0000 (18:35 +0300)]
mmc: sdhci: check host->clock before using it as a denominator

Sometimes host->clock could be zero which is a legal situation. This
patch checks host->clock before usage as a denominator when timeout is
calculated. A similar patch is applied for mmc core (see commit e9b8684,
"mmc: fix division by zero in MMC core").

Without this patch, the execution of the sdhci_calc_timeout could end up
with a backtrace:

<0>[    4.014319] divide error: 0000 [#1] PREEMPT SMP
<4>[    4.014352] Modules linked in: g_ether
<4>[    4.014376]
<4>[    4.014393] Pid: 33, comm: kworker/u:2 Not tainted 3.0.0+ #646
<4>[    4.014421] EIP: 0060:[<c12fa38e>] EFLAGS: 00010046 CPU: 1
<4>[    4.014449] EIP is at sdhci_calc_timeout+0x2e/0x100
<4>[    4.014468] EAX: 00000000 EBX: f5930fc8 ECX: 00000000 EDX: 00000000
<4>[    4.014488] ESI: f5291de8 EDI: f5291db8 EBP: f5291c6c ESP: f5291c50
<4>[    4.014508]  DS: 007b ES: 007b FS: 00d8 GS: 0000 SS: 0068
<0>[    4.014529] Process kworker/u:2 (pid: 33, ti=f5290000 task=f53065a0 task.ti=f5290000)
<0>[    4.014546] Stack:
<4>[    4.014557]  00000082 c1054fdd f5291c78 04000000 f5930fc8 f5291de8 f5291db8 f5291cac
<4>[    4.014611]  c12fab7c c107a98b f5291c88 c13b6d3f f593109c f5882000 f5291cac c1054fdd
<4>[    4.014663]  00000000 00000000 f5882000 00000082 f5930fc8 f5291db8 0000000a f5291ccc
<0>[    4.014716] Call Trace:
<4>[    4.014743]  [<c1054fdd>] ? mod_timer+0x11d/0x380
<4>[    4.014770]  [<c12fab7c>] sdhci_prepare_data+0x2c/0x3a0
<4>[    4.014798]  [<c107a98b>] ? trace_hardirqs_off+0xb/0x10
<4>[    4.014827]  [<c13b6d3f>] ? _raw_spin_unlock_irqrestore+0x2f/0x60
<4>[    4.014854]  [<c1054fdd>] ? mod_timer+0x11d/0x380
<4>[    4.014880]  [<c12fc7db>] sdhci_send_command+0xdb/0x210
<4>[    4.014906]  [<c12fd5f3>] sdhci_request+0xc3/0x150
<4>[    4.014932]  [<c12ec56a>] mmc_start_request+0xda/0x200
<4>[    4.014960]  [<c120d7c2>] ? __raw_spin_lock_init+0x32/0x60
<4>[    4.014989]  [<c1066a85>] ? __init_waitqueue_head+0x35/0x50
<4>[    4.015015]  [<c12ec70b>] mmc_wait_for_req+0x7b/0x90
<4>[    4.015045]  [<c12f0c67>] mmc_send_cxd_data+0xf7/0x130
<4>[    4.015076]  [<c12ecbc0>] ? mmc_erase+0x140/0x140
<4>[    4.015102]  [<c12f139d>] mmc_send_ext_csd+0x1d/0x20
<4>[    4.015125]  [<c12efef0>] mmc_get_ext_csd+0x70/0x140
<4>[    4.015151]  [<c12effe8>] mmc_compare_ext_csds+0x28/0x190
<4>[    4.015176]  [<c12f039f>] mmc_init_card+0x24f/0x650
<4>[    4.015201]  [<c13b6d5d>] ? _raw_spin_unlock_irqrestore+0x4d/0x60
<4>[    4.015226]  [<c107fd9c>] ? trace_hardirqs_on_caller+0x11c/0x160
<4>[    4.015255]  [<c12f09a4>] mmc_attach_mmc+0xa4/0x190
<4>[    4.015282]  [<c12ee3f0>] mmc_rescan+0x210/0x240
<4>[    4.015311]  [<c105f9b6>] process_one_work+0x176/0x550
<4>[    4.015336]  [<c105f93a>] ? process_one_work+0xfa/0x550
<4>[    4.015360]  [<c12ee1e0>] ? mmc_init_erase+0x140/0x140
<4>[    4.015385]  [<c1061c2a>] worker_thread+0x12a/0x2c0
<4>[    4.015410]  [<c1061b00>] ? manage_workers.clone.18+0x100/0x100
<4>[    4.015437]  [<c1066244>] kthread+0x74/0x80
<4>[    4.015463]  [<c10661d0>] ? __init_kthread_worker+0x60/0x60
<4>[    4.015490]  [<c13b7dfa>] kernel_thread_helper+0x6/0xd
<0>[    4.015507] Code: 57 89 d7 56 53 89 c3 83 ec 10 8b 40 04 8b 72 28 f6 c4 10 89 45 f0 0f 85 91 00 00 00 85 f6 0f 84 c1 00 00 00 8b 4e 04 31 d2 89 c8 <f7> 73 58 ba d3 4d 62 10 89 c1 8b 06 f7 e2 c1 ea 06 01 d1 f7 45
<0>[    4.015829] EIP: [<c12fa38e>] sdhci_calc_timeout+0x2e/0x100 SS:ESP 0068:f5291c50

Reported-by: Alexander Shishkin <alexander.shishkin@linux.intel.com>
Signed-off-by: Andy Shevchenko <andriy.shevchenko@linux.intel.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: Revert "mmc: sdhci: Fix SDHCI_QUIRK_TIMEOUT_USES_SDCLK"
Andy Shevchenko [Wed, 3 Aug 2011 15:35:58 +0000 (18:35 +0300)]
mmc: Revert "mmc: sdhci: Fix SDHCI_QUIRK_TIMEOUT_USES_SDCLK"

This reverts commit 4b01681c7764, which introduced a new potential
divide by zero in the process of fixing one.  The subsequent commits
attempt to fix the issue properly.

Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: tmio: eliminate unused variable 'mmc' warning
Axel Lin [Wed, 3 Aug 2011 06:48:58 +0000 (14:48 +0800)]
mmc: tmio: eliminate unused variable 'mmc' warning

Fix below compile warning:
  CC      drivers/mmc/host/tmio_mmc.o
drivers/mmc/host/tmio_mmc.c: In function 'tmio_mmc_suspend':
drivers/mmc/host/tmio_mmc.c:30: warning: unused variable 'mmc'
drivers/mmc/host/tmio_mmc.c: In function 'tmio_mmc_resume':
drivers/mmc/host/tmio_mmc.c:45: warning: unused variable 'mmc'

Signed-off-by: Axel Lin <axel.lin@gmail.com>
Acked-by: Guennadi Liakhovetski <g.liakhovetski@gmx.de>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: esdhc-imx: fix card interrupt loss on freescale eSDHC
Tony Lin [Thu, 11 Aug 2011 20:45:59 +0000 (16:45 -0400)]
mmc: esdhc-imx: fix card interrupt loss on freescale eSDHC

Apply a workaround for the imx eSDHC controller to avoid missing
card interrupts.  This makes SDIO work.

Signed-off-by: Tony Lin <tony.lin@freescale.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: sdhci-s3c: Fix build for header change
Mark Brown [Fri, 29 Jul 2011 14:35:00 +0000 (15:35 +0100)]
mmc: sdhci-s3c: Fix build for header change

A header change has removed an implicit inclusion of module.h, breaking
the build due to the use of THIS_MODULE. Fix that.

Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: dw_mmc: Fix mask in IDMAC_SET_BUFFER1_SIZE macro
Shashidhar Hiremath [Fri, 29 Jul 2011 12:49:50 +0000 (08:49 -0400)]
mmc: dw_mmc: Fix mask in IDMAC_SET_BUFFER1_SIZE macro

The mask used inside this macro was assuming Buffer_Size1's [BS1's]
width to be 14 bits, it is actually 13 bits.  Modify masks used in
IDMAC_SET_BUFFER1_SIZE such that they use only 13 bits instead of
current 14.

Signed-off-by: Shashidhar Hiremath <shashidharh@vayavyalabs.com>
Acked-by: Will Newton <will.newton@imgtec.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: cb710: fix possible pci_dev leak in cb710_pci_configure()
Michał Mirosław [Thu, 28 Jul 2011 18:55:27 +0000 (20:55 +0200)]
mmc: cb710: fix possible pci_dev leak in cb710_pci_configure()

Reported-by: Julia Lawall <julia@diku.dk>
Signed-off-by: Michał Mirosław <mirq-linux@rere.qmqm.pl>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: core: Detect eMMC v4.5 ext_csd entries
Kyungmin Park [Tue, 26 Jul 2011 08:12:37 +0000 (17:12 +0900)]
mmc: core: Detect eMMC v4.5 ext_csd entries

The eMMC v4.5 Spec is released now:

EXT_CSD_REV Extended CSD Revision
255-7 Reserved
6 Revision 1.6 (for MMC v4.5)
5 Revision 1.5 (for MMV v4.41)
...

Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: mmc_test: avoid stalled file in debugfs
Andy Shevchenko [Fri, 22 Jul 2011 13:13:36 +0000 (16:13 +0300)]
mmc: mmc_test: avoid stalled file in debugfs

During card removal and inserting cycle the test file in the debugfs could be
stalled until the host driver removes it. Let's keep the file in the linked
list and destroy it when card is removed.

Signed-off-by: Andy Shevchenko <andriy.shevchenko@linux.intel.com>
Acked-by: Per Forlin <per.forlin@linaro.org>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: sdhci-s3c: add BROKEN_ADMA_ZEROLEN_DESC quirk
Jaehoon Chung [Tue, 12 Jul 2011 08:30:47 +0000 (17:30 +0900)]
mmc: sdhci-s3c: add BROKEN_ADMA_ZEROLEN_DESC quirk

Samsung SoCs need to set BROKEN_ADMA_ZEROLEN_DESC.
(If ADMA operation is more than 65535, maybe set by zero.)

Signed-off-by: Jaehoon Chung <jh80.chung@samsung.com>
Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: sdhci: pxav3: controller needs 32 bit ADMA addressing
Philip Rakity [Mon, 11 Jul 2011 21:47:54 +0000 (14:47 -0700)]
mmc: sdhci: pxav3: controller needs 32 bit ADMA addressing

Enable the quirk.

(Best used in conjunction with patch downgrading ADMA to SDMA when
transfer is not aligned.)

Signed-off-by: Philip Rakity <prakity@marvell.com>
Acked-by: Zhangfei Gao <zhangfei.gao@marvell.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agommc: sdhci: fix retuning timer wrongly deleted in sdhci_tasklet_finish
Aaron Lu [Mon, 11 Jul 2011 05:27:11 +0000 (13:27 +0800)]
mmc: sdhci: fix retuning timer wrongly deleted in sdhci_tasklet_finish

Currently, the retuning timer for retuning mode 1 will be deleted in
function sdhci_tasklet_finish after a mmc request done, which will make
retuning timing never trigger again. This patch fixed this problem.

Signed-off-by: Aaron Lu <Aaron.Lu@amd.com>
Reviewed-by: Philip Rakity <prakity@marvell.com>
Signed-off-by: Chris Ball <cjb@laptop.org>
12 years agoMerge branch 'devicetree/merge' of git://git.secretlab.ca/git/linux-2.6
Linus Torvalds [Sat, 13 Aug 2011 04:59:09 +0000 (21:59 -0700)]
Merge branch 'devicetree/merge' of git://git.secretlab.ca/git/linux-2.6

* 'devicetree/merge' of git://git.secretlab.ca/git/linux-2.6:
  dt: add empty of_get_property for non-dt

12 years agoMerge branch 'usb-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh...
Linus Torvalds [Sat, 13 Aug 2011 04:56:53 +0000 (21:56 -0700)]
Merge branch 'usb-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/usb-2.6

* 'usb-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/usb-2.6: (30 commits)
  USB: Serial: Add PID(0xF7C0) to FTDI SIO driver for a zeitcontrol-device
  USB: Serial: Add device ID for Sierra Wireless MC8305
  USB: Serial: Added device ID for Qualcomm Modem in Sagemcom's HiLo3G
  usb/host/pci-quirks.c: correct annotation of `ehci_dmi_nohandoff_table'
  USB: option driver: add PID for Vodafone-Huawei K4511
  USB: option driver: add PID for Vodafone-Huawei K4510
  USB: option driver: add PID for Vodafone-Huawei K3771
  USB: option driver: add PID for Vodafone-Huawei K3770
  usb: serial: ftdi_sio.c: For the FT232H FTDI_SIO_SET_BAUDRATE_REQUEST, index needs to be shifted too
  usb/isp1760: Added missing call to usb_hcd_check_unlink_urb() during unlink
  USB: EHCI: Fix test mode sequence
  USB: ftdi_sio: fix minor typo in get_ftdi_divisor
  USB: at91_udc: include linux/prefetch.h explicitly
  USB: usb-storage: unusual_devs entry for ARM V2M motherboard.
  usb/ehci-mxc: add missing inclusion of mach/hardware.h
  USB: assign instead of equal in usbtmc.c
  usb: renesas_usbhs: fixup usbhsg_for_each_uep 1st pos
  usb: renesas_usbhs: fix DMA build by including dma-mapping.h
  usb: gadget: net2272 - Correct includes
  usb: musb: fix oops on musb_gadget_pullup
  ...

12 years agoMerge branch 'staging-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh...
Linus Torvalds [Sat, 13 Aug 2011 03:55:49 +0000 (20:55 -0700)]
Merge branch 'staging-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/staging-2.6

* 'staging-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/staging-2.6:
  zcache: Fix build error when sysfs is not defined
  zcache: Use div_u64 for 64-bit division
  staging:rts_pstor: fix thread synchronization flow
  drivers:staging:solo6x10:add the missed slab.h
  staging: zcache: include module.h for MODULE_LICENSE
  drivers/staging/hv/blkvsc_drv.c: eliminate NULL pointer dereference
  Staging: Add clk API note to nvec/TODO
  drivers/staging/ath6kl/miscdrv/ar3kps/ar3kpsparser.c: adjust array index
  staging: more missing slab.h inclusions
  drivers/staging/solo6x10/p2m.c needs slab.h
  drivers/staging/solo6x10/core.c needs slab.h
  drivers/staging/dt3155v4l/dt3155v4l.c needs slab.h
  drivers/staging/speakup/devsynth.c: fix "buffer size is not provably correct" error
  Staging: iio: add some unlocks to raw_read() functions
  staging: ft1000_proc needs asm/io.h for inw/outw on sparc
  staging: rtl8192u: declare MODULE_FIRMWARE
  gma500: Fix clashes with DRM updates
  staging: zcache: module is GPL
  staging: fix zcache building

12 years agoMerge branch 'x86-vdso-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git...
Linus Torvalds [Sat, 13 Aug 2011 03:46:24 +0000 (20:46 -0700)]
Merge branch 'x86-vdso-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-tip

* 'x86-vdso-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-tip:
  x86-64: Rework vsyscall emulation and add vsyscall= parameter
  x86-64: Wire up getcpu syscall
  x86: Remove unnecessary compile flag tweaks for vsyscall code
  x86-64: Add vsyscall:emulate_vsyscall trace event
  x86-64: Add user_64bit_mode paravirt op
  x86-64, xen: Enable the vvar mapping
  x86-64: Work around gold bug 13023
  x86-64: Move the "user" vsyscall segment out of the data segment.
  x86-64: Pad vDSO to a page boundary

12 years agoMerge branch 'for-linus' of git://oss.sgi.com/xfs/xfs
Linus Torvalds [Sat, 13 Aug 2011 03:43:01 +0000 (20:43 -0700)]
Merge branch 'for-linus' of git://oss.sgi.com/xfs/xfs

* 'for-linus' of git://oss.sgi.com/xfs/xfs:
  xfs: replace xfs_buf_geterror() with bp->b_error
  xfs: Check the return value of xfs_buf_read() for NULL
  "xfs: fix error handling for synchronous writes" revisited
  xfs: set cursor in xfs_ail_splice() even when AIL was empty
  xfs: Remove the macro XFS_BUFTARG_NAME
  xfs: Remove the macro XFS_BUF_TARGET
  xfs: Remove the macro XFS_BUF_SET_TARGET
  Replace the macro XFS_BUF_ISPINNED with helper xfs_buf_ispinned
  xfs: Remove the macro XFS_BUF_SET_PTR
  xfs: Remove the macro XFS_BUF_PTR
  xfs: Remove macro XFS_BUF_SET_START
  xfs: Remove macro XFS_BUF_HOLD
  xfs: Remove macro XFS_BUF_BUSY and family
  xfs: Remove the macro XFS_BUF_ERROR and family
  xfs: Remove the macro XFS_BUF_BFLAGS

12 years agoMerge branch 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/linux-arm-soc
Linus Torvalds [Sat, 13 Aug 2011 03:42:02 +0000 (20:42 -0700)]
Merge branch 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/linux-arm-soc

* 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/linux-arm-soc: (32 commits)
  ARM: mmp: Change the way we use timer 0 as clockevent timer.
  ARM: mmp: Switch to using timer 1 as clocksource timer.
  ARM: mmp: Also start timer 1 on boot.
  ARM: pxa168/gplugd: free correct GPIO
  ARM: pxa168/gplugd: get rid of mfp-gplugd.h
  ARM: pxa: fix logic error in PJ4 iWMMXt handling
  mach-sa1100: fix PCI build problem
  omap: timer: Set dmtimer used as clocksource in autoreload mode
  OMAP3: am3517crane: remove NULL board_mux from board file
  arm: mach-omap2: mux: use kstrdup()
  arch:arm:plat-omap:iovmm: remove unused variable 'va'
  Update Nook Color machine 3284 to common Encore name
  am3505/3517: Various platform defines for UART4
  OMAP: hwmod: fix build break on non-OMAP4 multi-OMAP2 builds
  OMAP: Fix linking error in twl-common.c for OMAP2/3/4 only builds
  iMX: Fix build for iMX53
  ARM: mx5: board-cpuimx51.c fixup irq_to_gpio() usage
  OMAP2+: PM: SmartReflex: use put_sync_suspend for IRQ-safe disabling
  OMAP3: beagle: don't touch omap_device internals
  OMAP1: enable GENERIC_IRQ_CHIP
  ...

12 years agoxfs: replace xfs_buf_geterror() with bp->b_error
Chandra Seetharaman [Wed, 3 Aug 2011 02:18:34 +0000 (02:18 +0000)]
xfs: replace xfs_buf_geterror() with bp->b_error

Since we just checked bp for NULL, it is ok to replace
xfs_buf_geterror() with bp->b_error in these places.

Signed-off-by: Chandra Seetharaman <sekharan@us.ibm.com>
Signed-off-by: Alex Elder <aelder@sgi.com>
12 years agoxfs: Check the return value of xfs_buf_read() for NULL
Chandra Seetharaman [Wed, 3 Aug 2011 02:18:29 +0000 (02:18 +0000)]
xfs: Check the return value of xfs_buf_read() for NULL

Check the return value of xfs_buf_read() for NULL and return ENOMEM
if it is NULL.  This is necessary in a few spots to avoid subsequent
code blindly dereferencing the null buffer pointer.

Signed-off-by: Chandra Seetharaman <sekharan@us.ibm.com>
Signed-off-by: Alex Elder <aelder@sgi.com>
12 years agoMerge branch 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/tmlind/linux...
Arnd Bergmann [Fri, 12 Aug 2011 18:37:43 +0000 (20:37 +0200)]
Merge branch 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/tmlind/linux-omap-2.6 into fixes

12 years agoMerge branch 'fix/asoc' into for-linus
Takashi Iwai [Fri, 12 Aug 2011 16:26:38 +0000 (18:26 +0200)]
Merge branch 'fix/asoc' into for-linus

12 years agoASoC: Fix compile warning in wm8750.c
Takashi Iwai [Fri, 12 Aug 2011 16:22:10 +0000 (18:22 +0200)]
ASoC: Fix compile warning in wm8750.c

sound/soc/codecs/wm8750.c:784:2: warning: missing braces around initializer
sound/soc/codecs/wm8750.c:784:2: warning: (near initialization for ‘wm8750_spi_ids[2].name’)

It's because struct spi_device_id.name is a char array, not a pointer,
while the driver initializes explicitly with 0.

Signed-off-by: Takashi Iwai <tiwai@suse.de>
12 years agoMerge branch 'fix' of git://git.kernel.org/pub/scm/linux/kernel/git/ycmiao/pxa-linux...
Arnd Bergmann [Fri, 12 Aug 2011 15:49:38 +0000 (15:49 +0000)]
Merge branch 'fix' of git://git.kernel.org/pub/scm/linux/kernel/git/ycmiao/pxa-linux-2.6 into fixes

12 years agoMerge branch 'imx-fixes-for-arnd' of git://git.pengutronix.de/git/imx/linux-2.6 into...
Arnd Bergmann [Fri, 12 Aug 2011 15:45:44 +0000 (15:45 +0000)]
Merge branch 'imx-fixes-for-arnd' of git://git.pengutronix.de/git/imx/linux-2.6 into fixes

12 years agoMerge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net
Linus Torvalds [Fri, 12 Aug 2011 13:43:53 +0000 (06:43 -0700)]
Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net

* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (44 commits)
  e1000e: increase driver version number
  e1000e: alternate MAC address update
  e1000e: do not disable receiver on 82574/82583
  e1000e: alternate MAC address does not work on device id 0x1060
  PCnet: Fix section mismatch
  bnx2x: disable dcb on 578xx since not supported yet
  bnx2x: properly clean indirect addresses
  bnx2x: prevent race between undi_unload and load flows
  bnx2x: fix select_queue when FCoE is disabled
  bnx2x: init FCOE FP only once
  ipv4: some rt_iif -> rt_route_iif conversions
  net/bridge/netfilter/ebtables.c: use available error handling code
  net/netlabel/netlabel_kapi.c: add missing cleanup code
  net/irda: sh_sir: tidyup compile warning
  net/irda: sh_sir: add missing header
  net/irda: sh_irda: add missing header
  slcan: ldisc generated skbs are received in softirq context
  scm: Capture the full credentials of the scm sender
  tcp: initialize variable ecn_ok in syncookies path
  drivers/net/wireless/wl1251: add missing kfree
  ...

12 years agoMerge git://git.kernel.org/pub/scm/linux/kernel/git/davem/sparc
Linus Torvalds [Fri, 12 Aug 2011 07:35:46 +0000 (00:35 -0700)]
Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/sparc

* git://git.kernel.org/pub/scm/linux/kernel/git/davem/sparc:
  sparc: Don't do hypervisor calls on non-sun4v in DS driver.

12 years agoMerge branch 'for-davem' of git://git.kernel.org/pub/scm/linux/kernel/git/linville...
David S. Miller [Fri, 12 Aug 2011 06:09:46 +0000 (23:09 -0700)]
Merge branch 'for-davem' of git://git.kernel.org/pub/scm/linux/kernel/git/linville/wireless

12 years agoASoC: omap: Update e-mail address of Jarkko Nikula
Jarkko Nikula [Thu, 11 Aug 2011 12:44:57 +0000 (15:44 +0300)]
ASoC: omap: Update e-mail address of Jarkko Nikula

My gmail account got disabled and I'm not going to reopen it.

Signed-off-by: Jarkko Nikula <jarkko.nikula@bitmer.com>
Acked-by: Liam Girdwood <lrg@ti.com>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
12 years agosparc: Don't do hypervisor calls on non-sun4v in DS driver.
David S. Miller [Fri, 12 Aug 2011 00:58:59 +0000 (17:58 -0700)]
sparc: Don't do hypervisor calls on non-sun4v in DS driver.

Reported-by: Pieter-Paul Giesberts <pieterpg@broadcom.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agopnfs: Automatically select blocks & objects layouts
Boaz Harrosh [Thu, 11 Aug 2011 21:29:25 +0000 (14:29 -0700)]
pnfs: Automatically select blocks & objects layouts

Just like files-layout, blocks & objects layouts are part of the
NFS 4.1 protocol and should be automatically selected if NFS_4_1
is selected. The small problem is that these depend on other
Kernel support being present, while files only depends on NFS
itself.

This patch removes from the user choice the presence of objects
and blocks layout. But makes sure these are selected only if
the depended subsystems are present in the Kernel.

Signed-off-by: Boaz Harrosh <bharrosh@panasas.com>
Acked-by: Peng Tao <peng_tao@emc.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoASoC: SAMSUNG: Add I2S0 internal dma driver
Sangbeom Kim [Wed, 20 Jul 2011 08:07:13 +0000 (17:07 +0900)]
ASoC: SAMSUNG: Add I2S0 internal dma driver

I2S in Exynos4 and S5PC110(S5PV210) has a internal dma.
It can be used low power audio mode and 2nd channel transfer.
This patch can support idma.

[Reapplied after dependencies propagated through in 3.1-rc1. --broonie]

Signed-off-by: Sangbeom Kim <sbkim73@samsung.com>
Acked-by: Jassi Brar <jassisinghbrar@gmail.com>
Acked-by: Liam Girdwood <lrg@ti.com>
Acked-by: Jassi Brar <jassisinghbrar@gmail.com>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
12 years agoext4: Properly count journal credits for long symlinks
Eric Sandeen [Thu, 11 Aug 2011 14:54:31 +0000 (09:54 -0500)]
ext4: Properly count journal credits for long symlinks

Commit df5e6223407e ("ext4: fix deadlock in ext4_symlink() in ENOSPC
conditions") recalculated the number of credits needed for a long
symlink, in the process of splitting it into two transactions.  However,
the first credit calculation under-counted because if selinux is
enabled, credits are needed to create the selinux xattr as well.

Overrunning the reservation will result in an OOPS in
jbd2_journal_dirty_metadata() due to this assert:

  J_ASSERT_JH(jh, handle->h_buffer_credits > 0);

Fix this by increasing the reservation size.

Signed-off-by: Eric Sandeen <sandeen@redhat.com>
Reviewed-by: Jan Kara <jack@suse.cz>
Acked-by: "Theodore Ts'o" <tytso@mit.edu>
Cc: stable@kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoext3: Properly count journal credits for long symlinks
Eric Sandeen [Thu, 11 Aug 2011 14:51:46 +0000 (09:51 -0500)]
ext3: Properly count journal credits for long symlinks

Commit ae54870a1dc9 ("ext3: Fix lock inversion in ext3_symlink()")
recalculated the number of credits needed for a long symlink, in the
process of splitting it into two transactions.  However, the first
credit calculation under-counted because if selinux is enabled, credits
are needed to create the selinux xattr as well.

Overrunning the reservation will result in an OOPS in
journal_dirty_metadata() due to this assert:

  J_ASSERT_JH(jh, handle->h_buffer_credits > 0);

Fix this by increasing the reservation size.

Signed-off-by: Eric Sandeen <sandeen@redhat.com>
Reviewed-by: Jan Kara <jack@suse.cz>
Acked-by: "Theodore Ts'o" <tytso@mit.edu>
Cc: stable@kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoe1000e: increase driver version number
Bruce Allan [Fri, 22 Jul 2011 06:22:02 +0000 (06:22 +0000)]
e1000e: increase driver version number

Signed-off-by: Bruce Allan <bruce.w.allan@intel.com>
Tested-by: Aaron Brown <aaron.f.brown@intel.com>
Signed-off-by: Jeff Kirsher <jeffrey.t.kirsher@intel.com>
12 years agoe1000e: alternate MAC address update
Bruce Allan [Fri, 29 Jul 2011 05:53:07 +0000 (05:53 +0000)]
e1000e: alternate MAC address update

If word 0x37 in the EEPROM is 0xFFFF _or_ 0x0000, then there is no
alternate MAC address in the EEPROM.

Signed-off-by: Bruce Allan <bruce.w.allan@intel.com>
Tested-by: Aaron Brown <aaron.f.brown@intel.com>
Signed-off-by: Jeff Kirsher <jeffrey.t.kirsher@intel.com>
12 years agoe1000e: do not disable receiver on 82574/82583
Bruce Allan [Fri, 22 Jul 2011 06:21:35 +0000 (06:21 +0000)]
e1000e: do not disable receiver on 82574/82583

Due to a hardware erratum, the receiver on 82574 and 82583 should not be
stopped once it has been started.

Signed-off-by: Bruce Allan <bruce.w.allan@intel.com>
Tested-by: Aaron Brown <aaron.f.brown@intel.com>
Signed-off-by: Jeff Kirsher <jeffrey.t.kirsher@intel.com>
12 years agoe1000e: alternate MAC address does not work on device id 0x1060
Bruce Allan [Fri, 22 Jul 2011 06:21:51 +0000 (06:21 +0000)]
e1000e: alternate MAC address does not work on device id 0x1060

This issue is present all the way back to 2.6.34 kernels.

CC: <stable@kernel.org>
Signed-off-by: Bruce Allan <bruce.w.allan@intel.com>
Tested-by: Jeffrey Pieper <jeffrey.e.pieper@intel.com>
Signed-off-by: Jeff Kirsher <jeffrey.t.kirsher@intel.com>
12 years agomove RLIMIT_NPROC check from set_user() to do_execve_common()
Vasiliy Kulikov [Mon, 8 Aug 2011 15:02:04 +0000 (19:02 +0400)]
move RLIMIT_NPROC check from set_user() to do_execve_common()

The patch http://lkml.org/lkml/2003/7/13/226 introduced an RLIMIT_NPROC
check in set_user() to check for NPROC exceeding via setuid() and
similar functions.

Before the check there was a possibility to greatly exceed the allowed
number of processes by an unprivileged user if the program relied on
rlimit only.  But the check created new security threat: many poorly
written programs simply don't check setuid() return code and believe it
cannot fail if executed with root privileges.  So, the check is removed
in this patch because of too often privilege escalations related to
buggy programs.

The NPROC can still be enforced in the common code flow of daemons
spawning user processes.  Most of daemons do fork()+setuid()+execve().
The check introduced in execve() (1) enforces the same limit as in
setuid() and (2) doesn't create similar security issues.

Neil Brown suggested to track what specific process has exceeded the
limit by setting PF_NPROC_EXCEEDED process flag.  With the change only
this process would fail on execve(), and other processes' execve()
behaviour is not changed.

Solar Designer suggested to re-check whether NPROC limit is still
exceeded at the moment of execve().  If the process was sleeping for
days between set*uid() and execve(), and the NPROC counter step down
under the limit, the defered execve() failure because NPROC limit was
exceeded days ago would be unexpected.  If the limit is not exceeded
anymore, we clear the flag on successful calls to execve() and fork().

The flag is also cleared on successful calls to set_user() as the limit
was exceeded for the previous user, not the current one.

Similar check was introduced in -ow patches (without the process flag).

v3 - clear PF_NPROC_EXCEEDED on successful calls to set_user().

Reviewed-by: James Morris <jmorris@namei.org>
Signed-off-by: Vasiliy Kulikov <segoon@openwall.com>
Acked-by: NeilBrown <neilb@suse.de>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoMerge branch 'master' of git://git.kernel.org/pub/scm/linux/kernel/git/linville/wirel...
John W. Linville [Thu, 11 Aug 2011 17:37:26 +0000 (13:37 -0400)]
Merge branch 'master' of git://git.kernel.org/pub/scm/linux/kernel/git/linville/wireless into for-davem

12 years agohwmon: (ibmaem) add missing kfree
Julia Lawall [Tue, 9 Aug 2011 15:10:56 +0000 (11:10 -0400)]
hwmon: (ibmaem) add missing kfree

rs_resp is dynamically allocated in aem_read_sensor(), so it should be freed
before exiting in every case.  This collects the kfree and the return at
the end of the function.

Signed-off-by: Julia Lawall <julia@diku.dk>
Signed-off-by: Guenter Roeck <guenter.roeck@ericsson.com>
Cc: stable@kernel.org # 2.6.27+
12 years agohwmon: (pmbus/lm25066) Ignore byte writes to non-zero pages
Guenter Roeck [Sat, 30 Jul 2011 06:05:25 +0000 (23:05 -0700)]
hwmon: (pmbus/lm25066) Ignore byte writes to non-zero pages

pmbus_clear_faults() attempts to clear faults on non-existing real pages.
As a result, the command error bit in the status register is set, and faults
are not really cleared.

All byte writes to non-zero pages are requests to clear the status register
on that page. Since non-zero pages are virtual and do not exist on the chip,
there is nothing to do, and such requests have to be ignored. This fixes
above problem.

Signed-off-by: Guenter Roeck <guenter.roeck@ericsson.com>
Reviewed-by: Robert Coulson <robert.coulson@ericsson.com>
12 years agohwmon: (pmbus) Virtualize pmbus_write_byte
Guenter Roeck [Sat, 30 Jul 2011 05:08:07 +0000 (22:08 -0700)]
hwmon: (pmbus) Virtualize pmbus_write_byte

With virtual pages and to be able to handle more chips, it is necessary to
virtualise pmbus_write_byte().

Signed-off-by: Guenter Roeck <guenter.roeck@ericsson.com>
Reviewed-by: Robert Coulson <robert.coulson@ericsson.com>
12 years agoMerge branch 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Thu, 11 Aug 2011 16:03:48 +0000 (09:03 -0700)]
Merge branch 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip

* 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip:
  perf symbols: Check '/tmp/perf-' symbol file ownership
  perf sched: Usage leftover from trace -> script rename
  perf sched: Do not delete session object prematurely
  perf tools: Check $HOME/.perfconfig ownership
  perf, x86: Add model 45 SandyBridge support
  perf tools: Add support to install perf python extension
  perf tools: do not look at ./config for configuration
  perf tools: Make clean leaves some files
  perf lock: Dropping unsupported ':r' modifier
  perf probe: Fix coredump introduced by probe module option
  jump label: Reduce the cycle count by changing the link order
  perf report: Use ui__warning in some more places
  perf python: Add PERF_RECORD_{LOST,READ,SAMPLE} routine tables
  perf evlist: Introduce 'disable' method
  trace events: Update version number reference to new 3.x scheme for EVENT_POWER_TRACING_DEPRECATED
  perf buildid-cache: Zero out buffer of filenames when adding/removing buildid

12 years agoMAINTAINERS: Update linus' git repository
Tracey Dent [Thu, 11 Aug 2011 06:59:00 +0000 (02:59 -0400)]
MAINTAINERS: Update linus' git repository

Change to new git tree -
 (git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git).

Signed-off-by: Tracey Dent <tdent48227@gmail.com>
Acked-by: WANG Cong <xiyou.wangcong@gmail.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoRevert "EDAC: Correct Kconfig dependencies"
Linus Torvalds [Thu, 11 Aug 2011 15:58:41 +0000 (08:58 -0700)]
Revert "EDAC: Correct Kconfig dependencies"

This reverts commit af9d220bac41dc3201893e1601cc7c44f7da4498.

It turns out that one was meant to be applied on top of the edac.git
tree in -next that has more i7core_edac changes, but that wasn't clear
in the original email.

Reported-by: Stephen Rothwell <sfr@canb.auug.org.au>
Acked-by: Borislav Petkov <borislav.petkov@amd.com>
Cc: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoNFS41: make PNFS_BLOCK selectable
Peng Tao [Wed, 10 Aug 2011 22:29:21 +0000 (18:29 -0400)]
NFS41: make PNFS_BLOCK selectable

PNFS_BLOCK needs BLK_DEV_DM/MD, which is not a dependency for other
pnfs layout drivers. Seperate it out so others can still build when
BLK_DEV_DM/MD is not enabled.

Also change select to depends on to avoid build failures.

Reported-and-tested-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Peng Tao <peng_tao@emc.com>
Acked-by: Benny Halevy <bhalevy@tonian.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
12 years agoPCnet: Fix section mismatch
Ralf Baechle [Wed, 10 Aug 2011 05:23:46 +0000 (05:23 +0000)]
PCnet: Fix section mismatch

Building MIPS mtx1_defconfig results in:

  MODPOST 735 modules
WARNING: drivers/net/pcnet32.o(.devinit.text+0x11ec): Section mismatch in reference from the function pcnet32_probe_vlbus.constprop.22() to the variable .init.data:pcnet32_portlist
The function __devinit pcnet32_probe_vlbus.constprop.22() references
a variable __initdata pcnet32_portlist.
If pcnet32_portlist is only used by pcnet32_probe_vlbus.constprop.22 then
annotate pcnet32_portlist with a matching annotation.

Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agobnx2x: disable dcb on 578xx since not supported yet
Dmitry Kravkov [Tue, 9 Aug 2011 03:11:13 +0000 (03:11 +0000)]
bnx2x: disable dcb on 578xx since not supported yet

Signed-off-by: Dmitry Kravkov <dmitry@broadcom.com>
Signed-off-by: Eilon Greenstein <eilong@broadcom.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agobnx2x: properly clean indirect addresses
Dmitry Kravkov [Tue, 9 Aug 2011 03:10:29 +0000 (03:10 +0000)]
bnx2x: properly clean indirect addresses

Signed-off-by: Dmitry Kravkov <dmitry@broadcom.com>
Signed-off-by: Eilon Greenstein <eilong@broadcom.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agobnx2x: prevent race between undi_unload and load flows
Dmitry Kravkov [Tue, 9 Aug 2011 03:09:52 +0000 (03:09 +0000)]
bnx2x: prevent race between undi_unload and load flows

Signed-off-by: Dmitry Kravkov <dmitry@broadcom.com>
Signed-off-by: Eilon Greenstein <eilong@broadcom.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agobnx2x: fix select_queue when FCoE is disabled
Vladislav Zolotarov [Tue, 9 Aug 2011 03:08:55 +0000 (03:08 +0000)]
bnx2x: fix select_queue when FCoE is disabled

Signed-off-by: Dmitry Kravkov <dmitry@broadcom.com>
Signed-off-by: Eilon Greenstein <eilong@broadcom.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agobnx2x: init FCOE FP only once
Vladislav Zolotarov [Tue, 9 Aug 2011 03:08:09 +0000 (03:08 +0000)]
bnx2x: init FCOE FP only once

Signed-off-by: Dmitry Kravkov <dmitry@broadcom.com>
Signed-off-by: Eilon Greenstein <eilong@broadcom.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agoipv4: some rt_iif -> rt_route_iif conversions
Julian Anastasov [Tue, 9 Aug 2011 04:01:16 +0000 (04:01 +0000)]
ipv4: some rt_iif -> rt_route_iif conversions

As rt_iif represents input device even for packets
coming from loopback with output route, it is not an unique
key specific to input routes. Now rt_route_iif has such role,
it was fl.iif in 2.6.38, so better to change the checks at
some places to save CPU cycles and to restore 2.6.38 semantics.

compare_keys:
- input routes: only rt_route_iif matters, rt_iif is same
- output routes: only rt_oif matters, rt_iif is not
used for matching in __ip_route_output_key
- now we are back to 2.6.38 state

ip_route_input_common:
- matching rt_route_iif implies input route
- compared to 2.6.38 we eliminated one rth->fl.oif check
because it was not needed even for 2.6.38

compare_hash_inputs:
Only the change here is not an optimization, it has
effect only for output routes. I assume I'm restoring
the original intention to ignore oif, it was using fl.iif
- now we are back to 2.6.38 state

Signed-off-by: Julian Anastasov <ja@ssi.bg>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agonet/bridge/netfilter/ebtables.c: use available error handling code
Julia Lawall [Thu, 11 Aug 2011 01:59:38 +0000 (01:59 +0000)]
net/bridge/netfilter/ebtables.c: use available error handling code

Free the locally allocated table and newinfo as done in adjacent error
handling code.

Signed-off-by: Julia Lawall <julia@diku.dk>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agonet/netlabel/netlabel_kapi.c: add missing cleanup code
Julia Lawall [Thu, 11 Aug 2011 00:06:04 +0000 (00:06 +0000)]
net/netlabel/netlabel_kapi.c: add missing cleanup code

Call cipso_v4_doi_putdef in the case of the failure of the allocation of
entry.  Reverse the order of the error handling code at the end of the
function and insert more labels in order to reduce the number of
unnecessary calls to kfree.

Signed-off-by: Julia Lawall <julia@diku.dk>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agonet/irda: sh_sir: tidyup compile warning
Kuninori Morimoto [Wed, 10 Aug 2011 23:26:37 +0000 (23:26 +0000)]
net/irda: sh_sir: tidyup compile warning

This patch tidyup below warning

${LINUX}/drivers/net/irda/sh_sir.c:514:6: warning:
 'val' may be used uninitialized in this function

Signed-off-by: Kuninori Morimoto <kuninori.morimoto.gx@renesas.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agonet/irda: sh_sir: add missing header
Kuninori Morimoto [Wed, 10 Aug 2011 23:26:09 +0000 (23:26 +0000)]
net/irda: sh_sir: add missing header

This patch fixup below build error on sh_sir

sh_sir.c: In function 'sh_sir_write':
sh_sir.c:127:2: error: implicit declaration of function 'iowrite16'
sh_sir.c: In function 'sh_sir_read':
sh_sir.c:132:2: error: implicit declaration of function 'ioread16'
sh_sir.c: At top level:
sh_sir.c:561:20: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'sh_sir_irq'
sh_sir.c: In function 'sh_sir_probe':
sh_sir.c:727:2: error: implicit declaration of function 'ioremap_nocache'
sh_sir.c:727:16: warning: assignment makes pointer from integer without a cast
sh_sir.c:762:2: error: implicit declaration of function 'request_irq'
sh_sir.c:762:23: error: 'sh_sir_irq' undeclared (first use in this function)
sh_sir.c:762:23: note: each undeclared identifier is reported only once for each function it appears in
sh_sir.c:762:35: error: 'IRQF_DISABLED' undeclared (first use in this function)
sh_sir.c:776:2: error: implicit declaration of function 'iounmap'
sh_sir.c: At top level:
sh_sir.c:436:13: warning: 'sh_sir_clear_all_err' defined but not used
sh_sir.c:474:12: warning: 'sh_sir_is_which_phase' defined but not used
sh_sir.c:490:13: warning: 'sh_sir_tx' defined but not used
sh_sir.c:540:13: warning: 'sh_sir_rx' defined but not used

Signed-off-by: Kuninori Morimoto <kuninori.morimoto.gx@renesas.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agonet/irda: sh_irda: add missing header
Kuninori Morimoto [Wed, 10 Aug 2011 23:25:42 +0000 (23:25 +0000)]
net/irda: sh_irda: add missing header

This patch fixup below build error on sh_irda

sh_irda.c: In function 'sh_irda_write':
sh_irda.c:174: error: implicit declaration of function 'iowrite16'
sh_irda.c: In function 'sh_irda_read':
sh_irda.c:184: error: implicit declaration of function 'ioread16'
sh_irda.c: At top level:
sh_irda.c:492: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'sh_irda_irq'
sh_irda.c: In function 'sh_irda_probe':
sh_irda.c:776: error: implicit declaration of function 'ioremap_nocache'
sh_irda.c:776: warning: assignment makes pointer from integer without a cast
sh_irda.c:811: error: implicit declaration of function 'request_irq'
sh_irda.c:811: error: 'sh_irda_irq' undeclared (first use in this function)
sh_irda.c:811: error: (Each undeclared identifier is reported only once
sh_irda.c:811: error: for each function it appears in.)
sh_irda.c:811: error: 'IRQF_DISABLED' undeclared (first use in this function)
sh_irda.c:825: error: implicit declaration of function 'iounmap'

Signed-off-by: Kuninori Morimoto <kuninori.morimoto.gx@renesas.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agoslcan: ldisc generated skbs are received in softirq context
Oliver Hartkopp [Wed, 10 Aug 2011 05:18:59 +0000 (05:18 +0000)]
slcan: ldisc generated skbs are received in softirq context

As this discussion pointed out

http://marc.info/?l=linux-netdev&m=131257225602375

netdevices that are based on serial line disciplines should use netif_rx_ni()
when pushing received socketbuffers into the netdev rx queue.

Following commit 614851601c121b1320a35757ab88292d6272f906 ("slip: fix NOHZ
local_softirq_pending 08 warning") this patch updates the slcan driver
accordingly.

Signed-off-by: Oliver Hartkopp <socketcan@hartkopp.net>
CC: Matvejchikov Ilya <matvejchikov@gmail.com>
CC: Alan Cox <alan@lxorguk.ukuu.org.uk>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agoscm: Capture the full credentials of the scm sender
Tim Chen [Tue, 9 Aug 2011 06:48:32 +0000 (06:48 +0000)]
scm: Capture the full credentials of the scm sender

This patch corrects an erroneous update of credential's gid with uid
introduced in commit 257b5358b32f17 since 2.6.36.

Signed-off-by: Tim Chen <tim.c.chen@linux.intel.com>
Acked-by: Eric Dumazet <eric.dumazet@gmail.com>
Reviewed-by: James Morris <jmorris@namei.org>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agoUSB: Serial: Add PID(0xF7C0) to FTDI SIO driver for a zeitcontrol-device
Artur Zimmer [Wed, 10 Aug 2011 01:51:28 +0000 (03:51 +0200)]
USB: Serial: Add PID(0xF7C0) to FTDI SIO driver for a zeitcontrol-device

Here is a patch for a new PID (zeitcontrol-device mifare-reader FT232BL(like FT232BM but lead free)).

Signed-off-by: Artur Zimmer <artur128@3dzimmer.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
12 years agoUSB: Serial: Add device ID for Sierra Wireless MC8305
Florian Echtler [Tue, 9 Aug 2011 11:37:49 +0000 (13:37 +0200)]
USB: Serial: Add device ID for Sierra Wireless MC8305

A new device ID pair is added for Sierra Wireless MC8305.

Signed-off-by: Florian Echtler <floe@butterbrot.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
12 years agotcp: initialize variable ecn_ok in syncookies path
Mike Waychison [Thu, 11 Aug 2011 04:59:57 +0000 (21:59 -0700)]
tcp: initialize variable ecn_ok in syncookies path

Using a gcc 4.4.3, warnings are emitted for a possibly uninitialized use
of ecn_ok.

This can happen if cookie_check_timestamp() returns due to not having
seen a timestamp.  Defaulting to ecn off seems like a reasonable thing
to do in this case, so initialized ecn_ok to false.

Signed-off-by: Mike Waychison <mikew@google.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
12 years agoASoC: Terminate WM8750 SPI device ID table
Mark Brown [Thu, 11 Aug 2011 03:23:22 +0000 (12:23 +0900)]
ASoC: Terminate WM8750 SPI device ID table

Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Reported-by: Stephen Rothwell <sfr@canb.auug.org.au>
12 years agoARM: mmp: Change the way we use timer 0 as clockevent timer.
Lennert Buytenhek [Tue, 9 Aug 2011 18:37:55 +0000 (02:37 +0800)]
ARM: mmp: Change the way we use timer 0 as clockevent timer.

Instead of setting up a match interrupt for 'current_time + delta'
on ->set_next_event(), program timer 0 to count down from 'delta - 1'
and trigger an interrupt when it reaches zero.

Signed-off-by: Lennert Buytenhek <buytenh@laptop.org>
Acked-by: Haojian Zhuang <haojian.zhuang@gmail.com>
Signed-off-by: Eric Miao <eric.y.miao@gmail.com>
12 years agoARM: mmp: Switch to using timer 1 as clocksource timer.
Lennert Buytenhek [Tue, 9 Aug 2011 18:37:34 +0000 (02:37 +0800)]
ARM: mmp: Switch to using timer 1 as clocksource timer.

Signed-off-by: Lennert Buytenhek <buytenh@laptop.org>
Acked-by: Haojian Zhuang <haojian.zhuang@gmail.com>
Signed-off-by: Eric Miao <eric.y.miao@gmail.com>
12 years agoARM: mmp: Also start timer 1 on boot.
Lennert Buytenhek [Tue, 9 Aug 2011 18:36:59 +0000 (02:36 +0800)]
ARM: mmp: Also start timer 1 on boot.

Currently, arch-mmp/time.c uses timer 0 both as a clocksource timer
and as a clockevent timer, the latter by setting up a comparator
interrupt to match on 'current_time + delta'.  This is problematic
if delta is small enough, as that can lead to 'current_time + delta'
already being in the past when comparator setup has finished, leading
to the requested event not triggering.

As there is also a silicon issue that requires stopping a timer's
counter while writing to one of its match registers, we'll switch to
using two separate timers -- timer 0 as clockevent timer, which we'll
start and stop on every invocation of ->set_next_event(), and timer 1
as clocksource timer, which will be free-running.

This first patch enables timer 1 on boot, so that we can use it as
clocksource timer.

Signed-off-by: Lennert Buytenhek <buytenh@laptop.org>
Acked-by: Haojian Zhuang <haojian.zhuang@gmail.com>
Signed-off-by: Eric Miao <eric.y.miao@gmail.com>
12 years agoARM: pxa168/gplugd: free correct GPIO
Tanmay Upadhyay [Thu, 14 Jul 2011 09:37:16 +0000 (15:07 +0530)]
ARM: pxa168/gplugd: free correct GPIO

Signed-off-by: Tanmay Upadhyay <tanmay.upadhyay@einfochips.com>
Signed-off-by: Eric Miao <eric.y.miao@gmail.com>
12 years agoARM: pxa168/gplugd: get rid of mfp-gplugd.h
Tanmay Upadhyay [Thu, 14 Jul 2011 09:37:15 +0000 (15:07 +0530)]
ARM: pxa168/gplugd: get rid of mfp-gplugd.h

Move definitions from mfp-gplugd.h to mfp-pxa168.h as they aren't
gplugD specific.

Signed-off-by: Tanmay Upadhyay <tanmay.upadhyay@einfochips.com>
Signed-off-by: Eric Miao <eric.y.miao@gmail.com>
12 years agoARM: pxa: fix logic error in PJ4 iWMMXt handling
Lennert Buytenhek [Thu, 11 Aug 2011 01:56:06 +0000 (09:56 +0800)]
ARM: pxa: fix logic error in PJ4 iWMMXt handling

This got added in:

commit ef6c84454f8567d4968c210d7d194fb711ed3739
Author: Haojian Zhuang <haojian.zhuang@marvell.com>
Date:   Wed Nov 24 11:54:25 2010 +0800

    ARM: pxa: add iwmmx support for PJ4

which does:

-       mrc     p15, 0, r2, c15, c1, 0
-       orr     r2, r2, #0x3                    @ enable access to CP0 and CP1
-       mcr     p15, 0, r2, c15, c1, 0
+       @ enable access to CP0 and CP1
+       XSC(mrc p15, 0, r2, c15, c1, 0)
+       XSC(orr r2, r2, #0x3)
+       XSC(mcr p15, 0, r2, c15, c1, 0)

but then later does:

-       mrc     p15, 0, r4, c15, c1, 0
-       orr     r4, r4, #0x3                    @ enable access to CP0 and CP1
-       mcr     p15, 0, r4, c15, c1, 0
+       @ enable access to CP0 and CP1
+       XSC(mrc p15, 0, r4, c15, c1, 0)
+       XSC(orr r4, r4, #0xf)
+       XSC(mcr p15, 0, r4, c15, c1, 0)

Signed-off-by: Lennert Buytenhek <buytenh@laptop.org>
Acked-by Haojian <haojian.zhuang@gmail.com>
Signed-off-by: Eric Miao <eric.y.miao@gmail.com>
12 years agoASoC: Add missing break in WM8994 probe
Mark Brown [Wed, 10 Aug 2011 13:19:19 +0000 (22:19 +0900)]
ASoC: Add missing break in WM8994 probe

This error would have no effect on current silicon revisions, the fall
through case has the same behaviour.

Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Acked-by: Liam Girdwood <lrg@ti.com>
12 years agoMerge branch 'fixes' of master.kernel.org:/home/rmk/linux-2.6-arm
Linus Torvalds [Thu, 11 Aug 2011 00:37:17 +0000 (17:37 -0700)]
Merge branch 'fixes' of master.kernel.org:/home/rmk/linux-2.6-arm

* 'fixes' of master.kernel.org:/home/rmk/linux-2.6-arm:
  ARM: drop experimental status for ARM_PATCH_PHYS_VIRT
  ARM: 7008/1: alignment: Make SIGBUS sent to userspace POSIXly correct
  ARM: 7007/1: alignment: Prevent ignoring of faults with ARMv6 unaligned access model
  ARM: 7010/1: mm: fix invalid loop for poison_init_mem
  ARM: 7005/1: freshen up mm/proc-arm946.S
  dmaengine: PL08x: Fix trivial build error
  ARM: Fix build error for SMP=n builds

12 years agox86-64: Rework vsyscall emulation and add vsyscall= parameter
Andy Lutomirski [Wed, 10 Aug 2011 15:15:32 +0000 (11:15 -0400)]
x86-64: Rework vsyscall emulation and add vsyscall= parameter

There are three choices:

vsyscall=native: Vsyscalls are native code that issues the
corresponding syscalls.

vsyscall=emulate (default): Vsyscalls are emulated by instruction
fault traps, tested in the bad_area path.  The actual contents of
the vsyscall page is the same as the vsyscall=native case except
that it's marked NX.  This way programs that make assumptions about
what the code in the page does will not be confused when they read
that code.

vsyscall=none: Trying to execute a vsyscall will segfault.

Signed-off-by: Andy Lutomirski <luto@mit.edu>
Link: http://lkml.kernel.org/r/8449fb3abf89851fd6b2260972666a6f82542284.1312988155.git.luto@mit.edu
Signed-off-by: H. Peter Anvin <hpa@linux.intel.com>
12 years agox86-64: Wire up getcpu syscall
Andy Lutomirski [Wed, 10 Aug 2011 15:15:31 +0000 (11:15 -0400)]
x86-64: Wire up getcpu syscall

getcpu is available as a vdso entry and an emulated vsyscall.
Programs that for some reason don't want to use the vdso should
still be able to call getcpu without relying on the slow emulated
vsyscall.  It costs almost nothing to expose it as a real syscall.

We also need this for the following patch in vsyscall=native mode.

Signed-off-by: Andy Lutomirski <luto@mit.edu>
Link: http://lkml.kernel.org/r/6b19f55bdb06a0c32c2fa6dba9b6f222e1fde999.1312988155.git.luto@mit.edu
Signed-off-by: H. Peter Anvin <hpa@linux.intel.com>
12 years agox86: Remove unnecessary compile flag tweaks for vsyscall code
Andy Lutomirski [Wed, 10 Aug 2011 15:15:30 +0000 (11:15 -0400)]
x86: Remove unnecessary compile flag tweaks for vsyscall code

As of commit 98d0ac38ca7b1b7a552c9a2359174ff84decb600
Author: Andy Lutomirski <luto@mit.edu>
Date:   Thu Jul 14 06:47:22 2011 -0400

    x86-64: Move vread_tsc and vread_hpet into the vDSO

user code no longer directly calls into code in arch/x86/kernel/, so
we don't need compile flag hacks to make it safe.  All vdso code is
in the vdso directory now.

Signed-off-by: Andy Lutomirski <luto@mit.edu>
Link: http://lkml.kernel.org/r/835cd05a4c7740544d09723d6ba48f4406f9826c.1312988155.git.luto@mit.edu
Signed-off-by: H. Peter Anvin <hpa@linux.intel.com>
12 years ago"xfs: fix error handling for synchronous writes" revisited
Ajeet Yadav [Fri, 29 Jul 2011 07:42:59 +0000 (07:42 +0000)]
"xfs: fix error handling for synchronous writes" revisited

xfs: fix for hang during synchronous buffer write error

If removed storage while synchronous buffer write underway,
"xfslogd" hangs.

Detailed log http://oss.sgi.com/archives/xfs/2011-07/msg00740.html

Related work bfc60177f8ab509bc225becbb58f7e53a0e33e81
"xfs: fix error handling for synchronous writes"

Given that xfs_bwrite actually does the shutdown already after
waiting for the b_iodone completion and given that we actually
found that calling xfs_force_shutdown from inside
xfs_buf_iodone_callbacks was a major contributor the problem
it better to drop this call.

Signed-off-by: Ajeet Yadav <ajeet.yadav.77@gmail.com>
Reviewed-by: Christoph Hellwig <hch@lst.de>
Signed-off-by: Alex Elder <aelder@sgi.com>
12 years agoMerge branch 'merge' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc
Linus Torvalds [Wed, 10 Aug 2011 19:36:45 +0000 (12:36 -0700)]
Merge branch 'merge' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc

* 'merge' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc:
  powerpc: Really fix build without CONFIG_PCI
  powerpc: Fix build without CONFIG_PCI
  powerpc/4xx: Fix build of PCI code on 405
  powerpc/pseries: Simplify vpa deregistration functions
  powerpc/pseries: Cleanup VPA registration and deregistration errors
  powerpc/pseries: Fix kexec on recent firmware versions
  MAINTAINERS: change maintainership of mpc5xxx
  powerpc: Make KVM_GUEST default to n
  powerpc/kvm: Fix build errors with older toolchains
  powerpc: Lack of ibm,io-events not that important!
  powerpc: Move kdump default base address to half RMO size on 64bit
  powerpc/perf: Disable pagefaults during callchain stack read
  ppc: Remove duplicate definition of PV_POWER7
  powerpc: pseries: Fix kexec on machines with more than 4TB of RAM
  powerpc: Jump label misalignment causes oops at boot
  powerpc: Clean up some panic messages in prom_init
  powerpc: Fix device tree claim code
  powerpc: Return the_cpu_ spec from identify_cpu
  powerpc: mtspr/mtmsr should take an unsigned long

12 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ecryptfs...
Linus Torvalds [Wed, 10 Aug 2011 18:08:06 +0000 (11:08 -0700)]
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ecryptfs/ecryptfs-2.6

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ecryptfs/ecryptfs-2.6:
  Ecryptfs: Add mount option to check uid of device being mounted = expect uid
  eCryptfs: Fix payload_len unitialized variable warning
  eCryptfs: fix compile error
  eCryptfs: Return error when lower file pointer is NULL

12 years agodrivers/net/wireless/wl1251: add missing kfree
Julia Lawall [Mon, 8 Aug 2011 11:18:03 +0000 (13:18 +0200)]
drivers/net/wireless/wl1251: add missing kfree

In each case, the kfree already at the end of the function is also needed
in the error case.

A simplified version of the semantic match that finds this problem is as
follows: (http://coccinelle.lip6.fr/)

// <smpl>
@exists@
local idexpression x;
statement S,S1;
expression E;
identifier fl;
expression *ptr != NULL;
@@

x = \(kmalloc\|kzalloc\|kcalloc\)(...);
...
if (x == NULL) S
<... when != x
     when != if (...) { <+...kfree(x)...+> }
     when any
     when != true x == NULL
x->fl
...>
(
if (x == NULL) S1
|
if (...) { ... when != x
               when forall
(
 return \(0\|<+...x...+>\|ptr\);
|
* return ...;
)
}
)
// </smpl>

Signed-off-by: Julia Lawall <julia@diku.dk>
Signed-off-by: John W. Linville <linville@tuxdriver.com>
12 years agoALSA: snd-usb-caiaq: Correct offset fields of outbound iso_frame_desc
Daniel Mack [Fri, 5 Aug 2011 11:49:52 +0000 (13:49 +0200)]
ALSA: snd-usb-caiaq: Correct offset fields of outbound iso_frame_desc

This fixes faulty outbount packets in case the inbound packets
received from the hardware are fragmented and contain bogus input
iso frames. The bug has been there for ages, but for some strange
reasons, it was only triggered by newer machines in 64bit mode.

Signed-off-by: Daniel Mack <zonque@gmail.com>
Reported-and-tested-by: William Light <wrl@illest.net>
Reported-by: Pedro Ribeiro <pedrib@gmail.com>
Cc: stable@kernel.org
Signed-off-by: Takashi Iwai <tiwai@suse.de>
12 years agoEDAC: Correct Kconfig dependencies
Borislav Petkov [Wed, 10 Aug 2011 12:43:30 +0000 (14:43 +0200)]
EDAC: Correct Kconfig dependencies

Both AMD and Intel i7 EDAC drivers use MCE features and are thus
dependent of this functionality present in the kernel. Express this in
Kconfig so that randconfig builds don't break.

Reported-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Borislav Petkov <borislav.petkov@amd.com>
Acked-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>