]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/kernel-video.git/shortlog
android-sdk/kernel-video.git
2013-04-08 Felipe BalbiMerge tag 'v3.8.6' into connectivity-linux-3.8.y
2013-04-05 Felipe BalbiARM: omap2plus_defconfig: enable ocp2scp driver
2013-04-05 Greg Kroah... Linux 3.8.6 v3.8.6
2013-04-05 Veaceslav Falicobonding: get netdev_rx_handler_unregister out of locks
2013-04-05 Steve Glendinningsmsc75xx: fix jumbo frame support
2013-04-05 Veaceslav Falicopch_gbe: fix ip_summed checksum reporting on rx
2013-04-05 Vijay Subramaniannet: fq_codel: Fix off-by-one error
2013-04-05 Li RongQingnet: fix the use of this_cpu_ptr
2013-04-05 Lothar Waßmannnet: ethernet: cpsw: fix erroneous condition in error...
2013-04-05 Eric Dumazetnet: add a synchronize_net() in netdev_rx_handler_unreg...
2013-04-05 Max.Nekludov... ks8851: Fix interpretation of rxlen field.
2013-04-05 Hannes Frederic... ipv6: don't accept node local multicast traffic from...
2013-04-05 Hannes Frederic... ipv6: don't accept multicast traffic with scope 0
2013-04-05 Hong Zhiguoipv6: fix bad free of addrconf_init_net
2013-04-05 Fabio Estevamfec: Fix the build as module
2013-04-05 Joseph CHANGDM9000B: driver initialization upgrade
2013-04-05 Hannes Frederic... atl1e: drop pci-msi support because of packet corruption
2013-04-05 Eric Dumazetaoe: reserve enough headroom on skbs
2013-04-05 Andrey Vaginnet: fix *_DIAG_MAX constants
2013-04-05 Mugunthan V Ndrivers: net: ethernet: cpsw: use netif_wake_queue...
2013-04-05 Mugunthan V Ndrivers: net: ethernet: davinci_emac: use netif_wake_qu...
2013-04-05 nikolay@redhat.combonding: fix disabling of arp_interval and miimon
2013-04-05 Veaceslav Falicobonding: remove already created master sysfs link on...
2013-04-05 Paul Mooreunix: fix a race condition in unix_release()
2013-04-05 Masatake YAMATOthermal: shorten too long mcast group name
2013-04-05 Cong Wang8021q: fix a potential use-after-free
2013-04-05 Yuchung Chengtcp: undo spurious timeout after SACK reneging
2013-04-05 Eric Dumazettcp: preserve ACK clocking in TSO
2013-04-05 Mirko Lindnersky2: Threshold for Pause Packet is set wrong
2013-04-05 Mirko Lindnersky2: Receive Overflows not counted
2013-04-05 Eric Dumazetnet: remove a WARN_ON() in net_enable_timestamp()
2013-04-05 Russ Dillregulator: Fix memory garbage dev_err printout.
2013-04-05 Matt Flemingefivars: Handle duplicate names from get_next_variable()
2013-04-05 Matt Flemingefivars: explicitly calculate length of VariableName
2013-04-05 Steven Rostedt... tracing: Prevent buffer overwrite disabled for latency...
2013-04-05 David Vrabelxen/events: avoid race with raising an event in unmask_...
2013-04-05 Josef BacikBtrfs: fix space leak when we fail to reserve metadata...
2013-04-05 Emmanuel Grumbachiwlwifi: dvm: don't send HCMD in restart flow
2013-04-05 Ville Syrjälädrm/i915: Don't clobber crtc->fb when queue_flip fails
2013-04-05 Takashi Iwaidrm/i915: Use the fixed pixel clock for eDP in intel_dp...
2013-04-05 J. Bruce Fieldsnfsd4: reject "negative" acl lengths
2013-04-05 Amit Shahvirtio: console: add locking around c_ovq operations
2013-04-05 Amit Shahvirtio: console: rename cvq_lock to c_ivq_lock
2013-04-05 Rajendra NayakARM: OMAP: clocks: Delay clk inits atleast until slab...
2013-04-05 Eric HutterARM: kirkwood: Fix chip-delay for GoFlex Net
2013-04-05 Shawn GuoARM: imx: fix sync issue between imx_cpu_die and imx_cp...
2013-04-05 Mac LinARM: cns3xxx: fix mapping of private memory region
2013-04-05 Anatol Pomozovloop: prevent bdev freeing while device in use
2013-04-05 Andrew Mortonkernel/signal.c: use __ARCH_HAS_SA_RESTORER instead...
2013-04-05 Ben Hutchingssignal: Define __ARCH_HAS_SA_RESTORER so we know whethe...
2013-04-05 Alan Sternusb: gadget: udc-core: fix a regression during gadget...
2013-04-05 Johan HovoldUSB: ti_usb_3410_5052: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: cypress_m8: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: mct_u232: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: ark3116: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: f81232: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: io_edgeport: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: ch341: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: ssu100: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: spcp8x5: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: mos7840: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: pl2303: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: ftdi_sio: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: oti6858: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: io_ti: fix use-after-free in TIOCMIWAIT
2013-04-05 Johan HovoldUSB: mos7840: fix broken TIOCMIWAIT
2013-04-05 Johan HovoldUSB: quatech2: fix use-after-free in TIOCMIWAIT
2013-04-05 Ming LeiUSB: serial: fix hang when opening port
2013-04-05 Johan HovoldUSB: serial: add modem-status-change wait queue
2013-04-05 Josef BacikBtrfs: don't drop path when printing out tree errors...
2013-04-05 Josef BacikBtrfs: limit the global reserve to 512mb
2013-04-05 Chris MasonBtrfs: fix race between mmap writes and compression
2013-04-05 Jan SchmidtBtrfs: fix locking on ROOT_REPLACE operations in tree...
2013-04-05 Josef BacikBtrfs: use set_nlink if our i_nlink is 0
2013-04-05 Eric W. Biedermanuserns: Restrict when proc and sysfs can be mounted
2013-04-05 Eric W. Biedermanipc: Restrict mounting the mqueue filesystem
2013-04-05 Eric W. Biedermanvfs: Carefully propogate mounts across user namespaces
2013-04-05 Eric W. Biedermanvfs: Add a mount flag to lock read only bind mounts
2013-04-05 Eric W. Biedermanuserns: Don't allow creation if the user is chrooted
2013-04-05 Eric W. Biedermanpid: Handle the exit of a multi-threaded init.
2013-04-05 Eric W. Biedermanscm: Require CAP_SYS_ADMIN over the current pidns to...
2013-04-05 Johannes Bergmac80211: prevent spurious HT/VHT downgrade message
2013-04-05 Hans de Goedemedia: [REGRESSION] bt8xx: Fix too large height in...
2013-04-05 Nicholas Bellingertarget: Fix RESERVATION_CONFLICT status regression...
2013-04-05 Vivek Gautamusb: xhci: Fix TRB transfer length macro used for Event...
2013-04-05 Soeren MochUSB: EHCI: fix bug in iTD/siTD DMA pool allocation
2013-04-05 Al ViroNest rename_lock inside vfsmount_lock
2013-04-05 Kees Cooknet/irda: add missing error path release_sock call
2013-04-05 Trond MyklebustNFSv4.1: Always clear the NFS_INO_LAYOUTCOMMIT in layou...
2013-04-05 Trond MyklebustNFSv4.1: Fix a race in pNFS layoutcommit
2013-04-05 Trond MyklebustNFSv4: Fix the string length returned by the idmapper
2013-04-05 fanchaotingpnfs-block: removing DM device maybe cause oops when...
2013-04-05 Bing Zhaomwifiex: cancel cmd timer and free curr_cmd in shutdown...
2013-04-05 Bing Zhaomwifiex: skip pending commands after function shutdown
2013-04-05 Amitkumar Karwarmwifiex: fix race when queuing commands
2013-04-05 Al Virovt: synchronize_rcu() under spinlock is not nice...
2013-04-05 Konstantin... usb: ftdi_sio: Add support for Mitsubishi FX-USB-AW/-BD
2013-04-05 Pawel Wieczorkiewicztty: atmel_serial_probe(): index of atmel_ports[] fix
2013-04-05 Roger Pau Monnexen-blkfront: switch from llist to list
2013-04-05 Jan Beulichxen-blkback: fix dispatch_rw_block_io() error path
next